/* * Functions related to generic timeout handling of requests. */ #include #include #include #include "blk.h" /* * blk_delete_timer - Delete/cancel timer for a given function. * @req: request that we are canceling timer for * */ void blk_delete_timer(struct request *req) { struct request_queue *q = req->q; /* * Nothing to detach */ if (!q->rq_timed_out_fn || !req->deadline) return; list_del_init(&req->timeout_list); if (list_empty(&q->timeout_list)) del_timer(&q->timeout); } static void blk_rq_timed_out(struct request *req) { struct request_queue *q = req->q; enum blk_eh_timer_return ret; ret = q->rq_timed_out_fn(req); switch (ret) { case BLK_EH_HANDLED: __blk_complete_request(req); break; case BLK_EH_RESET_TIMER: blk_clear_rq_complete(req); blk_add_timer(req); break; case BLK_EH_NOT_HANDLED: /* * LLD handles this for now but in the future * we can send a request msg to abort the command * and we can move more of the generic scsi eh code to * the blk layer. */ break; default: printk(KERN_ERR "block: bad eh return: %d\n", ret); break; } } void blk_rq_timed_out_timer(unsigned long data) { struct request_queue *q = (struct request_queue *) data; unsigned long flags, uninitialized_var(next), next_set = 0; struct request *rq, *tmp; spin_lock_irqsave(q->queue_lock, flags); list_for_each_entry_safe(rq, tmp, &q->timeout_list, timeout_list) { if (time_after_eq(jiffies, rq->deadline)) { list_del_init(&rq->timeout_list); /* * Check if we raced with end io completion */ if (blk_mark_rq_complete(rq)) continue; blk_rq_timed_out(rq); } if (!next_set) { next = rq->deadline; next_set = 1; } else if (time_after(next, rq->deadline)) next = rq->deadline; } if (next_set && !list_empty(&q->timeout_list)) mod_timer(&q->timeout, round_jiffies(next)); spin_unlock_irqrestore(q->queue_lock, flags); } /** * blk_abort_request -- Request request recovery for the specified command * @req: pointer to the request of interest * * This function requests that the block layer start recovery for the * request by deleting the timer and calling the q's timeout function. * LLDDs who implement their own error recovery MAY ignore the timeout * event if they generated blk_abort_req. Must hold queue lock. */ void blk_abort_request(struct request *req) { blk_delete_timer(req); blk_rq_timed_out(req); } EXPORT_SYMBOL_GPL(blk_abort_request); /** * blk_add_timer - Start timeout timer for a single request * @req: request that is about to start running. * * Notes: * Each request has its own timer, and as it is added to the queue, we * set up the timer. When the request completes, we cancel the timer. */ void blk_add_timer(struct request *req) { struct request_queue *q = req->q; unsigned long expiry; if (!q->rq_timed_out_fn) return; BUG_ON(!list_empty(&req->timeout_list)); BUG_ON(test_bit(REQ_ATOM_COMPLETE, &req->atomic_flags)); if (req->timeout) req->deadline = jiffies + req->timeout; else { req->deadline = jiffies + q->rq_timeout; /* * Some LLDs, like scsi, peek at the timeout to prevent * a command from being retried forever. */ req->timeout = q->rq_timeout; } list_add_tail(&req->timeout_list, &q->timeout_list); /* * If the timer isn't already pending or this timeout is earlier * than an existing one, modify the timer. Round to next nearest * second. */ expiry = round_jiffies(req->deadline); /* * We use ->deadline == 0 to detect whether a timer was added or * not, so just increase to next jiffy for that specific case */ if (unlikely(!req->deadline)) req->deadline = 1; if (!timer_pending(&q->timeout) || time_before(expiry, q->timeout.expires)) mod_timer(&q->timeout, expiry); } /** * blk_abort_queue -- Abort all request on given queue * @queue: pointer to queue * */ void blk_abort_queue(struct request_queue *q) { unsigned long flags; struct request *rq, *tmp; spin_lock_irqsave(q->queue_lock, flags); elv_abort_queue(q); list_for_each_entry_safe(rq, tmp, &q->timeout_list, timeout_list) blk_abort_request(rq); spin_unlock_irqrestore(q->queue_lock, flags); } EXPORT_SYMBOL_GPL(blk_abort_queue);