/* * sysctl.h: General linux system control interface * * Begun 24 March 1995, Stephen Tweedie * **************************************************************** **************************************************************** ** ** WARNING: ** The values in this file are exported to user space via ** the sysctl() binary interface. Do *NOT* change the ** numbering of any existing values here, and do not change ** any numbers within any one set of values. If you have to ** redefine an existing interface, use a new number for it. ** The kernel will then return -ENOTDIR to any application using ** the old binary interface. ** **************************************************************** **************************************************************** */ #ifndef _LINUX_SYSCTL_H #define _LINUX_SYSCTL_H #include #include #include #include #include /* For the /proc/sys support */ struct ctl_table; struct nsproxy; struct ctl_table_root; struct ctl_table_header; struct ctl_dir; typedef struct ctl_table ctl_table; typedef int proc_handler (struct ctl_table *ctl, int write, void __user *buffer, size_t *lenp, loff_t *ppos); extern int proc_dostring(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_dointvec(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_dointvec_minmax(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_dointvec_jiffies(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_dointvec_userhz_jiffies(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_dointvec_ms_jiffies(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_doulongvec_minmax(struct ctl_table *, int, void __user *, size_t *, loff_t *); extern int proc_doulongvec_ms_jiffies_minmax(struct ctl_table *table, int, void __user *, size_t *, loff_t *); extern int proc_do_large_bitmap(struct ctl_table *, int, void __user *, size_t *, loff_t *); /* * Register a set of sysctl names by calling register_sysctl_table * with an initialised array of struct ctl_table's. An entry with * NULL procname terminates the table. table->de will be * set up by the registration and need not be initialised in advance. * * sysctl names can be mirrored automatically under /proc/sys. The * procname supplied controls /proc naming. * * The table's mode will be honoured both for sys_sysctl(2) and * proc-fs access. * * Leaf nodes in the sysctl tree will be represented by a single file * under /proc; non-leaf nodes will be represented by directories. A * null procname disables /proc mirroring at this node. * * sysctl(2) can automatically manage read and write requests through * the sysctl table. The data and maxlen fields of the ctl_table * struct enable minimal validation of the values being written to be * performed, and the mode field allows minimal authentication. * * There must be a proc_handler routine for any terminal nodes * mirrored under /proc/sys (non-terminals are handled by a built-in * directory handler). Several default handlers are available to * cover common cases. */ /* Support for userspace poll() to watch for changes */ struct ctl_table_poll { atomic_t event; wait_queue_head_t wait; }; static inline void *proc_sys_poll_event(struct ctl_table_poll *poll) { return (void *)(unsigned long)atomic_read(&poll->event); } #define __CTL_TABLE_POLL_INITIALIZER(name) { \ .event = ATOMIC_INIT(0), \ .wait = __WAIT_QUEUE_HEAD_INITIALIZER(name.wait) } #define DEFINE_CTL_TABLE_POLL(name) \ struct ctl_table_poll name = __CTL_TABLE_POLL_INITIALIZER(name) /* A sysctl table is an array of struct ctl_table: */ struct ctl_table { const char *procname; /* Text ID for /proc/sys, or zero */ void *data; int maxlen; umode_t mode; struct ctl_table *child; /* Deprecated */ proc_handler *proc_handler; /* Callback for text formatting */ struct ctl_table_poll *poll; void *extra1; void *extra2; }; struct ctl_node { struct rb_node node; struct ctl_table_header *header; }; /* struct ctl_table_header is used to maintain dynamic lists of struct ctl_table trees. */ struct ctl_table_header { union { struct { struct ctl_table *ctl_table; int used; int count; int nreg; }; struct rcu_head rcu; }; struct completion *unregistering; struct ctl_table *ctl_table_arg; struct ctl_table_root *root; struct ctl_table_set *set; struct ctl_dir *parent; struct ctl_node *node; }; struct ctl_dir { /* Header must be at the start of ctl_dir */ struct ctl_table_header header; struct rb_root root; }; struct ctl_table_set { int (*is_seen)(struct ctl_table_set *); struct ctl_dir dir; }; struct ctl_table_root { struct ctl_table_set default_set; struct ctl_table_set *(*lookup)(struct ctl_table_root *root, struct nsproxy *namespaces); int (*permissions)(struct ctl_table_header *head, struct ctl_table *table); }; /* struct ctl_path describes where in the hierarchy a table is added */ struct ctl_path { const char *procname; }; #ifdef CONFIG_SYSCTL void proc_sys_poll_notify(struct ctl_table_poll *poll); extern void setup_sysctl_set(struct ctl_table_set *p, struct ctl_table_root *root, int (*is_seen)(struct ctl_table_set *)); extern void retire_sysctl_set(struct ctl_table_set *set); void register_sysctl_root(struct ctl_table_root *root); struct ctl_table_header *__register_sysctl_table( struct ctl_table_set *set, const char *path, struct ctl_table *table); struct ctl_table_header *__register_sysctl_paths( struct ctl_table_set *set, const struct ctl_path *path, struct ctl_table *table); struct ctl_table_header *register_sysctl(const char *path, struct ctl_table *table); struct ctl_table_header *register_sysctl_table(struct ctl_table * table); struct ctl_table_header *register_sysctl_paths(const struct ctl_path *path, struct ctl_table *table); void unregister_sysctl_table(struct ctl_table_header * table); extern int sysctl_init(void); #else /* CONFIG_SYSCTL */ static inline struct ctl_table_header *register_sysctl_table(struct ctl_table * table) { return NULL; } static inline struct ctl_table_header *register_sysctl_paths( const struct ctl_path *path, struct ctl_table *table) { return NULL; } static inline void unregister_sysctl_table(struct ctl_table_header * table) { } static inline void setup_sysctl_set(struct ctl_table_set *p, struct ctl_table_root *root, int (*is_seen)(struct ctl_table_set *)) { } #endif /* CONFIG_SYSCTL */ #endif /* _LINUX_SYSCTL_H */