/***************************************************************************** * * * Copyright (c) David L. Mills 1993 * * * * Permission to use, copy, modify, and distribute this software and its * * documentation for any purpose and without fee is hereby granted, provided * * that the above copyright notice appears in all copies and that both the * * copyright notice and this permission notice appear in supporting * * documentation, and that the name University of Delaware not be used in * * advertising or publicity pertaining to distribution of the software * * without specific, written prior permission. The University of Delaware * * makes no representations about the suitability this software for any * * purpose. It is provided "as is" without express or implied warranty. * * * *****************************************************************************/ /* * Modification history timex.h * * 29 Dec 97 Russell King * Moved CLOCK_TICK_RATE, CLOCK_TICK_FACTOR and FINETUNE to asm/timex.h * for ARM machines * * 9 Jan 97 Adrian Sun * Shifted LATCH define to allow access to alpha machines. * * 26 Sep 94 David L. Mills * Added defines for hybrid phase/frequency-lock loop. * * 19 Mar 94 David L. Mills * Moved defines from kernel routines to header file and added new * defines for PPS phase-lock loop. * * 20 Feb 94 David L. Mills * Revised status codes and structures for external clock and PPS * signal discipline. * * 28 Nov 93 David L. Mills * Adjusted parameters to improve stability and increase poll * interval. * * 17 Sep 93 David L. Mills * Created file $NTP/include/sys/timex.h * 07 Oct 93 Torsten Duwe * Derived linux/timex.h * 1995-08-13 Torsten Duwe * kernel PLL updated to 1994-12-13 specs (rfc-1589) * 1997-08-30 Ulrich Windl * Added new constant NTP_PHASE_LIMIT * 2004-08-12 Christoph Lameter * Reworked time interpolation logic */ #ifndef _LINUX_TIMEX_H #define _LINUX_TIMEX_H #include #define ADJ_ADJTIME 0x8000 /* switch between adjtime/adjtimex modes */ #define ADJ_OFFSET_SINGLESHOT 0x0001 /* old-fashioned adjtime */ #define ADJ_OFFSET_READONLY 0x2000 /* read-only adjtime */ #include #include #include #include /* * SHIFT_PLL is used as a dampening factor to define how much we * adjust the frequency correction for a given offset in PLL mode. * It also used in dampening the offset correction, to define how * much of the current value in time_offset we correct for each * second. Changing this value changes the stiffness of the ntp * adjustment code. A lower value makes it more flexible, reducing * NTP convergence time. A higher value makes it stiffer, increasing * convergence time, but making the clock more stable. * * In David Mills' nanokernel reference implementation SHIFT_PLL is 4. * However this seems to increase convergence time much too long. * * https://lists.ntp.org/pipermail/hackers/2008-January/003487.html * * In the above mailing list discussion, it seems the value of 4 * was appropriate for other Unix systems with HZ=100, and that * SHIFT_PLL should be decreased as HZ increases. However, Linux's * clock steering implementation is HZ independent. * * Through experimentation, a SHIFT_PLL value of 2 was found to allow * for fast convergence (very similar to the NTPv3 code used prior to * v2.6.19), with good clock stability. * * * SHIFT_FLL is used as a dampening factor to define how much we * adjust the frequency correction for a given offset in FLL mode. * In David Mills' nanokernel reference implementation SHIFT_FLL is 2. * * MAXTC establishes the maximum time constant of the PLL. */ #define SHIFT_PLL 2 /* PLL frequency factor (shift) */ #define SHIFT_FLL 2 /* FLL frequency factor (shift) */ #define MAXTC 10 /* maximum time constant (shift) */ /* * SHIFT_USEC defines the scaling (shift) of the time_freq and * time_tolerance variables, which represent the current frequency * offset and maximum frequency tolerance. */ #define SHIFT_USEC 16 /* frequency offset scale (shift) */ #define PPM_SCALE ((s64)NSEC_PER_USEC << (NTP_SCALE_SHIFT - SHIFT_USEC)) #define PPM_SCALE_INV_SHIFT 19 #define PPM_SCALE_INV ((1LL << (PPM_SCALE_INV_SHIFT + NTP_SCALE_SHIFT)) / \ PPM_SCALE + 1) #define MAXPHASE 500000000L /* max phase error (ns) */ #define MAXFREQ 500000 /* max frequency error (ns/s) */ #define MAXFREQ_SCALED ((s64)MAXFREQ << NTP_SCALE_SHIFT) #define MINSEC 256 /* min interval between updates (s) */ #define MAXSEC 2048 /* max interval between updates (s) */ #define NTP_PHASE_LIMIT ((MAXPHASE / NSEC_PER_USEC) << 5) /* beyond max. dispersion */ /* * kernel variables * Note: maximum error = NTP synch distance = dispersion + delay / 2; * estimated error = NTP dispersion. */ extern unsigned long tick_usec; /* USER_HZ period (usec) */ extern unsigned long tick_nsec; /* SHIFTED_HZ period (nsec) */ extern void ntp_init(void); extern void ntp_clear(void); /* Required to safely shift negative values */ #define shift_right(x, s) ({ \ __typeof__(x) __x = (x); \ __typeof__(s) __s = (s); \ __x < 0 ? -(-__x >> __s) : __x >> __s; \ }) #define NTP_SCALE_SHIFT 32 #define NTP_INTERVAL_FREQ (HZ) #define NTP_INTERVAL_LENGTH (NSEC_PER_SEC/NTP_INTERVAL_FREQ) /* Returns how long ticks are at present, in ns / 2^NTP_SCALE_SHIFT. */ extern u64 ntp_tick_length(void); extern int second_overflow(unsigned long secs); extern int do_adjtimex(struct timex *); extern void hardpps(const struct timespec *, const struct timespec *); int read_current_timer(unsigned long *timer_val); /* The clock frequency of the i8253/i8254 PIT */ #define PIT_TICK_RATE 1193182ul #endif /* LINUX_TIMEX_H */