/* * Generic implementation of 64-bit atomics using spinlocks, * useful on processors that don't have 64-bit atomic instructions. * * Copyright © 2009 Paul Mackerras, IBM Corp. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * as published by the Free Software Foundation; either version * 2 of the License, or (at your option) any later version. */ #include #include #include #include #include #include /* * We use a hashed array of spinlocks to provide exclusive access * to each atomic64_t variable. Since this is expected to used on * systems with small numbers of CPUs (<= 4 or so), we use a * relatively small array of 16 spinlocks to avoid wasting too much * memory on the spinlock array. */ #define NR_LOCKS 16 /* * Ensure each lock is in a separate cacheline. */ static union { raw_spinlock_t lock; char pad[L1_CACHE_BYTES]; } atomic64_lock[NR_LOCKS] __cacheline_aligned_in_smp = { [0 ... (NR_LOCKS - 1)] = { .lock = __RAW_SPIN_LOCK_UNLOCKED(atomic64_lock.lock), }, }; static inline raw_spinlock_t *lock_addr(const atomic64_t *v) { unsigned long addr = (unsigned long) v; addr >>= L1_CACHE_SHIFT; addr ^= (addr >> 8) ^ (addr >> 16); return &atomic64_lock[addr & (NR_LOCKS - 1)].lock; } long long atomic64_read(const atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_read); void atomic64_set(atomic64_t *v, long long i) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); raw_spin_lock_irqsave(lock, flags); v->counter = i; raw_spin_unlock_irqrestore(lock, flags); } EXPORT_SYMBOL(atomic64_set); void atomic64_add(long long a, atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); raw_spin_lock_irqsave(lock, flags); v->counter += a; raw_spin_unlock_irqrestore(lock, flags); } EXPORT_SYMBOL(atomic64_add); long long atomic64_add_return(long long a, atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter += a; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_add_return); void atomic64_sub(long long a, atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); raw_spin_lock_irqsave(lock, flags); v->counter -= a; raw_spin_unlock_irqrestore(lock, flags); } EXPORT_SYMBOL(atomic64_sub); long long atomic64_sub_return(long long a, atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter -= a; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_sub_return); long long atomic64_dec_if_positive(atomic64_t *v) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter - 1; if (val >= 0) v->counter = val; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_dec_if_positive); long long atomic64_cmpxchg(atomic64_t *v, long long o, long long n) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter; if (val == o) v->counter = n; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_cmpxchg); long long atomic64_xchg(atomic64_t *v, long long new) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); long long val; raw_spin_lock_irqsave(lock, flags); val = v->counter; v->counter = new; raw_spin_unlock_irqrestore(lock, flags); return val; } EXPORT_SYMBOL(atomic64_xchg); int atomic64_add_unless(atomic64_t *v, long long a, long long u) { unsigned long flags; raw_spinlock_t *lock = lock_addr(v); int ret = 0; raw_spin_lock_irqsave(lock, flags); if (v->counter != u) { v->counter += a; ret = 1; } raw_spin_unlock_irqrestore(lock, flags); return ret; } EXPORT_SYMBOL(atomic64_add_unless);