/* * kobject.c - library routines for handling generic kernel objects * * Copyright (c) 2002-2003 Patrick Mochel * Copyright (c) 2006-2007 Greg Kroah-Hartman * Copyright (c) 2006-2007 Novell Inc. * * This file is released under the GPLv2. * * * Please see the file Documentation/kobject.txt for critical information * about using the kobject interface. */ #include #include #include #include #include /* * populate_dir - populate directory with attributes. * @kobj: object we're working on. * * Most subsystems have a set of default attributes that are associated * with an object that registers with them. This is a helper called during * object registration that loops through the default attributes of the * subsystem and creates attributes files for them in sysfs. */ static int populate_dir(struct kobject *kobj) { struct kobj_type *t = get_ktype(kobj); struct attribute *attr; int error = 0; int i; if (t && t->default_attrs) { for (i = 0; (attr = t->default_attrs[i]) != NULL; i++) { error = sysfs_create_file(kobj, attr); if (error) break; } } return error; } static int create_dir(struct kobject *kobj) { int error = 0; if (kobject_name(kobj)) { error = sysfs_create_dir(kobj); if (!error) { error = populate_dir(kobj); if (error) sysfs_remove_dir(kobj); } } return error; } static int get_kobj_path_length(struct kobject *kobj) { int length = 1; struct kobject *parent = kobj; /* walk up the ancestors until we hit the one pointing to the * root. * Add 1 to strlen for leading '/' of each level. */ do { if (kobject_name(parent) == NULL) return 0; length += strlen(kobject_name(parent)) + 1; parent = parent->parent; } while (parent); return length; } static void fill_kobj_path(struct kobject *kobj, char *path, int length) { struct kobject *parent; --length; for (parent = kobj; parent; parent = parent->parent) { int cur = strlen(kobject_name(parent)); /* back up enough to print this name with '/' */ length -= cur; strncpy(path + length, kobject_name(parent), cur); *(path + --length) = '/'; } pr_debug("kobject: '%s' (%p): %s: path = '%s'\n", kobject_name(kobj), kobj, __func__, path); } /** * kobject_get_path - generate and return the path associated with a given kobj and kset pair. * * @kobj: kobject in question, with which to build the path * @gfp_mask: the allocation type used to allocate the path * * The result must be freed by the caller with kfree(). */ char *kobject_get_path(struct kobject *kobj, gfp_t gfp_mask) { char *path; int len; len = get_kobj_path_length(kobj); if (len == 0) return NULL; path = kzalloc(len, gfp_mask); if (!path) return NULL; fill_kobj_path(kobj, path, len); return path; } EXPORT_SYMBOL_GPL(kobject_get_path); /* add the kobject to its kset's list */ static void kobj_kset_join(struct kobject *kobj) { if (!kobj->kset) return; kset_get(kobj->kset); spin_lock(&kobj->kset->list_lock); list_add_tail(&kobj->entry, &kobj->kset->list); spin_unlock(&kobj->kset->list_lock); } /* remove the kobject from its kset's list */ static void kobj_kset_leave(struct kobject *kobj) { if (!kobj->kset) return; spin_lock(&kobj->kset->list_lock); list_del_init(&kobj->entry); spin_unlock(&kobj->kset->list_lock); kset_put(kobj->kset); } static void kobject_init_internal(struct kobject *kobj) { if (!kobj) return; kref_init(&kobj->kref); INIT_LIST_HEAD(&kobj->entry); kobj->state_in_sysfs = 0; kobj->state_add_uevent_sent = 0; kobj->state_remove_uevent_sent = 0; kobj->state_initialized = 1; } static int kobject_add_internal(struct kobject *kobj) { int error = 0; struct kobject *parent; if (!kobj) return -ENOENT; if (!kobj->name || !kobj->name[0]) { WARN(1, "kobject: (%p): attempted to be registered with empty " "name!\n", kobj); return -EINVAL; } parent = kobject_get(kobj->parent); /* join kset if set, use it as parent if we do not already have one */ if (kobj->kset) { if (!parent) parent = kobject_get(&kobj->kset->kobj); kobj_kset_join(kobj); kobj->parent = parent; } pr_debug("kobject: '%s' (%p): %s: parent: '%s', set: '%s'\n", kobject_name(kobj), kobj, __func__, parent ? kobject_name(parent) : "", kobj->kset ? kobject_name(&kobj->kset->kobj) : ""); error = create_dir(kobj); if (error) { kobj_kset_leave(kobj); kobject_put(parent); kobj->parent = NULL; /* be noisy on error issues */ if (error == -EEXIST) printk(KERN_ERR "%s failed for %s with " "-EEXIST, don't try to register things with " "the same name in the same directory.\n", __func__, kobject_name(kobj)); else printk(KERN_ERR "%s failed for %s (%d)\n", __func__, kobject_name(kobj), error); dump_stack(); } else kobj->state_in_sysfs = 1; return error; } /** * kobject_set_name_vargs - Set the name of an kobject * @kobj: struct kobject to set the name of * @fmt: format string used to build the name * @vargs: vargs to format the string. */ int kobject_set_name_vargs(struct kobject *kobj, const char *fmt, va_list vargs) { const char *old_name = kobj->name; char *s; if (kobj->name && !fmt) return 0; kobj->name = kvasprintf(GFP_KERNEL, fmt, vargs); if (!kobj->name) return -ENOMEM; /* ewww... some of these buggers have '/' in the name ... */ while ((s = strchr(kobj->name, '/'))) s[0] = '!'; kfree(old_name); return 0; } /** * kobject_set_name - Set the name of a kobject * @kobj: struct kobject to set the name of * @fmt: format string used to build the name * * This sets the name of the kobject. If you have already added the * kobject to the system, you must call kobject_rename() in order to * change the name of the kobject. */ int kobject_set_name(struct kobject *kobj, const char *fmt, ...) { va_list vargs; int retval; va_start(vargs, fmt); retval = kobject_set_name_vargs(kobj, fmt, vargs); va_end(vargs); return retval; } EXPORT_SYMBOL(kobject_set_name); /** * kobject_init - initialize a kobject structure * @kobj: pointer to the kobject to initialize * @ktype: pointer to the ktype for this kobject. * * This function will properly initialize a kobject such that it can then * be passed to the kobject_add() call. * * After this function is called, the kobject MUST be cleaned up by a call * to kobject_put(), not by a call to kfree directly to ensure that all of * the memory is cleaned up properly. */ void kobject_init(struct kobject *kobj, struct kobj_type *ktype) { char *err_str; if (!kobj) { err_str = "invalid kobject pointer!"; goto error; } if (!ktype) { err_str = "must have a ktype to be initialized properly!\n"; goto error; } if (kobj->state_initialized) { /* do not error out as sometimes we can recover */ printk(KERN_ERR "kobject (%p): tried to init an initialized " "object, something is seriously wrong.\n", kobj); dump_stack(); } kobject_init_internal(kobj); kobj->ktype = ktype; return; error: printk(KERN_ERR "kobject (%p): %s\n", kobj, err_str); dump_stack(); } EXPORT_SYMBOL(kobject_init); static int kobject_add_varg(struct kobject *kobj, struct kobject *parent, const char *fmt, va_list vargs) { int retval; retval = kobject_set_name_vargs(kobj, fmt, vargs); if (retval) { printk(KERN_ERR "kobject: can not set name properly!\n"); return retval; } kobj->parent = parent; return kobject_add_internal(kobj); } /** * kobject_add - the main kobject add function * @kobj: the kobject to add * @parent: pointer to the parent of the kobject. * @fmt: format to name the kobject with. * * The kobject name is set and added to the kobject hierarchy in this * function. * * If @parent is set, then the parent of the @kobj will be set to it. * If @parent is NULL, then the parent of the @kobj will be set to the * kobject associted with the kset assigned to this kobject. If no kset * is assigned to the kobject, then the kobject will be located in the * root of the sysfs tree. * * If this function returns an error, kobject_put() must be called to * properly clean up the memory associated with the object. * Under no instance should the kobject that is passed to this function * be directly freed with a call to kfree(), that can leak memory. * * Note, no "add" uevent will be created with this call, the caller should set * up all of the necessary sysfs files for the object and then call * kobject_uevent() with the UEVENT_ADD parameter to ensure that * userspace is properly notified of this kobject's creation. */ int kobject_add(struct kobject *kobj, struct kobject *parent, const char *fmt, ...) { va_list args; int retval; if (!kobj) return -EINVAL; if (!kobj->state_initialized) { printk(KERN_ERR "kobject '%s' (%p): tried to add an " "uninitialized object, something is seriously wrong.\n", kobject_name(kobj), kobj); dump_stack(); return -EINVAL; } va_start(args, fmt); retval = kobject_add_varg(kobj, parent, fmt, args); va_end(args); return retval; } EXPORT_SYMBOL(kobject_add); /** * kobject_init_and_add - initialize a kobject structure and add it to the kobject hierarchy * @kobj: pointer to the kobject to initialize * @ktype: pointer to the ktype for this kobject. * @parent: pointer to the parent of this kobject. * @fmt: the name of the kobject. * * This function combines the call to kobject_init() and * kobject_add(). The same type of error handling after a call to * kobject_add() and kobject lifetime rules are the same here. */ int kobject_init_and_add(struct kobject *kobj, struct kobj_type *ktype, struct kobject *parent, const char *fmt, ...) { va_list args; int retval; kobject_init(kobj, ktype); va_start(args, fmt); retval = kobject_add_varg(kobj, parent, fmt, args); va_end(args); return retval; } EXPORT_SYMBOL_GPL(kobject_init_and_add); /** * kobject_rename - change the name of an object * @kobj: object in question. * @new_name: object's new name * * It is the responsibility of the caller to provide mutual * exclusion between two different calls of kobject_rename * on the same kobject and to ensure that new_name is valid and * won't conflict with other kobjects. */ int kobject_rename(struct kobject *kobj, const char *new_name) { int error = 0; const char *devpath = NULL; const char *dup_name = NULL, *name; char *devpath_string = NULL; char *envp[2]; kobj = kobject_get(kobj); if (!kobj) return -EINVAL; if (!kobj->parent) return -EINVAL; devpath = kobject_get_path(kobj, GFP_KERNEL); if (!devpath) { error = -ENOMEM; goto out; } devpath_string = kmalloc(strlen(devpath) + 15, GFP_KERNEL); if (!devpath_string) { error = -ENOMEM; goto out; } sprintf(devpath_string, "DEVPATH_OLD=%s", devpath); envp[0] = devpath_string; envp[1] = NULL; name = dup_name = kstrdup(new_name, GFP_KERNEL); if (!name) { error = -ENOMEM; goto out; } error = sysfs_rename_dir(kobj, new_name); if (error) goto out; /* Install the new kobject name */ dup_name = kobj->name; kobj->name = name; /* This function is mostly/only used for network interface. * Some hotplug package track interfaces by their name and * therefore want to know when the name is changed by the user. */ kobject_uevent_env(kobj, KOBJ_MOVE, envp); out: kfree(dup_name); kfree(devpath_string); kfree(devpath); kobject_put(kobj); return error; } EXPORT_SYMBOL_GPL(kobject_rename); /** * kobject_move - move object to another parent * @kobj: object in question. * @new_parent: object's new parent (can be NULL) */ int kobject_move(struct kobject *kobj, struct kobject *new_parent) { int error; struct kobject *old_parent; const char *devpath = NULL; char *devpath_string = NULL; char *envp[2]; kobj = kobject_get(kobj); if (!kobj) return -EINVAL; new_parent = kobject_get(new_parent); if (!new_parent) { if (kobj->kset) new_parent = kobject_get(&kobj->kset->kobj); } /* old object path */ devpath = kobject_get_path(kobj, GFP_KERNEL); if (!devpath) { error = -ENOMEM; goto out; } devpath_string = kmalloc(strlen(devpath) + 15, GFP_KERNEL); if (!devpath_string) { error = -ENOMEM; goto out; } sprintf(devpath_string, "DEVPATH_OLD=%s", devpath); envp[0] = devpath_string; envp[1] = NULL; error = sysfs_move_dir(kobj, new_parent); if (error) goto out; old_parent = kobj->parent; kobj->parent = new_parent; new_parent = NULL; kobject_put(old_parent); kobject_uevent_env(kobj, KOBJ_MOVE, envp); out: kobject_put(new_parent); kobject_put(kobj); kfree(devpath_string); kfree(devpath); return error; } /** * kobject_del - unlink kobject from hierarchy. * @kobj: object. */ void kobject_del(struct kobject *kobj) { if (!kobj) return; sysfs_remove_dir(kobj); kobj->state_in_sysfs = 0; kobj_kset_leave(kobj); kobject_put(kobj->parent); kobj->parent = NULL; } /** * kobject_get - increment refcount for object. * @kobj: object. */ struct kobject *kobject_get(struct kobject *kobj) { if (kobj) kref_get(&kobj->kref); return kobj; } /* * kobject_cleanup - free kobject resources. * @kobj: object to cleanup */ static void kobject_cleanup(struct kobject *kobj) { struct kobj_type *t = get_ktype(kobj); const char *name = kobj->name; pr_debug("kobject: '%s' (%p): %s\n", kobject_name(kobj), kobj, __func__); if (t && !t->release) pr_debug("kobject: '%s' (%p): does not have a release() " "function, it is broken and must be fixed.\n", kobject_name(kobj), kobj); /* send "remove" if the caller did not do it but sent "add" */ if (kobj->state_add_uevent_sent && !kobj->state_remove_uevent_sent) { pr_debug("kobject: '%s' (%p): auto cleanup 'remove' event\n", kobject_name(kobj), kobj); kobject_uevent(kobj, KOBJ_REMOVE); } /* remove from sysfs if the caller did not do it */ if (kobj->state_in_sysfs) { pr_debug("kobject: '%s' (%p): auto cleanup kobject_del\n", kobject_name(kobj), kobj); kobject_del(kobj); } if (t && t->release) { pr_debug("kobject: '%s' (%p): calling ktype release\n", kobject_name(kobj), kobj); t->release(kobj); } /* free name if we allocated it */ if (name) { pr_debug("kobject: '%s': free name\n", name); kfree(name); } } static void kobject_release(struct kref *kref) { kobject_cleanup(container_of(kref, struct kobject, kref)); } /** * kobject_put - decrement refcount for object. * @kobj: object. * * Decrement the refcount, and if 0, call kobject_cleanup(). */ void kobject_put(struct kobject *kobj) { if (kobj) { if (!kobj->state_initialized) WARN(1, KERN_WARNING "kobject: '%s' (%p): is not " "initialized, yet kobject_put() is being " "called.\n", kobject_name(kobj), kobj); kref_put(&kobj->kref, kobject_release); } } static void dynamic_kobj_release(struct kobject *kobj) { pr_debug("kobject: (%p): %s\n", kobj, __func__); kfree(kobj); } static struct kobj_type dynamic_kobj_ktype = { .release = dynamic_kobj_release, .sysfs_ops = &kobj_sysfs_ops, }; /** * kobject_create - create a struct kobject dynamically * * This function creates a kobject structure dynamically and sets it up * to be a "dynamic" kobject with a default release function set up. * * If the kobject was not able to be created, NULL will be returned. * The kobject structure returned from here must be cleaned up with a * call to kobject_put() and not kfree(), as kobject_init() has * already been called on this structure. */ struct kobject *kobject_create(void) { struct kobject *kobj; kobj = kzalloc(sizeof(*kobj), GFP_KERNEL); if (!kobj) return NULL; kobject_init(kobj, &dynamic_kobj_ktype); return kobj; } /** * kobject_create_and_add - create a struct kobject dynamically and register it with sysfs * * @name: the name for the kset * @parent: the parent kobject of this kobject, if any. * * This function creates a kobject structure dynamically and registers it * with sysfs. When you are finished with this structure, call * kobject_put() and the structure will be dynamically freed when * it is no longer being used. * * If the kobject was not able to be created, NULL will be returned. */ struct kobject *kobject_create_and_add(const char *name, struct kobject *parent) { struct kobject *kobj; int retval; kobj = kobject_create(); if (!kobj) return NULL; retval = kobject_add(kobj, parent, "%s", name); if (retval) { printk(KERN_WARNING "%s: kobject_add error: %d\n", __func__, retval); kobject_put(kobj); kobj = NULL; } return kobj; } EXPORT_SYMBOL_GPL(kobject_create_and_add); /** * kset_init - initialize a kset for use * @k: kset */ void kset_init(struct kset *k) { kobject_init_internal(&k->kobj); INIT_LIST_HEAD(&k->list); spin_lock_init(&k->list_lock); } /* default kobject attribute operations */ static ssize_t kobj_attr_show(struct kobject *kobj, struct attribute *attr, char *buf) { struct kobj_attribute *kattr; ssize_t ret = -EIO; kattr = container_of(attr, struct kobj_attribute, attr); if (kattr->show) ret = kattr->show(kobj, kattr, buf); return ret; } static ssize_t kobj_attr_store(struct kobject *kobj, struct attribute *attr, const char *buf, size_t count) { struct kobj_attribute *kattr; ssize_t ret = -EIO; kattr = container_of(attr, struct kobj_attribute, attr); if (kattr->store) ret = kattr->store(kobj, kattr, buf, count); return ret; } const struct sysfs_ops kobj_sysfs_ops = { .show = kobj_attr_show, .store = kobj_attr_store, }; /** * kset_register - initialize and add a kset. * @k: kset. */ int kset_register(struct kset *k) { int err; if (!k) return -EINVAL; kset_init(k); err = kobject_add_internal(&k->kobj); if (err) return err; kobject_uevent(&k->kobj, KOBJ_ADD); return 0; } /** * kset_unregister - remove a kset. * @k: kset. */ void kset_unregister(struct kset *k) { if (!k) return; kobject_put(&k->kobj); } /** * kset_find_obj - search for object in kset. * @kset: kset we're looking in. * @name: object's name. * * Lock kset via @kset->subsys, and iterate over @kset->list, * looking for a matching kobject. If matching object is found * take a reference and return the object. */ struct kobject *kset_find_obj(struct kset *kset, const char *name) { return kset_find_obj_hinted(kset, name, NULL); } /** * kset_find_obj_hinted - search for object in kset given a predecessor hint. * @kset: kset we're looking in. * @name: object's name. * @hint: hint to possible object's predecessor. * * Check the hint's next object and if it is a match return it directly, * otherwise, fall back to the behavior of kset_find_obj(). Either way * a reference for the returned object is held and the reference on the * hinted object is released. */ struct kobject *kset_find_obj_hinted(struct kset *kset, const char *name, struct kobject *hint) { struct kobject *k; struct kobject *ret = NULL; spin_lock(&kset->list_lock); if (!hint) goto slow_search; /* end of list detection */ if (hint->entry.next == kset->list.next) goto slow_search; k = container_of(hint->entry.next, struct kobject, entry); if (!kobject_name(k) || strcmp(kobject_name(k), name)) goto slow_search; ret = kobject_get(k); goto unlock_exit; slow_search: list_for_each_entry(k, &kset->list, entry) { if (kobject_name(k) && !strcmp(kobject_name(k), name)) { ret = kobject_get(k); break; } } unlock_exit: spin_unlock(&kset->list_lock); if (hint) kobject_put(hint); return ret; } static void kset_release(struct kobject *kobj) { struct kset *kset = container_of(kobj, struct kset, kobj); pr_debug("kobject: '%s' (%p): %s\n", kobject_name(kobj), kobj, __func__); kfree(kset); } static struct kobj_type kset_ktype = { .sysfs_ops = &kobj_sysfs_ops, .release = kset_release, }; /** * kset_create - create a struct kset dynamically * * @name: the name for the kset * @uevent_ops: a struct kset_uevent_ops for the kset * @parent_kobj: the parent kobject of this kset, if any. * * This function creates a kset structure dynamically. This structure can * then be registered with the system and show up in sysfs with a call to * kset_register(). When you are finished with this structure, if * kset_register() has been called, call kset_unregister() and the * structure will be dynamically freed when it is no longer being used. * * If the kset was not able to be created, NULL will be returned. */ static struct kset *kset_create(const char *name, const struct kset_uevent_ops *uevent_ops, struct kobject *parent_kobj) { struct kset *kset; int retval; kset = kzalloc(sizeof(*kset), GFP_KERNEL); if (!kset) return NULL; retval = kobject_set_name(&kset->kobj, name); if (retval) { kfree(kset); return NULL; } kset->uevent_ops = uevent_ops; kset->kobj.parent = parent_kobj; /* * The kobject of this kset will have a type of kset_ktype and belong to * no kset itself. That way we can properly free it when it is * finished being used. */ kset->kobj.ktype = &kset_ktype; kset->kobj.kset = NULL; return kset; } /** * kset_create_and_add - create a struct kset dynamically and add it to sysfs * * @name: the name for the kset * @uevent_ops: a struct kset_uevent_ops for the kset * @parent_kobj: the parent kobject of this kset, if any. * * This function creates a kset structure dynamically and registers it * with sysfs. When you are finished with this structure, call * kset_unregister() and the structure will be dynamically freed when it * is no longer being used. * * If the kset was not able to be created, NULL will be returned. */ struct kset *kset_create_and_add(const char *name, const struct kset_uevent_ops *uevent_ops, struct kobject *parent_kobj) { struct kset *kset; int error; kset = kset_create(name, uevent_ops, parent_kobj); if (!kset) return NULL; error = kset_register(kset); if (error) { kfree(kset); return NULL; } return kset; } EXPORT_SYMBOL_GPL(kset_create_and_add); static DEFINE_SPINLOCK(kobj_ns_type_lock); static const struct kobj_ns_type_operations *kobj_ns_ops_tbl[KOBJ_NS_TYPES]; int kobj_ns_type_register(const struct kobj_ns_type_operations *ops) { enum kobj_ns_type type = ops->type; int error; spin_lock(&kobj_ns_type_lock); error = -EINVAL; if (type >= KOBJ_NS_TYPES) goto out; error = -EINVAL; if (type <= KOBJ_NS_TYPE_NONE) goto out; error = -EBUSY; if (kobj_ns_ops_tbl[type]) goto out; error = 0; kobj_ns_ops_tbl[type] = ops; out: spin_unlock(&kobj_ns_type_lock); return error; } int kobj_ns_type_registered(enum kobj_ns_type type) { int registered = 0; spin_lock(&kobj_ns_type_lock); if ((type > KOBJ_NS_TYPE_NONE) && (type < KOBJ_NS_TYPES)) registered = kobj_ns_ops_tbl[type] != NULL; spin_unlock(&kobj_ns_type_lock); return registered; } const struct kobj_ns_type_operations *kobj_child_ns_ops(struct kobject *parent) { const struct kobj_ns_type_operations *ops = NULL; if (parent && parent->ktype->child_ns_type) ops = parent->ktype->child_ns_type(parent); return ops; } const struct kobj_ns_type_operations *kobj_ns_ops(struct kobject *kobj) { return kobj_child_ns_ops(kobj->parent); } void *kobj_ns_grab_current(enum kobj_ns_type type) { void *ns = NULL; spin_lock(&kobj_ns_type_lock); if ((type > KOBJ_NS_TYPE_NONE) && (type < KOBJ_NS_TYPES) && kobj_ns_ops_tbl[type]) ns = kobj_ns_ops_tbl[type]->grab_current_ns(); spin_unlock(&kobj_ns_type_lock); return ns; } const void *kobj_ns_netlink(enum kobj_ns_type type, struct sock *sk) { const void *ns = NULL; spin_lock(&kobj_ns_type_lock); if ((type > KOBJ_NS_TYPE_NONE) && (type < KOBJ_NS_TYPES) && kobj_ns_ops_tbl[type]) ns = kobj_ns_ops_tbl[type]->netlink_ns(sk); spin_unlock(&kobj_ns_type_lock); return ns; } const void *kobj_ns_initial(enum kobj_ns_type type) { const void *ns = NULL; spin_lock(&kobj_ns_type_lock); if ((type > KOBJ_NS_TYPE_NONE) && (type < KOBJ_NS_TYPES) && kobj_ns_ops_tbl[type]) ns = kobj_ns_ops_tbl[type]->initial_ns(); spin_unlock(&kobj_ns_type_lock); return ns; } void kobj_ns_drop(enum kobj_ns_type type, void *ns) { spin_lock(&kobj_ns_type_lock); if ((type > KOBJ_NS_TYPE_NONE) && (type < KOBJ_NS_TYPES) && kobj_ns_ops_tbl[type] && kobj_ns_ops_tbl[type]->drop_ns) kobj_ns_ops_tbl[type]->drop_ns(ns); spin_unlock(&kobj_ns_type_lock); } EXPORT_SYMBOL(kobject_get); EXPORT_SYMBOL(kobject_put); EXPORT_SYMBOL(kobject_del); EXPORT_SYMBOL(kset_register); EXPORT_SYMBOL(kset_unregister);