/* * linux/mm/mmu_notifier.c * * Copyright (C) 2008 Qumranet, Inc. * Copyright (C) 2008 SGI * Christoph Lameter * * This work is licensed under the terms of the GNU GPL, version 2. See * the COPYING file in the top-level directory. */ #include #include #include #include #include #include #include #include #include /* global SRCU for all MMs */ static struct srcu_struct srcu; /* * This function can't run concurrently against mmu_notifier_register * because mm->mm_users > 0 during mmu_notifier_register and exit_mmap * runs with mm_users == 0. Other tasks may still invoke mmu notifiers * in parallel despite there being no task using this mm any more, * through the vmas outside of the exit_mmap context, such as with * vmtruncate. This serializes against mmu_notifier_unregister with * the mmu_notifier_mm->lock in addition to SRCU and it serializes * against the other mmu notifiers with SRCU. struct mmu_notifier_mm * can't go away from under us as exit_mmap holds an mm_count pin * itself. */ void __mmu_notifier_release(struct mm_struct *mm) { struct mmu_notifier *mn; int id; /* * srcu_read_lock() here will block synchronize_srcu() in * mmu_notifier_unregister() until all registered * ->release() callouts this function makes have * returned. */ id = srcu_read_lock(&srcu); spin_lock(&mm->mmu_notifier_mm->lock); while (unlikely(!hlist_empty(&mm->mmu_notifier_mm->list))) { mn = hlist_entry(mm->mmu_notifier_mm->list.first, struct mmu_notifier, hlist); /* * Unlink. This will prevent mmu_notifier_unregister() * from also making the ->release() callout. */ hlist_del_init_rcu(&mn->hlist); spin_unlock(&mm->mmu_notifier_mm->lock); /* * Clear sptes. (see 'release' description in mmu_notifier.h) */ if (mn->ops->release) mn->ops->release(mn, mm); spin_lock(&mm->mmu_notifier_mm->lock); } spin_unlock(&mm->mmu_notifier_mm->lock); /* * All callouts to ->release() which we have done are complete. * Allow synchronize_srcu() in mmu_notifier_unregister() to complete */ srcu_read_unlock(&srcu, id); /* * mmu_notifier_unregister() may have unlinked a notifier and may * still be calling out to it. Additionally, other notifiers * may have been active via vmtruncate() et. al. Block here * to ensure that all notifier callouts for this mm have been * completed and the sptes are really cleaned up before returning * to exit_mmap(). */ synchronize_srcu(&srcu); } /* * If no young bitflag is supported by the hardware, ->clear_flush_young can * unmap the address and return 1 or 0 depending if the mapping previously * existed or not. */ int __mmu_notifier_clear_flush_young(struct mm_struct *mm, unsigned long address) { struct mmu_notifier *mn; struct hlist_node *n; int young = 0, id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->clear_flush_young) young |= mn->ops->clear_flush_young(mn, mm, address); } srcu_read_unlock(&srcu, id); return young; } int __mmu_notifier_test_young(struct mm_struct *mm, unsigned long address) { struct mmu_notifier *mn; struct hlist_node *n; int young = 0, id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->test_young) { young = mn->ops->test_young(mn, mm, address); if (young) break; } } srcu_read_unlock(&srcu, id); return young; } void __mmu_notifier_change_pte(struct mm_struct *mm, unsigned long address, pte_t pte) { struct mmu_notifier *mn; struct hlist_node *n; int id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->change_pte) mn->ops->change_pte(mn, mm, address, pte); /* * Some drivers don't have change_pte, * so we must call invalidate_page in that case. */ else if (mn->ops->invalidate_page) mn->ops->invalidate_page(mn, mm, address); } srcu_read_unlock(&srcu, id); } void __mmu_notifier_invalidate_page(struct mm_struct *mm, unsigned long address) { struct mmu_notifier *mn; struct hlist_node *n; int id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->invalidate_page) mn->ops->invalidate_page(mn, mm, address); } srcu_read_unlock(&srcu, id); } void __mmu_notifier_invalidate_range_start(struct mm_struct *mm, unsigned long start, unsigned long end) { struct mmu_notifier *mn; struct hlist_node *n; int id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->invalidate_range_start) mn->ops->invalidate_range_start(mn, mm, start, end); } srcu_read_unlock(&srcu, id); } void __mmu_notifier_invalidate_range_end(struct mm_struct *mm, unsigned long start, unsigned long end) { struct mmu_notifier *mn; struct hlist_node *n; int id; id = srcu_read_lock(&srcu); hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) { if (mn->ops->invalidate_range_end) mn->ops->invalidate_range_end(mn, mm, start, end); } srcu_read_unlock(&srcu, id); } static int do_mmu_notifier_register(struct mmu_notifier *mn, struct mm_struct *mm, int take_mmap_sem) { struct mmu_notifier_mm *mmu_notifier_mm; int ret; BUG_ON(atomic_read(&mm->mm_users) <= 0); /* * Verify that mmu_notifier_init() already run and the global srcu is * initialized. */ BUG_ON(!srcu.per_cpu_ref); ret = -ENOMEM; mmu_notifier_mm = kmalloc(sizeof(struct mmu_notifier_mm), GFP_KERNEL); if (unlikely(!mmu_notifier_mm)) goto out; if (take_mmap_sem) down_write(&mm->mmap_sem); ret = mm_take_all_locks(mm); if (unlikely(ret)) goto out_cleanup; if (!mm_has_notifiers(mm)) { INIT_HLIST_HEAD(&mmu_notifier_mm->list); spin_lock_init(&mmu_notifier_mm->lock); mm->mmu_notifier_mm = mmu_notifier_mm; mmu_notifier_mm = NULL; } atomic_inc(&mm->mm_count); /* * Serialize the update against mmu_notifier_unregister. A * side note: mmu_notifier_release can't run concurrently with * us because we hold the mm_users pin (either implicitly as * current->mm or explicitly with get_task_mm() or similar). * We can't race against any other mmu notifier method either * thanks to mm_take_all_locks(). */ spin_lock(&mm->mmu_notifier_mm->lock); hlist_add_head(&mn->hlist, &mm->mmu_notifier_mm->list); spin_unlock(&mm->mmu_notifier_mm->lock); mm_drop_all_locks(mm); out_cleanup: if (take_mmap_sem) up_write(&mm->mmap_sem); /* kfree() does nothing if mmu_notifier_mm is NULL */ kfree(mmu_notifier_mm); out: BUG_ON(atomic_read(&mm->mm_users) <= 0); return ret; } /* * Must not hold mmap_sem nor any other VM related lock when calling * this registration function. Must also ensure mm_users can't go down * to zero while this runs to avoid races with mmu_notifier_release, * so mm has to be current->mm or the mm should be pinned safely such * as with get_task_mm(). If the mm is not current->mm, the mm_users * pin should be released by calling mmput after mmu_notifier_register * returns. mmu_notifier_unregister must be always called to * unregister the notifier. mm_count is automatically pinned to allow * mmu_notifier_unregister to safely run at any time later, before or * after exit_mmap. ->release will always be called before exit_mmap * frees the pages. */ int mmu_notifier_register(struct mmu_notifier *mn, struct mm_struct *mm) { return do_mmu_notifier_register(mn, mm, 1); } EXPORT_SYMBOL_GPL(mmu_notifier_register); /* * Same as mmu_notifier_register but here the caller must hold the * mmap_sem in write mode. */ int __mmu_notifier_register(struct mmu_notifier *mn, struct mm_struct *mm) { return do_mmu_notifier_register(mn, mm, 0); } EXPORT_SYMBOL_GPL(__mmu_notifier_register); /* this is called after the last mmu_notifier_unregister() returned */ void __mmu_notifier_mm_destroy(struct mm_struct *mm) { BUG_ON(!hlist_empty(&mm->mmu_notifier_mm->list)); kfree(mm->mmu_notifier_mm); mm->mmu_notifier_mm = LIST_POISON1; /* debug */ } /* * This releases the mm_count pin automatically and frees the mm * structure if it was the last user of it. It serializes against * running mmu notifiers with SRCU and against mmu_notifier_unregister * with the unregister lock + SRCU. All sptes must be dropped before * calling mmu_notifier_unregister. ->release or any other notifier * method may be invoked concurrently with mmu_notifier_unregister, * and only after mmu_notifier_unregister returned we're guaranteed * that ->release or any other method can't run anymore. */ void mmu_notifier_unregister(struct mmu_notifier *mn, struct mm_struct *mm) { BUG_ON(atomic_read(&mm->mm_count) <= 0); spin_lock(&mm->mmu_notifier_mm->lock); if (!hlist_unhashed(&mn->hlist)) { int id; /* * Ensure we synchronize up with __mmu_notifier_release(). */ id = srcu_read_lock(&srcu); hlist_del_rcu(&mn->hlist); spin_unlock(&mm->mmu_notifier_mm->lock); if (mn->ops->release) mn->ops->release(mn, mm); /* * Allow __mmu_notifier_release() to complete. */ srcu_read_unlock(&srcu, id); } else spin_unlock(&mm->mmu_notifier_mm->lock); /* * Wait for any running method to finish, including ->release() if it * was run by __mmu_notifier_release() instead of us. */ synchronize_srcu(&srcu); BUG_ON(atomic_read(&mm->mm_count) <= 0); mmdrop(mm); } EXPORT_SYMBOL_GPL(mmu_notifier_unregister); static int __init mmu_notifier_init(void) { return init_srcu_struct(&srcu); } module_init(mmu_notifier_init);