aboutsummaryrefslogtreecommitdiffstats
blob: 6aed1ce36737540d7d05a4bd9f7afb49cff58866 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
     CPU frequency and voltage scaling code in the Linux(TM) kernel


		         L i n u x    C P U F r e q

		      C P U F r e q   G o v e r n o r s

		   - information for users and developers -


		    Dominik Brodowski  <linux@brodo.de>
            some additions and corrections by Nico Golde <nico@ngolde.de>



   Clock scaling allows you to change the clock speed of the CPUs on the
    fly. This is a nice method to save battery power, because the lower
            the clock speed, the less power the CPU consumes.


Contents:
---------
1.   What is a CPUFreq Governor?

2.   Governors In the Linux Kernel
2.1  Performance
2.2  Powersave
2.3  Userspace
2.4  Ondemand
2.5  Conservative
2.6  Interactive

3.   The Governor Interface in the CPUfreq Core



1. What Is A CPUFreq Governor?
==============================

Most cpufreq drivers (in fact, all except one, longrun) or even most
cpu frequency scaling algorithms only offer the CPU to be set to one
frequency. In order to offer dynamic frequency scaling, the cpufreq
core must be able to tell these drivers of a "target frequency". So
these specific drivers will be transformed to offer a "->target"
call instead of the existing "->setpolicy" call. For "longrun", all
stays the same, though.

How to decide what frequency within the CPUfreq policy should be used?
That's done using "cpufreq governors". Two are already in this patch
-- they're the already existing "powersave" and "performance" which
set the frequency statically to the lowest or highest frequency,
respectively. At least two more such governors will be ready for
addition in the near future, but likely many more as there are various
different theories and models about dynamic frequency scaling
around. Using such a generic interface as cpufreq offers to scaling
governors, these can be tested extensively, and the best one can be
selected for each specific use.

Basically, it's the following flow graph:

CPU can be set to switch independently	 |	   CPU can only be set
      within specific "limits"		 |       to specific frequencies

                                 "CPUfreq policy"
		consists of frequency limits (policy->{min,max})
  		     and CPUfreq governor to be used
			 /		      \
			/		       \
		       /		       the cpufreq governor decides
		      /			       (dynamically or statically)
		     /			       what target_freq to set within
		    /			       the limits of policy->{min,max}
		   /			            \
		  /				     \
	Using the ->setpolicy call,		 Using the ->target call,
	    the limits and the			  the frequency closest
	     "policy" is set.			  to target_freq is set.
						  It is assured that it
						  is within policy->{min,max}


2. Governors In the Linux Kernel
================================

2.1 Performance
---------------

The CPUfreq governor "performance" sets the CPU statically to the
highest frequency within the borders of scaling_min_freq and
scaling_max_freq.


2.2 Powersave
-------------

The CPUfreq governor "powersave" sets the CPU statically to the
lowest frequency within the borders of scaling_min_freq and
scaling_max_freq.


2.3 Userspace
-------------

The CPUfreq governor "userspace" allows the user, or any userspace
program running with UID "root", to set the CPU to a specific frequency
by making a sysfs file "scaling_setspeed" available in the CPU-device
directory.


2.4 Ondemand
------------

The CPUfreq governor "ondemand" sets the CPU depending on the
current usage. To do this the CPU must have the capability to
switch the frequency very quickly.  There are a number of sysfs file
accessible parameters:

sampling_rate: measured in uS (10^-6 seconds), this is how often you
want the kernel to look at the CPU usage and to make decisions on
what to do about the frequency.  Typically this is set to values of
around '10000' or more. It's default value is (cmp. with users-guide.txt):
transition_latency * 1000
Be aware that transition latency is in ns and sampling_rate is in us, so you
get the same sysfs value by default.
Sampling rate should always get adjusted considering the transition latency
To set the sampling rate 750 times as high as the transition latency
in the bash (as said, 1000 is default), do:
echo `$(($(cat cpuinfo_transition_latency) * 750 / 1000)) \
    >ondemand/sampling_rate

sampling_rate_min:
The sampling rate is limited by the HW transition latency:
transition_latency * 100
Or by kernel restrictions:
If CONFIG_NO_HZ is set, the limit is 10ms fixed.
If CONFIG_NO_HZ is not set or nohz=off boot parameter is used, the
limits depend on the CONFIG_HZ option:
HZ=1000: min=20000us  (20ms)
HZ=250:  min=80000us  (80ms)
HZ=100:  min=200000us (200ms)
The highest value of kernel and HW latency restrictions is shown and
used as the minimum sampling rate.

up_threshold: defines what the average CPU usage between the samplings
of 'sampling_rate' needs to be for the kernel to make a decision on
whether it should increase the frequency.  For example when it is set
to its default value of '95' it means that between the checking
intervals the CPU needs to be on average more than 95% in use to then
decide that the CPU frequency needs to be increased.  

ignore_nice_load: this parameter takes a value of '0' or '1'. When
set to '0' (its default), all processes are counted towards the
'cpu utilisation' value.  When set to '1', the processes that are
run with a 'nice' value will not count (and thus be ignored) in the
overall usage calculation.  This is useful if you are running a CPU
intensive calculation on your laptop that you do not care how long it
takes to complete as you can 'nice' it and prevent it from taking part
in the deciding process of whether to increase your CPU frequency.

sampling_down_factor: this parameter controls the rate at which the
kernel makes a decision on when to decrease the frequency while running
at top speed. When set to 1 (the default) decisions to reevaluate load
are made at the same interval regardless of current clock speed. But
when set to greater than 1 (e.g. 100) it acts as a multiplier for the
scheduling interval for reevaluating load when the CPU is at its top
speed due to high load. This improves performance by reducing the overhead
of load evaluation and helping the CPU stay at its top speed when truly
busy, rather than shifting back and forth in speed. This tunable has no
effect on behavior at lower speeds/lower CPU loads.


2.5 Conservative
----------------

The CPUfreq governor "conservative", much like the "ondemand"
governor, sets the CPU depending on the current usage.  It differs in
behaviour in that it gracefully increases and decreases the CPU speed
rather than jumping to max speed the moment there is any load on the
CPU.  This behaviour more suitable in a battery powered environment.
The governor is tweaked in the same manner as the "ondemand" governor
through sysfs with the addition of:

freq_step: this describes what percentage steps the cpu freq should be
increased and decreased smoothly by.  By default the cpu frequency will
increase in 5% chunks of your maximum cpu frequency.  You can change this
value to anywhere between 0 and 100 where '0' will effectively lock your
CPU at a speed regardless of its load whilst '100' will, in theory, make
it behave identically to the "ondemand" governor.

down_threshold: same as the 'up_threshold' found for the "ondemand"
governor but for the opposite direction.  For example when set to its
default value of '20' it means that if the CPU usage needs to be below
20% between samples to have the frequency decreased.


2.6 Interactive
---------------

The CPUfreq governor "interactive" is designed for latency-sensitive,
interactive workloads. This governor sets the CPU speed depending on
usage, similar to "ondemand" and "conservative" governors.  However,
the governor is more aggressive about scaling the CPU speed up in
response to CPU-intensive activity.

Sampling the CPU load every X ms can lead to under-powering the CPU
for X ms, leading to dropped frames, stuttering UI, etc.  Instead of
sampling the cpu at a specified rate, the interactive governor will
check whether to scale the cpu frequency up soon after coming out of
idle.  When the cpu comes out of idle, a timer is configured to fire
within 1-2 ticks.  If the cpu is very busy between exiting idle and
when the timer fires then we assume the cpu is underpowered and ramp
to MAX speed.

If the cpu was not sufficiently busy to immediately ramp to MAX speed,
then governor evaluates the cpu load since the last speed adjustment,
choosing the highest value between that longer-term load or the
short-term load since idle exit to determine the cpu speed to ramp to.

The tuneable values for this governor are:

min_sample_time: The minimum amount of time to spend at the current
frequency before ramping down. This is to ensure that the governor has
seen enough historic cpu load data to determine the appropriate
workload.  Default is 80000 uS.

hispeed_freq: An intermediate "hi speed" at which to initially ramp
when CPU load hits the value specified in go_hispeed_load.  If load
stays high for the amount of time specified in above_hispeed_delay,
then speed may be bumped higher.  Default is maximum speed.

go_hispeed_load: The CPU load at which to ramp to the intermediate "hi
speed".  Default is 85%.

above_hispeed_delay: Once speed is set to hispeed_freq, wait for this
long before bumping speed higher in response to continued high load.
Default is 20000 uS.

timer_rate: Sample rate for reevaluating cpu load when the system is
not idle.  Default is 20000 uS.

input_boost: If non-zero, boost speed of all CPUs to hispeed_freq on
touchscreen activity.  Default is 0.

boost: If non-zero, immediately boost speed of all CPUs to at least
hispeed_freq until zero is written to this attribute.  If zero, allow
CPU speeds to drop below hispeed_freq according to load as usual.

boostpulse: Immediately boost speed of all CPUs to hispeed_freq for
min_sample_time, after which speeds are allowed to drop below
hispeed_freq according to load as usual.


3. The Governor Interface in the CPUfreq Core
=============================================

A new governor must register itself with the CPUfreq core using
"cpufreq_register_governor". The struct cpufreq_governor, which has to
be passed to that function, must contain the following values:

governor->name -	    A unique name for this governor
governor->governor -	    The governor callback function
governor->owner	-	    .THIS_MODULE for the governor module (if 
			    appropriate)

The governor->governor callback is called with the current (or to-be-set)
cpufreq_policy struct for that CPU, and an unsigned int event. The
following events are currently defined:

CPUFREQ_GOV_START:   This governor shall start its duty for the CPU
		     policy->cpu
CPUFREQ_GOV_STOP:    This governor shall end its duty for the CPU
		     policy->cpu
CPUFREQ_GOV_LIMITS:  The limits for CPU policy->cpu have changed to
		     policy->min and policy->max.

If you need other "events" externally of your driver, _only_ use the
cpufreq_governor_l(unsigned int cpu, unsigned int event) call to the
CPUfreq core to ensure proper locking.


The CPUfreq governor may call the CPU processor driver using one of
these two functions:

int cpufreq_driver_target(struct cpufreq_policy *policy,
                                 unsigned int target_freq,
                                 unsigned int relation);

int __cpufreq_driver_target(struct cpufreq_policy *policy,
                                   unsigned int target_freq,
                                   unsigned int relation);

target_freq must be within policy->min and policy->max, of course.
What's the difference between these two functions? When your governor
still is in a direct code path of a call to governor->governor, the
per-CPU cpufreq lock is still held in the cpufreq core, and there's
no need to lock it again (in fact, this would cause a deadlock). So
use __cpufreq_driver_target only in these cases. In all other cases 
(for example, when there's a "daemonized" function that wakes up 
every second), use cpufreq_driver_target to lock the cpufreq per-CPU
lock before the command is passed to the cpufreq processor driver.