aboutsummaryrefslogtreecommitdiffstats
blob: 2cf3e2608de324b5622673943807b8e8b353e2da (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121

XZ data compression in Linux
============================

Introduction

    XZ is a general purpose data compression format with high compression
    ratio and relatively fast decompression. The primary compression
    algorithm (filter) is LZMA2. Additional filters can be used to improve
    compression ratio even further. E.g. Branch/Call/Jump (BCJ) filters
    improve compression ratio of executable data.

    The XZ decompressor in Linux is called XZ Embedded. It supports
    the LZMA2 filter and optionally also BCJ filters. CRC32 is supported
    for integrity checking. The home page of XZ Embedded is at
    <http://tukaani.org/xz/embedded.html>, where you can find the
    latest version and also information about using the code outside
    the Linux kernel.

    For userspace, XZ Utils provide a zlib-like compression library
    and a gzip-like command line tool. XZ Utils can be downloaded from
    <http://tukaani.org/xz/>.

XZ related components in the kernel

    The xz_dec module provides XZ decompressor with single-call (buffer
    to buffer) and multi-call (stateful) APIs. The usage of the xz_dec
    module is documented in include/linux/xz.h.

    The xz_dec_test module is for testing xz_dec. xz_dec_test is not
    useful unless you are hacking the XZ decompressor. xz_dec_test
    allocates a char device major dynamically to which one can write
    .xz files from userspace. The decompressed output is thrown away.
    Keep an eye on dmesg to see diagnostics printed by xz_dec_test.
    See the xz_dec_test source code for the details.

    For decompressing the kernel image, initramfs, and initrd, there
    is a wrapper function in lib/decompress_unxz.c. Its API is the
    same as in other decompress_*.c files, which is defined in
    include/linux/decompress/generic.h.

    scripts/xz_wrap.sh is a wrapper for the xz command line tool found
    from XZ Utils. The wrapper sets compression options to values suitable
    for compressing the kernel image.

    For kernel makefiles, two commands are provided for use with
    $(call if_needed). The kernel image should be compressed with
    $(call if_needed,xzkern) which will use a BCJ filter and a big LZMA2
    dictionary. It will also append a four-byte trailer containing the
    uncompressed size of the file, which is needed by the boot code.
    Other things should be compressed with $(call if_needed,xzmisc)
    which will use no BCJ filter and 1 MiB LZMA2 dictionary.

Notes on compression options

    Since the XZ Embedded supports only streams with no integrity check or
    CRC32, make sure that you don't use some other integrity check type
    when encoding files that are supposed to be decoded by the kernel. With
    liblzma, you need to use either LZMA_CHECK_NONE or LZMA_CHECK_CRC32
    when encoding. With the xz command line tool, use --check=none or
    --check=crc32.

    Using CRC32 is strongly recommended unless there is some other layer
    which will verify the integrity of the uncompressed data anyway.
    Double checking the integrity would probably be waste of CPU cycles.
    Note that the headers will always have a CRC32 which will be validated
    by the decoder; you can only change the integrity check type (or
    disable it) for the actual uncompressed data.

    In userspace, LZMA2 is typically used with dictionary sizes of several
    megabytes. The decoder needs to have the dictionary in RAM, thus big
    dictionaries cannot be used for files that are intended to be decoded
    by the kernel. 1 MiB is probably the maximum reasonable dictionary
    size for in-kernel use (maybe more is OK for initramfs). The presets
    in XZ Utils may not be optimal when creating files for the kernel,
    so don't hesitate to use custom settings. Example:

        xz --check=crc32 --lzma2=dict=512KiB inputfile

    An exception to above dictionary size limitation is when the decoder
    is used in single-call mode. Decompressing the kernel itself is an
    example of this situation. In single-call mode, the memory usage
    doesn't depend on the dictionary size, and it is perfectly fine to
    use a big dictionary: for maximum compression, the dictionary should
    be at least as big as the uncompressed data itself.

Future plans

    Creating a limited XZ encoder may be considered if people think it is
    useful. LZMA2 is slower to compress than e.g. Deflate or LZO even at
    the fastest settings, so it isn't clear if LZMA2 encoder is wanted
    into the kernel.

    Support for limited random-access reading is planned for the
    decompression code. I don't know if it could have any use in the
    kernel, but I know that it would be useful in some embedded projects
    outside the Linux kernel.

Conformance to the .xz file format specification

    There are a couple of corner cases where things have been simplified
    at expense of detecting errors as early as possible. These should not
    matter in practice all, since they don't cause security issues. But
    it is good to know this if testing the code e.g. with the test files
    from XZ Utils.

Reporting bugs

    Before reporting a bug, please check that it's not fixed already
    at upstream. See <http://tukaani.org/xz/embedded.html> to get the
    latest code.

    Report bugs to <lasse.collin@tukaani.org> or visit #tukaani on
    Freenode and talk to Larhzu. I don't actively read LKML or other
    kernel-related mailing lists, so if there's something I should know,
    you should email to me personally or use IRC.

    Don't bother Igor Pavlov with questions about the XZ implementation
    in the kernel or about XZ Utils. While these two implementations
    include essential code that is directly based on Igor Pavlov's code,
    these implementations aren't maintained nor supported by him.