aboutsummaryrefslogtreecommitdiffstats
blob: 615fa9061b57cde4f8cdb10ac574904eec6e1147 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
#ifndef _ASM_X86_IPI_H
#define _ASM_X86_IPI_H

#ifdef CONFIG_X86_LOCAL_APIC

/*
 * Copyright 2004 James Cleverdon, IBM.
 * Subject to the GNU Public License, v.2
 *
 * Generic APIC InterProcessor Interrupt code.
 *
 * Moved to include file by James Cleverdon from
 * arch/x86-64/kernel/smp.c
 *
 * Copyrights from kernel/smp.c:
 *
 * (c) 1995 Alan Cox, Building #3 <alan@redhat.com>
 * (c) 1998-99, 2000 Ingo Molnar <mingo@redhat.com>
 * (c) 2002,2003 Andi Kleen, SuSE Labs.
 * Subject to the GNU Public License, v.2
 */

#include <asm/hw_irq.h>
#include <asm/apic.h>
#include <asm/smp.h>

/*
 * the following functions deal with sending IPIs between CPUs.
 *
 * We use 'broadcast', CPU->CPU IPIs and self-IPIs too.
 */

static inline unsigned int __prepare_ICR(unsigned int shortcut, int vector,
					 unsigned int dest)
{
	unsigned int icr = shortcut | dest;

	switch (vector) {
	default:
		icr |= APIC_DM_FIXED | vector;
		break;
	case NMI_VECTOR:
		icr |= APIC_DM_NMI;
		break;
	}
	return icr;
}

static inline int __prepare_ICR2(unsigned int mask)
{
	return SET_APIC_DEST_FIELD(mask);
}

static inline void __xapic_wait_icr_idle(void)
{
	while (native_apic_mem_read(APIC_ICR) & APIC_ICR_BUSY)
		cpu_relax();
}

static inline void
__default_send_IPI_shortcut(unsigned int shortcut, int vector, unsigned int dest)
{
	/*
	 * Subtle. In the case of the 'never do double writes' workaround
	 * we have to lock out interrupts to be safe.  As we don't care
	 * of the value read we use an atomic rmw access to avoid costly
	 * cli/sti.  Otherwise we use an even cheaper single atomic write
	 * to the APIC.
	 */
	unsigned int cfg;

	/*
	 * Wait for idle.
	 */
	__xapic_wait_icr_idle();

	/*
	 * No need to touch the target chip field
	 */
	cfg = __prepare_ICR(shortcut, vector, dest);

	/*
	 * Send the IPI. The write to APIC_ICR fires this off.
	 */
	native_apic_mem_write(APIC_ICR, cfg);
}

/*
 * This is used to send an IPI with no shorthand notation (the destination is
 * specified in bits 56 to 63 of the ICR).
 */
static inline void
 __default_send_IPI_dest_field(unsigned int mask, int vector, unsigned int dest)
{
	unsigned long cfg;

	/*
	 * Wait for idle.
	 */
	if (unlikely(vector == NMI_VECTOR))
		safe_apic_wait_icr_idle();
	else
		__xapic_wait_icr_idle();

	/*
	 * prepare target chip field
	 */
	cfg = __prepare_ICR2(mask);
	native_apic_mem_write(APIC_ICR2, cfg);

	/*
	 * program the ICR
	 */
	cfg = __prepare_ICR(0, vector, dest);

	/*
	 * Send the IPI. The write to APIC_ICR fires this off.
	 */
	native_apic_mem_write(APIC_ICR, cfg);
}

extern void default_send_IPI_mask_sequence_phys(const struct cpumask *mask,
						 int vector);
extern void default_send_IPI_mask_allbutself_phys(const struct cpumask *mask,
							 int vector);

/* Avoid include hell */
#define NMI_VECTOR 0x02

extern int no_broadcast;

static inline void __default_local_send_IPI_allbutself(int vector)
{
	if (no_broadcast || vector == NMI_VECTOR)
		apic->send_IPI_mask_allbutself(cpu_online_mask, vector);
	else
		__default_send_IPI_shortcut(APIC_DEST_ALLBUT, vector, apic->dest_logical);
}

static inline void __default_local_send_IPI_all(int vector)
{
	if (no_broadcast || vector == NMI_VECTOR)
		apic->send_IPI_mask(cpu_online_mask, vector);
	else
		__default_send_IPI_shortcut(APIC_DEST_ALLINC, vector, apic->dest_logical);
}

#ifdef CONFIG_X86_32
extern void default_send_IPI_mask_sequence_logical(const struct cpumask *mask,
							 int vector);
extern void default_send_IPI_mask_allbutself_logical(const struct cpumask *mask,
							 int vector);
extern void default_send_IPI_mask_logical(const struct cpumask *mask,
						 int vector);
extern void default_send_IPI_allbutself(int vector);
extern void default_send_IPI_all(int vector);
extern void default_send_IPI_self(int vector);
#endif

#endif

#endif /* _ASM_X86_IPI_H */