aboutsummaryrefslogtreecommitdiffstats
blob: 7ab9046ae0eca5fe64ea930206c18a7cdeda1420 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
/* Special Initializers for certain USB Mass Storage devices
 *
 * Current development and maintenance by:
 *   (c) 1999, 2000 Matthew Dharm (mdharm-usb@one-eyed-alien.net)
 *
 * This driver is based on the 'USB Mass Storage Class' document. This
 * describes in detail the protocol used to communicate with such
 * devices.  Clearly, the designers had SCSI and ATAPI commands in
 * mind when they created this document.  The commands are all very
 * similar to commands in the SCSI-II and ATAPI specifications.
 *
 * It is important to note that in a number of cases this class
 * exhibits class-specific exemptions from the USB specification.
 * Notably the usage of NAK, STALL and ACK differs from the norm, in
 * that they are used to communicate wait, failed and OK on commands.
 *
 * Also, for certain devices, the interrupt endpoint is used to convey
 * status of a command.
 *
 * Please see http://www.one-eyed-alien.net/~mdharm/linux-usb for more
 * information about this driver.
 *
 * This program is free software; you can redistribute it and/or modify it
 * under the terms of the GNU General Public License as published by the
 * Free Software Foundation; either version 2, or (at your option) any
 * later version.
 *
 * This program is distributed in the hope that it will be useful, but
 * WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
 * General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License along
 * with this program; if not, write to the Free Software Foundation, Inc.,
 * 675 Mass Ave, Cambridge, MA 02139, USA.
 */

#include <linux/errno.h>

#include "usb.h"
#include "initializers.h"
#include "debug.h"
#include "transport.h"

/* This places the Shuttle/SCM USB<->SCSI bridge devices in multi-target
 * mode */
int usb_stor_euscsi_init(struct us_data *us)
{
	int result;

	US_DEBUGP("Attempting to init eUSCSI bridge...\n");
	us->iobuf[0] = 0x1;
	result = usb_stor_control_msg(us, us->send_ctrl_pipe,
			0x0C, USB_RECIP_INTERFACE | USB_TYPE_VENDOR,
			0x01, 0x0, us->iobuf, 0x1, 5000);
	US_DEBUGP("-- result is %d\n", result);

	return 0;
}

/* This function is required to activate all four slots on the UCR-61S2B
 * flash reader */
int usb_stor_ucr61s2b_init(struct us_data *us)
{
	struct bulk_cb_wrap *bcb = (struct bulk_cb_wrap*) us->iobuf;
	struct bulk_cs_wrap *bcs = (struct bulk_cs_wrap*) us->iobuf;
	int res;
	unsigned int partial;
	static char init_string[] = "\xec\x0a\x06\x00$PCCHIPS";

	US_DEBUGP("Sending UCR-61S2B initialization packet...\n");

	bcb->Signature = cpu_to_le32(US_BULK_CB_SIGN);
	bcb->Tag = 0;
	bcb->DataTransferLength = cpu_to_le32(0);
	bcb->Flags = bcb->Lun = 0;
	bcb->Length = sizeof(init_string) - 1;
	memset(bcb->CDB, 0, sizeof(bcb->CDB));
	memcpy(bcb->CDB, init_string, sizeof(init_string) - 1);

	res = usb_stor_bulk_transfer_buf(us, us->send_bulk_pipe, bcb,
			US_BULK_CB_WRAP_LEN, &partial);
	if (res)
		return -EIO;

	US_DEBUGP("Getting status packet...\n");
	res = usb_stor_bulk_transfer_buf(us, us->recv_bulk_pipe, bcs,
			US_BULK_CS_WRAP_LEN, &partial);
	if (res)
		return -EIO;

	return 0;
}

/* This places the HUAWEI usb dongles in multi-port mode */
static int usb_stor_huawei_feature_init(struct us_data *us)
{
	int result;

	result = usb_stor_control_msg(us, us->send_ctrl_pipe,
				      USB_REQ_SET_FEATURE,
				      USB_TYPE_STANDARD | USB_RECIP_DEVICE,
				      0x01, 0x0, NULL, 0x0, 1000);
	US_DEBUGP("Huawei mode set result is %d\n", result);
	return 0;
}

/*
 * It will send a scsi switch command called rewind' to huawei dongle.
 * When the dongle receives this command at the first time,
 * it will reboot immediately. After rebooted, it will ignore this command.
 * So it is  unnecessary to read its response.
 */
static int usb_stor_huawei_scsi_init(struct us_data *us)
{
	int result = 0;
	int act_len = 0;
	struct bulk_cb_wrap *bcbw = (struct bulk_cb_wrap *) us->iobuf;
	char rewind_cmd[] = {0x11, 0x06, 0x20, 0x00, 0x00, 0x01, 0x01, 0x00,
			0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};

	bcbw->Signature = cpu_to_le32(US_BULK_CB_SIGN);
	bcbw->Tag = 0;
	bcbw->DataTransferLength = 0;
	bcbw->Flags = bcbw->Lun = 0;
	bcbw->Length = sizeof(rewind_cmd);
	memset(bcbw->CDB, 0, sizeof(bcbw->CDB));
	memcpy(bcbw->CDB, rewind_cmd, sizeof(rewind_cmd));

	result = usb_stor_bulk_transfer_buf(us, us->send_bulk_pipe, bcbw,
					US_BULK_CB_WRAP_LEN, &act_len);
	US_DEBUGP("transfer actual length=%d, result=%d\n", act_len, result);
	return result;
}

/*
 * It tries to find the supported Huawei USB dongles.
 * In Huawei, they assign the following product IDs
 * for all of their mobile broadband dongles,
 * including the new dongles in the future.
 * So if the product ID is not included in this list,
 * it means it is not Huawei's mobile broadband dongles.
 */
static int usb_stor_huawei_dongles_pid(struct us_data *us)
{
	struct usb_interface_descriptor *idesc;
	int idProduct;

	idesc = &us->pusb_intf->cur_altsetting->desc;
	idProduct = le16_to_cpu(us->pusb_dev->descriptor.idProduct);
	/* The first port is CDROM,
	 * means the dongle in the single port mode,
	 * and a switch command is required to be sent. */
	if (idesc && idesc->bInterfaceNumber == 0) {
		if ((idProduct == 0x1001)
			|| (idProduct == 0x1003)
			|| (idProduct == 0x1004)
			|| (idProduct >= 0x1401 && idProduct <= 0x1500)
			|| (idProduct >= 0x1505 && idProduct <= 0x1600)
			|| (idProduct >= 0x1c02 && idProduct <= 0x2202)) {
			return 1;
		}
	}
	return 0;
}

int usb_stor_huawei_init(struct us_data *us)
{
	int result = 0;

	if (usb_stor_huawei_dongles_pid(us)) {
		if (le16_to_cpu(us->pusb_dev->descriptor.idProduct) >= 0x1446)
			result = usb_stor_huawei_scsi_init(us);
		else
			result = usb_stor_huawei_feature_init(us);
	}
	return result;
}