aboutsummaryrefslogtreecommitdiffstats
blob: 34c4498b800fc7b288bedceb375a7788d375f4d4 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
/*
 * posix-clock.h - support for dynamic clock devices
 *
 * Copyright (C) 2010 OMICRON electronics GmbH
 *
 *  This program is free software; you can redistribute it and/or modify
 *  it under the terms of the GNU General Public License as published by
 *  the Free Software Foundation; either version 2 of the License, or
 *  (at your option) any later version.
 *
 *  This program is distributed in the hope that it will be useful,
 *  but WITHOUT ANY WARRANTY; without even the implied warranty of
 *  MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 *  GNU General Public License for more details.
 *
 *  You should have received a copy of the GNU General Public License
 *  along with this program; if not, write to the Free Software
 *  Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
 */
#ifndef _LINUX_POSIX_CLOCK_H_
#define _LINUX_POSIX_CLOCK_H_

#include <linux/cdev.h>
#include <linux/fs.h>
#include <linux/poll.h>
#include <linux/posix-timers.h>
#include <linux/rwsem.h>

struct posix_clock;

/**
 * struct posix_clock_operations - functional interface to the clock
 *
 * Every posix clock is represented by a character device. Drivers may
 * optionally offer extended capabilities by implementing the
 * character device methods. The character device file operations are
 * first handled by the clock device layer, then passed on to the
 * driver by calling these functions.
 *
 * @owner:          The clock driver should set to THIS_MODULE
 * @clock_adjtime:  Adjust the clock
 * @clock_gettime:  Read the current time
 * @clock_getres:   Get the clock resolution
 * @clock_settime:  Set the current time value
 * @timer_create:   Create a new timer
 * @timer_delete:   Remove a previously created timer
 * @timer_gettime:  Get remaining time and interval of a timer
 * @timer_settime: Set a timer's initial expiration and interval
 * @fasync:         Optional character device fasync method
 * @mmap:           Optional character device mmap method
 * @open:           Optional character device open method
 * @release:        Optional character device release method
 * @ioctl:          Optional character device ioctl method
 * @read:           Optional character device read method
 * @poll:           Optional character device poll method
 */
struct posix_clock_operations {
	struct module *owner;

	int  (*clock_adjtime)(struct posix_clock *pc, struct timex *tx);

	int  (*clock_gettime)(struct posix_clock *pc, struct timespec *ts);

	int  (*clock_getres) (struct posix_clock *pc, struct timespec *ts);

	int  (*clock_settime)(struct posix_clock *pc,
			      const struct timespec *ts);

	int  (*timer_create) (struct posix_clock *pc, struct k_itimer *kit);

	int  (*timer_delete) (struct posix_clock *pc, struct k_itimer *kit);

	void (*timer_gettime)(struct posix_clock *pc,
			      struct k_itimer *kit, struct itimerspec *tsp);

	int  (*timer_settime)(struct posix_clock *pc,
			      struct k_itimer *kit, int flags,
			      struct itimerspec *tsp, struct itimerspec *old);
	/*
	 * Optional character device methods:
	 */
	int     (*fasync)  (struct posix_clock *pc,
			    int fd, struct file *file, int on);

	long    (*ioctl)   (struct posix_clock *pc,
			    unsigned int cmd, unsigned long arg);

	int     (*mmap)    (struct posix_clock *pc,
			    struct vm_area_struct *vma);

	int     (*open)    (struct posix_clock *pc, fmode_t f_mode);

	uint    (*poll)    (struct posix_clock *pc,
			    struct file *file, poll_table *wait);

	int     (*release) (struct posix_clock *pc);

	ssize_t (*read)    (struct posix_clock *pc,
			    uint flags, char __user *buf, size_t cnt);
};

/**
 * struct posix_clock - represents a dynamic posix clock
 *
 * @ops:     Functional interface to the clock
 * @cdev:    Character device instance for this clock
 * @kref:    Reference count.
 * @rwsem:   Protects the 'zombie' field from concurrent access.
 * @zombie:  If 'zombie' is true, then the hardware has disappeared.
 * @release: A function to free the structure when the reference count reaches
 *           zero. May be NULL if structure is statically allocated.
 *
 * Drivers should embed their struct posix_clock within a private
 * structure, obtaining a reference to it during callbacks using
 * container_of().
 */
struct posix_clock {
	struct posix_clock_operations ops;
	struct cdev cdev;
	struct kref kref;
	struct rw_semaphore rwsem;
	bool zombie;
	void (*release)(struct posix_clock *clk);
};

/**
 * posix_clock_register() - register a new clock
 * @clk:   Pointer to the clock. Caller must provide 'ops' and 'release'
 * @devid: Allocated device id
 *
 * A clock driver calls this function to register itself with the
 * clock device subsystem. If 'clk' points to dynamically allocated
 * memory, then the caller must provide a 'release' function to free
 * that memory.
 *
 * Returns zero on success, non-zero otherwise.
 */
int posix_clock_register(struct posix_clock *clk, dev_t devid);

/**
 * posix_clock_unregister() - unregister a clock
 * @clk: Clock instance previously registered via posix_clock_register()
 *
 * A clock driver calls this function to remove itself from the clock
 * device subsystem. The posix_clock itself will remain (in an
 * inactive state) until its reference count drops to zero, at which
 * point it will be deallocated with its 'release' method.
 */
void posix_clock_unregister(struct posix_clock *clk);

#endif