aboutsummaryrefslogtreecommitdiffstats
blob: 2f322c38bd4d61d01e63bb89d2fa134e9b809ae6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
#ifndef _LINUX_TRACEPOINT_H
#define _LINUX_TRACEPOINT_H

/*
 * Kernel Tracepoint API.
 *
 * See Documentation/trace/tracepoints.txt.
 *
 * (C) Copyright 2008 Mathieu Desnoyers <mathieu.desnoyers@polymtl.ca>
 *
 * Heavily inspired from the Linux Kernel Markers.
 *
 * This file is released under the GPLv2.
 * See the file COPYING for more details.
 */

#include <linux/errno.h>
#include <linux/types.h>
#include <linux/rcupdate.h>
#include <linux/static_key.h>

struct module;
struct tracepoint;

struct tracepoint_func {
	void *func;
	void *data;
};

struct tracepoint {
	const char *name;		/* Tracepoint name */
	struct static_key key;
	void (*regfunc)(void);
	void (*unregfunc)(void);
	struct tracepoint_func __rcu *funcs;
};

/*
 * Connect a probe to a tracepoint.
 * Internal API, should not be used directly.
 */
extern int tracepoint_probe_register(const char *name, void *probe, void *data);

/*
 * Disconnect a probe from a tracepoint.
 * Internal API, should not be used directly.
 */
extern int
tracepoint_probe_unregister(const char *name, void *probe, void *data);

extern int tracepoint_probe_register_noupdate(const char *name, void *probe,
					      void *data);
extern int tracepoint_probe_unregister_noupdate(const char *name, void *probe,
						void *data);
extern void tracepoint_probe_update_all(void);

#ifdef CONFIG_MODULES
struct tp_module {
	struct list_head list;
	unsigned int num_tracepoints;
	struct tracepoint * const *tracepoints_ptrs;
};
#endif /* CONFIG_MODULES */

struct tracepoint_iter {
#ifdef CONFIG_MODULES
	struct tp_module *module;
#endif /* CONFIG_MODULES */
	struct tracepoint * const *tracepoint;
};

extern void tracepoint_iter_start(struct tracepoint_iter *iter);
extern void tracepoint_iter_next(struct tracepoint_iter *iter);
extern void tracepoint_iter_stop(struct tracepoint_iter *iter);
extern void tracepoint_iter_reset(struct tracepoint_iter *iter);

/*
 * tracepoint_synchronize_unregister must be called between the last tracepoint
 * probe unregistration and the end of module exit to make sure there is no
 * caller executing a probe when it is freed.
 */
static inline void tracepoint_synchronize_unregister(void)
{
	synchronize_sched();
}

#define PARAMS(args...) args

#endif /* _LINUX_TRACEPOINT_H */

/*
 * Note: we keep the TRACE_EVENT and DECLARE_TRACE outside the include
 *  file ifdef protection.
 *  This is due to the way trace events work. If a file includes two
 *  trace event headers under one "CREATE_TRACE_POINTS" the first include
 *  will override the TRACE_EVENT and break the second include.
 */

#ifndef DECLARE_TRACE

#define TP_PROTO(args...)	args
#define TP_ARGS(args...)	args
#define TP_CONDITION(args...)	args

#ifdef CONFIG_TRACEPOINTS

/*
 * it_func[0] is never NULL because there is at least one element in the array
 * when the array itself is non NULL.
 *
 * Note, the proto and args passed in includes "__data" as the first parameter.
 * The reason for this is to handle the "void" prototype. If a tracepoint
 * has a "void" prototype, then it is invalid to declare a function
 * as "(void *, void)". The DECLARE_TRACE_NOARGS() will pass in just
 * "void *data", where as the DECLARE_TRACE() will pass in "void *data, proto".
 */
#define __DO_TRACE(tp, proto, args, cond, prercu, postrcu)		\
	do {								\
		struct tracepoint_func *it_func_ptr;			\
		void *it_func;						\
		void *__data;						\
									\
		if (!(cond))						\
			return;						\
		prercu;							\
		rcu_read_lock_sched_notrace();				\
		it_func_ptr = rcu_dereference_sched((tp)->funcs);	\
		if (it_func_ptr) {					\
			do {						\
				it_func = (it_func_ptr)->func;		\
				__data = (it_func_ptr)->data;		\
				((void(*)(proto))(it_func))(args);	\
			} while ((++it_func_ptr)->func);		\
		}							\
		rcu_read_unlock_sched_notrace();			\
		postrcu;						\
	} while (0)

#ifndef MODULE
#define __DECLARE_TRACE_RCU(name, proto, args, cond, data_proto, data_args)	\
	static inline void trace_##name##_rcuidle(proto)		\
	{								\
		if (static_key_false(&__tracepoint_##name.key))		\
			__DO_TRACE(&__tracepoint_##name,		\
				TP_PROTO(data_proto),			\
				TP_ARGS(data_args),			\
				TP_CONDITION(cond),			\
				rcu_idle_exit(),			\
				rcu_idle_enter());			\
	}
#else
#define __DECLARE_TRACE_RCU(name, proto, args, cond, data_proto, data_args)
#endif

/*
 * Make sure the alignment of the structure in the __tracepoints section will
 * not add unwanted padding between the beginning of the section and the
 * structure. Force alignment to the same alignment as the section start.
 */
#define __DECLARE_TRACE(name, proto, args, cond, data_proto, data_args) \
	extern struct tracepoint __tracepoint_##name;			\
	static inline void trace_##name(proto)				\
	{								\
		if (static_key_false(&__tracepoint_##name.key))		\
			__DO_TRACE(&__tracepoint_##name,		\
				TP_PROTO(data_proto),			\
				TP_ARGS(data_args),			\
				TP_CONDITION(cond),,);			\
	}								\
	__DECLARE_TRACE_RCU(name, PARAMS(proto), PARAMS(args),		\
		PARAMS(cond), PARAMS(data_proto), PARAMS(data_args))	\
	static inline int						\
	register_trace_##name(void (*probe)(data_proto), void *data)	\
	{								\
		return tracepoint_probe_register(#name, (void *)probe,	\
						 data);			\
	}								\
	static inline int						\
	unregister_trace_##name(void (*probe)(data_proto), void *data)	\
	{								\
		return tracepoint_probe_unregister(#name, (void *)probe, \
						   data);		\
	}								\
	static inline void						\
	check_trace_callback_type_##name(void (*cb)(data_proto))	\
	{								\
	}

/*
 * We have no guarantee that gcc and the linker won't up-align the tracepoint
 * structures, so we create an array of pointers that will be used for iteration
 * on the tracepoints.
 */
#define DEFINE_TRACE_FN(name, reg, unreg)				 \
	static const char __tpstrtab_##name[]				 \
	__attribute__((section("__tracepoints_strings"))) = #name;	 \
	struct tracepoint __tracepoint_##name				 \
	__attribute__((section("__tracepoints"))) =			 \
		{ __tpstrtab_##name, STATIC_KEY_INIT_FALSE, reg, unreg, NULL };\
	static struct tracepoint * const __tracepoint_ptr_##name __used	 \
	__attribute__((section("__tracepoints_ptrs"))) =		 \
		&__tracepoint_##name;

#define DEFINE_TRACE(name)						\
	DEFINE_TRACE_FN(name, NULL, NULL);

#define EXPORT_TRACEPOINT_SYMBOL_GPL(name)				\
	EXPORT_SYMBOL_GPL(__tracepoint_##name)
#define EXPORT_TRACEPOINT_SYMBOL(name)					\
	EXPORT_SYMBOL(__tracepoint_##name)

#else /* !CONFIG_TRACEPOINTS */
#define __DECLARE_TRACE(name, proto, args, cond, data_proto, data_args) \
	static inline void trace_##name(proto)				\
	{ }								\
	static inline void trace_##name##_rcuidle(proto)		\
	{ }								\
	static inline int						\
	register_trace_##name(void (*probe)(data_proto),		\
			      void *data)				\
	{								\
		return -ENOSYS;						\
	}								\
	static inline int						\
	unregister_trace_##name(void (*probe)(data_proto),		\
				void *data)				\
	{								\
		return -ENOSYS;						\
	}								\
	static inline void check_trace_callback_type_##name(void (*cb)(data_proto)) \
	{								\
	}

#define DEFINE_TRACE_FN(name, reg, unreg)
#define DEFINE_TRACE(name)
#define EXPORT_TRACEPOINT_SYMBOL_GPL(name)
#define EXPORT_TRACEPOINT_SYMBOL(name)

#endif /* CONFIG_TRACEPOINTS */

/*
 * The need for the DECLARE_TRACE_NOARGS() is to handle the prototype
 * (void). "void" is a special value in a function prototype and can
 * not be combined with other arguments. Since the DECLARE_TRACE()
 * macro adds a data element at the beginning of the prototype,
 * we need a way to differentiate "(void *data, proto)" from
 * "(void *data, void)". The second prototype is invalid.
 *
 * DECLARE_TRACE_NOARGS() passes "void" as the tracepoint prototype
 * and "void *__data" as the callback prototype.
 *
 * DECLARE_TRACE() passes "proto" as the tracepoint protoype and
 * "void *__data, proto" as the callback prototype.
 */
#define DECLARE_TRACE_NOARGS(name)					\
		__DECLARE_TRACE(name, void, , 1, void *__data, __data)

#define DECLARE_TRACE(name, proto, args)				\
		__DECLARE_TRACE(name, PARAMS(proto), PARAMS(args), 1,	\
				PARAMS(void *__data, proto),		\
				PARAMS(__data, args))

#define DECLARE_TRACE_CONDITION(name, proto, args, cond)		\
	__DECLARE_TRACE(name, PARAMS(proto), PARAMS(args), PARAMS(cond), \
			PARAMS(void *__data, proto),			\
			PARAMS(__data, args))

#define TRACE_EVENT_FLAGS(event, flag)

#endif /* DECLARE_TRACE */

#ifndef TRACE_EVENT
/*
 * For use with the TRACE_EVENT macro:
 *
 * We define a tracepoint, its arguments, its printk format
 * and its 'fast binay record' layout.
 *
 * Firstly, name your tracepoint via TRACE_EVENT(name : the
 * 'subsystem_event' notation is fine.
 *
 * Think about this whole construct as the
 * 'trace_sched_switch() function' from now on.
 *
 *
 *  TRACE_EVENT(sched_switch,
 *
 *	*
 *	* A function has a regular function arguments
 *	* prototype, declare it via TP_PROTO():
 *	*
 *
 *	TP_PROTO(struct rq *rq, struct task_struct *prev,
 *		 struct task_struct *next),
 *
 *	*
 *	* Define the call signature of the 'function'.
 *	* (Design sidenote: we use this instead of a
 *	*  TP_PROTO1/TP_PROTO2/TP_PROTO3 ugliness.)
 *	*
 *
 *	TP_ARGS(rq, prev, next),
 *
 *	*
 *	* Fast binary tracing: define the trace record via
 *	* TP_STRUCT__entry(). You can think about it like a
 *	* regular C structure local variable definition.
 *	*
 *	* This is how the trace record is structured and will
 *	* be saved into the ring buffer. These are the fields
 *	* that will be exposed to user-space in
 *	* /sys/kernel/debug/tracing/events/<*>/format.
 *	*
 *	* The declared 'local variable' is called '__entry'
 *	*
 *	* __field(pid_t, prev_prid) is equivalent to a standard declariton:
 *	*
 *	*	pid_t	prev_pid;
 *	*
 *	* __array(char, prev_comm, TASK_COMM_LEN) is equivalent to:
 *	*
 *	*	char	prev_comm[TASK_COMM_LEN];
 *	*
 *
 *	TP_STRUCT__entry(
 *		__array(	char,	prev_comm,	TASK_COMM_LEN	)
 *		__field(	pid_t,	prev_pid			)
 *		__field(	int,	prev_prio			)
 *		__array(	char,	next_comm,	TASK_COMM_LEN	)
 *		__field(	pid_t,	next_pid			)
 *		__field(	int,	next_prio			)
 *	),
 *
 *	*
 *	* Assign the entry into the trace record, by embedding
 *	* a full C statement block into TP_fast_assign(). You
 *	* can refer to the trace record as '__entry' -
 *	* otherwise you can put arbitrary C code in here.
 *	*
 *	* Note: this C code will execute every time a trace event
 *	* happens, on an active tracepoint.
 *	*
 *
 *	TP_fast_assign(
 *		memcpy(__entry->next_comm, next->comm, TASK_COMM_LEN);
 *		__entry->prev_pid	= prev->pid;
 *		__entry->prev_prio	= prev->prio;
 *		memcpy(__entry->prev_comm, prev->comm, TASK_COMM_LEN);
 *		__entry->next_pid	= next->pid;
 *		__entry->next_prio	= next->prio;
 *	),
 *
 *	*
 *	* Formatted output of a trace record via TP_printk().
 *	* This is how the tracepoint will appear under ftrace
 *	* plugins that make use of this tracepoint.
 *	*
 *	* (raw-binary tracing wont actually perform this step.)
 *	*
 *
 *	TP_printk("task %s:%d [%d] ==> %s:%d [%d]",
 *		__entry->prev_comm, __entry->prev_pid, __entry->prev_prio,
 *		__entry->next_comm, __entry->next_pid, __entry->next_prio),
 *
 * );
 *
 * This macro construct is thus used for the regular printk format
 * tracing setup, it is used to construct a function pointer based
 * tracepoint callback (this is used by programmatic plugins and
 * can also by used by generic instrumentation like SystemTap), and
 * it is also used to expose a structured trace record in
 * /sys/kernel/debug/tracing/events/.
 *
 * A set of (un)registration functions can be passed to the variant
 * TRACE_EVENT_FN to perform any (un)registration work.
 */

#define DECLARE_EVENT_CLASS(name, proto, args, tstruct, assign, print)
#define DEFINE_EVENT(template, name, proto, args)		\
	DECLARE_TRACE(name, PARAMS(proto), PARAMS(args))
#define DEFINE_EVENT_PRINT(template, name, proto, args, print)	\
	DECLARE_TRACE(name, PARAMS(proto), PARAMS(args))
#define DEFINE_EVENT_CONDITION(template, name, proto,		\
			       args, cond)			\
	DECLARE_TRACE_CONDITION(name, PARAMS(proto),		\
				PARAMS(args), PARAMS(cond))

#define TRACE_EVENT(name, proto, args, struct, assign, print)	\
	DECLARE_TRACE(name, PARAMS(proto), PARAMS(args))
#define TRACE_EVENT_FN(name, proto, args, struct,		\
		assign, print, reg, unreg)			\
	DECLARE_TRACE(name, PARAMS(proto), PARAMS(args))
#define TRACE_EVENT_CONDITION(name, proto, args, cond,		\
			      struct, assign, print)		\
	DECLARE_TRACE_CONDITION(name, PARAMS(proto),		\
				PARAMS(args), PARAMS(cond))

#define TRACE_EVENT_FLAGS(event, flag)

#endif /* ifdef TRACE_EVENT (see note above) */