aboutsummaryrefslogtreecommitdiffstats
blob: 267739d851791b0a3e4526a3be5fb4944d8b507e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
/*
 * init/noinitramfs.c
 *
 * Copyright (C) 2006, NXP Semiconductors, All Rights Reserved
 * Author: Jean-Paul Saman <jean-paul.saman@nxp.com>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; version 2 of the License.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
 */
#include <linux/init.h>
#include <linux/stat.h>
#include <linux/kdev_t.h>
#include <linux/syscalls.h>

/*
 * Create a simple rootfs that is similar to the default initramfs
 */
static int __init default_rootfs(void)
{
	int err;

	err = sys_mkdir((const char __user __force *) "/dev", 0755);
	if (err < 0)
		goto out;

	err = sys_mknod((const char __user __force *) "/dev/console",
			S_IFCHR | S_IRUSR | S_IWUSR,
			new_encode_dev(MKDEV(5, 1)));
	if (err < 0)
		goto out;

	err = sys_mkdir((const char __user __force *) "/root", 0700);
	if (err < 0)
		goto out;

	return 0;

out:
	printk(KERN_WARNING "Failed to create a rootfs\n");
	return err;
}
rootfs_initcall(default_rootfs);