aboutsummaryrefslogtreecommitdiffstats
blob: 75cdb77fa49d2cc84459360ad939a76be2596f7e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
#
# Library configuration
#

config BINARY_PRINTF
	def_bool n

menu "Library routines"

config RAID6_PQ
	tristate

config BITREVERSE
	tristate

config RATIONAL
	boolean

config GENERIC_STRNCPY_FROM_USER
	bool

config GENERIC_STRNLEN_USER
	bool

config GENERIC_FIND_FIRST_BIT
	bool

config NO_GENERIC_PCI_IOPORT_MAP
	bool

config GENERIC_PCI_IOMAP
	bool

config GENERIC_IOMAP
	bool
	select GENERIC_PCI_IOMAP

config GENERIC_IO
	boolean
	default n

config STMP_DEVICE
	bool

config PERCPU_RWSEM
	boolean

config CRC_CCITT
	tristate "CRC-CCITT functions"
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC-CCITT functions, but a module built outside
	  the kernel tree does. Such modules that use library CRC-CCITT
	  functions require M here.

config CRC16
	tristate "CRC16 functions"
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC16 functions, but a module built outside
	  the kernel tree does. Such modules that use library CRC16
	  functions require M here.

config CRC_T10DIF
	tristate "CRC calculation for the T10 Data Integrity Field"
	help
	  This option is only needed if a module that's not in the
	  kernel tree needs to calculate CRC checks for use with the
	  SCSI data integrity subsystem.

config CRC_ITU_T
	tristate "CRC ITU-T V.41 functions"
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC ITU-T V.41 functions, but a module built outside
	  the kernel tree does. Such modules that use library CRC ITU-T V.41
	  functions require M here.

config CRC32
	tristate "CRC32/CRC32c functions"
	default y
	select BITREVERSE
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC32/CRC32c functions, but a module built outside
	  the kernel tree does. Such modules that use library CRC32/CRC32c
	  functions require M here.

config CRC32_SELFTEST
	bool "CRC32 perform self test on init"
	default n
	depends on CRC32
	help
	  This option enables the CRC32 library functions to perform a
	  self test on initialization. The self test computes crc32_le
	  and crc32_be over byte strings with random alignment and length
	  and computes the total elapsed time and number of bytes processed.

choice
	prompt "CRC32 implementation"
	depends on CRC32
	default CRC32_SLICEBY8
	help
	  This option allows a kernel builder to override the default choice
	  of CRC32 algorithm.  Choose the default ("slice by 8") unless you
	  know that you need one of the others.

config CRC32_SLICEBY8
	bool "Slice by 8 bytes"
	help
	  Calculate checksum 8 bytes at a time with a clever slicing algorithm.
	  This is the fastest algorithm, but comes with a 8KiB lookup table.
	  Most modern processors have enough cache to hold this table without
	  thrashing the cache.

	  This is the default implementation choice.  Choose this one unless
	  you have a good reason not to.

config CRC32_SLICEBY4
	bool "Slice by 4 bytes"
	help
	  Calculate checksum 4 bytes at a time with a clever slicing algorithm.
	  This is a bit slower than slice by 8, but has a smaller 4KiB lookup
	  table.

	  Only choose this option if you know what you are doing.

config CRC32_SARWATE
	bool "Sarwate's Algorithm (one byte at a time)"
	help
	  Calculate checksum a byte at a time using Sarwate's algorithm.  This
	  is not particularly fast, but has a small 256 byte lookup table.

	  Only choose this option if you know what you are doing.

config CRC32_BIT
	bool "Classic Algorithm (one bit at a time)"
	help
	  Calculate checksum one bit at a time.  This is VERY slow, but has
	  no lookup table.  This is provided as a debugging option.

	  Only choose this option if you are debugging crc32.

endchoice

config CRC7
	tristate "CRC7 functions"
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC7 functions, but a module built outside
	  the kernel tree does. Such modules that use library CRC7
	  functions require M here.

config LIBCRC32C
	tristate "CRC32c (Castagnoli, et al) Cyclic Redundancy-Check"
	select CRYPTO
	select CRYPTO_CRC32C
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require CRC32c functions, but a module built outside the
	  kernel tree does. Such modules that use library CRC32c functions
	  require M here.  See Castagnoli93.
	  Module will be libcrc32c.

config CRC8
	tristate "CRC8 function"
	help
	  This option provides CRC8 function. Drivers may select this
	  when they need to do cyclic redundancy check according CRC8
	  algorithm. Module will be called crc8.

config AUDIT_GENERIC
	bool
	depends on AUDIT && !AUDIT_ARCH
	default y

#
# compression support is select'ed if needed
#
config ZLIB_INFLATE
	tristate

config ZLIB_DEFLATE
	tristate

config LZO_COMPRESS
	tristate

config LZO_DECOMPRESS
	tristate

source "lib/xz/Kconfig"

#
# These all provide a common interface (hence the apparent duplication with
# ZLIB_INFLATE; DECOMPRESS_GZIP is just a wrapper.)
#
config DECOMPRESS_GZIP
	select ZLIB_INFLATE
	tristate

config DECOMPRESS_BZIP2
	tristate

config DECOMPRESS_LZMA
	tristate

config DECOMPRESS_XZ
	select XZ_DEC
	tristate

config DECOMPRESS_LZO
	select LZO_DECOMPRESS
	tristate

#
# Generic allocator support is selected if needed
#
config GENERIC_ALLOCATOR
	boolean

#
# reed solomon support is select'ed if needed
#
config REED_SOLOMON
	tristate
	
config REED_SOLOMON_ENC8
	boolean

config REED_SOLOMON_DEC8
	boolean

config REED_SOLOMON_ENC16
	boolean

config REED_SOLOMON_DEC16
	boolean

#
# BCH support is selected if needed
#
config BCH
	tristate

config BCH_CONST_PARAMS
	boolean
	help
	  Drivers may select this option to force specific constant
	  values for parameters 'm' (Galois field order) and 't'
	  (error correction capability). Those specific values must
	  be set by declaring default values for symbols BCH_CONST_M
	  and BCH_CONST_T.
	  Doing so will enable extra compiler optimizations,
	  improving encoding and decoding performance up to 2x for
	  usual (m,t) values (typically such that m*t < 200).
	  When this option is selected, the BCH library supports
	  only a single (m,t) configuration. This is mainly useful
	  for NAND flash board drivers requiring known, fixed BCH
	  parameters.

config BCH_CONST_M
	int
	range 5 15
	help
	  Constant value for Galois field order 'm'. If 'k' is the
	  number of data bits to protect, 'm' should be chosen such
	  that (k + m*t) <= 2**m - 1.
	  Drivers should declare a default value for this symbol if
	  they select option BCH_CONST_PARAMS.

config BCH_CONST_T
	int
	help
	  Constant value for error correction capability in bits 't'.
	  Drivers should declare a default value for this symbol if
	  they select option BCH_CONST_PARAMS.

#
# Textsearch support is select'ed if needed
#
config TEXTSEARCH
	boolean

config TEXTSEARCH_KMP
	tristate

config TEXTSEARCH_BM
	tristate

config TEXTSEARCH_FSM
	tristate

config BTREE
	boolean

config HAS_IOMEM
	boolean
	depends on !NO_IOMEM
	select GENERIC_IO
	default y

config HAS_IOPORT
	boolean
	depends on HAS_IOMEM && !NO_IOPORT
	default y

config HAS_DMA
	boolean
	depends on !NO_DMA
	default y

config CHECK_SIGNATURE
	bool

config CPUMASK_OFFSTACK
	bool "Force CPU masks off stack" if DEBUG_PER_CPU_MAPS
	help
	  Use dynamic allocation for cpumask_var_t, instead of putting
	  them on the stack.  This is a bit more expensive, but avoids
	  stack overflow.

config DISABLE_OBSOLETE_CPUMASK_FUNCTIONS
       bool "Disable obsolete cpumask functions" if DEBUG_PER_CPU_MAPS
       depends on EXPERIMENTAL && BROKEN

config CPU_RMAP
	bool
	depends on SMP

config DQL
	bool

#
# Netlink attribute parsing support is select'ed if needed
#
config NLATTR
	bool

#
# Generic 64-bit atomic support is selected if needed
#
config GENERIC_ATOMIC64
       bool

config ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE
	def_bool y if GENERIC_ATOMIC64

config LRU_CACHE
	tristate

config AVERAGE
	bool "Averaging functions"
	help
	  This option is provided for the case where no in-kernel-tree
	  modules require averaging functions, but a module built outside
	  the kernel tree does. Such modules that use library averaging
	  functions require Y here.

	  If unsure, say N.

config CLZ_TAB
	bool

config CORDIC
	tristate "CORDIC algorithm"
	help
	  This option provides an implementation of the CORDIC algorithm;
	  calculations are in fixed point. Module will be called cordic.

config DDR
	bool "JEDEC DDR data"
	help
	  Data from JEDEC specs for DDR SDRAM memories,
	  particularly the AC timing parameters and addressing
	  information. This data is useful for drivers handling
	  DDR SDRAM controllers.

config MPILIB
	tristate
	select CLZ_TAB
	help
	  Multiprecision maths library from GnuPG.
	  It is used to implement RSA digital signature verification,
	  which is used by IMA/EVM digital signature extension.

config SIGNATURE
	tristate
	depends on KEYS && CRYPTO
	select CRYPTO_SHA1
	select MPILIB
	help
	  Digital signature verification. Currently only RSA is supported.
	  Implementation is done using GnuPG MPI library

#
# libfdt files, only selected if needed.
#
config LIBFDT
	bool

config OID_REGISTRY
	tristate
	help
	  Enable fast lookup object identifier registry.

endmenu