aboutsummaryrefslogtreecommitdiffstats
blob: 88fa54d158e49bb5cc981e5b15fb718543e506f6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
/*
 *  linux/mm/mmu_notifier.c
 *
 *  Copyright (C) 2008  Qumranet, Inc.
 *  Copyright (C) 2008  SGI
 *             Christoph Lameter <clameter@sgi.com>
 *
 *  This work is licensed under the terms of the GNU GPL, version 2. See
 *  the COPYING file in the top-level directory.
 */

#include <linux/rculist.h>
#include <linux/mmu_notifier.h>
#include <linux/module.h>
#include <linux/mm.h>
#include <linux/err.h>
#include <linux/srcu.h>
#include <linux/rcupdate.h>
#include <linux/sched.h>
#include <linux/slab.h>

/* global SRCU for all MMs */
static struct srcu_struct srcu;

/*
 * This function can't run concurrently against mmu_notifier_register
 * because mm->mm_users > 0 during mmu_notifier_register and exit_mmap
 * runs with mm_users == 0. Other tasks may still invoke mmu notifiers
 * in parallel despite there being no task using this mm any more,
 * through the vmas outside of the exit_mmap context, such as with
 * vmtruncate. This serializes against mmu_notifier_unregister with
 * the mmu_notifier_mm->lock in addition to SRCU and it serializes
 * against the other mmu notifiers with SRCU. struct mmu_notifier_mm
 * can't go away from under us as exit_mmap holds an mm_count pin
 * itself.
 */
void __mmu_notifier_release(struct mm_struct *mm)
{
	struct mmu_notifier *mn;
	int id;

	/*
	 * srcu_read_lock() here will block synchronize_srcu() in
	 * mmu_notifier_unregister() until all registered
	 * ->release() callouts this function makes have
	 * returned.
	 */
	id = srcu_read_lock(&srcu);
	spin_lock(&mm->mmu_notifier_mm->lock);
	while (unlikely(!hlist_empty(&mm->mmu_notifier_mm->list))) {
		mn = hlist_entry(mm->mmu_notifier_mm->list.first,
				 struct mmu_notifier,
				 hlist);

		/*
		 * Unlink.  This will prevent mmu_notifier_unregister()
		 * from also making the ->release() callout.
		 */
		hlist_del_init_rcu(&mn->hlist);
		spin_unlock(&mm->mmu_notifier_mm->lock);

		/*
		 * Clear sptes. (see 'release' description in mmu_notifier.h)
		 */
		if (mn->ops->release)
			mn->ops->release(mn, mm);

		spin_lock(&mm->mmu_notifier_mm->lock);
	}
	spin_unlock(&mm->mmu_notifier_mm->lock);

	/*
	 * All callouts to ->release() which we have done are complete.
	 * Allow synchronize_srcu() in mmu_notifier_unregister() to complete
	 */
	srcu_read_unlock(&srcu, id);

	/*
	 * mmu_notifier_unregister() may have unlinked a notifier and may
	 * still be calling out to it.	Additionally, other notifiers
	 * may have been active via vmtruncate() et. al. Block here
	 * to ensure that all notifier callouts for this mm have been
	 * completed and the sptes are really cleaned up before returning
	 * to exit_mmap().
	 */
	synchronize_srcu(&srcu);
}

/*
 * If no young bitflag is supported by the hardware, ->clear_flush_young can
 * unmap the address and return 1 or 0 depending if the mapping previously
 * existed or not.
 */
int __mmu_notifier_clear_flush_young(struct mm_struct *mm,
					unsigned long address)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int young = 0, id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->clear_flush_young)
			young |= mn->ops->clear_flush_young(mn, mm, address);
	}
	srcu_read_unlock(&srcu, id);

	return young;
}

int __mmu_notifier_test_young(struct mm_struct *mm,
			      unsigned long address)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int young = 0, id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->test_young) {
			young = mn->ops->test_young(mn, mm, address);
			if (young)
				break;
		}
	}
	srcu_read_unlock(&srcu, id);

	return young;
}

void __mmu_notifier_change_pte(struct mm_struct *mm, unsigned long address,
			       pte_t pte)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->change_pte)
			mn->ops->change_pte(mn, mm, address, pte);
		/*
		 * Some drivers don't have change_pte,
		 * so we must call invalidate_page in that case.
		 */
		else if (mn->ops->invalidate_page)
			mn->ops->invalidate_page(mn, mm, address);
	}
	srcu_read_unlock(&srcu, id);
}

void __mmu_notifier_invalidate_page(struct mm_struct *mm,
					  unsigned long address)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->invalidate_page)
			mn->ops->invalidate_page(mn, mm, address);
	}
	srcu_read_unlock(&srcu, id);
}

void __mmu_notifier_invalidate_range_start(struct mm_struct *mm,
				  unsigned long start, unsigned long end)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->invalidate_range_start)
			mn->ops->invalidate_range_start(mn, mm, start, end);
	}
	srcu_read_unlock(&srcu, id);
}

void __mmu_notifier_invalidate_range_end(struct mm_struct *mm,
				  unsigned long start, unsigned long end)
{
	struct mmu_notifier *mn;
	struct hlist_node *n;
	int id;

	id = srcu_read_lock(&srcu);
	hlist_for_each_entry_rcu(mn, n, &mm->mmu_notifier_mm->list, hlist) {
		if (mn->ops->invalidate_range_end)
			mn->ops->invalidate_range_end(mn, mm, start, end);
	}
	srcu_read_unlock(&srcu, id);
}

static int do_mmu_notifier_register(struct mmu_notifier *mn,
				    struct mm_struct *mm,
				    int take_mmap_sem)
{
	struct mmu_notifier_mm *mmu_notifier_mm;
	int ret;

	BUG_ON(atomic_read(&mm->mm_users) <= 0);

	/*
	* Verify that mmu_notifier_init() already run and the global srcu is
	* initialized.
	*/
	BUG_ON(!srcu.per_cpu_ref);

	ret = -ENOMEM;
	mmu_notifier_mm = kmalloc(sizeof(struct mmu_notifier_mm), GFP_KERNEL);
	if (unlikely(!mmu_notifier_mm))
		goto out;

	if (take_mmap_sem)
		down_write(&mm->mmap_sem);
	ret = mm_take_all_locks(mm);
	if (unlikely(ret))
		goto out_cleanup;

	if (!mm_has_notifiers(mm)) {
		INIT_HLIST_HEAD(&mmu_notifier_mm->list);
		spin_lock_init(&mmu_notifier_mm->lock);
		mm->mmu_notifier_mm = mmu_notifier_mm;
		mmu_notifier_mm = NULL;
	}
	atomic_inc(&mm->mm_count);

	/*
	 * Serialize the update against mmu_notifier_unregister. A
	 * side note: mmu_notifier_release can't run concurrently with
	 * us because we hold the mm_users pin (either implicitly as
	 * current->mm or explicitly with get_task_mm() or similar).
	 * We can't race against any other mmu notifier method either
	 * thanks to mm_take_all_locks().
	 */
	spin_lock(&mm->mmu_notifier_mm->lock);
	hlist_add_head(&mn->hlist, &mm->mmu_notifier_mm->list);
	spin_unlock(&mm->mmu_notifier_mm->lock);

	mm_drop_all_locks(mm);
out_cleanup:
	if (take_mmap_sem)
		up_write(&mm->mmap_sem);
	/* kfree() does nothing if mmu_notifier_mm is NULL */
	kfree(mmu_notifier_mm);
out:
	BUG_ON(atomic_read(&mm->mm_users) <= 0);
	return ret;
}

/*
 * Must not hold mmap_sem nor any other VM related lock when calling
 * this registration function. Must also ensure mm_users can't go down
 * to zero while this runs to avoid races with mmu_notifier_release,
 * so mm has to be current->mm or the mm should be pinned safely such
 * as with get_task_mm(). If the mm is not current->mm, the mm_users
 * pin should be released by calling mmput after mmu_notifier_register
 * returns. mmu_notifier_unregister must be always called to
 * unregister the notifier. mm_count is automatically pinned to allow
 * mmu_notifier_unregister to safely run at any time later, before or
 * after exit_mmap. ->release will always be called before exit_mmap
 * frees the pages.
 */
int mmu_notifier_register(struct mmu_notifier *mn, struct mm_struct *mm)
{
	return do_mmu_notifier_register(mn, mm, 1);
}
EXPORT_SYMBOL_GPL(mmu_notifier_register);

/*
 * Same as mmu_notifier_register but here the caller must hold the
 * mmap_sem in write mode.
 */
int __mmu_notifier_register(struct mmu_notifier *mn, struct mm_struct *mm)
{
	return do_mmu_notifier_register(mn, mm, 0);
}
EXPORT_SYMBOL_GPL(__mmu_notifier_register);

/* this is called after the last mmu_notifier_unregister() returned */
void __mmu_notifier_mm_destroy(struct mm_struct *mm)
{
	BUG_ON(!hlist_empty(&mm->mmu_notifier_mm->list));
	kfree(mm->mmu_notifier_mm);
	mm->mmu_notifier_mm = LIST_POISON1; /* debug */
}

/*
 * This releases the mm_count pin automatically and frees the mm
 * structure if it was the last user of it. It serializes against
 * running mmu notifiers with SRCU and against mmu_notifier_unregister
 * with the unregister lock + SRCU. All sptes must be dropped before
 * calling mmu_notifier_unregister. ->release or any other notifier
 * method may be invoked concurrently with mmu_notifier_unregister,
 * and only after mmu_notifier_unregister returned we're guaranteed
 * that ->release or any other method can't run anymore.
 */
void mmu_notifier_unregister(struct mmu_notifier *mn, struct mm_struct *mm)
{
	BUG_ON(atomic_read(&mm->mm_count) <= 0);

	spin_lock(&mm->mmu_notifier_mm->lock);
	if (!hlist_unhashed(&mn->hlist)) {
		int id;

		/*
		 * Ensure we synchronize up with __mmu_notifier_release().
		 */
		id = srcu_read_lock(&srcu);

		hlist_del_rcu(&mn->hlist);
		spin_unlock(&mm->mmu_notifier_mm->lock);

		if (mn->ops->release)
			mn->ops->release(mn, mm);

		/*
		 * Allow __mmu_notifier_release() to complete.
		 */
		srcu_read_unlock(&srcu, id);
	} else
		spin_unlock(&mm->mmu_notifier_mm->lock);

	/*
	 * Wait for any running method to finish, including ->release() if it
	 * was run by __mmu_notifier_release() instead of us.
	 */
	synchronize_srcu(&srcu);

	BUG_ON(atomic_read(&mm->mm_count) <= 0);

	mmdrop(mm);
}
EXPORT_SYMBOL_GPL(mmu_notifier_unregister);

static int __init mmu_notifier_init(void)
{
	return init_srcu_struct(&srcu);
}

module_init(mmu_notifier_init);