1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
|
#
# Network configuration
#
menuconfig NET
bool "Networking support"
select NLATTR
---help---
Unless you really know what you are doing, you should say Y here.
The reason is that some programs need kernel networking support even
when running on a stand-alone machine that isn't connected to any
other computer.
If you are upgrading from an older kernel, you
should consider updating your networking tools too because changes
in the kernel and the tools often go hand in hand. The tools are
contained in the package net-tools, the location and version number
of which are given in <file:Documentation/Changes>.
For a general introduction to Linux networking, it is highly
recommended to read the NET-HOWTO, available from
<http://www.tldp.org/docs.html#howto>.
if NET
config WANT_COMPAT_NETLINK_MESSAGES
bool
help
This option can be selected by other options that need compat
netlink messages.
config COMPAT_NETLINK_MESSAGES
def_bool y
depends on COMPAT
depends on WEXT_CORE || WANT_COMPAT_NETLINK_MESSAGES
help
This option makes it possible to send different netlink messages
to tasks depending on whether the task is a compat task or not. To
achieve this, you need to set skb_shinfo(skb)->frag_list to the
compat skb before sending the skb, the netlink code will sort out
which message to actually pass to the task.
Newly written code should NEVER need this option but do
compat-independent messages instead!
menu "Networking options"
source "net/packet/Kconfig"
source "net/unix/Kconfig"
source "net/xfrm/Kconfig"
source "net/iucv/Kconfig"
config INET
bool "TCP/IP networking"
select CRYPTO
select CRYPTO_AES
---help---
These are the protocols used on the Internet and on most local
Ethernets. It is highly recommended to say Y here (this will enlarge
your kernel by about 400 KB), since some programs (e.g. the X window
system) use TCP/IP even if your machine is not connected to any
other computer. You will get the so-called loopback device which
allows you to ping yourself (great fun, that!).
For an excellent introduction to Linux networking, please read the
Linux Networking HOWTO, available from
<http://www.tldp.org/docs.html#howto>.
If you say Y here and also to "/proc file system support" and
"Sysctl support" below, you can change various aspects of the
behavior of the TCP/IP code by writing to the (virtual) files in
/proc/sys/net/ipv4/*; the options are explained in the file
<file:Documentation/networking/ip-sysctl.txt>.
Short answer: say Y.
if INET
source "net/ipv4/Kconfig"
source "net/ipv6/Kconfig"
source "net/netlabel/Kconfig"
endif # if INET
config ANDROID_PARANOID_NETWORK
bool "Only allow certain groups to create sockets"
default y
help
none
config NET_ACTIVITY_STATS
bool "Network activity statistics tracking"
default y
help
Network activity statistics are useful for tracking wireless
modem activity on 2G, 3G, 4G wireless networks. Counts number of
transmissions and groups them in specified time buckets.
config NETWORK_SECMARK
bool "Security Marking"
help
This enables security marking of network packets, similar
to nfmark, but designated for security purposes.
If you are unsure how to answer this question, answer N.
config NETWORK_PHY_TIMESTAMPING
bool "Timestamping in PHY devices"
depends on EXPERIMENTAL
help
This allows timestamping of network packets by PHYs with
hardware timestamping capabilities. This option adds some
overhead in the transmit and receive paths.
If you are unsure how to answer this question, answer N.
menuconfig NETFILTER
bool "Network packet filtering framework (Netfilter)"
---help---
Netfilter is a framework for filtering and mangling network packets
that pass through your Linux box.
The most common use of packet filtering is to run your Linux box as
a firewall protecting a local network from the Internet. The type of
firewall provided by this kernel support is called a "packet
filter", which means that it can reject individual network packets
based on type, source, destination etc. The other kind of firewall,
a "proxy-based" one, is more secure but more intrusive and more
bothersome to set up; it inspects the network traffic much more
closely, modifies it and has knowledge about the higher level
protocols, which a packet filter lacks. Moreover, proxy-based
firewalls often require changes to the programs running on the local
clients. Proxy-based firewalls don't need support by the kernel, but
they are often combined with a packet filter, which only works if
you say Y here.
You should also say Y here if you intend to use your Linux box as
the gateway to the Internet for a local network of machines without
globally valid IP addresses. This is called "masquerading": if one
of the computers on your local network wants to send something to
the outside, your box can "masquerade" as that computer, i.e. it
forwards the traffic to the intended outside destination, but
modifies the packets to make it look like they came from the
firewall box itself. It works both ways: if the outside host
replies, the Linux box will silently forward the traffic to the
correct local computer. This way, the computers on your local net
are completely invisible to the outside world, even though they can
reach the outside and can receive replies. It is even possible to
run globally visible servers from within a masqueraded local network
using a mechanism called portforwarding. Masquerading is also often
called NAT (Network Address Translation).
Another use of Netfilter is in transparent proxying: if a machine on
the local network tries to connect to an outside host, your Linux
box can transparently forward the traffic to a local server,
typically a caching proxy server.
Yet another use of Netfilter is building a bridging firewall. Using
a bridge with Network packet filtering enabled makes iptables "see"
the bridged traffic. For filtering on the lower network and Ethernet
protocols over the bridge, use ebtables (under bridge netfilter
configuration).
Various modules exist for netfilter which replace the previous
masquerading (ipmasqadm), packet filtering (ipchains), transparent
proxying, and portforwarding mechanisms. Please see
<file:Documentation/Changes> under "iptables" for the location of
these packages.
if NETFILTER
config NETFILTER_DEBUG
bool "Network packet filtering debugging"
depends on NETFILTER
help
You can say Y here if you want to get additional messages useful in
debugging the netfilter code.
config NETFILTER_ADVANCED
bool "Advanced netfilter configuration"
depends on NETFILTER
default y
help
If you say Y here you can select between all the netfilter modules.
If you say N the more unusual ones will not be shown and the
basic ones needed by most people will default to 'M'.
If unsure, say Y.
config BRIDGE_NETFILTER
bool "Bridged IP/ARP packets filtering"
depends on BRIDGE && NETFILTER && INET
depends on NETFILTER_ADVANCED
default y
---help---
Enabling this option will let arptables resp. iptables see bridged
ARP resp. IP traffic. If you want a bridging firewall, you probably
want this option enabled.
Enabling or disabling this option doesn't enable or disable
ebtables.
If unsure, say N.
source "net/netfilter/Kconfig"
source "net/ipv4/netfilter/Kconfig"
source "net/ipv6/netfilter/Kconfig"
source "net/decnet/netfilter/Kconfig"
source "net/bridge/netfilter/Kconfig"
endif
source "net/dccp/Kconfig"
source "net/sctp/Kconfig"
source "net/rds/Kconfig"
source "net/tipc/Kconfig"
source "net/atm/Kconfig"
source "net/l2tp/Kconfig"
source "net/802/Kconfig"
source "net/bridge/Kconfig"
source "net/dsa/Kconfig"
source "net/8021q/Kconfig"
source "net/decnet/Kconfig"
source "net/llc/Kconfig"
source "net/ipx/Kconfig"
source "drivers/net/appletalk/Kconfig"
source "net/x25/Kconfig"
source "net/lapb/Kconfig"
source "net/wanrouter/Kconfig"
source "net/phonet/Kconfig"
source "net/ieee802154/Kconfig"
source "net/mac802154/Kconfig"
source "net/sched/Kconfig"
source "net/dcb/Kconfig"
source "net/dns_resolver/Kconfig"
source "net/batman-adv/Kconfig"
source "net/openvswitch/Kconfig"
config RPS
boolean "RPS"
depends on SMP && SYSFS && USE_GENERIC_SMP_HELPERS
default y
config RFS_ACCEL
boolean
depends on RPS && GENERIC_HARDIRQS
select CPU_RMAP
default y
config XPS
boolean
depends on SMP && SYSFS && USE_GENERIC_SMP_HELPERS
default y
config NETPRIO_CGROUP
tristate "Network priority cgroup"
depends on CGROUPS
---help---
Cgroup subsystem for use in assigning processes to network priorities on
a per-interface basis
config BQL
boolean
depends on SYSFS
select DQL
default y
config BPF_JIT
bool "enable BPF Just In Time compiler"
depends on HAVE_BPF_JIT
depends on MODULES
---help---
Berkeley Packet Filter filtering capabilities are normally handled
by an interpreter. This option allows kernel to generate a native
code when filter is loaded in memory. This should speedup
packet sniffing (libpcap/tcpdump). Note : Admin should enable
this feature changing /proc/sys/net/core/bpf_jit_enable
menu "Network testing"
config NET_PKTGEN
tristate "Packet Generator (USE WITH CAUTION)"
depends on PROC_FS
---help---
This module will inject preconfigured packets, at a configurable
rate, out of a given interface. It is used for network interface
stress testing and performance analysis. If you don't understand
what was just said, you don't need it: say N.
Documentation on how to use the packet generator can be found
at <file:Documentation/networking/pktgen.txt>.
To compile this code as a module, choose M here: the
module will be called pktgen.
config NET_TCPPROBE
tristate "TCP connection probing"
depends on INET && EXPERIMENTAL && PROC_FS && KPROBES
---help---
This module allows for capturing the changes to TCP connection
state in response to incoming packets. It is used for debugging
TCP congestion avoidance modules. If you don't understand
what was just said, you don't need it: say N.
Documentation on how to use TCP connection probing can be found
at:
http://www.linuxfoundation.org/collaborate/workgroups/networking/tcpprobe
To compile this code as a module, choose M here: the
module will be called tcp_probe.
config NET_DROP_MONITOR
tristate "Network packet drop alerting service"
depends on INET && EXPERIMENTAL && TRACEPOINTS
---help---
This feature provides an alerting service to userspace in the
event that packets are discarded in the network stack. Alerts
are broadcast via netlink socket to any listening user space
process. If you don't need network drop alerts, or if you are ok
just checking the various proc files and other utilities for
drop statistics, say N here.
endmenu
endmenu
source "net/ax25/Kconfig"
source "net/can/Kconfig"
source "net/irda/Kconfig"
source "net/bluetooth/Kconfig"
source "net/rxrpc/Kconfig"
config FIB_RULES
bool
menuconfig WIRELESS
bool "Wireless"
depends on !S390
default y
if WIRELESS
source "net/wireless/Kconfig"
source "net/mac80211/Kconfig"
endif # WIRELESS
source "net/wimax/Kconfig"
source "net/rfkill/Kconfig"
source "net/9p/Kconfig"
source "net/caif/Kconfig"
source "net/ceph/Kconfig"
source "net/nfc/Kconfig"
endif # if NET
# Used by archs to tell that they support BPF_JIT
config HAVE_BPF_JIT
bool
|