aboutsummaryrefslogtreecommitdiffstats
blob: 8d9b55a1202372a3d63494ac7babf4d752a8969e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
/*
 * Sample kobject implementation
 *
 * Copyright (C) 2004-2007 Greg Kroah-Hartman <greg@kroah.com>
 * Copyright (C) 2007 Novell Inc.
 *
 * Released under the GPL version 2 only.
 *
 */
#include <linux/kobject.h>
#include <linux/string.h>
#include <linux/sysfs.h>
#include <linux/module.h>
#include <linux/init.h>

/*
 * This module shows how to create a simple subdirectory in sysfs called
 * /sys/kernel/kobject-example  In that directory, 3 files are created:
 * "foo", "baz", and "bar".  If an integer is written to these files, it can be
 * later read out of it.
 */

static int foo;
static int baz;
static int bar;

/*
 * The "foo" file where a static variable is read from and written to.
 */
static ssize_t foo_show(struct kobject *kobj, struct kobj_attribute *attr,
			char *buf)
{
	return sprintf(buf, "%d\n", foo);
}

static ssize_t foo_store(struct kobject *kobj, struct kobj_attribute *attr,
			 const char *buf, size_t count)
{
	sscanf(buf, "%du", &foo);
	return count;
}

static struct kobj_attribute foo_attribute =
	__ATTR(foo, 0666, foo_show, foo_store);

/*
 * More complex function where we determine which varible is being accessed by
 * looking at the attribute for the "baz" and "bar" files.
 */
static ssize_t b_show(struct kobject *kobj, struct kobj_attribute *attr,
		      char *buf)
{
	int var;

	if (strcmp(attr->attr.name, "baz") == 0)
		var = baz;
	else
		var = bar;
	return sprintf(buf, "%d\n", var);
}

static ssize_t b_store(struct kobject *kobj, struct kobj_attribute *attr,
		       const char *buf, size_t count)
{
	int var;

	sscanf(buf, "%du", &var);
	if (strcmp(attr->attr.name, "baz") == 0)
		baz = var;
	else
		bar = var;
	return count;
}

static struct kobj_attribute baz_attribute =
	__ATTR(baz, 0666, b_show, b_store);
static struct kobj_attribute bar_attribute =
	__ATTR(bar, 0666, b_show, b_store);


/*
 * Create a group of attributes so that we can create and destory them all
 * at once.
 */
static struct attribute *attrs[] = {
	&foo_attribute.attr,
	&baz_attribute.attr,
	&bar_attribute.attr,
	NULL,	/* need to NULL terminate the list of attributes */
};

/*
 * An unnamed attribute group will put all of the attributes directly in
 * the kobject directory.  If we specify a name, a subdirectory will be
 * created for the attributes with the directory being the name of the
 * attribute group.
 */
static struct attribute_group attr_group = {
	.attrs = attrs,
};

static struct kobject *example_kobj;

static int __init example_init(void)
{
	int retval;

	/*
	 * Create a simple kobject with the name of "kobject_example",
	 * located under /sys/kernel/
	 *
	 * As this is a simple directory, no uevent will be sent to
	 * userspace.  That is why this function should not be used for
	 * any type of dynamic kobjects, where the name and number are
	 * not known ahead of time.
	 */
	example_kobj = kobject_create_and_add("kobject_example", kernel_kobj);
	if (!example_kobj)
		return -ENOMEM;

	/* Create the files associated with this kobject */
	retval = sysfs_create_group(example_kobj, &attr_group);
	if (retval)
		kobject_put(example_kobj);

	return retval;
}

static void __exit example_exit(void)
{
	kobject_put(example_kobj);
}

module_init(example_init);
module_exit(example_exit);
MODULE_LICENSE("GPL");
MODULE_AUTHOR("Greg Kroah-Hartman <greg@kroah.com>");