aboutsummaryrefslogtreecommitdiffstats
blob: 6af373236d7318729528bc288510363071725649 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
/*
 * If TRACE_SYSTEM is defined, that will be the directory created
 * in the ftrace directory under /sys/kernel/debug/tracing/events/<system>
 *
 * The define_trace.h below will also look for a file name of
 * TRACE_SYSTEM.h where TRACE_SYSTEM is what is defined here.
 * In this case, it would look for sample.h
 *
 * If the header name will be different than the system name
 * (as in this case), then you can override the header name that
 * define_trace.h will look up by defining TRACE_INCLUDE_FILE
 *
 * This file is called trace-events-sample.h but we want the system
 * to be called "sample". Therefore we must define the name of this
 * file:
 *
 * #define TRACE_INCLUDE_FILE trace-events-sample
 *
 * As we do an the bottom of this file.
 *
 * Notice that TRACE_SYSTEM should be defined outside of #if
 * protection, just like TRACE_INCLUDE_FILE.
 */
#undef TRACE_SYSTEM
#define TRACE_SYSTEM sample

/*
 * Notice that this file is not protected like a normal header.
 * We also must allow for rereading of this file. The
 *
 *  || defined(TRACE_HEADER_MULTI_READ)
 *
 * serves this purpose.
 */
#if !defined(_TRACE_EVENT_SAMPLE_H) || defined(TRACE_HEADER_MULTI_READ)
#define _TRACE_EVENT_SAMPLE_H

/*
 * All trace headers should include tracepoint.h, until we finally
 * make it into a standard header.
 */
#include <linux/tracepoint.h>

/*
 * The TRACE_EVENT macro is broken up into 5 parts.
 *
 * name: name of the trace point. This is also how to enable the tracepoint.
 *   A function called trace_foo_bar() will be created.
 *
 * proto: the prototype of the function trace_foo_bar()
 *   Here it is trace_foo_bar(char *foo, int bar).
 *
 * args:  must match the arguments in the prototype.
 *    Here it is simply "foo, bar".
 *
 * struct:  This defines the way the data will be stored in the ring buffer.
 *    There are currently two types of elements. __field and __array.
 *    a __field is broken up into (type, name). Where type can be any
 *    type but an array.
 *    For an array. there are three fields. (type, name, size). The
 *    type of elements in the array, the name of the field and the size
 *    of the array.
 *
 *    __array( char, foo, 10) is the same as saying   char foo[10].
 *
 * fast_assign: This is a C like function that is used to store the items
 *    into the ring buffer.
 *
 * printk: This is a way to print out the data in pretty print. This is
 *    useful if the system crashes and you are logging via a serial line,
 *    the data can be printed to the console using this "printk" method.
 *
 * Note, that for both the assign and the printk, __entry is the handler
 * to the data structure in the ring buffer, and is defined by the
 * TP_STRUCT__entry.
 */
TRACE_EVENT(foo_bar,

	TP_PROTO(char *foo, int bar),

	TP_ARGS(foo, bar),

	TP_STRUCT__entry(
		__array(	char,	foo,    10		)
		__field(	int,	bar			)
	),

	TP_fast_assign(
		strncpy(__entry->foo, foo, 10);
		__entry->bar	= bar;
	),

	TP_printk("foo %s %d", __entry->foo, __entry->bar)
);
#endif

/***** NOTICE! The #if protection ends here. *****/


/*
 * There are several ways I could have done this. If I left out the
 * TRACE_INCLUDE_PATH, then it would default to the kernel source
 * include/trace/events directory.
 *
 * I could specify a path from the define_trace.h file back to this
 * file.
 *
 * #define TRACE_INCLUDE_PATH ../../samples/trace_events
 *
 * But the safest and easiest way to simply make it use the directory
 * that the file is in is to add in the Makefile:
 *
 * CFLAGS_trace-events-sample.o := -I$(src)
 *
 * This will make sure the current path is part of the include
 * structure for our file so that define_trace.h can find it.
 *
 * I could have made only the top level directory the include:
 *
 * CFLAGS_trace-events-sample.o := -I$(PWD)
 *
 * And then let the path to this directory be the TRACE_INCLUDE_PATH:
 *
 * #define TRACE_INCLUDE_PATH samples/trace_events
 *
 * But then if something defines "samples" or "trace_events" as a macro
 * then we could risk that being converted too, and give us an unexpected
 * result.
 */
#undef TRACE_INCLUDE_PATH
#undef TRACE_INCLUDE_FILE
#define TRACE_INCLUDE_PATH .
/*
 * TRACE_INCLUDE_FILE is not needed if the filename and TRACE_SYSTEM are equal
 */
#define TRACE_INCLUDE_FILE trace-events-sample
#include <trace/define_trace.h>