aboutsummaryrefslogtreecommitdiffstats
blob: 43ce6e19015fc81e80786c26a07e2ac47e71109b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
/*
 *  inode.c - securityfs
 *
 *  Copyright (C) 2005 Greg Kroah-Hartman <gregkh@suse.de>
 *
 *	This program is free software; you can redistribute it and/or
 *	modify it under the terms of the GNU General Public License version
 *	2 as published by the Free Software Foundation.
 *
 *  Based on fs/debugfs/inode.c which had the following copyright notice:
 *    Copyright (C) 2004 Greg Kroah-Hartman <greg@kroah.com>
 *    Copyright (C) 2004 IBM Inc.
 */

/* #define DEBUG */
#include <linux/module.h>
#include <linux/fs.h>
#include <linux/mount.h>
#include <linux/pagemap.h>
#include <linux/init.h>
#include <linux/namei.h>
#include <linux/security.h>
#include <linux/magic.h>

static struct vfsmount *mount;
static int mount_count;

static inline int positive(struct dentry *dentry)
{
	return dentry->d_inode && !d_unhashed(dentry);
}

static int fill_super(struct super_block *sb, void *data, int silent)
{
	static struct tree_descr files[] = {{""}};

	return simple_fill_super(sb, SECURITYFS_MAGIC, files);
}

static struct dentry *get_sb(struct file_system_type *fs_type,
		  int flags, const char *dev_name,
		  void *data)
{
	return mount_single(fs_type, flags, data, fill_super);
}

static struct file_system_type fs_type = {
	.owner =	THIS_MODULE,
	.name =		"securityfs",
	.mount =	get_sb,
	.kill_sb =	kill_litter_super,
};

/**
 * securityfs_create_file - create a file in the securityfs filesystem
 *
 * @name: a pointer to a string containing the name of the file to create.
 * @mode: the permission that the file should have
 * @parent: a pointer to the parent dentry for this file.  This should be a
 *          directory dentry if set.  If this parameter is %NULL, then the
 *          file will be created in the root of the securityfs filesystem.
 * @data: a pointer to something that the caller will want to get to later
 *        on.  The inode.i_private pointer will point to this value on
 *        the open() call.
 * @fops: a pointer to a struct file_operations that should be used for
 *        this file.
 *
 * This is the basic "create a file" function for securityfs.  It allows for a
 * wide range of flexibility in creating a file, or a directory (if you
 * want to create a directory, the securityfs_create_dir() function is
 * recommended to be used instead).
 *
 * This function returns a pointer to a dentry if it succeeds.  This
 * pointer must be passed to the securityfs_remove() function when the file is
 * to be removed (no automatic cleanup happens if your module is unloaded,
 * you are responsible here).  If an error occurs, the function will return
 * the erorr value (via ERR_PTR).
 *
 * If securityfs is not enabled in the kernel, the value %-ENODEV is
 * returned.
 */
struct dentry *securityfs_create_file(const char *name, umode_t mode,
				   struct dentry *parent, void *data,
				   const struct file_operations *fops)
{
	struct dentry *dentry;
	int is_dir = S_ISDIR(mode);
	struct inode *dir, *inode;
	int error;

	if (!is_dir) {
		BUG_ON(!fops);
		mode = (mode & S_IALLUGO) | S_IFREG;
	}

	pr_debug("securityfs: creating file '%s'\n",name);

	error = simple_pin_fs(&fs_type, &mount, &mount_count);
	if (error)
		return ERR_PTR(error);

	if (!parent)
		parent = mount->mnt_root;

	dir = parent->d_inode;

	mutex_lock(&dir->i_mutex);
	dentry = lookup_one_len(name, parent, strlen(name));
	if (IS_ERR(dentry))
		goto out;

	if (dentry->d_inode) {
		error = -EEXIST;
		goto out1;
	}

	inode = new_inode(dir->i_sb);
	if (!inode) {
		error = -ENOMEM;
		goto out1;
	}

	inode->i_ino = get_next_ino();
	inode->i_mode = mode;
	inode->i_atime = inode->i_mtime = inode->i_ctime = CURRENT_TIME;
	inode->i_private = data;
	if (is_dir) {
		inode->i_op = &simple_dir_inode_operations;
		inode->i_fop = &simple_dir_operations;
		inc_nlink(inode);
		inc_nlink(dir);
	} else {
		inode->i_fop = fops;
	}
	d_instantiate(dentry, inode);
	dget(dentry);
	mutex_unlock(&dir->i_mutex);
	return dentry;

out1:
	dput(dentry);
	dentry = ERR_PTR(error);
out:
	mutex_unlock(&dir->i_mutex);
	simple_release_fs(&mount, &mount_count);
	return dentry;
}
EXPORT_SYMBOL_GPL(securityfs_create_file);

/**
 * securityfs_create_dir - create a directory in the securityfs filesystem
 *
 * @name: a pointer to a string containing the name of the directory to
 *        create.
 * @parent: a pointer to the parent dentry for this file.  This should be a
 *          directory dentry if set.  If this parameter is %NULL, then the
 *          directory will be created in the root of the securityfs filesystem.
 *
 * This function creates a directory in securityfs with the given @name.
 *
 * This function returns a pointer to a dentry if it succeeds.  This
 * pointer must be passed to the securityfs_remove() function when the file is
 * to be removed (no automatic cleanup happens if your module is unloaded,
 * you are responsible here).  If an error occurs, %NULL will be returned.
 *
 * If securityfs is not enabled in the kernel, the value %-ENODEV is
 * returned.  It is not wise to check for this value, but rather, check for
 * %NULL or !%NULL instead as to eliminate the need for #ifdef in the calling
 * code.
 */
struct dentry *securityfs_create_dir(const char *name, struct dentry *parent)
{
	return securityfs_create_file(name,
				      S_IFDIR | S_IRWXU | S_IRUGO | S_IXUGO,
				      parent, NULL, NULL);
}
EXPORT_SYMBOL_GPL(securityfs_create_dir);

/**
 * securityfs_remove - removes a file or directory from the securityfs filesystem
 *
 * @dentry: a pointer to a the dentry of the file or directory to be removed.
 *
 * This function removes a file or directory in securityfs that was previously
 * created with a call to another securityfs function (like
 * securityfs_create_file() or variants thereof.)
 *
 * This function is required to be called in order for the file to be
 * removed. No automatic cleanup of files will happen when a module is
 * removed; you are responsible here.
 */
void securityfs_remove(struct dentry *dentry)
{
	struct dentry *parent;

	if (!dentry || IS_ERR(dentry))
		return;

	parent = dentry->d_parent;
	if (!parent || !parent->d_inode)
		return;

	mutex_lock(&parent->d_inode->i_mutex);
	if (positive(dentry)) {
		if (dentry->d_inode) {
			if (S_ISDIR(dentry->d_inode->i_mode))
				simple_rmdir(parent->d_inode, dentry);
			else
				simple_unlink(parent->d_inode, dentry);
			dput(dentry);
		}
	}
	mutex_unlock(&parent->d_inode->i_mutex);
	simple_release_fs(&mount, &mount_count);
}
EXPORT_SYMBOL_GPL(securityfs_remove);

static struct kobject *security_kobj;

static int __init securityfs_init(void)
{
	int retval;

	security_kobj = kobject_create_and_add("security", kernel_kobj);
	if (!security_kobj)
		return -EINVAL;

	retval = register_filesystem(&fs_type);
	if (retval)
		kobject_put(security_kobj);
	return retval;
}

core_initcall(securityfs_init);
MODULE_LICENSE("GPL");