aboutsummaryrefslogtreecommitdiffstats
blob: d35379781c2c44ab188cb7aed071579da189bb53 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
/*
 * Network port table
 *
 * SELinux must keep a mapping of network ports to labels/SIDs.  This
 * mapping is maintained as part of the normal policy but a fast cache is
 * needed to reduce the lookup overhead.
 *
 * Author: Paul Moore <paul@paul-moore.com>
 *
 * This code is heavily based on the "netif" concept originally developed by
 * James Morris <jmorris@redhat.com>
 *   (see security/selinux/netif.c for more information)
 *
 */

/*
 * (c) Copyright Hewlett-Packard Development Company, L.P., 2008
 *
 * This program is free software: you can redistribute it and/or modify
 * it under the terms of version 2 of the GNU General Public License as
 * published by the Free Software Foundation.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 */

#include <linux/types.h>
#include <linux/rcupdate.h>
#include <linux/list.h>
#include <linux/slab.h>
#include <linux/spinlock.h>
#include <linux/in.h>
#include <linux/in6.h>
#include <linux/ip.h>
#include <linux/ipv6.h>
#include <net/ip.h>
#include <net/ipv6.h>

#include "netport.h"
#include "objsec.h"

#define SEL_NETPORT_HASH_SIZE       256
#define SEL_NETPORT_HASH_BKT_LIMIT   16

struct sel_netport_bkt {
	int size;
	struct list_head list;
};

struct sel_netport {
	struct netport_security_struct psec;

	struct list_head list;
	struct rcu_head rcu;
};

/* NOTE: we are using a combined hash table for both IPv4 and IPv6, the reason
 * for this is that I suspect most users will not make heavy use of both
 * address families at the same time so one table will usually end up wasted,
 * if this becomes a problem we can always add a hash table for each address
 * family later */

static LIST_HEAD(sel_netport_list);
static DEFINE_SPINLOCK(sel_netport_lock);
static struct sel_netport_bkt sel_netport_hash[SEL_NETPORT_HASH_SIZE];

/**
 * sel_netport_hashfn - Hashing function for the port table
 * @pnum: port number
 *
 * Description:
 * This is the hashing function for the port table, it returns the bucket
 * number for the given port.
 *
 */
static unsigned int sel_netport_hashfn(u16 pnum)
{
	return (pnum & (SEL_NETPORT_HASH_SIZE - 1));
}

/**
 * sel_netport_find - Search for a port record
 * @protocol: protocol
 * @port: pnum
 *
 * Description:
 * Search the network port table and return the matching record.  If an entry
 * can not be found in the table return NULL.
 *
 */
static struct sel_netport *sel_netport_find(u8 protocol, u16 pnum)
{
	unsigned int idx;
	struct sel_netport *port;

	idx = sel_netport_hashfn(pnum);
	list_for_each_entry_rcu(port, &sel_netport_hash[idx].list, list)
		if (port->psec.port == pnum && port->psec.protocol == protocol)
			return port;

	return NULL;
}

/**
 * sel_netport_insert - Insert a new port into the table
 * @port: the new port record
 *
 * Description:
 * Add a new port record to the network address hash table.
 *
 */
static void sel_netport_insert(struct sel_netport *port)
{
	unsigned int idx;

	/* we need to impose a limit on the growth of the hash table so check
	 * this bucket to make sure it is within the specified bounds */
	idx = sel_netport_hashfn(port->psec.port);
	list_add_rcu(&port->list, &sel_netport_hash[idx].list);
	if (sel_netport_hash[idx].size == SEL_NETPORT_HASH_BKT_LIMIT) {
		struct sel_netport *tail;
		tail = list_entry(
			rcu_dereference_protected(
				sel_netport_hash[idx].list.prev,
				lockdep_is_held(&sel_netport_lock)),
			struct sel_netport, list);
		list_del_rcu(&tail->list);
		kfree_rcu(tail, rcu);
	} else
		sel_netport_hash[idx].size++;
}

/**
 * sel_netport_sid_slow - Lookup the SID of a network address using the policy
 * @protocol: protocol
 * @pnum: port
 * @sid: port SID
 *
 * Description:
 * This function determines the SID of a network port by quering the security
 * policy.  The result is added to the network port table to speedup future
 * queries.  Returns zero on success, negative values on failure.
 *
 */
static int sel_netport_sid_slow(u8 protocol, u16 pnum, u32 *sid)
{
	int ret = -ENOMEM;
	struct sel_netport *port;
	struct sel_netport *new = NULL;

	spin_lock_bh(&sel_netport_lock);
	port = sel_netport_find(protocol, pnum);
	if (port != NULL) {
		*sid = port->psec.sid;
		spin_unlock_bh(&sel_netport_lock);
		return 0;
	}
	new = kzalloc(sizeof(*new), GFP_ATOMIC);
	if (new == NULL)
		goto out;
	ret = security_port_sid(protocol, pnum, sid);
	if (ret != 0)
		goto out;

	new->psec.port = pnum;
	new->psec.protocol = protocol;
	new->psec.sid = *sid;
	sel_netport_insert(new);

out:
	spin_unlock_bh(&sel_netport_lock);
	if (unlikely(ret)) {
		printk(KERN_WARNING
		       "SELinux: failure in sel_netport_sid_slow(),"
		       " unable to determine network port label\n");
		kfree(new);
	}
	return ret;
}

/**
 * sel_netport_sid - Lookup the SID of a network port
 * @protocol: protocol
 * @pnum: port
 * @sid: port SID
 *
 * Description:
 * This function determines the SID of a network port using the fastest method
 * possible.  First the port table is queried, but if an entry can't be found
 * then the policy is queried and the result is added to the table to speedup
 * future queries.  Returns zero on success, negative values on failure.
 *
 */
int sel_netport_sid(u8 protocol, u16 pnum, u32 *sid)
{
	struct sel_netport *port;

	rcu_read_lock();
	port = sel_netport_find(protocol, pnum);
	if (port != NULL) {
		*sid = port->psec.sid;
		rcu_read_unlock();
		return 0;
	}
	rcu_read_unlock();

	return sel_netport_sid_slow(protocol, pnum, sid);
}

/**
 * sel_netport_flush - Flush the entire network port table
 *
 * Description:
 * Remove all entries from the network address table.
 *
 */
static void sel_netport_flush(void)
{
	unsigned int idx;
	struct sel_netport *port, *port_tmp;

	spin_lock_bh(&sel_netport_lock);
	for (idx = 0; idx < SEL_NETPORT_HASH_SIZE; idx++) {
		list_for_each_entry_safe(port, port_tmp,
					 &sel_netport_hash[idx].list, list) {
			list_del_rcu(&port->list);
			kfree_rcu(port, rcu);
		}
		sel_netport_hash[idx].size = 0;
	}
	spin_unlock_bh(&sel_netport_lock);
}

static int sel_netport_avc_callback(u32 event)
{
	if (event == AVC_CALLBACK_RESET) {
		sel_netport_flush();
		synchronize_net();
	}
	return 0;
}

static __init int sel_netport_init(void)
{
	int iter;
	int ret;

	if (!selinux_enabled)
		return 0;

	for (iter = 0; iter < SEL_NETPORT_HASH_SIZE; iter++) {
		INIT_LIST_HEAD(&sel_netport_hash[iter].list);
		sel_netport_hash[iter].size = 0;
	}

	ret = avc_add_callback(sel_netport_avc_callback, AVC_CALLBACK_RESET);
	if (ret != 0)
		panic("avc_add_callback() failed, error %d\n", ret);

	return ret;
}

__initcall(sel_netport_init);