aboutsummaryrefslogblamecommitdiffstats
blob: b030b9c7ed34ad05f62faf8f253cfb0efd1c01b4 (plain) (tree)









































                                                                               
menu "Certificates for signature checking"

config MODULE_SIG_KEY
	string "File name or PKCS#11 URI of module signing key"
	default "certs/signing_key.pem"
	depends on MODULE_SIG
	help
         Provide the file name of a private key/certificate in PEM format,
         or a PKCS#11 URI according to RFC7512. The file should contain, or
         the URI should identify, both the certificate and its corresponding
         private key.

         If this option is unchanged from its default "certs/signing_key.pem",
         then the kernel will automatically generate the private key and
         certificate as described in Documentation/module-signing.txt

config SYSTEM_TRUSTED_KEYRING
	bool "Provide system-wide ring of trusted keys"
	depends on KEYS
	help
	  Provide a system keyring to which trusted keys can be added.  Keys in
	  the keyring are considered to be trusted.  Keys may be added at will
	  by the kernel from compiled-in data and from hardware key stores, but
	  userspace may only add extra keys if those keys can be verified by
	  keys already in the keyring.

	  Keys in this keyring are used by module signature checking.

config SYSTEM_TRUSTED_KEYS
	string "Additional X.509 keys for default system keyring"
	depends on SYSTEM_TRUSTED_KEYRING
	help
	  If set, this option should be the filename of a PEM-formatted file
	  containing trusted X.509 certificates to be included in the default
	  system keyring. Any certificate used for module signing is implicitly
	  also trusted.

	  NOTE: If you previously provided keys for the system keyring in the
	  form of DER-encoded *.x509 files in the top-level build directory,
	  those are no longer used. You will need to set this option instead.

endmenu