#
# Mouse driver configuration
#
menuconfig INPUT_MOUSE
bool "Mice"
default y
help
Say Y here, and a list of supported mice will be displayed.
This option doesn't affect the kernel.
If unsure, say Y.
if INPUT_MOUSE
config MOUSE_PS2
tristate "PS/2 mouse"
default y
select SERIO
select SERIO_LIBPS2
select SERIO_I8042 if ARCH_MIGHT_HAVE_PC_SERIO
select SERIO_GSCPS2 if GSC
help
Say Y here if you have a PS/2 mouse connected to your system. This
includes the standard 2 or 3-button PS/2 mouse, as well as PS/2
mice with wheels and extra buttons, Microsoft, Logitech or Genius
compatible.
Synaptics, ALPS or Elantech TouchPad users might be interested
in a specialized Xorg/XFree86 driver at:
<http://w1.894.telia.com/~u89404340/touchpad/index.html>
and a new version of GPM at:
<http://www.geocities.com/dt_or/gpm/gpm.html>
<http://xorg.freedesktop.org/archive/individual/driver/>
to take advantage of the advanced features of the touchpad.
If unsure, say Y.
To compile this driver as a module, choose M here: the
module will be called psmouse.
config MOUSE_PS2_ALPS
bool "ALPS PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have an ALPS PS/2 touchpad connected to
your system.
If unsure, say Y.
config MOUSE_PS2_LOGIPS2PP
bool "Logitech PS/2++ mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have a Logitech PS/2++ mouse connected to
your system.
If unsure, say Y.
config MOUSE_PS2_SYNAPTICS
bool "Synaptics PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have a Synaptics PS/2 TouchPad connected to
your system.
If unsure, say Y.
config MOUSE_PS2_CYPRESS
bool "Cypress PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have a Cypress PS/2 Trackpad connected to
your system.
If unsure, say Y.
config MOUSE_PS2_LIFEBOOK
bool "Fujitsu Lifebook PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2 && X86 && DMI
help
Say Y here if you have a Fujitsu B-series Lifebook PS/2
TouchScreen connected to your system.
If unsure, say Y.
config MOUSE_PS2_TRACKPOINT
bool "IBM Trackpoint PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have an IBM Trackpoint PS/2 mouse connected
to your system.
If unsure, say Y.
config MOUSE_PS2_ELANTECH
bool "Elantech PS/2 protocol extension"
depends on MOUSE_PS2
help
Say Y here if you have an Elantech PS/2 touchpad connected
to your system.
This driver exposes some configuration registers via sysfs
entries. For further information,
see <file:Documentation/input/elantech.txt>.
If unsure, say N.
config MOUSE_PS2_SENTELIC
bool "Sentelic Finger Sensing Pad PS/2 protocol extension"
depends on MOUSE_PS2
help
Say Y here if you have a laptop (such as MSI WIND Netbook)
with Sentelic Finger Sensing Pad touchpad.
If unsure, say N.
config MOUSE_PS2_TOUCHKIT
bool "eGalax TouchKit PS/2 protocol extension"
depends on MOUSE_PS2
help
Say Y here if you have an eGalax TouchKit PS/2 touchscreen
connected to your system.
If unsure, say N.
config MOUSE_PS2_OLPC
bool "OLPC PS/2 mouse protocol extension"
depends on MOUSE_PS2 && OLPC
help
Say Y here if you have an OLPC XO-1 laptop (with built-in
PS/2 touchpad/tablet device). The manufacturer calls the
touchpad an HGPK.
If unsure, say N.
config MOUSE_PS2_FOCALTECH
bool "FocalTech PS/2 mouse protocol extension" if EXPERT
default y
depends on MOUSE_PS2
help
Say Y here if you have a FocalTech PS/2 TouchPad connected to
your system.
If unsure, say Y.
config MOUSE_PS2_VMMOUSE
bool "Virtual mouse (vmmouse)"
depends on MOUSE_PS2 && X86 && HYPERVISOR_GUEST
help
Say Y here if you are running under control of VMware hypervisor
(ESXi, Workstation or Fusion). Also make sure that when you enable
this option, you remove the xf86-input-vmmouse user-space driver
or upgrade it to at least xf86-input-vmmouse 13.1.0, which doesn't
load in the presence of an in-kernel vmmouse driver.
If unsure, say N.
config MOUSE_SERIAL
tristate "Serial mouse"
select SERIO
help
Say Y here if you have a serial (RS-232, COM port) mouse connected
to your system. This includes Sun, MouseSystems, Microsoft,
Logitech and all other compatible serial mice.
If unsure, say N.
To compile this driver as a module, choose M here: the
module will be called sermouse.
config MOUSE_APPLETOUCH
tristate "Apple USB Touchpad support"
depends on USB_ARCH_HAS_HCD
select USB
help
Say Y here if you want to use an Apple USB Touchpad.
These are the touchpads that can be found on post-February 2005
Apple Powerbooks (prior models have a Synaptics touchpad connected
to the ADB bus).
This driver provides a basic mouse driver but can be interfaced
with the synaptics X11 driver to provide acceleration and
scrolling in X11.
For further information, see
<file:Documentation/input/appletouch.txt>.
To compile this driver as a module, choose M here: the
module will be called appletouch.
config MOUSE_BCM5974
tristate "Apple USB BCM5974 Multitouch trackpad support"
depends on USB_ARCH_HAS_HCD
select USB
help
Say Y here if you have an Apple USB BCM5974 Multitouch
trackpad.
The BCM5974 is the multitouch trackpad found in the Macbook
Air (JAN2008) and Macbook Pro Penryn (FEB2008) laptops.
It is also found in the IPhone (2007) and Ipod Touch (2008).
This driver provides multitouch functionality together with
the synaptics X11 driver.
The interface is currently identical to the appletouch interface,
for further information, see
<file:Documentation/input/appletouch.txt>.
To compile this driver as a module, choose M here: the
module will be called bcm5974.
config MOUSE_CYAPA
tristate "Cypress APA I2C Trackpad support"
depends on I2C
select CRC_ITU_T
help
This driver adds support for Cypress All Points Addressable (APA)
I2C Trackpads, including the ones used in 2012 Samsung Chromebooks.
Say Y here if you have a Cypress APA I2C Trackpad.
To compile this driver as a module, choose M here: the module will be
called cyapa.
config MOUSE_ELAN_I2C
tristate "ELAN I2C Touchpad support"
depends on I2C
help
This driver adds support for Elan I2C/SMbus Trackpads.
Say Y here if you have a ELAN I2C/SMbus Touchpad.
To compile this driver as a module, choose M here: the module will be
called elan_i2c.
config MOUSE_ELAN_I2C_I2C
bool "Enable I2C support"
depends on MOUSE_ELAN_I2C
default y
help
Say Y here if Elan Touchpad in your system is connected to
a standard I2C controller.
If unsure, say Y.
config MOUSE_ELAN_I2C_SMBUS
bool "Enable SMbus support"
depends on MOUSE_ELAN_I2C
help
Say Y here if Elan Touchpad in your system is connected to
a SMbus adapter.
If unsure, say Y.
config MOUSE_INPORT
tristate "InPort/MS/ATIXL busmouse"
depends on ISA
help
Say Y here if you have an InPort, Microsoft or ATI XL busmouse.
They are rather rare these days.
To compile this driver as a module, choose M here: the
module will be called inport.
config MOUSE_ATIXL
bool "ATI XL variant"
depends on MOUSE_INPORT
help
Say Y here if your mouse is of the ATI XL variety.
config MOUSE_LOGIBM
tristate "Logitech busmouse"
depends on ISA
help
Say Y here if you have a Logitech busmouse.
They are rather rare these days.
To compile this driver as a module, choose M here: the
module will be called logibm.
config MOUSE_PC110PAD
tristate "IBM PC110 touchpad"
depends on ISA
help
Say Y if you have the IBM PC-110 micro-notebook and want its
touchpad supported.
To compile this driver as a module, choose M here: the
module will be called pc110pad.
config MOUSE_AMIGA
tristate "Amiga mouse"
depends on AMIGA
help
Say Y here if you have an Amiga and want its native mouse
supported by the kernel.
To compile this driver as a module, choose M here: the
module will be called amimouse.
config MOUSE_ATARI
tristate "Atari mouse"
depends on ATARI
select ATARI_KBD_CORE
help
Say Y here if you have an Atari and want its native mouse
supported by the kernel.
To compile this driver as a module, choose M here: the
module will be called atarimouse.
config MOUSE_RISCPC
tristate "Acorn RiscPC mouse"
depends on ARCH_ACORN
help
Say Y here if you have the Acorn RiscPC computer and want its
native mouse supported.
To compile this driver as a module, choose M here: the
module will be called rpcmouse.
config MOUSE_VSXXXAA
tristate "DEC VSXXX-AA/GA mouse and VSXXX-AB tablet"
select SERIO
help
Say Y (or M) if you want to use a DEC VSXXX-AA (hockey
puck) or a VSXXX-GA (rectangular) mouse. Theses mice are
typically used on DECstations or VAXstations, but can also
be used on any box capable of RS232 (with some adaptor
described in the source file). This driver also works with the
digitizer (VSXXX-AB) DEC produced.
config MOUSE_GPIO
tristate "GPIO mouse"
depends on GPIOLIB || COMPILE_TEST
select INPUT_POLLDEV
help
This driver simulates a mouse on GPIO lines of various CPUs (and some
other chips).
Say Y here if your device has buttons or a simple joystick connected
directly to GPIO lines. Your board-specific setup logic must also
provide a platform device and platform data saying which GPIOs are
used.
To compile this driver as a module, choose M here: the
module will be called gpio_mouse.
config MOUSE_PXA930_TRKBALL
tristate "PXA930 Trackball mouse"
depends on CPU_PXA930 || CPU_PXA935
help
Say Y here to support PXA930 Trackball mouse.
config MOUSE_MAPLE
tristate "Maple mouse (for the Dreamcast)"
depends on MAPLE
help
This driver supports the Maple mouse on the SEGA Dreamcast.
Most Dreamcast users, who have a mouse, will say Y here.
To compile this driver as a module choose M here: the module will be
called maplemouse.
config MOUSE_SYNAPTICS_I2C
tristate "Synaptics I2C Touchpad support"
depends on I2C
help
This driver supports Synaptics I2C touchpad controller on eXeda
mobile device.
The device will not work the synaptics X11 driver because
(i) it reports only relative coordinates and has no capabilities
to report absolute coordinates
(ii) the eXeda device itself uses Xfbdev as X Server and it does
not allow using xf86-input-* drivers.
Say y here if you have eXeda device and want to use a Synaptics
I2C Touchpad.
To compile this driver as a module, choose M here: the
module will be called synaptics_i2c.
config MOUSE_SYNAPTICS_USB
tristate "Synaptics USB device support"
depends on USB_ARCH_HAS_HCD
select USB
help
Say Y here if you want to use a Synaptics USB touchpad or pointing
stick.
While these devices emulate an USB mouse by default and can be used
with standard usbhid driver, this driver, together with its X.Org
counterpart, allows you to fully utilize capabilities of the device.
More information can be found at:
<http://jan-steinhoff.de/linux/synaptics-usb.html>
To compile this driver as a module, choose M here: the
module will be called synaptics_usb.
config MOUSE_NAVPOINT_PXA27x
tristate "Synaptics NavPoint (PXA27x SSP/SPI)"
depends on PXA27x && PXA_SSP
help
This driver adds support for the Synaptics NavPoint touchpad connected
to a PXA27x SSP port in SPI slave mode. The device emulates a mouse;
a tap or tap-and-a-half drag gesture emulates the left mouse button.
For example, use the xf86-input-evdev driver for an X pointing device.
To compile this driver as a module, choose M here: the
module will be called navpoint.
endif