aboutsummaryrefslogblamecommitdiffstats
blob: de6cbb7cf547037d91fd891a403dfd666045c4eb (plain) (tree)






















                                                                            
                         
                              
 




                                                                               






                                                                        
                                                                     
                                                            










                                                                       
                   
                           


                   
                    


                                     

  








                                                                               

                                                                             







                                                                               
                                                                           


















                                                                      




                                                          


























































































                                                                                

                                                     
                         

                   
                                         

  
                              
 




                                                                


                                                                    
 
                     
 







                                                              


                                                        
                                                          
                                                                           

                                                                   
                                        
                                                                                   


                                                                        
                                                             
 
                           
                     
                        




                              



                          
                                           
 
                                       
                                                
                                                   
                                            
 

                                                                    


                                                         
                           
                         


                                                                                  
                                                                               
                                                               
                                                         
                                                                                        





                                                                                                        

                                                                                        
 








                                            




                                                    

                                         
                               
 


                                                                   
                                                                        




                                                              

                                                        
                                                 







                                                          
                                    



                                                            
                           
                            

                         
                          

                                                                   
 



                                                                
 
                                                                              
                                                  
     
                                             
                                               
      

                                    
/* audit -- definition of audit_context structure and supporting types 
 *
 * Copyright 2003-2004 Red Hat, Inc.
 * Copyright 2005 Hewlett-Packard Development Company, L.P.
 * Copyright 2005 IBM Corporation
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
 */

#include <linux/fs.h>
#include <linux/audit.h>
#include <linux/skbuff.h>
#include <uapi/linux/mqueue.h>

/* AUDIT_NAMES is the number of slots we reserve in the audit_context
 * for saving names from getname().  If we get more names we will allocate
 * a name dynamically and also add those to the list anchored by names_list. */
#define AUDIT_NAMES	5

/* At task start time, the audit_state is set in the audit_context using
   a per-task filter.  At syscall entry, the audit_state is augmented by
   the syscall filter. */
enum audit_state {
	AUDIT_DISABLED,		/* Do not create per-task audit_context.
				 * No syscall-specific audit records can
				 * be generated. */
	AUDIT_BUILD_CONTEXT,	/* Create the per-task audit_context,
				 * and fill it in at syscall
				 * entry time.  This makes a full
				 * syscall record available if some
				 * other part of the kernel decides it
				 * should be recorded. */
	AUDIT_RECORD_CONTEXT	/* Create the per-task audit_context,
				 * always fill it in at syscall entry
				 * time, and always write out the audit
				 * record at syscall exit time.  */
};

/* Rule lists */
struct audit_watch;
struct audit_fsnotify_mark;
struct audit_tree;
struct audit_chunk;

struct audit_entry {
	struct list_head	list;
	struct rcu_head		rcu;
	struct audit_krule	rule;
};

struct audit_cap_data {
	kernel_cap_t		permitted;
	kernel_cap_t		inheritable;
	union {
		unsigned int	fE;		/* effective bit of file cap */
		kernel_cap_t	effective;	/* effective set of process */
	};
};

/* When fs/namei.c:getname() is called, we store the pointer in name and bump
 * the refcnt in the associated filename struct.
 *
 * Further, in fs/namei.c:path_lookup() we store the inode and device.
 */
struct audit_names {
	struct list_head	list;		/* audit_context->names_list */

	struct filename		*name;
	int			name_len;	/* number of chars to log */
	bool			hidden;		/* don't log this record */

	unsigned long		ino;
	dev_t			dev;
	umode_t			mode;
	kuid_t			uid;
	kgid_t			gid;
	dev_t			rdev;
	u32			osid;
	struct audit_cap_data	fcap;
	unsigned int		fcap_ver;
	unsigned char		type;		/* record type */
	/*
	 * This was an allocated audit_names and not from the array of
	 * names allocated in the task audit context.  Thus this name
	 * should be freed on syscall exit.
	 */
	bool			should_free;
};

struct audit_proctitle {
	int	len;	/* length of the cmdline field. */
	char	*value;	/* the cmdline field */
};

/* The per-task audit context. */
struct audit_context {
	int		    dummy;	/* must be the first element */
	int		    in_syscall;	/* 1 if task is in a syscall */
	enum audit_state    state, current_state;
	unsigned int	    serial;     /* serial number for record */
	int		    major;      /* syscall number */
	struct timespec	    ctime;      /* time of syscall entry */
	unsigned long	    argv[4];    /* syscall arguments */
	long		    return_code;/* syscall return code */
	u64		    prio;
	int		    return_valid; /* return code is valid */
	/*
	 * The names_list is the list of all audit_names collected during this
	 * syscall.  The first AUDIT_NAMES entries in the names_list will
	 * actually be from the preallocated_names array for performance
	 * reasons.  Except during allocation they should never be referenced
	 * through the preallocated_names array and should only be found/used
	 * by running the names_list.
	 */
	struct audit_names  preallocated_names[AUDIT_NAMES];
	int		    name_count; /* total records in names_list */
	struct list_head    names_list;	/* struct audit_names->list anchor */
	char		    *filterkey;	/* key for rule that triggered record */
	struct path	    pwd;
	struct audit_aux_data *aux;
	struct audit_aux_data *aux_pids;
	struct sockaddr_storage *sockaddr;
	size_t sockaddr_len;
				/* Save things to print about task_struct */
	pid_t		    pid, ppid;
	kuid_t		    uid, euid, suid, fsuid;
	kgid_t		    gid, egid, sgid, fsgid;
	unsigned long	    personality;
	int		    arch;

	pid_t		    target_pid;
	kuid_t		    target_auid;
	kuid_t		    target_uid;
	unsigned int	    target_sessionid;
	u32		    target_sid;
	char		    target_comm[TASK_COMM_LEN];

	struct audit_tree_refs *trees, *first_trees;
	struct list_head killed_trees;
	int tree_count;

	int type;
	union {
		struct {
			int nargs;
			long args[6];
		} socketcall;
		struct {
			kuid_t			uid;
			kgid_t			gid;
			umode_t			mode;
			u32			osid;
			int			has_perm;
			uid_t			perm_uid;
			gid_t			perm_gid;
			umode_t			perm_mode;
			unsigned long		qbytes;
		} ipc;
		struct {
			mqd_t			mqdes;
			struct mq_attr		mqstat;
		} mq_getsetattr;
		struct {
			mqd_t			mqdes;
			int			sigev_signo;
		} mq_notify;
		struct {
			mqd_t			mqdes;
			size_t			msg_len;
			unsigned int		msg_prio;
			struct timespec		abs_timeout;
		} mq_sendrecv;
		struct {
			int			oflag;
			umode_t			mode;
			struct mq_attr		attr;
		} mq_open;
		struct {
			pid_t			pid;
			struct audit_cap_data	cap;
		} capset;
		struct {
			int			fd;
			int			flags;
		} mmap;
		struct {
			int			argc;
		} execve;
	};
	int fds[2];
	struct audit_proctitle proctitle;
};

extern u32 audit_ever_enabled;

extern void audit_copy_inode(struct audit_names *name,
			     const struct dentry *dentry,
			     const struct inode *inode);
extern void audit_log_cap(struct audit_buffer *ab, char *prefix,
			  kernel_cap_t *cap);
extern void audit_log_name(struct audit_context *context,
			   struct audit_names *n, struct path *path,
			   int record_num, int *call_panic);

extern int audit_pid;

#define AUDIT_INODE_BUCKETS	32
extern struct list_head audit_inode_hash[AUDIT_INODE_BUCKETS];

static inline int audit_hash_ino(u32 ino)
{
	return (ino & (AUDIT_INODE_BUCKETS-1));
}

/* Indicates that audit should log the full pathname. */
#define AUDIT_NAME_FULL -1

extern int audit_match_class(int class, unsigned syscall);
extern int audit_comparator(const u32 left, const u32 op, const u32 right);
extern int audit_uid_comparator(kuid_t left, u32 op, kuid_t right);
extern int audit_gid_comparator(kgid_t left, u32 op, kgid_t right);
extern int parent_len(const char *path);
extern int audit_compare_dname_path(const char *dname, const char *path, int plen);
extern struct sk_buff *audit_make_reply(__u32 portid, int seq, int type,
					int done, int multi,
					const void *payload, int size);
extern void		    audit_panic(const char *message);

struct audit_netlink_list {
	__u32 portid;
	struct net *net;
	struct sk_buff_head q;
};

int audit_send_list(void *);

struct audit_net {
	struct sock *nlsk;
};

extern int selinux_audit_rule_update(void);

extern struct mutex audit_filter_mutex;
extern int audit_del_rule(struct audit_entry *);
extern void audit_free_rule_rcu(struct rcu_head *);
extern struct list_head audit_filter_list[];

extern struct audit_entry *audit_dupe_rule(struct audit_krule *old);

extern void audit_log_d_path_exe(struct audit_buffer *ab,
				 struct mm_struct *mm);

/* audit watch functions */
#ifdef CONFIG_AUDIT_WATCH
extern void audit_put_watch(struct audit_watch *watch);
extern void audit_get_watch(struct audit_watch *watch);
extern int audit_to_watch(struct audit_krule *krule, char *path, int len, u32 op);
extern int audit_add_watch(struct audit_krule *krule, struct list_head **list);
extern void audit_remove_watch_rule(struct audit_krule *krule);
extern char *audit_watch_path(struct audit_watch *watch);
extern int audit_watch_compare(struct audit_watch *watch, unsigned long ino, dev_t dev);

extern struct audit_fsnotify_mark *audit_alloc_mark(struct audit_krule *krule, char *pathname, int len);
extern char *audit_mark_path(struct audit_fsnotify_mark *mark);
extern void audit_remove_mark(struct audit_fsnotify_mark *audit_mark);
extern void audit_remove_mark_rule(struct audit_krule *krule);
extern int audit_mark_compare(struct audit_fsnotify_mark *mark, unsigned long ino, dev_t dev);
extern int audit_dupe_exe(struct audit_krule *new, struct audit_krule *old);
extern int audit_exe_compare(struct task_struct *tsk, struct audit_fsnotify_mark *mark);

#else
#define audit_put_watch(w) {}
#define audit_get_watch(w) {}
#define audit_to_watch(k, p, l, o) (-EINVAL)
#define audit_add_watch(k, l) (-EINVAL)
#define audit_remove_watch_rule(k) BUG()
#define audit_watch_path(w) ""
#define audit_watch_compare(w, i, d) 0

#define audit_alloc_mark(k, p, l) (ERR_PTR(-EINVAL))
#define audit_mark_path(m) ""
#define audit_remove_mark(m)
#define audit_remove_mark_rule(k)
#define audit_mark_compare(m, i, d) 0
#define audit_exe_compare(t, m) (-EINVAL)
#define audit_dupe_exe(n, o) (-EINVAL)
#endif /* CONFIG_AUDIT_WATCH */

#ifdef CONFIG_AUDIT_TREE
extern struct audit_chunk *audit_tree_lookup(const struct inode *);
extern void audit_put_chunk(struct audit_chunk *);
extern bool audit_tree_match(struct audit_chunk *, struct audit_tree *);
extern int audit_make_tree(struct audit_krule *, char *, u32);
extern int audit_add_tree_rule(struct audit_krule *);
extern int audit_remove_tree_rule(struct audit_krule *);
extern void audit_trim_trees(void);
extern int audit_tag_tree(char *old, char *new);
extern const char *audit_tree_path(struct audit_tree *);
extern void audit_put_tree(struct audit_tree *);
extern void audit_kill_trees(struct list_head *);
#else
#define audit_remove_tree_rule(rule) BUG()
#define audit_add_tree_rule(rule) -EINVAL
#define audit_make_tree(rule, str, op) -EINVAL
#define audit_trim_trees() (void)0
#define audit_put_tree(tree) (void)0
#define audit_tag_tree(old, new) -EINVAL
#define audit_tree_path(rule) ""	/* never called */
#define audit_kill_trees(list) BUG()
#endif

extern char *audit_unpack_string(void **, size_t *, size_t);

extern pid_t audit_sig_pid;
extern kuid_t audit_sig_uid;
extern u32 audit_sig_sid;

#ifdef CONFIG_AUDITSYSCALL
extern int __audit_signal_info(int sig, struct task_struct *t);
static inline int audit_signal_info(int sig, struct task_struct *t)
{
	if (unlikely((audit_pid && t->tgid == audit_pid) ||
		     (audit_signals && !audit_dummy_context())))
		return __audit_signal_info(sig, t);
	return 0;
}
extern void audit_filter_inodes(struct task_struct *, struct audit_context *);
extern struct list_head *audit_killed_trees(void);
#else
#define audit_signal_info(s,t) AUDIT_DISABLED
#define audit_filter_inodes(t,c) AUDIT_DISABLED
#endif

extern struct mutex audit_cmd_mutex;