aboutsummaryrefslogblamecommitdiffstats
blob: 75a2ab3d0b0208dfa51e40339ffd00206622732e (plain) (tree)
1
2
3
4
5
6
7
8




                                                          


                                                                             


                                 

                                        










                           
                          

                         
                           

                             
                         
                                       
                                           
                                       




                                                                 
                                                

                                                              
                                 

                                                



                                                               



                                                            
                                 

                                                                




                                                   

                                             
                                       
                                     

















                                                                
                             






                                               
                             




                                            






                                                                               
                                      


                                   










                                                                     
                                   

          
                                                     



                                                                  
           
                                                                          




                                         
                                          
 
                                                                     

 
                                    
 
                                               
 
                                         
 
                                         











                                                                    
                                 

                             







                                                                        
                                    


                                  

      





                                                        
                                 
                                 
                              
 
                                                                  
 
                                                               

                         
                                                          



                 
                                                
 
                                                              

                                             
                                                                




                                      
                                 
 








                                                         
                                                                


                                               


                                                      

                                                            








                                                                   


                                                  
                                                 
                                                                






                                                                                     
                                                           


                       
                                                    

               

                                       

                                          
                                           
 


                                                   



                                                                      
                                                                    






                                              
                                                              

                           
                                                                 

                            
                                                                       



                                                                      
                                                                       

                                           


                                                                   









                                                                 
                                           
                                 







                                                                             
                                    
                                                                

                                               
                                                                                       
                                                     









                                                             
                                                           
              
                                                            



                               


                                                                     
 



                                                    
 
                                                                       
 



                                                                 






                                      
 
                                                                                
                                                          

                                               



                                                       
 


                                                                       
 



                                           

 








                                                         
                                                              









                                                                   
 
                                 






                                                      
                                                











                                                             
                              
                                                                           

                                                        
                                                                                                       




                                                    
                             


                                                                                                   


                              


                                                    


                                                             
                                                                              
                                           

                                                                             
            

                                                                              
                              









                                                     
                                                  












                                                               

                                                              
                                       

                                     

                      

                                          
                         
 




                                                                          



                                           
                         
 




                                                                        

 
  
                                                                 

   

                                                                    
 
                
 


                                  
                                                                     
                          
                           
 
                            
                                                



                                            
                   
 

                          







                                                       

  
                                      
 
                            



                                                                        
 
/*
 * Detect hard and soft lockups on a system
 *
 * started by Don Zickus, Copyright (C) 2010 Red Hat, Inc.
 *
 * Note: Most of this code is borrowed heavily from the original softlockup
 * detector, so thanks to Ingo for the initial implementation.
 * Some chunks also taken from the old x86-specific nmi watchdog code, thanks
 * to those contributors as well.
 */

#define pr_fmt(fmt) "NMI watchdog: " fmt

#include <linux/mm.h>
#include <linux/cpu.h>
#include <linux/nmi.h>
#include <linux/init.h>
#include <linux/delay.h>
#include <linux/freezer.h>
#include <linux/kthread.h>
#include <linux/lockdep.h>
#include <linux/notifier.h>
#include <linux/module.h>
#include <linux/sysctl.h>
#include <linux/smpboot.h>

#include <asm/irq_regs.h>
#include <linux/kvm_para.h>
#include <linux/perf_event.h>

int watchdog_enabled = 1;
int __read_mostly watchdog_thresh = 10;
static int __read_mostly watchdog_disabled;
static u64 __read_mostly sample_period;

static DEFINE_PER_CPU(unsigned long, watchdog_touch_ts);
static DEFINE_PER_CPU(struct task_struct *, softlockup_watchdog);
static DEFINE_PER_CPU(struct hrtimer, watchdog_hrtimer);
static DEFINE_PER_CPU(bool, softlockup_touch_sync);
static DEFINE_PER_CPU(bool, soft_watchdog_warn);
static DEFINE_PER_CPU(unsigned long, hrtimer_interrupts);
static DEFINE_PER_CPU(unsigned long, soft_lockup_hrtimer_cnt);
#ifdef CONFIG_HARDLOCKUP_DETECTOR
static DEFINE_PER_CPU(bool, hard_watchdog_warn);
static DEFINE_PER_CPU(bool, watchdog_nmi_touch);
static DEFINE_PER_CPU(unsigned long, hrtimer_interrupts_saved);
static DEFINE_PER_CPU(struct perf_event *, watchdog_ev);
#endif

/* boot commands */
/*
 * Should we panic when a soft-lockup or hard-lockup occurs:
 */
#ifdef CONFIG_HARDLOCKUP_DETECTOR
static int hardlockup_panic =
			CONFIG_BOOTPARAM_HARDLOCKUP_PANIC_VALUE;

static int __init hardlockup_panic_setup(char *str)
{
	if (!strncmp(str, "panic", 5))
		hardlockup_panic = 1;
	else if (!strncmp(str, "nopanic", 7))
		hardlockup_panic = 0;
	else if (!strncmp(str, "0", 1))
		watchdog_enabled = 0;
	return 1;
}
__setup("nmi_watchdog=", hardlockup_panic_setup);
#endif

unsigned int __read_mostly softlockup_panic =
			CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC_VALUE;

static int __init softlockup_panic_setup(char *str)
{
	softlockup_panic = simple_strtoul(str, NULL, 0);

	return 1;
}
__setup("softlockup_panic=", softlockup_panic_setup);

static int __init nowatchdog_setup(char *str)
{
	watchdog_enabled = 0;
	return 1;
}
__setup("nowatchdog", nowatchdog_setup);

/* deprecated */
static int __init nosoftlockup_setup(char *str)
{
	watchdog_enabled = 0;
	return 1;
}
__setup("nosoftlockup", nosoftlockup_setup);
/*  */

/*
 * Hard-lockup warnings should be triggered after just a few seconds. Soft-
 * lockups can have false positives under extreme conditions. So we generally
 * want a higher threshold for soft lockups than for hard lockups. So we couple
 * the thresholds with a factor: we make the soft threshold twice the amount of
 * time the hard threshold is.
 */
static int get_softlockup_thresh(void)
{
	return watchdog_thresh * 2;
}

/*
 * Returns seconds, approximately.  We don't need nanosecond
 * resolution, and we don't need to waste time with a big divide when
 * 2^30ns == 1.074s.
 */
static unsigned long get_timestamp(int this_cpu)
{
	return cpu_clock(this_cpu) >> 30LL;  /* 2^30 ~= 10^9 */
}

static void set_sample_period(void)
{
	/*
	 * convert watchdog_thresh from seconds to ns
	 * the divide by 5 is to give hrtimer several chances (two
	 * or three with the current relation between the soft
	 * and hard thresholds) to increment before the
	 * hardlockup detector generates a warning
	 */
	sample_period = get_softlockup_thresh() * ((u64)NSEC_PER_SEC / 5);
}

/* Commands for resetting the watchdog */
static void __touch_watchdog(void)
{
	int this_cpu = smp_processor_id();

	__this_cpu_write(watchdog_touch_ts, get_timestamp(this_cpu));
}

void touch_softlockup_watchdog(void)
{
	__this_cpu_write(watchdog_touch_ts, 0);
}
EXPORT_SYMBOL(touch_softlockup_watchdog);

void touch_all_softlockup_watchdogs(void)
{
	int cpu;

	/*
	 * this is done lockless
	 * do we care if a 0 races with a timestamp?
	 * all it means is the softlock check starts one cycle later
	 */
	for_each_online_cpu(cpu)
		per_cpu(watchdog_touch_ts, cpu) = 0;
}

#ifdef CONFIG_HARDLOCKUP_DETECTOR
void touch_nmi_watchdog(void)
{
	if (watchdog_enabled) {
		unsigned cpu;

		for_each_present_cpu(cpu) {
			if (per_cpu(watchdog_nmi_touch, cpu) != true)
				per_cpu(watchdog_nmi_touch, cpu) = true;
		}
	}
	touch_softlockup_watchdog();
}
EXPORT_SYMBOL(touch_nmi_watchdog);

#endif

void touch_softlockup_watchdog_sync(void)
{
	__raw_get_cpu_var(softlockup_touch_sync) = true;
	__raw_get_cpu_var(watchdog_touch_ts) = 0;
}

#ifdef CONFIG_HARDLOCKUP_DETECTOR
/* watchdog detector functions */
static int is_hardlockup(void)
{
	unsigned long hrint = __this_cpu_read(hrtimer_interrupts);

	if (__this_cpu_read(hrtimer_interrupts_saved) == hrint)
		return 1;

	__this_cpu_write(hrtimer_interrupts_saved, hrint);
	return 0;
}
#endif

static int is_softlockup(unsigned long touch_ts)
{
	unsigned long now = get_timestamp(smp_processor_id());

	/* Warn about unreasonable delays: */
	if (time_after(now, touch_ts + get_softlockup_thresh()))
		return now - touch_ts;

	return 0;
}

#ifdef CONFIG_HARDLOCKUP_DETECTOR

static struct perf_event_attr wd_hw_attr = {
	.type		= PERF_TYPE_HARDWARE,
	.config		= PERF_COUNT_HW_CPU_CYCLES,
	.size		= sizeof(struct perf_event_attr),
	.pinned		= 1,
	.disabled	= 1,
};

/* Callback function for perf event subsystem */
static void watchdog_overflow_callback(struct perf_event *event,
		 struct perf_sample_data *data,
		 struct pt_regs *regs)
{
	/* Ensure the watchdog never gets throttled */
	event->hw.interrupts = 0;

	if (__this_cpu_read(watchdog_nmi_touch) == true) {
		__this_cpu_write(watchdog_nmi_touch, false);
		return;
	}

	/* check for a hardlockup
	 * This is done by making sure our timer interrupt
	 * is incrementing.  The timer interrupt should have
	 * fired multiple times before we overflow'd.  If it hasn't
	 * then this is a good indication the cpu is stuck
	 */
	if (is_hardlockup()) {
		int this_cpu = smp_processor_id();

		/* only print hardlockups once */
		if (__this_cpu_read(hard_watchdog_warn) == true)
			return;

		if (hardlockup_panic)
			panic("Watchdog detected hard LOCKUP on cpu %d", this_cpu);
		else
			WARN(1, "Watchdog detected hard LOCKUP on cpu %d", this_cpu);

		__this_cpu_write(hard_watchdog_warn, true);
		return;
	}

	__this_cpu_write(hard_watchdog_warn, false);
	return;
}
#endif /* CONFIG_HARDLOCKUP_DETECTOR */

static void watchdog_interrupt_count(void)
{
	__this_cpu_inc(hrtimer_interrupts);
}

static int watchdog_nmi_enable(unsigned int cpu);
static void watchdog_nmi_disable(unsigned int cpu);

/* watchdog kicker functions */
static enum hrtimer_restart watchdog_timer_fn(struct hrtimer *hrtimer)
{
	unsigned long touch_ts = __this_cpu_read(watchdog_touch_ts);
	struct pt_regs *regs = get_irq_regs();
	int duration;

	/* kick the hardlockup detector */
	watchdog_interrupt_count();

	/* kick the softlockup detector */
	wake_up_process(__this_cpu_read(softlockup_watchdog));

	/* .. and repeat */
	hrtimer_forward_now(hrtimer, ns_to_ktime(sample_period));

	if (touch_ts == 0) {
		if (unlikely(__this_cpu_read(softlockup_touch_sync))) {
			/*
			 * If the time stamp was touched atomically
			 * make sure the scheduler tick is up to date.
			 */
			__this_cpu_write(softlockup_touch_sync, false);
			sched_clock_tick();
		}

		/* Clear the guest paused flag on watchdog reset */
		kvm_check_and_clear_guest_paused();
		__touch_watchdog();
		return HRTIMER_RESTART;
	}

	/* check for a softlockup
	 * This is done by making sure a high priority task is
	 * being scheduled.  The task touches the watchdog to
	 * indicate it is getting cpu time.  If it hasn't then
	 * this is a good indication some task is hogging the cpu
	 */
	duration = is_softlockup(touch_ts);
	if (unlikely(duration)) {
		/*
		 * If a virtual machine is stopped by the host it can look to
		 * the watchdog like a soft lockup, check to see if the host
		 * stopped the vm before we issue the warning
		 */
		if (kvm_check_and_clear_guest_paused())
			return HRTIMER_RESTART;

		/* only warn once */
		if (__this_cpu_read(soft_watchdog_warn) == true)
			return HRTIMER_RESTART;

		printk(KERN_EMERG "BUG: soft lockup - CPU#%d stuck for %us! [%s:%d]\n",
			smp_processor_id(), duration,
			current->comm, task_pid_nr(current));
		print_modules();
		print_irqtrace_events(current);
		if (regs)
			show_regs(regs);
		else
			dump_stack();

		if (softlockup_panic)
			panic("softlockup: hung tasks");
		__this_cpu_write(soft_watchdog_warn, true);
	} else
		__this_cpu_write(soft_watchdog_warn, false);

	return HRTIMER_RESTART;
}

static void watchdog_set_prio(unsigned int policy, unsigned int prio)
{
	struct sched_param param = { .sched_priority = prio };

	sched_setscheduler(current, policy, &param);
}

static void watchdog_enable(unsigned int cpu)
{
	struct hrtimer *hrtimer = &__raw_get_cpu_var(watchdog_hrtimer);

	/* kick off the timer for the hardlockup detector */
	hrtimer_init(hrtimer, CLOCK_MONOTONIC, HRTIMER_MODE_REL);
	hrtimer->function = watchdog_timer_fn;

	if (!watchdog_enabled) {
		kthread_park(current);
		return;
	}

	/* Enable the perf event */
	watchdog_nmi_enable(cpu);

	/* done here because hrtimer_start can only pin to smp_processor_id() */
	hrtimer_start(hrtimer, ns_to_ktime(sample_period),
		      HRTIMER_MODE_REL_PINNED);

	/* initialize timestamp */
	watchdog_set_prio(SCHED_FIFO, MAX_RT_PRIO - 1);
	__touch_watchdog();
}

static void watchdog_disable(unsigned int cpu)
{
	struct hrtimer *hrtimer = &__raw_get_cpu_var(watchdog_hrtimer);

	watchdog_set_prio(SCHED_NORMAL, 0);
	hrtimer_cancel(hrtimer);
	/* disable the perf event */
	watchdog_nmi_disable(cpu);
}

static int watchdog_should_run(unsigned int cpu)
{
	return __this_cpu_read(hrtimer_interrupts) !=
		__this_cpu_read(soft_lockup_hrtimer_cnt);
}

/*
 * The watchdog thread function - touches the timestamp.
 *
 * It only runs once every sample_period seconds (4 seconds by
 * default) to reset the softlockup timestamp. If this gets delayed
 * for more than 2*watchdog_thresh seconds then the debug-printout
 * triggers in watchdog_timer_fn().
 */
static void watchdog(unsigned int cpu)
{
	__this_cpu_write(soft_lockup_hrtimer_cnt,
			 __this_cpu_read(hrtimer_interrupts));
	__touch_watchdog();
}

#ifdef CONFIG_HARDLOCKUP_DETECTOR
/*
 * People like the simple clean cpu node info on boot.
 * Reduce the watchdog noise by only printing messages
 * that are different from what cpu0 displayed.
 */
static unsigned long cpu0_err;

static int watchdog_nmi_enable(unsigned int cpu)
{
	struct perf_event_attr *wd_attr;
	struct perf_event *event = per_cpu(watchdog_ev, cpu);

	/* is it already setup and enabled? */
	if (event && event->state > PERF_EVENT_STATE_OFF)
		goto out;

	/* it is setup but not enabled */
	if (event != NULL)
		goto out_enable;

	wd_attr = &wd_hw_attr;
	wd_attr->sample_period = hw_nmi_get_sample_period(watchdog_thresh);

	/* Try to register using hardware perf events */
	event = perf_event_create_kernel_counter(wd_attr, cpu, NULL, watchdog_overflow_callback, NULL);

	/* save cpu0 error for future comparision */
	if (cpu == 0 && IS_ERR(event))
		cpu0_err = PTR_ERR(event);

	if (!IS_ERR(event)) {
		/* only print for cpu0 or different than cpu0 */
		if (cpu == 0 || cpu0_err)
			pr_info("enabled on all CPUs, permanently consumes one hw-PMU counter.\n");
		goto out_save;
	}

	/* skip displaying the same error again */
	if (cpu > 0 && (PTR_ERR(event) == cpu0_err))
		return PTR_ERR(event);

	/* vary the KERN level based on the returned errno */
	if (PTR_ERR(event) == -EOPNOTSUPP)
		pr_info("disabled (cpu%i): not supported (no LAPIC?)\n", cpu);
	else if (PTR_ERR(event) == -ENOENT)
		pr_warning("disabled (cpu%i): hardware events not enabled\n",
			 cpu);
	else
		pr_err("disabled (cpu%i): unable to create perf event: %ld\n",
			cpu, PTR_ERR(event));
	return PTR_ERR(event);

	/* success path */
out_save:
	per_cpu(watchdog_ev, cpu) = event;
out_enable:
	perf_event_enable(per_cpu(watchdog_ev, cpu));
out:
	return 0;
}

static void watchdog_nmi_disable(unsigned int cpu)
{
	struct perf_event *event = per_cpu(watchdog_ev, cpu);

	if (event) {
		perf_event_disable(event);
		per_cpu(watchdog_ev, cpu) = NULL;

		/* should be in cleanup, but blocks oprofile */
		perf_event_release_kernel(event);
	}
	return;
}
#else
static int watchdog_nmi_enable(unsigned int cpu) { return 0; }
static void watchdog_nmi_disable(unsigned int cpu) { return; }
#endif /* CONFIG_HARDLOCKUP_DETECTOR */

/* prepare/enable/disable routines */
/* sysctl functions */
#ifdef CONFIG_SYSCTL
static void watchdog_enable_all_cpus(void)
{
	unsigned int cpu;

	if (watchdog_disabled) {
		watchdog_disabled = 0;
		for_each_online_cpu(cpu)
			kthread_unpark(per_cpu(softlockup_watchdog, cpu));
	}
}

static void watchdog_disable_all_cpus(void)
{
	unsigned int cpu;

	if (!watchdog_disabled) {
		watchdog_disabled = 1;
		for_each_online_cpu(cpu)
			kthread_park(per_cpu(softlockup_watchdog, cpu));
	}
}

/*
 * proc handler for /proc/sys/kernel/nmi_watchdog,watchdog_thresh
 */

int proc_dowatchdog(struct ctl_table *table, int write,
		    void __user *buffer, size_t *lenp, loff_t *ppos)
{
	int ret;

	if (watchdog_disabled < 0)
		return -ENODEV;

	ret = proc_dointvec_minmax(table, write, buffer, lenp, ppos);
	if (ret || !write)
		return ret;

	set_sample_period();
	if (watchdog_enabled && watchdog_thresh)
		watchdog_enable_all_cpus();
	else
		watchdog_disable_all_cpus();

	return ret;
}
#endif /* CONFIG_SYSCTL */

static struct smp_hotplug_thread watchdog_threads = {
	.store			= &softlockup_watchdog,
	.thread_should_run	= watchdog_should_run,
	.thread_fn		= watchdog,
	.thread_comm		= "watchdog/%u",
	.setup			= watchdog_enable,
	.park			= watchdog_disable,
	.unpark			= watchdog_enable,
};

void __init lockup_detector_init(void)
{
	set_sample_period();
	if (smpboot_register_percpu_thread(&watchdog_threads)) {
		pr_err("Failed to create watchdog threads, disabled\n");
		watchdog_disabled = -ENODEV;
	}
}