include ../scripts/Makefile.include
# The default target of this Makefile is...
all:
include config/utilities.mak
# Define V to have a more verbose compile.
#
# Define O to save output files in a separate directory.
#
# Define ARCH as name of target architecture if you want cross-builds.
#
# Define CROSS_COMPILE as prefix name of compiler if you want cross-builds.
#
# Define NO_LIBPERL to disable perl script extension.
#
# Define NO_LIBPYTHON to disable python script extension.
#
# Define PYTHON to point to the python binary if the default
# `python' is not correct; for example: PYTHON=python2
#
# Define PYTHON_CONFIG to point to the python-config binary if
# the default `$(PYTHON)-config' is not correct.
#
# Define ASCIIDOC8 if you want to format documentation with AsciiDoc 8
#
# Define DOCBOOK_XSL_172 if you want to format man pages with DocBook XSL v1.72.
#
# Define LDFLAGS=-static to build a static binary.
#
# Define EXTRA_CFLAGS=-m64 or EXTRA_CFLAGS=-m32 as appropriate for cross-builds.
#
# Define NO_DWARF if you do not want debug-info analysis feature at all.
#
# Define WERROR=0 to disable treating any warnings as errors.
#
# Define NO_NEWT if you do not want TUI support.
#
# Define NO_GTK2 if you do not want GTK+ GUI support.
#
# Define NO_DEMANGLE if you do not want C++ symbol demangling.
#
# Define NO_LIBELF if you do not want libelf dependency (e.g. cross-builds)
#
# Define NO_LIBUNWIND if you do not want libunwind dependency for dwarf
# backtrace post unwind.
#
# Define NO_BACKTRACE if you do not want stack backtrace debug feature
$(OUTPUT)PERF-VERSION-FILE: .FORCE-PERF-VERSION-FILE
@$(SHELL_PATH) util/PERF-VERSION-GEN $(OUTPUT)
-include $(OUTPUT)PERF-VERSION-FILE
uname_M := $(shell uname -m 2>/dev/null || echo not)
ARCH ?= $(shell echo $(uname_M) | sed -e s/i.86/i386/ -e s/sun4u/sparc64/ \
-e s/arm.*/arm/ -e s/sa110/arm/ \
-e s/s390x/s390/ -e s/parisc64/parisc/ \
-e s/ppc.*/powerpc/ -e s/mips.*/mips/ \
-e s/sh[234].*/sh/ -e s/aarch64.*/arm64/ )
NO_PERF_REGS := 1
CC = $(CROSS_COMPILE)gcc
AR = $(CROSS_COMPILE)ar
# Additional ARCH settings for x86
ifeq ($(ARCH),i386)
override ARCH := x86
NO_PERF_REGS := 0
LIBUNWIND_LIBS = -lunwind -lunwind-x86
endif
ifeq ($(ARCH),x86_64)
override ARCH := x86
IS_X86_64 := 0
ifeq (, $(findstring m32,$(EXTRA_CFLAGS)))
IS_X86_64 := $(shell echo __x86_64__ | ${CC} -E -x c - | tail -n 1)
endif
ifeq (${IS_X86_64}, 1)
RAW_ARCH := x86_64
ARCH_CFLAGS := -DARCH_X86_64
ARCH_INCLUDE = ../../arch/x86/lib/memcpy_64.S ../../arch/x86/lib/memset_64.S
endif
NO_PERF_REGS := 0
LIBUNWIND_LIBS = -lunwind -lunwind-x86_64
endif
# Treat warnings as errors unless directed not to
ifneq ($(WERROR),0)
CFLAGS_WERROR := -Werror
endif
ifeq ("$(origin DEBUG)", "command line")
PERF_DEBUG = $(DEBUG)
endif
ifndef PERF_DEBUG
CFLAGS_OPTIMIZE = -O6 -D_FORTIFY_SOURCE=2
endif
ifdef PARSER_DEBUG
PARSER_DEBUG_BISON := -t
PARSER_DEBUG_FLEX := -d
PARSER_DEBUG_CFLAGS := -DPARSER_DEBUG
endif
CFLAGS = -fno-omit-frame-pointer -ggdb3 -funwind-tables -Wall -Wextra -std=gnu99 $(CFLAGS_WERROR) $(CFLAGS_OPTIMIZE) $(EXTRA_WARNINGS) $(EXTRA_CFLAGS) $(PARSER_DEBUG_CFLAGS)
EXTLIBS = -lpthread -lrt -lelf -lm
ALL_CFLAGS = $(CFLAGS) -D_LARGEFILE64_SOURCE -D_FILE_OFFSET_BITS=64 -D_GNU_SOURCE
ALL_LDFLAGS = $(LDFLAGS)
STRIP ?= strip
# Among the variables below, these:
# perfexecdir
# template_dir
# mandir
# infodir
# htmldir
# ETC_PERFCONFIG (but not sysconfdir)
# can be specified as a relative path some/where/else;
# this is interpreted as relative to $(prefix) and "perf" at
# runtime figures out where they are based on the path to the executable.
# This can help installing the suite in a relocatable way.
# Make the path relative to DESTDIR, not to prefix
ifndef DESTDIR
prefix = $(HOME)
endif
bindir_relative = bin
bindir = $(prefix)/$(bindir_relative)
mandir = share/man
infodir = share/info
perfexecdir = libexec/perf-core
sharedir = $(prefix)/share
template_dir = share/perf-core/templates
htmldir = share/doc/perf-doc
ifeq ($(prefix),/usr)
sysconfdir = /etc
ETC_PERFCONFIG = $(sysconfdir)/perfconfig
else
sysconfdir = $(prefix)/etc
ETC_PERFCONFIG = etc/perfconfig
endif
lib = lib
export prefix bindir sharedir sysconfdir
RM = rm -f
MKDIR = mkdir
FIND = find
INSTALL = install
# sparse is architecture-neutral, which means that we need to tell it
# explicitly what architecture to check for. Fix this up for yours..
SPARSE_FLAGS = -D__BIG_ENDIAN__ -D__powerpc__
-include config/feature-tests.mak
ifeq ($(call try-cc,$(SOURCE_HELLO),$(CFLAGS) -Werror -fstack-protector-all,-fstack-protector-all),y)
CFLAGS := $(CFLAGS) -fstack-protector-all
endif
ifeq ($(call try-cc,$(SOURCE_HELLO),$(CFLAGS) -Werror -Wstack-protector,-Wstack-protector),y)
CFLAGS := $(CFLAGS) -Wstack-protector
endif
ifeq ($(call try-cc,$(SOURCE_HELLO),$(CFLAGS) -Werror -Wvolatile-register-var,-Wvolatile-register-var),y)
CFLAGS := $(CFLAGS) -Wvolatile-register-var
endif
### --- END CONFIGURATION SECTION ---
ifeq ($(srctree),)
srctree := $(patsubst %/,%,$(dir $(shell pwd)))
srctree := $(patsubst %/,%,$(dir $(srctree)))
#$(info Determined 'srctree' to be $(srctree))
endif
ifneq ($(objtree),)
#$(info Determined 'objtree' to be $(objtree))
endif
ifneq ($(OUTPUT),)
#$(info Determined 'OUTPUT' to be $(OUTPUT))
endif
BASIC_CFLAGS = \
-Iutil/include \
-Iarch/$(ARCH)/include \
$(if $(objtree),-I$(objtree)/arch/$(ARCH)/include/generated/uapi) \
-I$(srctree)/arch/$(ARCH)/include/uapi \
-I$(srctree)/arch/$(ARCH)/include \
$(if $(objtree),-I$(objtree)/include/generated/uapi) \
-I$(srctree)/include/uapi \
-I$(srctree)/include \
-I$(OUTPUT)util \
-Iutil \
-I. \
-I$(TRACE_EVENT_DIR) \
-D_LARGEFILE64_SOURCE -D_FILE_OFFSET_BITS=64 -D_GNU_SOURCE
BASIC_LDFLAGS =
ifeq ($(call try-cc,$(SOURCE_BIONIC),$(CFLAGS),bionic),y)
BIONIC := 1
EXTLIBS := $(filter-out -lrt,$(EXTLIBS))
EXTLIBS := $(filter-out -lpthread,$(EXTLIBS))
BASIC_CFLAGS += -I.
endif
# Guard against environment variables
BUILTIN_OBJS =
LIB_H =
LIB_OBJS =
PYRF_OBJS =
SCRIPT_SH =
SCRIPT_SH += perf-archive.sh
grep-libs = $(filter -l%,$(1))
strip-libs = $(filter-out -l%,$(1))
TRACE_EVENT_DIR = ../lib/traceevent/
ifneq ($(OUTPUT),)
TE_PATH=$(OUTPUT)
else
TE_PATH=$(TRACE_EVENT_DIR)
endif
LIBTRACEEVENT = $(TE_PATH)libtraceevent.a
TE_LIB := -L$(TE_PATH) -ltraceevent
PYTHON_EXT_SRCS := $(shell grep -v ^\# util/python-ext-sources)
PYTHON_EXT_DEPS := util/python-ext-sources util/setup.py
export LIBTRACEEVENT
$(OUTPUT)python/perf.so: $(PYTHON_EXT_SRCS) $(PYTHON_EXT_DEPS)
$(QUIET_GEN)CFLAGS='$(BASIC_CFLAGS)' $(PYTHON_WORD) util/setup.py \
--quiet build_ext; \
mkdir -p $(OUTPUT)python && \
cp $(PYTHON_EXTBUILD_LIB)perf.so $(OUTPUT)python/
#
# No Perl scripts right now:
#
SCRIPTS = $(patsubst %.sh,%,$(SCRIPT_SH))
#
# Single 'perf' binary right now:
#
PROGRAMS += $(OUTPUT)perf
LANG_BINDINGS =
# what 'all' will build and 'install' will install, in perfexecdir
ALL_PROGRAMS = $(PROGRAMS) $(SCRIPTS)
# what 'all' will build but not install in perfexecdir
OTHER_PROGRAMS = $(OUTPUT)perf
# Set paths to tools early so that they can be used for version tests.
ifndef SHELL_PATH
SHELL_PATH = /bin/sh
endif
ifndef PERL_PATH
PERL_PATH = /usr/bin/perl
endif
export PERL_PATH
FLEX = flex
BISON= bison
$(OUTPUT)util/parse-events-flex.c: util/parse-events.l $(OUTPUT)util/parse-events-bison.c
$(QUIET_FLEX)$(FLEX) --header-file=$(OUTPUT)util/parse-events-flex.h $(PARSER_DEBUG_FLEX) -t util/parse-events.l > $(OUTPUT)util/parse-events-flex.c
$(OUTPUT)util/parse-events-bison.c: util/parse-events.y
$(QUIET_BISON)$(BISON) -v util/parse-events.y -d $(PARSER_DEBUG_BISON) -o $(OUTPUT)util/parse-events-bison.c
$(OUTPUT)util/pmu-flex.c: util/pmu.l $(OUTPUT)util/pmu-bison.c
$(QUIET_FLEX)$(FLEX) --header-file=$(OUTPUT)util/pmu-flex.h -t util/pmu.l > $(OUTPUT)util/pmu-flex.c
$(OUTPUT)util/pmu-bison.c: util/pmu.y
$(QUIET_BISON)$(BISON) -v util/pmu.y -d -o $(OUTPUT)util/pmu-bison.c
$(OUTPUT)util/parse-events.o: $(OUTPUT)util/parse-events-flex.c $(OUTPUT)util/parse-events-bison.c
$(OUTPUT)util/pmu.o: $(OUTPUT)util/pmu-flex.c $(OUTPUT)util/pmu-bison.c
LIB_FILE=$(OUTPUT)libperf.a
LIB_H += ../../include/uapi/linux/perf_event.h
LIB_H += ../../include/linux/rbtree.h
LIB_H += ../../include/linux/list.h
LIB_H += ../../include/uapi/linux/const.h
LIB_H += ../../include/linux/hash.h
LIB_H += ../../include/linux/stringify.h
LIB_H += util/include/linux/bitmap.h
LIB_H += util/include/linux/bitops.h
LIB_H += util/include/linux/compiler.h
LIB_H += util/include/linux/const.h
LIB_H += util/include/linux/ctype.h
LIB_H += util/include/linux/kernel.h
LIB_H += util/include/linux/list.h
LIB_H += util/include/linux/export.h
LIB_H += util/include/linux/magic.h
LIB_H += util/include/linux/poison.h
LIB_H += util/include/linux/prefetch.h
LIB_H += util/include/linux/rbtree.h
LIB_H += util/include/linux/rbtree_augmented.h
LIB_H += util/include/linux/string.h
LIB_H += util/include/linux/types.h
LIB_H += util/include/linux/linkage.h
LIB_H += util/include/asm/asm-offsets.h
LIB_H += util/include/asm/bug.h
LIB_H += util/include/asm/byteorder.h
LIB_H += util/include/asm/hweight.h
LIB_H += util/include/asm/swab.h
LIB_H += util/include/asm/system.h
LIB_H += util/include/asm/uaccess.h
LIB_H += util/include/dwarf-regs.h
LIB_H += util/include/asm/dwarf2.h
LIB_H += util/include/asm/cpufeature.h
LIB_H += util/include/asm/unistd_32.h
LIB_H += util/include/asm/unistd_64.h
LIB_H += perf.h
LIB_H += util/annotate.h
LIB_H += util/cache.h
LIB_H += util/callchain.h
LIB_H += util/build-id.h
LIB_H += util/debug.h
LIB_H += util/debugfs.h
LIB_H += util/sysfs.h
LIB_H += util/pmu.h
LIB_H += util/event.h
LIB_H += util/evsel.h
LIB_H += util/evlist.h
LIB_H += util/exec_cmd.h
LIB_H += util/types.h
LIB_H += util/levenshtein.h
LIB_H += util/machine.h
LIB_H += util/map.h
LIB_H += util/parse-options.h
LIB_H += util/parse-events.h
LIB_H += util/quote.h
LIB_H += util/util.h
LIB_H += util/xyarray.h
LIB_H += util/header.h
LIB_H += util/help.h
LIB_H += util/session.h
LIB_H += util/strbuf.h
LIB_H += util/strlist.h
LIB_H += util/strfilter.h
LIB_H += util/svghelper.h
LIB_H += util/tool.h
LIB_H += util/run-command.h
LIB_H += util/sigchain.h
LIB_H += util/dso.h
LIB_H += util/symbol.h
LIB_H += util/color.h
LIB_H += util/values.h
LIB_H += util/sort.h
LIB_H += util/hist.h
LIB_H += util/thread.h
LIB_H += util/thread_map.h
LIB_H += util/trace-event.h
LIB_H += util/probe-finder.h
LIB_H += util/dwarf-aux.h
LIB_H += util/probe-event.h
LIB_H += util/pstack.h
LIB_H += util/cpumap.h
LIB_H += util/top.h
LIB_H += $(ARCH_INCLUDE)
LIB_H += util/cgroup.h
LIB_H += $(TRACE_EVENT_DIR)event-parse.h
LIB_H += util/target.h
LIB_H += util/rblist.h
LIB_H += util/intlist.h
LIB_H += util/perf_regs.h
LIB_H += util/unwind.h
LIB_H += ui/helpline.h
LIB_H += util/vdso.h
LIB_OBJS += $(OUTPUT)util/abspath.o
LIB_OBJS += $(OUTPUT)util/alias.o
LIB_OBJS += $(OUTPUT)util/annotate.o
LIB_OBJS += $(OUTPUT)util/build-id.o
LIB_OBJS += $(OUTPUT)util/config.o
LIB_OBJS += $(OUTPUT)util/ctype.o
LIB_OBJS += $(OUTPUT)util/debugfs.o
LIB_OBJS += $(OUTPUT)util/sysfs.o
LIB_OBJS += $(OUTPUT)util/pmu.o
LIB_OBJS += $(OUTPUT)util/environment.o
LIB_OBJS += $(OUTPUT)util/event.o
LIB_OBJS += $(OUTPUT)util/evlist.o
LIB_OBJS += $(OUTPUT)util/evsel.o
LIB_OBJS += $(OUTPUT)util/exec_cmd.o
LIB_OBJS += $(OUTPUT)util/help.o
LIB_OBJS += $(OUTPUT)util/levenshtein.o
LIB_OBJS += $(OUTPUT)util/parse-options.o
LIB_OBJS += $(OUTPUT)util/parse-events.o
LIB_OBJS += $(OUTPUT)util/path.o
LIB_OBJS += $(OUTPUT)util/rbtree.o
LIB_OBJS += $(OUTPUT)util/bitmap.o
LIB_OBJS += $(OUTPUT)util/hweight.o
LIB_OBJS += $(OUTPUT)util/run-command.o
LIB_OBJS += $(OUTPUT)util/quote.o
LIB_OBJS += $(OUTPUT)util/strbuf.o
LIB_OBJS += $(OUTPUT)util/string.o
LIB_OBJS += $(OUTPUT)util/strlist.o
LIB_OBJS += $(OUTPUT)util/strfilter.o
LIB_OBJS += $(OUTPUT)util/top.o
LIB_OBJS += $(OUTPUT)util/usage.o
LIB_OBJS += $(OUTPUT)util/wrapper.o
LIB_OBJS += $(OUTPUT)util/sigchain.o
LIB_OBJS += $(OUTPUT)util/dso.o
LIB_OBJS += $(OUTPUT)util/symbol.o
LIB_OBJS += $(OUTPUT)util/symbol-elf.o
LIB_OBJS += $(OUTPUT)util/color.o
LIB_OBJS += $(OUTPUT)util/pager.o
LIB_OBJS += $(OUTPUT)util/header.o
LIB_OBJS += $(OUTPUT)util/callchain.o
LIB_OBJS += $(OUTPUT)util/values.o
LIB_OBJS += $(OUTPUT)util/debug.o
LIB_OBJS += $(OUTPUT)util/machine.o
LIB_OBJS += $(OUTPUT)util/map.o
LIB_OBJS += $(OUTPUT)util/pstack.o
LIB_OBJS += $(OUTPUT)util/session.o
LIB_OBJS += $(OUTPUT)util/thread.o
LIB_OBJS += $(OUTPUT)util/thread_map.o
LIB_OBJS += $(OUTPUT)util/trace-event-parse.o
LIB_OBJS += $(OUTPUT)util/parse-events-flex.o
LIB_OBJS += $(OUTPUT)util/parse-events-bison.o
LIB_OBJS += $(OUTPUT)util/pmu-flex.o
LIB_OBJS += $(OUTPUT)util/pmu-bison.o
LIB_OBJS += $(OUTPUT)util/trace-event-read.o
LIB_OBJS += $(OUTPUT)util/trace-event-info.o
LIB_OBJS += $(OUTPUT)util/trace-event-scripting.o
LIB_OBJS += $(OUTPUT)util/svghelper.o
LIB_OBJS += $(OUTPUT)util/sort.o
LIB_OBJS += $(OUTPUT)util/hist.o
LIB_OBJS += $(OUTPUT)util/probe-event.o
LIB_OBJS += $(OUTPUT)util/util.o
LIB_OBJS += $(OUTPUT)util/xyarray.o
LIB_OBJS += $(OUTPUT)util/cpumap.o
LIB_OBJS += $(OUTPUT)util/cgroup.o
LIB_OBJS += $(OUTPUT)util/target.o
LIB_OBJS += $(OUTPUT)util/rblist.o
LIB_OBJS += $(OUTPUT)util/intlist.o
LIB_OBJS += $(OUTPUT)util/vdso.o
LIB_OBJS += $(OUTPUT)util/stat.o
LIB_OBJS += $(OUTPUT)ui/setup.o
LIB_OBJS += $(OUTPUT)ui/helpline.o
LIB_OBJS += $(OUTPUT)ui/progress.o
LIB_OBJS += $(OUTPUT)ui/hist.o
LIB_OBJS += $(OUTPUT)ui/stdio/hist.o
LIB_OBJS += $(OUTPUT)arch/common.o
LIB_OBJS += $(OUTPUT)tests/parse-events.o
LIB_OBJS += $(OUTPUT)tests/dso-data.o
LIB_OBJS += $(OUTPUT)tests/attr.o
LIB_OBJS += $(OUTPUT)tests/vmlinux-kallsyms.o
LIB_OBJS += $(OUTPUT)tests/open-syscall.o
LIB_OBJS += $(OUTPUT)tests/open-syscall-all-cpus.o
LIB_OBJS += $(OUTPUT)tests/open-syscall-tp-fields.o
LIB_OBJS += $(OUTPUT)tests/mmap-basic.o
LIB_OBJS += $(OUTPUT)tests/perf-record.o
LIB_OBJS += $(OUTPUT)tests/rdpmc.o
LIB_OBJS += $(OUTPUT)tests/evsel-roundtrip-name.o
LIB_OBJS += $(OUTPUT)tests/evsel-tp-sched.o
LIB_OBJS += $(OUTPUT)tests/pmu.o
LIB_OBJS += $(OUTPUT)tests/util.o
BUILTIN_OBJS += $(OUTPUT)builtin-annotate.o
BUILTIN_OBJS += $(OUTPUT)builtin-bench.o
# Benchmark modules
BUILTIN_OBJS += $(OUTPUT)bench/sched-messaging.o
BUILTIN_OBJS += $(OUTPUT)bench/sched-pipe.o
ifeq ($(RAW_ARCH),x86_64)
BUILTIN_OBJS += $(OUTPUT)bench/mem-memcpy-x86-64-asm.o
BUILTIN_OBJS += $(OUTPUT)bench/mem-memset-x86-64-asm.o
endif
BUILTIN_OBJS += $(OUTPUT)bench/mem-memcpy.o
BUILTIN_OBJS += $(OUTPUT)bench/mem-memset.o
BUILTIN_OBJS += $(OUTPUT)builtin-diff.o
BUILTIN_OBJS += $(OUTPUT)builtin-evlist.o
BUILTIN_OBJS += $(OUTPUT)builtin-help.o
BUILTIN_OBJS += $(OUTPUT)builtin-sched.o
BUILTIN_OBJS += $(OUTPUT)builtin-buildid-list.o
BUILTIN_OBJS += $(OUTPUT)builtin-buildid-cache.o
BUILTIN_OBJS += $(OUTPUT)builtin-list.o
BUILTIN_OBJS += $(OUTPUT)builtin-record.o
BUILTIN_OBJS += $(OUTPUT)builtin-report.o
BUILTIN_OBJS += $(OUTPUT)builtin-stat.o
BUILTIN_OBJS += $(OUTPUT)builtin-timechart.o
BUILTIN_OBJS += $(OUTPUT)builtin-top.o
BUILTIN_OBJS += $(OUTPUT)builtin-script.o
BUILTIN_OBJS += $(OUTPUT)builtin-probe.o
BUILTIN_OBJS += $(OUTPUT)builtin-kmem.o
BUILTIN_OBJS += $(OUTPUT)builtin-lock.o
BUILTIN_OBJS += $(OUTPUT)builtin-kvm.o
BUILTIN_OBJS += $(OUTPUT)builtin-inject.o
BUILTIN_OBJS += $(OUTPUT)tests/builtin-test.o
PERFLIBS = $(LIB_FILE) $(LIBTRACEEVENT)
#
# Platform specific tweaks
#
# We choose to avoid "if .. else if .. else .. endif endif"
# because maintaining the nesting to match is a pain. If
# we had "elif" things would have been much nicer...
-include config.mak.autogen
-include config.mak
ifdef NO_LIBELF
NO_DWARF := 1
NO_DEMANGLE := 1
NO_LIBUNWIND := 1
else
FLAGS_LIBELF=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS)
ifneq ($(call try-cc,$(SOURCE_LIBELF),$(FLAGS_LIBELF),libelf),y)
FLAGS_GLIBC=$(ALL_CFLAGS) $(ALL_LDFLAGS)
ifeq ($(call try-cc,$(SOURCE_GLIBC),$(FLAGS_GLIBC),glibc),y)
LIBC_SUPPORT := 1
endif
ifeq ($(BIONIC),1)
LIBC_SUPPORT := 1
endif
ifeq ($(LIBC_SUPPORT),1)
msg := $(warning No libelf found, disables 'probe' tool, please install elfutils-libelf-devel/libelf-dev);
NO_LIBELF := 1
NO_DWARF := 1
NO_DEMANGLE := 1
else
msg := $(error No gnu/libc-version.h found, please install glibc-dev[el]/glibc-static);
endif
else
# for linking with debug library, run like:
# make DEBUG=1 LIBDW_DIR=/opt/libdw/
ifdef LIBDW_DIR
LIBDW_CFLAGS := -I$(LIBDW_DIR)/include
LIBDW_LDFLAGS := -L$(LIBDW_DIR)/lib
endif
FLAGS_DWARF=$(ALL_CFLAGS) $(LIBDW_CFLAGS) -ldw -lelf $(LIBDW_LDFLAGS) $(ALL_LDFLAGS) $(EXTLIBS)
ifneq ($(call try-cc,$(SOURCE_DWARF),$(FLAGS_DWARF),libdw),y)
msg := $(warning No libdw.h found or old libdw.h found or elfutils is older than 0.138, disables dwarf support. Please install new elfutils-devel/libdw-dev);
NO_DWARF := 1
endif # Dwarf support
endif # SOURCE_LIBELF
endif # NO_LIBELF
ifndef NO_LIBUNWIND
# for linking with debug library, run like:
# make DEBUG=1 LIBUNWIND_DIR=/opt/libunwind/
ifdef LIBUNWIND_DIR
LIBUNWIND_CFLAGS := -I$(LIBUNWIND_DIR)/include
LIBUNWIND_LDFLAGS := -L$(LIBUNWIND_DIR)/lib
endif
FLAGS_UNWIND=$(LIBUNWIND_CFLAGS) $(ALL_CFLAGS) $(LIBUNWIND_LDFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) $(LIBUNWIND_LIBS)
ifneq ($(call try-cc,$(SOURCE_LIBUNWIND),$(FLAGS_UNWIND),libunwind),y)
msg := $(warning No libunwind found, disabling post unwind support. Please install libunwind-dev[el] >= 0.99);
NO_LIBUNWIND := 1
endif # Libunwind support
endif # NO_LIBUNWIND
-include arch/$(ARCH)/Makefile
ifneq ($(OUTPUT),)
BASIC_CFLAGS += -I$(OUTPUT)
endif
ifdef NO_LIBELF
EXTLIBS := $(filter-out -lelf,$(EXTLIBS))
# Remove ELF/DWARF dependent codes
LIB_OBJS := $(filter-out $(OUTPUT)util/symbol-elf.o,$(LIB_OBJS))
LIB_OBJS := $(filter-out $(OUTPUT)util/dwarf-aux.o,$(LIB_OBJS))
LIB_OBJS := $(filter-out $(OUTPUT)util/probe-event.o,$(LIB_OBJS))
LIB_OBJS := $(filter-out $(OUTPUT)util/probe-finder.o,$(LIB_OBJS))
BUILTIN_OBJS := $(filter-out $(OUTPUT)builtin-probe.o,$(BUILTIN_OBJS))
# Use minimal symbol handling
LIB_OBJS += $(OUTPUT)util/symbol-minimal.o
else # NO_LIBELF
BASIC_CFLAGS += -DLIBELF_SUPPORT
FLAGS_LIBELF=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS)
ifeq ($(call try-cc,$(SOURCE_ELF_MMAP),$(FLAGS_LIBELF),-DLIBELF_MMAP),y)
BASIC_CFLAGS += -DLIBELF_MMAP
endif
ifndef NO_DWARF
ifeq ($(origin PERF_HAVE_DWARF_REGS), undefined)
msg := $(warning DWARF register mappings have not been defined for architecture $(ARCH), DWARF support disabled);
else
BASIC_CFLAGS := -DDWARF_SUPPORT $(LIBDW_CFLAGS) $(BASIC_CFLAGS)
BASIC_LDFLAGS := $(LIBDW_LDFLAGS) $(BASIC_LDFLAGS)
EXTLIBS += -lelf -ldw
LIB_OBJS += $(OUTPUT)util/probe-finder.o
LIB_OBJS += $(OUTPUT)util/dwarf-aux.o
endif # PERF_HAVE_DWARF_REGS
endif # NO_DWARF
endif # NO_LIBELF
ifndef NO_LIBUNWIND
BASIC_CFLAGS += -DLIBUNWIND_SUPPORT
EXTLIBS += $(LIBUNWIND_LIBS)
BASIC_CFLAGS := $(LIBUNWIND_CFLAGS) $(BASIC_CFLAGS)
BASIC_LDFLAGS := $(LIBUNWIND_LDFLAGS) $(BASIC_LDFLAGS)
LIB_OBJS += $(OUTPUT)util/unwind.o
endif
ifndef NO_LIBAUDIT
FLAGS_LIBAUDIT = $(ALL_CFLAGS) $(ALL_LDFLAGS) -laudit
ifneq ($(call try-cc,$(SOURCE_LIBAUDIT),$(FLAGS_LIBAUDIT),libaudit),y)
msg := $(warning No libaudit.h found, disables 'trace' tool, please install audit-libs-devel or libaudit-dev);
else
BASIC_CFLAGS += -DLIBAUDIT_SUPPORT
BUILTIN_OBJS += $(OUTPUT)builtin-trace.o
EXTLIBS += -laudit
endif
endif
ifndef NO_NEWT
FLAGS_NEWT=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) -lnewt
ifneq ($(call try-cc,$(SOURCE_NEWT),$(FLAGS_NEWT),libnewt),y)
msg := $(warning newt not found, disables TUI support. Please install newt-devel or libnewt-dev);
else
# Fedora has /usr/include/slang/slang.h, but ubuntu /usr/include/slang.h
BASIC_CFLAGS += -I/usr/include/slang
BASIC_CFLAGS += -DNEWT_SUPPORT
EXTLIBS += -lnewt -lslang
LIB_OBJS += $(OUTPUT)ui/browser.o
LIB_OBJS += $(OUTPUT)ui/browsers/annotate.o
LIB_OBJS += $(OUTPUT)ui/browsers/hists.o
LIB_OBJS += $(OUTPUT)ui/browsers/map.o
LIB_OBJS += $(OUTPUT)ui/browsers/scripts.o
LIB_OBJS += $(OUTPUT)ui/util.o
LIB_OBJS += $(OUTPUT)ui/tui/setup.o
LIB_OBJS += $(OUTPUT)ui/tui/util.o
LIB_OBJS += $(OUTPUT)ui/tui/helpline.o
LIB_OBJS += $(OUTPUT)ui/tui/progress.o
LIB_H += ui/browser.h
LIB_H += ui/browsers/map.h
LIB_H += ui/keysyms.h
LIB_H += ui/libslang.h
LIB_H += ui/progress.h
LIB_H += ui/util.h
LIB_H += ui/ui.h
endif
endif
ifndef NO_GTK2
FLAGS_GTK2=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) $(shell pkg-config --libs --cflags gtk+-2.0 2>/dev/null)
ifneq ($(call try-cc,$(SOURCE_GTK2),$(FLAGS_GTK2),gtk2),y)
msg := $(warning GTK2 not found, disables GTK2 support. Please install gtk2-devel or libgtk2.0-dev);
else
ifeq ($(call try-cc,$(SOURCE_GTK2_INFOBAR),$(FLAGS_GTK2),-DHAVE_GTK_INFO_BAR),y)
BASIC_CFLAGS += -DHAVE_GTK_INFO_BAR
endif
BASIC_CFLAGS += -DGTK2_SUPPORT
BASIC_CFLAGS += $(shell pkg-config --cflags gtk+-2.0 2>/dev/null)
EXTLIBS += $(shell pkg-config --libs gtk+-2.0 2>/dev/null)
LIB_OBJS += $(OUTPUT)ui/gtk/browser.o
LIB_OBJS += $(OUTPUT)ui/gtk/setup.o
LIB_OBJS += $(OUTPUT)ui/gtk/util.o
LIB_OBJS += $(OUTPUT)ui/gtk/helpline.o
LIB_OBJS += $(OUTPUT)ui/gtk/progress.o
# Make sure that it'd be included only once.
ifeq ($(findstring -DNEWT_SUPPORT,$(BASIC_CFLAGS)),)
LIB_OBJS += $(OUTPUT)ui/util.o
endif
endif
endif
ifdef NO_LIBPERL
BASIC_CFLAGS += -DNO_LIBPERL
else
PERL_EMBED_LDOPTS = $(shell perl -MExtUtils::Embed -e ldopts 2>/dev/null)
PERL_EMBED_LDFLAGS = $(call strip-libs,$(PERL_EMBED_LDOPTS))
PERL_EMBED_LIBADD = $(call grep-libs,$(PERL_EMBED_LDOPTS))
PERL_EMBED_CCOPTS = `perl -MExtUtils::Embed -e ccopts 2>/dev/null`
FLAGS_PERL_EMBED=$(PERL_EMBED_CCOPTS) $(PERL_EMBED_LDOPTS)
ifneq ($(call try-cc,$(SOURCE_PERL_EMBED),$(FLAGS_PERL_EMBED),perl),y)
BASIC_CFLAGS += -DNO_LIBPERL
else
ALL_LDFLAGS += $(PERL_EMBED_LDFLAGS)
EXTLIBS += $(PERL_EMBED_LIBADD)
LIB_OBJS += $(OUTPUT)util/scripting-engines/trace-event-perl.o
LIB_OBJS += $(OUTPUT)scripts/perl/Perf-Trace-Util/Context.o
endif
endif
disable-python = $(eval $(disable-python_code))
define disable-python_code
BASIC_CFLAGS += -DNO_LIBPYTHON
$(if $(1),$(warning No $(1) was found))
$(warning Python support won't be built)
endef
override PYTHON := \
$(call get-executable-or-default,PYTHON,python)
ifndef PYTHON
$(call disable-python,python interpreter)
python-clean :=
else
PYTHON_WORD := $(call shell-wordify,$(PYTHON))
# python extension build directories
PYTHON_EXTBUILD := $(OUTPUT)python_ext_build/
PYTHON_EXTBUILD_LIB := $(PYTHON_EXTBUILD)lib/
PYTHON_EXTBUILD_TMP := $(PYTHON_EXTBUILD)tmp/
export PYTHON_EXTBUILD_LIB PYTHON_EXTBUILD_TMP
python-clean := rm -rf $(PYTHON_EXTBUILD) $(OUTPUT)python/perf.so
ifdef NO_LIBPYTHON
$(call disable-python)
else
override PYTHON_CONFIG := \
$(call get-executable-or-default,PYTHON_CONFIG,$(PYTHON)-config)
ifndef PYTHON_CONFIG
$(call disable-python,python-config tool)
else
PYTHON_CONFIG_SQ := $(call shell-sq,$(PYTHON_CONFIG))
PYTHON_EMBED_LDOPTS := $(shell $(PYTHON_CONFIG_SQ) --ldflags 2>/dev/null)
PYTHON_EMBED_LDFLAGS := $(call strip-libs,$(PYTHON_EMBED_LDOPTS))
PYTHON_EMBED_LIBADD := $(call grep-libs,$(PYTHON_EMBED_LDOPTS))
PYTHON_EMBED_CCOPTS := $(shell $(PYTHON_CONFIG_SQ) --cflags 2>/dev/null)
FLAGS_PYTHON_EMBED := $(PYTHON_EMBED_CCOPTS) $(PYTHON_EMBED_LDOPTS)
ifneq ($(call try-cc,$(SOURCE_PYTHON_EMBED),$(FLAGS_PYTHON_EMBED),python),y)
$(call disable-python,Python.h (for Python 2.x))
else
ifneq ($(call try-cc,$(SOURCE_PYTHON_VERSION),$(FLAGS_PYTHON_EMBED),python version),y)
$(warning Python 3 is not yet supported; please set)
$(warning PYTHON and/or PYTHON_CONFIG appropriately.)
$(warning If you also have Python 2 installed, then)
$(warning try something like:)
$(warning $(and ,))
$(warning $(and ,) make PYTHON=python2)
$(warning $(and ,))
$(warning Otherwise, disable Python support entirely:)
$(warning $(and ,))
$(warning $(and ,) make NO_LIBPYTHON=1)
$(warning $(and ,))
$(error $(and ,))
else
ALL_LDFLAGS += $(PYTHON_EMBED_LDFLAGS)
EXTLIBS += $(PYTHON_EMBED_LIBADD)
LIB_OBJS += $(OUTPUT)util/scripting-engines/trace-event-python.o
LIB_OBJS += $(OUTPUT)scripts/python/Perf-Trace-Util/Context.o
LANG_BINDINGS += $(OUTPUT)python/perf.so
endif
endif
endif
endif
endif
ifdef NO_DEMANGLE
BASIC_CFLAGS += -DNO_DEMANGLE
else
ifdef HAVE_CPLUS_DEMANGLE
EXTLIBS += -liberty
BASIC_CFLAGS += -DHAVE_CPLUS_DEMANGLE
else
FLAGS_BFD=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) -DPACKAGE='perf' -lbfd
has_bfd := $(call try-cc,$(SOURCE_BFD),$(FLAGS_BFD),libbfd)
ifeq ($(has_bfd),y)
EXTLIBS += -lbfd
else
FLAGS_BFD_IBERTY=$(FLAGS_BFD) -liberty
has_bfd_iberty := $(call try-cc,$(SOURCE_BFD),$(FLAGS_BFD_IBERTY),liberty)
ifeq ($(has_bfd_iberty),y)
EXTLIBS += -lbfd -liberty
else
FLAGS_BFD_IBERTY_Z=$(FLAGS_BFD_IBERTY) -lz
has_bfd_iberty_z := $(call try-cc,$(SOURCE_BFD),$(FLAGS_BFD_IBERTY_Z),libz)
ifeq ($(has_bfd_iberty_z),y)
EXTLIBS += -lbfd -liberty -lz
else
FLAGS_CPLUS_DEMANGLE=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) -liberty
has_cplus_demangle := $(call try-cc,$(SOURCE_CPLUS_DEMANGLE),$(FLAGS_CPLUS_DEMANGLE),demangle)
ifeq ($(has_cplus_demangle),y)
EXTLIBS += -liberty
BASIC_CFLAGS += -DHAVE_CPLUS_DEMANGLE
else
msg := $(warning No bfd.h/libbfd found, install binutils-dev[el]/zlib-static to gain symbol demangling)
BASIC_CFLAGS += -DNO_DEMANGLE
endif
endif
endif
endif
endif
endif
ifeq ($(NO_PERF_REGS),0)
ifeq ($(ARCH),x86)
LIB_H += arch/x86/include/perf_regs.h
endif
BASIC_CFLAGS += -DHAVE_PERF_REGS
endif
ifndef NO_STRLCPY
ifeq ($(call try-cc,$(SOURCE_STRLCPY),,-DHAVE_STRLCPY),y)
BASIC_CFLAGS += -DHAVE_STRLCPY
endif
endif
ifndef NO_ON_EXIT
ifeq ($(call try-cc,$(SOURCE_ON_EXIT),,-DHAVE_ON_EXIT),y)
BASIC_CFLAGS += -DHAVE_ON_EXIT
endif
endif
ifndef NO_BACKTRACE
ifeq ($(call try-cc,$(SOURCE_BACKTRACE),,-DBACKTRACE_SUPPORT),y)
BASIC_CFLAGS += -DBACKTRACE_SUPPORT
endif
endif
ifdef ASCIIDOC8
export ASCIIDOC8
endif
# Shell quote (do not use $(call) to accommodate ancient setups);
ETC_PERFCONFIG_SQ = $(subst ','\'',$(ETC_PERFCONFIG))
DESTDIR_SQ = $(subst ','\'',$(DESTDIR))
bindir_SQ = $(subst ','\'',$(bindir))
bindir_relative_SQ = $(subst ','\'',$(bindir_relative))
mandir_SQ = $(subst ','\'',$(mandir))
infodir_SQ = $(subst ','\'',$(infodir))
perfexecdir_SQ = $(subst ','\'',$(perfexecdir))
template_dir_SQ = $(subst ','\'',$(template_dir))
htmldir_SQ = $(subst ','\'',$(htmldir))
prefix_SQ = $(subst ','\'',$(prefix))
sysconfdir_SQ = $(subst ','\'',$(sysconfdir))
SHELL_PATH_SQ = $(subst ','\'',$(SHELL_PATH))
LIBS = -Wl,--whole-archive $(PERFLIBS) -Wl,--no-whole-archive -Wl,--start-group $(EXTLIBS) -Wl,--end-group
ALL_CFLAGS += $(BASIC_CFLAGS)
ALL_CFLAGS += $(ARCH_CFLAGS)
ALL_LDFLAGS += $(BASIC_LDFLAGS)
export INSTALL SHELL_PATH
### Build rules
SHELL = $(SHELL_PATH)
all: shell_compatibility_test $(ALL_PROGRAMS) $(LANG_BINDINGS) $(OTHER_PROGRAMS)
please_set_SHELL_PATH_to_a_more_modern_shell:
@$$(:)
shell_compatibility_test: please_set_SHELL_PATH_to_a_more_modern_shell
strip: $(PROGRAMS) $(OUTPUT)perf
$(STRIP) $(STRIP_OPTS) $(PROGRAMS) $(OUTPUT)perf
$(OUTPUT)perf.o: perf.c $(OUTPUT)common-cmds.h $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -DPERF_VERSION='"$(PERF_VERSION)"' \
'-DPERF_HTML_PATH="$(htmldir_SQ)"' \
$(ALL_CFLAGS) -c $(filter %.c,$^) -o $@
$(OUTPUT)perf: $(OUTPUT)perf.o $(BUILTIN_OBJS) $(PERFLIBS)
$(QUIET_LINK)$(CC) $(ALL_CFLAGS) $(ALL_LDFLAGS) $(OUTPUT)perf.o \
$(BUILTIN_OBJS) $(LIBS) -o $@
$(OUTPUT)builtin-help.o: builtin-help.c $(OUTPUT)common-cmds.h $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) \
'-DPERF_HTML_PATH="$(htmldir_SQ)"' \
'-DPERF_MAN_PATH="$(mandir_SQ)"' \
'-DPERF_INFO_PATH="$(infodir_SQ)"' $<
$(OUTPUT)builtin-timechart.o: builtin-timechart.c $(OUTPUT)common-cmds.h $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) \
'-DPERF_HTML_PATH="$(htmldir_SQ)"' \
'-DPERF_MAN_PATH="$(mandir_SQ)"' \
'-DPERF_INFO_PATH="$(infodir_SQ)"' $<
$(OUTPUT)common-cmds.h: util/generate-cmdlist.sh command-list.txt
$(OUTPUT)common-cmds.h: $(wildcard Documentation/perf-*.txt)
$(QUIET_GEN). util/generate-cmdlist.sh > $@+ && mv $@+ $@
$(SCRIPTS) : % : %.sh
$(QUIET_GEN)$(INSTALL) '$@.sh' '$(OUTPUT)$@'
# These can record PERF_VERSION
$(OUTPUT)perf.o perf.spec \
$(SCRIPTS) \
: $(OUTPUT)PERF-VERSION-FILE
.SUFFIXES:
.SUFFIXES: .o .c .S .s
# These two need to be here so that when O= is not used they take precedence
# over the general rule for .o
$(OUTPUT)util/%-flex.o: $(OUTPUT)util/%-flex.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c -Iutil/ $(ALL_CFLAGS) -w $<
$(OUTPUT)util/%-bison.o: $(OUTPUT)util/%-bison.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c -Iutil/ $(ALL_CFLAGS) -DYYENABLE_NLS=0 -DYYLTYPE_IS_TRIVIAL=0 -w $<
$(OUTPUT)%.o: %.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $<
$(OUTPUT)%.i: %.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -E $(ALL_CFLAGS) $<
$(OUTPUT)%.s: %.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -S $(ALL_CFLAGS) $<
$(OUTPUT)%.o: %.S
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $<
$(OUTPUT)%.s: %.S
$(QUIET_CC)$(CC) -o $@ -E $(ALL_CFLAGS) $<
$(OUTPUT)util/exec_cmd.o: util/exec_cmd.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) \
'-DPERF_EXEC_PATH="$(perfexecdir_SQ)"' \
'-DPREFIX="$(prefix_SQ)"' \
$<
$(OUTPUT)tests/attr.o: tests/attr.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) \
'-DBINDIR="$(bindir_SQ)"' \
$<
$(OUTPUT)util/config.o: util/config.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DETC_PERFCONFIG='"$(ETC_PERFCONFIG_SQ)"' $<
$(OUTPUT)ui/browser.o: ui/browser.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DENABLE_SLFUTURE_CONST $<
$(OUTPUT)ui/browsers/annotate.o: ui/browsers/annotate.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DENABLE_SLFUTURE_CONST $<
$(OUTPUT)ui/browsers/hists.o: ui/browsers/hists.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DENABLE_SLFUTURE_CONST $<
$(OUTPUT)ui/browsers/map.o: ui/browsers/map.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DENABLE_SLFUTURE_CONST $<
$(OUTPUT)ui/browsers/scripts.o: ui/browsers/scripts.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -DENABLE_SLFUTURE_CONST $<
$(OUTPUT)util/rbtree.o: ../../lib/rbtree.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -Wno-unused-parameter -DETC_PERFCONFIG='"$(ETC_PERFCONFIG_SQ)"' $<
$(OUTPUT)util/parse-events.o: util/parse-events.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) -Wno-redundant-decls $<
$(OUTPUT)util/scripting-engines/trace-event-perl.o: util/scripting-engines/trace-event-perl.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $(PERL_EMBED_CCOPTS) -Wno-redundant-decls -Wno-strict-prototypes -Wno-unused-parameter -Wno-shadow $<
$(OUTPUT)scripts/perl/Perf-Trace-Util/Context.o: scripts/perl/Perf-Trace-Util/Context.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $(PERL_EMBED_CCOPTS) -Wno-redundant-decls -Wno-strict-prototypes -Wno-unused-parameter -Wno-nested-externs $<
$(OUTPUT)util/scripting-engines/trace-event-python.o: util/scripting-engines/trace-event-python.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $(PYTHON_EMBED_CCOPTS) -Wno-redundant-decls -Wno-strict-prototypes -Wno-unused-parameter -Wno-shadow $<
$(OUTPUT)scripts/python/Perf-Trace-Util/Context.o: scripts/python/Perf-Trace-Util/Context.c $(OUTPUT)PERF-CFLAGS
$(QUIET_CC)$(CC) -o $@ -c $(ALL_CFLAGS) $(PYTHON_EMBED_CCOPTS) -Wno-redundant-decls -Wno-strict-prototypes -Wno-unused-parameter -Wno-nested-externs $<
$(OUTPUT)perf-%: %.o $(PERFLIBS)
$(QUIET_LINK)$(CC) $(ALL_CFLAGS) -o $@ $(ALL_LDFLAGS) $(filter %.o,$^) $(LIBS)
$(LIB_OBJS) $(BUILTIN_OBJS): $(LIB_H)
$(patsubst perf-%,%.o,$(PROGRAMS)): $(LIB_H) $(wildcard */*.h)
# we compile into subdirectories. if the target directory is not the source directory, they might not exists. So
# we depend the various files onto their directories.
DIRECTORY_DEPS = $(LIB_OBJS) $(BUILTIN_OBJS) $(OUTPUT)PERF-VERSION-FILE $(OUTPUT)common-cmds.h
$(DIRECTORY_DEPS): | $(sort $(dir $(DIRECTORY_DEPS)))
# In the second step, we make a rule to actually create these directories
$(sort $(dir $(DIRECTORY_DEPS))):
$(QUIET_MKDIR)$(MKDIR) -p $@ 2>/dev/null
$(LIB_FILE): $(LIB_OBJS)
$(QUIET_AR)$(RM) $@ && $(AR) rcs $@ $(LIB_OBJS)
# libtraceevent.a
$(LIBTRACEEVENT):
$(QUIET_SUBDIR0)$(TRACE_EVENT_DIR) $(QUIET_SUBDIR1) O=$(OUTPUT) libtraceevent.a
$(LIBTRACEEVENT)-clean:
$(QUIET_SUBDIR0)$(TRACE_EVENT_DIR) $(QUIET_SUBDIR1) O=$(OUTPUT) clean
help:
@echo 'Perf make targets:'
@echo ' doc - make *all* documentation (see below)'
@echo ' man - make manpage documentation (access with man <foo>)'
@echo ' html - make html documentation'
@echo ' info - make GNU info documentation (access with info <foo>)'
@echo ' pdf - make pdf documentation'
@echo ' TAGS - use etags to make tag information for source browsing'
@echo ' tags - use ctags to make tag information for source browsing'
@echo ' cscope - use cscope to make interactive browsing database'
@echo ''
@echo 'Perf install targets:'
@echo ' NOTE: documentation build requires asciidoc, xmlto packages to be installed'
@echo ' HINT: use "make prefix=<path> <install target>" to install to a particular'
@echo ' path like make prefix=/usr/local install install-doc'
@echo ' install - install compiled binaries'
@echo ' install-doc - install *all* documentation'
@echo ' install-man - install manpage documentation'
@echo ' install-html - install html documentation'
@echo ' install-info - install GNU info documentation'
@echo ' install-pdf - install pdf documentation'
@echo ''
@echo ' quick-install-doc - alias for quick-install-man'
@echo ' quick-install-man - install the documentation quickly'
@echo ' quick-install-html - install the html documentation quickly'
@echo ''
@echo 'Perf maintainer targets:'
@echo ' clean - clean all binary objects and build output'
DOC_TARGETS := doc man html info pdf
INSTALL_DOC_TARGETS := $(patsubst %,install-%,$(DOC_TARGETS)) try-install-man
INSTALL_DOC_TARGETS += quick-install-doc quick-install-man quick-install-html
# 'make doc' should call 'make -C Documentation all'
$(DOC_TARGETS):
$(QUIET_SUBDIR0)Documentation $(QUIET_SUBDIR1) $(@:doc=all)
TAGS:
$(RM) TAGS
$(FIND) . -name '*.[hcS]' -print | xargs etags -a
tags:
$(RM) tags
$(FIND) . -name '*.[hcS]' -print | xargs ctags -a
cscope:
$(RM) cscope*
$(FIND) . -name '*.[hcS]' -print | xargs cscope -b
### Detect prefix changes
TRACK_CFLAGS = $(subst ','\'',$(ALL_CFLAGS)):\
$(bindir_SQ):$(perfexecdir_SQ):$(template_dir_SQ):$(prefix_SQ)
$(OUTPUT)PERF-CFLAGS: .FORCE-PERF-CFLAGS
@FLAGS='$(TRACK_CFLAGS)'; \
if test x"$$FLAGS" != x"`cat $(OUTPUT)PERF-CFLAGS 2>/dev/null`" ; then \
echo 1>&2 " * new build flags or prefix"; \
echo "$$FLAGS" >$(OUTPUT)PERF-CFLAGS; \
fi
### Testing rules
# GNU make supports exporting all variables by "export" without parameters.
# However, the environment gets quite big, and some programs have problems
# with that.
check: $(OUTPUT)common-cmds.h
if sparse; \
then \
for i in *.c */*.c; \
do \
sparse $(ALL_CFLAGS) $(SPARSE_FLAGS) $$i || exit; \
done; \
else \
exit 1; \
fi
### Installation rules
ifneq ($(filter /%,$(firstword $(perfexecdir))),)
perfexec_instdir = $(perfexecdir)
else
perfexec_instdir = $(prefix)/$(perfexecdir)
endif
perfexec_instdir_SQ = $(subst ','\'',$(perfexec_instdir))
install: all try-install-man
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(bindir_SQ)'
$(INSTALL) $(OUTPUT)perf '$(DESTDIR_SQ)$(bindir_SQ)'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/perl/Perf-Trace-Util/lib/Perf/Trace'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/perl/bin'
$(INSTALL) $(OUTPUT)perf-archive -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)'
$(INSTALL) scripts/perl/Perf-Trace-Util/lib/Perf/Trace/* -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/perl/Perf-Trace-Util/lib/Perf/Trace'
$(INSTALL) scripts/perl/*.pl -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/perl'
$(INSTALL) scripts/perl/bin/* -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/perl/bin'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/python/Perf-Trace-Util/lib/Perf/Trace'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/python/bin'
$(INSTALL) scripts/python/Perf-Trace-Util/lib/Perf/Trace/* -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/python/Perf-Trace-Util/lib/Perf/Trace'
$(INSTALL) scripts/python/*.py -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/python'
$(INSTALL) scripts/python/bin/* -t '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/scripts/python/bin'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(sysconfdir_SQ)/bash_completion.d'
$(INSTALL) bash_completion '$(DESTDIR_SQ)$(sysconfdir_SQ)/bash_completion.d/perf'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/tests'
$(INSTALL) tests/attr.py '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/tests'
$(INSTALL) -d -m 755 '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/tests/attr'
$(INSTALL) tests/attr/* '$(DESTDIR_SQ)$(perfexec_instdir_SQ)/tests/attr'
install-python_ext:
$(PYTHON_WORD) util/setup.py --quiet install --root='/$(DESTDIR_SQ)'
# 'make install-doc' should call 'make -C Documentation install'
$(INSTALL_DOC_TARGETS):
$(QUIET_SUBDIR0)Documentation $(QUIET_SUBDIR1) $(@:-doc=)
### Cleaning rules
clean: $(LIBTRACEEVENT)-clean
$(RM) $(LIB_OBJS) $(BUILTIN_OBJS) $(LIB_FILE) $(OUTPUT)perf-archive $(OUTPUT)perf.o $(LANG_BINDINGS)
$(RM) $(ALL_PROGRAMS) perf
$(RM) *.spec *.pyc *.pyo */*.pyc */*.pyo $(OUTPUT)common-cmds.h TAGS tags cscope*
$(QUIET_SUBDIR0)Documentation $(QUIET_SUBDIR1) clean
$(RM) $(OUTPUT)PERF-VERSION-FILE $(OUTPUT)PERF-CFLAGS
$(RM) $(OUTPUT)util/*-bison*
$(RM) $(OUTPUT)util/*-flex*
$(python-clean)
.PHONY: all install clean strip $(LIBTRACEEVENT)
.PHONY: shell_compatibility_test please_set_SHELL_PATH_to_a_more_modern_shell
.PHONY: .FORCE-PERF-VERSION-FILE TAGS tags cscope .FORCE-PERF-CFLAGS