aboutsummaryrefslogblamecommitdiffstats
blob: de38a034b129e62b91ad73d2564fe5b5e7617b7f (plain) (tree)





















                                                                             









                        


                      
                         
                           
                        
                       
                         
                               
                              
                             
 
                                                    
                                 


                                  
                         
                       
                        
                       
                           
                        
                        
                     

                                                   
                                
                                     
                           
                             
                                 
         
 
                                                              
                                             
 
                                                                      
                
 
                                                                    



                                                                             
 

                                      
                                                   
                                                 
                                               

                   

 
























                                                                    
                                                              
 
                                      

                  



                                           

                                    



                                           
                                           
         


                               
                



                                           
                                                          
         
                                 
                                     
                  
                   

 

                                                                        
 

                                         
                                              
              
                         

 

                                                                         

                  
                                         


                                                                  



                 
                                                                    
                                                 



















                                                           
                    

                                                                    
 

                    








                                                                        
                                 

                                                             

                   
 
 

                                                                   















                                                                        
      
 

                                                                    








                                                          
                                                                              







                                                                            
 






                                                                                 
                    

                                                             
      
                    
  
                                         
                                          
                                                                    
                                                     
                                                    

                                                                                
                                      
                    
                                                                        
                                    
     
                                                              
      
                                                 

                                                     
                                            
                                                                  
                                                                  
                    
                                              


                                                                      
                                                                    
                                                          


                                                                              
                                     
                                                                          
                                           
                    
                                       
                                                                  
                                                                


                                                                             

                                                                      

                                                             

                                                             


                                                                        
      
                                           

                                                                        

                                                            




                                                                               

                                                                          
                 
          

                
                                                              
                                                           




                                                                       




                                                                     
         
 


                                                     
                                                                         
                                                       

                                                         




                                                                          
                                 
                                        
                                                                                

                                                                 
                                        
                                                                           

                                                                 



                                                                          



                                                                            



                                                                               




                                                                            
         













                                                                            


                                                                           

                                                                        
                                                 




                                                                   
 
                    
                                                   






                                                                          

                                                                 
 
                                                                         


                                                                             
         





                                                                 



                                                                          
                                                                        
                                                                  
                                                        
                                                        
                                                                
                                                 



                                                                            

      
                             
                                                            
                                                



                                                                                

         

                                                                          
                                                                    
                                                          
                                                              




                                                                             

                 
/*
 * builtin-probe.c
 *
 * Builtin probe command: Set up probe events by C expression
 *
 * Written by Masami Hiramatsu <mhiramat@redhat.com>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA.
 *
 */
#include <sys/utsname.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <errno.h>
#include <stdio.h>
#include <unistd.h>
#include <stdlib.h>
#include <string.h>

#include "perf.h"
#include "builtin.h"
#include "util/util.h"
#include "util/strlist.h"
#include "util/strfilter.h"
#include "util/symbol.h"
#include "util/debug.h"
#include "util/debugfs.h"
#include "util/parse-options.h"
#include "util/probe-finder.h"
#include "util/probe-event.h"

#define DEFAULT_VAR_FILTER "!__k???tab_* & !__crc_*"
#define DEFAULT_FUNC_FILTER "!_*"

/* Session management structure */
static struct {
	bool list_events;
	bool force_add;
	bool show_lines;
	bool show_vars;
	bool show_ext_vars;
	bool show_funcs;
	bool mod_events;
	bool uprobes;
	int nevents;
	struct perf_probe_event events[MAX_PROBES];
	struct strlist *dellist;
	struct line_range line_range;
	const char *target;
	int max_probe_points;
	struct strfilter *filter;
} params;

/* Parse an event definition. Note that any error must die. */
static int parse_probe_event(const char *str)
{
	struct perf_probe_event *pev = &params.events[params.nevents];
	int ret;

	pr_debug("probe-definition(%d): %s\n", params.nevents, str);
	if (++params.nevents == MAX_PROBES) {
		pr_err("Too many probes (> %d) were specified.", MAX_PROBES);
		return -1;
	}

	pev->uprobes = params.uprobes;

	/* Parse a perf-probe command into event */
	ret = parse_perf_probe_command(str, pev);
	pr_debug("%d arguments\n", pev->nargs);

	return ret;
}

static int set_target(const char *ptr)
{
	int found = 0;
	const char *buf;

	/*
	 * The first argument after options can be an absolute path
	 * to an executable / library or kernel module.
	 *
	 * TODO: Support relative path, and $PATH, $LD_LIBRARY_PATH,
	 * short module name.
	 */
	if (!params.target && ptr && *ptr == '/') {
		params.target = ptr;
		found = 1;
		buf = ptr + (strlen(ptr) - 3);

		if (strcmp(buf, ".ko"))
			params.uprobes = true;

	}

	return found;
}

static int parse_probe_event_argv(int argc, const char **argv)
{
	int i, len, ret, found_target;
	char *buf;

	found_target = set_target(argv[0]);
	if (found_target && argc == 1)
		return 0;

	/* Bind up rest arguments */
	len = 0;
	for (i = 0; i < argc; i++) {
		if (i == 0 && found_target)
			continue;

		len += strlen(argv[i]) + 1;
	}
	buf = zalloc(len + 1);
	if (buf == NULL)
		return -ENOMEM;
	len = 0;
	for (i = 0; i < argc; i++) {
		if (i == 0 && found_target)
			continue;

		len += sprintf(&buf[len], "%s ", argv[i]);
	}
	params.mod_events = true;
	ret = parse_probe_event(buf);
	free(buf);
	return ret;
}

static int opt_add_probe_event(const struct option *opt __maybe_unused,
			      const char *str, int unset __maybe_unused)
{
	if (str) {
		params.mod_events = true;
		return parse_probe_event(str);
	} else
		return 0;
}

static int opt_del_probe_event(const struct option *opt __maybe_unused,
			       const char *str, int unset __maybe_unused)
{
	if (str) {
		params.mod_events = true;
		if (!params.dellist)
			params.dellist = strlist__new(true, NULL);
		strlist__add(params.dellist, str);
	}
	return 0;
}

static int opt_set_target(const struct option *opt, const char *str,
			int unset __maybe_unused)
{
	int ret = -ENOENT;

	if  (str && !params.target) {
		if (!strcmp(opt->long_name, "exec"))
			params.uprobes = true;
#ifdef DWARF_SUPPORT
		else if (!strcmp(opt->long_name, "module"))
			params.uprobes = false;
#endif
		else
			return ret;

		params.target = str;
		ret = 0;
	}

	return ret;
}

#ifdef DWARF_SUPPORT
static int opt_show_lines(const struct option *opt __maybe_unused,
			  const char *str, int unset __maybe_unused)
{
	int ret = 0;

	if (!str)
		return 0;

	if (params.show_lines) {
		pr_warning("Warning: more than one --line options are"
			   " detected. Only the first one is valid.\n");
		return 0;
	}

	params.show_lines = true;
	ret = parse_line_range_desc(str, &params.line_range);
	INIT_LIST_HEAD(&params.line_range.line_list);

	return ret;
}

static int opt_show_vars(const struct option *opt __maybe_unused,
			 const char *str, int unset __maybe_unused)
{
	struct perf_probe_event *pev = &params.events[params.nevents];
	int ret;

	if (!str)
		return 0;

	ret = parse_probe_event(str);
	if (!ret && pev->nargs != 0) {
		pr_err("  Error: '--vars' doesn't accept arguments.\n");
		return -EINVAL;
	}
	params.show_vars = true;

	return ret;
}
#endif

static int opt_set_filter(const struct option *opt __maybe_unused,
			  const char *str, int unset __maybe_unused)
{
	const char *err;

	if (str) {
		pr_debug2("Set filter: %s\n", str);
		if (params.filter)
			strfilter__delete(params.filter);
		params.filter = strfilter__new(str, &err);
		if (!params.filter) {
			pr_err("Filter parse error at %td.\n", err - str + 1);
			pr_err("Source: \"%s\"\n", str);
			pr_err("         %*c\n", (int)(err - str + 1), '^');
			return -EINVAL;
		}
	}

	return 0;
}

int cmd_probe(int argc, const char **argv, const char *prefix __maybe_unused)
{
	const char * const probe_usage[] = {
		"perf probe [<options>] 'PROBEDEF' ['PROBEDEF' ...]",
		"perf probe [<options>] --add 'PROBEDEF' [--add 'PROBEDEF' ...]",
		"perf probe [<options>] --del '[GROUP:]EVENT' ...",
		"perf probe --list",
#ifdef DWARF_SUPPORT
		"perf probe [<options>] --line 'LINEDESC'",
		"perf probe [<options>] --vars 'PROBEPOINT'",
#endif
		NULL
};
	const struct option options[] = {
	OPT_INCR('v', "verbose", &verbose,
		    "be more verbose (show parsed arguments, etc)"),
	OPT_BOOLEAN('l', "list", &params.list_events,
		    "list up current probe events"),
	OPT_CALLBACK('d', "del", NULL, "[GROUP:]EVENT", "delete a probe event.",
		opt_del_probe_event),
	OPT_CALLBACK('a', "add", NULL,
#ifdef DWARF_SUPPORT
		"[EVENT=]FUNC[@SRC][+OFF|%return|:RL|;PT]|SRC:AL|SRC;PT"
		" [[NAME=]ARG ...]",
#else
		"[EVENT=]FUNC[+OFF|%return] [[NAME=]ARG ...]",
#endif
		"probe point definition, where\n"
		"\t\tGROUP:\tGroup name (optional)\n"
		"\t\tEVENT:\tEvent name\n"
		"\t\tFUNC:\tFunction name\n"
		"\t\tOFF:\tOffset from function entry (in byte)\n"
		"\t\t%return:\tPut the probe at function return\n"
#ifdef DWARF_SUPPORT
		"\t\tSRC:\tSource code path\n"
		"\t\tRL:\tRelative line number from function entry.\n"
		"\t\tAL:\tAbsolute line number in file.\n"
		"\t\tPT:\tLazy expression of line code.\n"
		"\t\tARG:\tProbe argument (local variable name or\n"
		"\t\t\tkprobe-tracer argument format.)\n",
#else
		"\t\tARG:\tProbe argument (kprobe-tracer argument format.)\n",
#endif
		opt_add_probe_event),
	OPT_BOOLEAN('f', "force", &params.force_add, "forcibly add events"
		    " with existing name"),
#ifdef DWARF_SUPPORT
	OPT_CALLBACK('L', "line", NULL,
		     "FUNC[:RLN[+NUM|-RLN2]]|SRC:ALN[+NUM|-ALN2]",
		     "Show source code lines.", opt_show_lines),
	OPT_CALLBACK('V', "vars", NULL,
		     "FUNC[@SRC][+OFF|%return|:RL|;PT]|SRC:AL|SRC;PT",
		     "Show accessible variables on PROBEDEF", opt_show_vars),
	OPT_BOOLEAN('\0', "externs", &params.show_ext_vars,
		    "Show external variables too (with --vars only)"),
	OPT_STRING('k', "vmlinux", &symbol_conf.vmlinux_name,
		   "file", "vmlinux pathname"),
	OPT_STRING('s', "source", &symbol_conf.source_prefix,
		   "directory", "path to kernel source"),
	OPT_CALLBACK('m', "module", NULL, "modname|path",
		"target module name (for online) or path (for offline)",
		opt_set_target),
#endif
	OPT__DRY_RUN(&probe_event_dry_run),
	OPT_INTEGER('\0', "max-probes", &params.max_probe_points,
		 "Set how many probe points can be found for a probe."),
	OPT_BOOLEAN('F', "funcs", &params.show_funcs,
		    "Show potential probe-able functions."),
	OPT_CALLBACK('\0', "filter", NULL,
		     "[!]FILTER", "Set a filter (with --vars/funcs only)\n"
		     "\t\t\t(default: \"" DEFAULT_VAR_FILTER "\" for --vars,\n"
		     "\t\t\t \"" DEFAULT_FUNC_FILTER "\" for --funcs)",
		     opt_set_filter),
	OPT_CALLBACK('x', "exec", NULL, "executable|path",
			"target executable name or path", opt_set_target),
	OPT_END()
	};
	int ret;

	argc = parse_options(argc, argv, options, probe_usage,
			     PARSE_OPT_STOP_AT_NON_OPTION);
	if (argc > 0) {
		if (strcmp(argv[0], "-") == 0) {
			pr_warning("  Error: '-' is not supported.\n");
			usage_with_options(probe_usage, options);
		}
		ret = parse_probe_event_argv(argc, argv);
		if (ret < 0) {
			pr_err("  Error: Parse Error.  (%d)\n", ret);
			return ret;
		}
	}

	if (params.max_probe_points == 0)
		params.max_probe_points = MAX_PROBES;

	if ((!params.nevents && !params.dellist && !params.list_events &&
	     !params.show_lines && !params.show_funcs))
		usage_with_options(probe_usage, options);

	/*
	 * Only consider the user's kernel image path if given.
	 */
	symbol_conf.try_vmlinux_path = (symbol_conf.vmlinux_name == NULL);

	if (params.list_events) {
		if (params.mod_events) {
			pr_err("  Error: Don't use --list with --add/--del.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_lines) {
			pr_err("  Error: Don't use --list with --line.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_vars) {
			pr_err(" Error: Don't use --list with --vars.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_funcs) {
			pr_err("  Error: Don't use --list with --funcs.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.uprobes) {
			pr_warning("  Error: Don't use --list with --exec.\n");
			usage_with_options(probe_usage, options);
		}
		ret = show_perf_probe_events();
		if (ret < 0)
			pr_err("  Error: Failed to show event list. (%d)\n",
			       ret);
		return ret;
	}
	if (params.show_funcs) {
		if (params.nevents != 0 || params.dellist) {
			pr_err("  Error: Don't use --funcs with"
			       " --add/--del.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_lines) {
			pr_err("  Error: Don't use --funcs with --line.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_vars) {
			pr_err("  Error: Don't use --funcs with --vars.\n");
			usage_with_options(probe_usage, options);
		}
		if (!params.filter)
			params.filter = strfilter__new(DEFAULT_FUNC_FILTER,
						       NULL);
		ret = show_available_funcs(params.target, params.filter,
					params.uprobes);
		strfilter__delete(params.filter);
		if (ret < 0)
			pr_err("  Error: Failed to show functions."
			       " (%d)\n", ret);
		return ret;
	}

#ifdef DWARF_SUPPORT
	if (params.show_lines && !params.uprobes) {
		if (params.mod_events) {
			pr_err("  Error: Don't use --line with"
			       " --add/--del.\n");
			usage_with_options(probe_usage, options);
		}
		if (params.show_vars) {
			pr_err(" Error: Don't use --line with --vars.\n");
			usage_with_options(probe_usage, options);
		}

		ret = show_line_range(&params.line_range, params.target);
		if (ret < 0)
			pr_err("  Error: Failed to show lines. (%d)\n", ret);
		return ret;
	}
	if (params.show_vars) {
		if (params.mod_events) {
			pr_err("  Error: Don't use --vars with"
			       " --add/--del.\n");
			usage_with_options(probe_usage, options);
		}
		if (!params.filter)
			params.filter = strfilter__new(DEFAULT_VAR_FILTER,
						       NULL);

		ret = show_available_vars(params.events, params.nevents,
					  params.max_probe_points,
					  params.target,
					  params.filter,
					  params.show_ext_vars);
		strfilter__delete(params.filter);
		if (ret < 0)
			pr_err("  Error: Failed to show vars. (%d)\n", ret);
		return ret;
	}
#endif

	if (params.dellist) {
		ret = del_perf_probe_events(params.dellist);
		strlist__delete(params.dellist);
		if (ret < 0) {
			pr_err("  Error: Failed to delete events. (%d)\n", ret);
			return ret;
		}
	}

	if (params.nevents) {
		ret = add_perf_probe_events(params.events, params.nevents,
					    params.max_probe_points,
					    params.target,
					    params.force_add);
		if (ret < 0) {
			pr_err("  Error: Failed to add events. (%d)\n", ret);
			return ret;
		}
	}
	return 0;
}