#ifndef LINUX_VIRTIO_H
#define LINUX_VIRTIO_H
#include <stdbool.h>
#include <stdlib.h>
#include <stddef.h>
#include <stdio.h>
#include <string.h>
#include <assert.h>
#include <linux/types.h>
#include <errno.h>
typedef unsigned long long dma_addr_t;
struct scatterlist {
unsigned long page_link;
unsigned int offset;
unsigned int length;
dma_addr_t dma_address;
};
struct page {
unsigned long long dummy;
};
#define BUG_ON(__BUG_ON_cond) assert(!(__BUG_ON_cond))
/* Physical == Virtual */
#define virt_to_phys(p) ((unsigned long)p)
#define phys_to_virt(a) ((void *)(unsigned long)(a))
/* Page address: Virtual / 4K */
#define virt_to_page(p) ((struct page*)((virt_to_phys(p) / 4096) * \
sizeof(struct page)))
#define offset_in_page(p) (((unsigned long)p) % 4096)
#define sg_phys(sg) ((sg->page_link & ~0x3) / sizeof(struct page) * 4096 + \
sg->offset)
static inline void sg_mark_end(struct scatterlist *sg)
{
/*
* Set termination bit, clear potential chain bit
*/
sg->page_link |= 0x02;
sg->page_link &= ~0x01;
}
static inline void sg_init_table(struct scatterlist *sgl, unsigned int nents)
{
memset(sgl, 0, sizeof(*sgl) * nents);
sg_mark_end(&sgl[nents - 1]);
}
static inline void sg_assign_page(struct scatterlist *sg, struct page *page)
{
unsigned long page_link = sg->page_link & 0x3;
/*
* In order for the low bit stealing approach to work, pages
* must be aligned at a 32-bit boundary as a minimum.
*/
BUG_ON((unsigned long) page & 0x03);
sg->page_link = page_link | (unsigned long) page;
}
static inline void sg_set_page(struct scatterlist *sg, struct page *page,
unsigned int len, unsigned int offset)
{
sg_assign_page(sg, page);
sg->offset = offset;
sg->length = len;
}
static inline void sg_set_buf(struct scatterlist *sg, const void *buf,
unsigned int buflen)
{
sg_set_page(sg, virt_to_page(buf), buflen, offset_in_page(buf));
}
static inline void sg_init_one(struct scatterlist *sg, const void *buf, unsigned int buflen)
{
sg_init_table(sg, 1);
sg_set_buf(sg, buf, buflen);
}
typedef __u16 u16;
typedef enum {
GFP_KERNEL,
GFP_ATOMIC,
} gfp_t;
typedef enum {
IRQ_NONE,
IRQ_HANDLED
} irqreturn_t;
static inline void *kmalloc(size_t s, gfp_t gfp)
{
return malloc(s);
}
static inline void kfree(void *p)
{
free(p);
}
#define container_of(ptr, type, member) ({ \
const typeof( ((type *)0)->member ) *__mptr = (ptr); \
(type *)( (char *)__mptr - offsetof(type,member) );})
#define uninitialized_var(x) x = x
# ifndef likely
# define likely(x) (__builtin_expect(!!(x), 1))
# endif
# ifndef unlikely
# define unlikely(x) (__builtin_expect(!!(x), 0))
# endif
#define pr_err(format, ...) fprintf (stderr, format, ## __VA_ARGS__)
#ifdef DEBUG
#define pr_debug(format, ...) fprintf (stderr, format, ## __VA_ARGS__)
#else
#define pr_debug(format, ...) do {} while (0)
#endif
#define dev_err(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__)
#define dev_warn(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__)
/* TODO: empty stubs for now. Broken but enough for virtio_ring.c */
#define list_add_tail(a, b) do {} while (0)
#define list_del(a) do {} while (0)
#define BIT_WORD(nr) ((nr) / BITS_PER_LONG)
#define BITS_PER_BYTE 8
#define BITS_PER_LONG (sizeof(long) * BITS_PER_BYTE)
#define BIT_MASK(nr) (1UL << ((nr) % BITS_PER_LONG))
/* TODO: Not atomic as it should be:
* we don't use this for anything important. */
static inline void clear_bit(int nr, volatile unsigned long *addr)
{
unsigned long mask = BIT_MASK(nr);
unsigned long *p = ((unsigned long *)addr) + BIT_WORD(nr);
*p &= ~mask;
}
static inline int test_bit(int nr, const volatile unsigned long *addr)
{
return 1UL & (addr[BIT_WORD(nr)] >> (nr & (BITS_PER_LONG-1)));
}
/* The only feature we care to support */
#define virtio_has_feature(dev, feature) \
test_bit((feature), (dev)->features)
/* end of stubs */
struct virtio_device {
void *dev;
unsigned long features[1];
};
struct virtqueue {
/* TODO: commented as list macros are empty stubs for now.
* Broken but enough for virtio_ring.c
* struct list_head list; */
void (*callback)(struct virtqueue *vq);
const char *name;
struct virtio_device *vdev;
void *priv;
};
#define EXPORT_SYMBOL_GPL(__EXPORT_SYMBOL_GPL_name) \
void __EXPORT_SYMBOL_GPL##__EXPORT_SYMBOL_GPL_name() { \
}
#define MODULE_LICENSE(__MODULE_LICENSE_value) \
const char *__MODULE_LICENSE_name = __MODULE_LICENSE_value
#define CONFIG_SMP
#if defined(__i386__) || defined(__x86_64__)
#define barrier() asm volatile("" ::: "memory")
#define mb() __sync_synchronize()
#define smp_mb() mb()
# define smp_rmb() barrier()
# define smp_wmb() barrier()
#else
#error Please fill in barrier macros
#endif
/* Interfaces exported by virtio_ring. */
int virtqueue_add_buf_gfp(struct virtqueue *vq,
struct scatterlist sg[],
unsigned int out_num,
unsigned int in_num,
void *data,
gfp_t gfp);
static inline int virtqueue_add_buf(struct virtqueue *vq,
struct scatterlist sg[],
unsigned int out_num,
unsigned int in_num,
void *data)
{
return virtqueue_add_buf_gfp(vq, sg, out_num, in_num, data, GFP_ATOMIC);
}
void virtqueue_kick(struct virtqueue *vq);
void *virtqueue_get_buf(struct virtqueue *vq, unsigned int *len);
void virtqueue_disable_cb(struct virtqueue *vq);
bool virtqueue_enable_cb(struct virtqueue *vq);
void *virtqueue_detach_unused_buf(struct virtqueue *vq);
struct virtqueue *vring_new_virtqueue(unsigned int num,
unsigned int vring_align,
struct virtio_device *vdev,
bool weak_barriers,
void *pages,
void (*notify)(struct virtqueue *vq),
void (*callback)(struct virtqueue *vq),
const char *name);
void vring_del_virtqueue(struct virtqueue *vq);
#endif