diff options
author | Mikulas Patocka | 2018-01-02 13:01:34 -0600 |
---|---|---|
committer | Greg Kroah-Hartman | 2018-02-16 13:09:46 -0600 |
commit | f6d7ea7a180177fcf5c0aabb45dc8e2503a5fd9e (patch) | |
tree | 94632ffc2ac328f9d9bd304b75cebe16e2d01b9e | |
parent | fbc1425f4544371b5fe20b9a93f73b85c08dfe29 (diff) | |
download | kernel-omap-f6d7ea7a180177fcf5c0aabb45dc8e2503a5fd9e.tar.gz kernel-omap-f6d7ea7a180177fcf5c0aabb45dc8e2503a5fd9e.tar.xz kernel-omap-f6d7ea7a180177fcf5c0aabb45dc8e2503a5fd9e.zip |
alpha: fix crash if pthread_create races with signal delivery
commit 21ffceda1c8b3807615c40d440d7815e0c85d366 upstream.
On alpha, a process will crash if it attempts to start a thread and a
signal is delivered at the same time. The crash can be reproduced with
this program: https://cygwin.com/ml/cygwin/2014-11/msg00473.html
The reason for the crash is this:
* we call the clone syscall
* we go to the function copy_process
* copy process calls copy_thread_tls, it is a wrapper around copy_thread
* copy_thread sets the tls pointer: childti->pcb.unique = regs->r20
* copy_thread sets regs->r20 to zero
* we go back to copy_process
* copy process checks "if (signal_pending(current))" and returns
-ERESTARTNOINTR
* the clone syscall is restarted, but this time, regs->r20 is zero, so
the new thread is created with zero tls pointer
* the new thread crashes in start_thread when attempting to access tls
The comment in the code says that setting the register r20 is some
compatibility with OSF/1. But OSF/1 doesn't use the CLONE_SETTLS flag, so
we don't have to zero r20 if CLONE_SETTLS is set. This patch fixes the bug
by zeroing regs->r20 only if CLONE_SETTLS is not set.
Signed-off-by: Mikulas Patocka <mpatocka@redhat.com>
Signed-off-by: Matt Turner <mattst88@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
-rw-r--r-- | arch/alpha/kernel/process.c | 3 |
1 files changed, 2 insertions, 1 deletions
diff --git a/arch/alpha/kernel/process.c b/arch/alpha/kernel/process.c index 84d13263ce46..8095fb2c5c94 100644 --- a/arch/alpha/kernel/process.c +++ b/arch/alpha/kernel/process.c | |||
@@ -273,12 +273,13 @@ copy_thread(unsigned long clone_flags, unsigned long usp, | |||
273 | application calling fork. */ | 273 | application calling fork. */ |
274 | if (clone_flags & CLONE_SETTLS) | 274 | if (clone_flags & CLONE_SETTLS) |
275 | childti->pcb.unique = regs->r20; | 275 | childti->pcb.unique = regs->r20; |
276 | else | ||
277 | regs->r20 = 0; /* OSF/1 has some strange fork() semantics. */ | ||
276 | childti->pcb.usp = usp ?: rdusp(); | 278 | childti->pcb.usp = usp ?: rdusp(); |
277 | *childregs = *regs; | 279 | *childregs = *regs; |
278 | childregs->r0 = 0; | 280 | childregs->r0 = 0; |
279 | childregs->r19 = 0; | 281 | childregs->r19 = 0; |
280 | childregs->r20 = 1; /* OSF/1 has some strange fork() semantics. */ | 282 | childregs->r20 = 1; /* OSF/1 has some strange fork() semantics. */ |
281 | regs->r20 = 0; | ||
282 | stack = ((struct switch_stack *) regs) - 1; | 283 | stack = ((struct switch_stack *) regs) - 1; |
283 | *childstack = *stack; | 284 | *childstack = *stack; |
284 | childstack->r26 = (unsigned long) ret_from_fork; | 285 | childstack->r26 = (unsigned long) ret_from_fork; |