aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorJosh Boyer2012-10-30 12:38:05 -0500
committerLen Brown2012-11-30 00:09:45 -0600
commit55f1f545f709a6023371848028a3029118855576 (patch)
tree5331928fe5745ff09cbfaa41fccf48f137965e43
parentee0778a3015370779f603d2b6119a6ec2b1c811a (diff)
downloadkernel-omap-55f1f545f709a6023371848028a3029118855576.tar.gz
kernel-omap-55f1f545f709a6023371848028a3029118855576.tar.xz
kernel-omap-55f1f545f709a6023371848028a3029118855576.zip
tools: Allow tools to be installed in a user specified location
When building x86_energy_perf_policy or turbostat within the confines of a packaging system such as RPM, we need to be able to have it install to the buildroot and not the root filesystem of the build machine. This adds a DESTDIR variable that when set will act as a prefix for the install location of these tools. Signed-off-by: Josh Boyer <jwboyer@redhat.com> Signed-off-by: Len Brown <len.brown@intel.com>
-rw-r--r--tools/power/x86/x86_energy_perf_policy/Makefile6
1 files changed, 4 insertions, 2 deletions
diff --git a/tools/power/x86/x86_energy_perf_policy/Makefile b/tools/power/x86/x86_energy_perf_policy/Makefile
index f458237fdd79..971c9ffdcb50 100644
--- a/tools/power/x86/x86_energy_perf_policy/Makefile
+++ b/tools/power/x86/x86_energy_perf_policy/Makefile
@@ -1,8 +1,10 @@
1DESTDIR ?=
2
1x86_energy_perf_policy : x86_energy_perf_policy.c 3x86_energy_perf_policy : x86_energy_perf_policy.c
2 4
3clean : 5clean :
4 rm -f x86_energy_perf_policy 6 rm -f x86_energy_perf_policy
5 7
6install : 8install :
7 install x86_energy_perf_policy /usr/bin/ 9 install x86_energy_perf_policy ${DESTDIR}/usr/bin/
8 install x86_energy_perf_policy.8 /usr/share/man/man8/ 10 install x86_energy_perf_policy.8 ${DESTDIR}/usr/share/man/man8/