diff options
author | Rusty Russell | 2012-01-11 23:14:42 -0600 |
---|---|---|
committer | Rusty Russell | 2012-01-11 23:14:42 -0600 |
commit | 7b21e34fd1c272e3a8c3846168f2f6287a4cd72b (patch) | |
tree | 0f94c9f834f5b7cd8ba87168df892ed17b09cb8f | |
parent | e343a895a9f342f239c5e3c5ffc6c0b1707e6244 (diff) | |
download | kernel-omap-7b21e34fd1c272e3a8c3846168f2f6287a4cd72b.tar.gz kernel-omap-7b21e34fd1c272e3a8c3846168f2f6287a4cd72b.tar.xz kernel-omap-7b21e34fd1c272e3a8c3846168f2f6287a4cd72b.zip |
virtio: harsher barriers for rpmsg.
We were cheating with our barriers; using the smp ones rather than the
real device ones. That was fine, until rpmsg came along, which is
used to talk to a real device (a non-SMP CPU).
Unfortunately, just putting back the real barriers (reverting
d57ed95d) causes a performance regression on virtio-pci. In
particular, Amos reports netbench's TCP_RR over virtio_net CPU
utilization increased up to 35% while throughput went down by up to
14%.
By comparison, this branch is in the noise.
Reference: https://lkml.org/lkml/2011/12/11/22
Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
-rw-r--r-- | drivers/lguest/lguest_device.c | 8 | ||||
-rw-r--r-- | drivers/s390/kvm/kvm_virtio.c | 2 | ||||
-rw-r--r-- | drivers/virtio/virtio_mmio.c | 4 | ||||
-rw-r--r-- | drivers/virtio/virtio_pci.c | 4 | ||||
-rw-r--r-- | drivers/virtio/virtio_ring.c | 34 | ||||
-rw-r--r-- | include/linux/virtio_ring.h | 1 | ||||
-rw-r--r-- | tools/virtio/linux/virtio.h | 1 | ||||
-rw-r--r-- | tools/virtio/virtio_test.c | 3 |
8 files changed, 35 insertions, 22 deletions
diff --git a/drivers/lguest/lguest_device.c b/drivers/lguest/lguest_device.c index 595d73197016..6a1d6447b864 100644 --- a/drivers/lguest/lguest_device.c +++ b/drivers/lguest/lguest_device.c | |||
@@ -292,10 +292,12 @@ static struct virtqueue *lg_find_vq(struct virtio_device *vdev, | |||
292 | 292 | ||
293 | /* | 293 | /* |
294 | * OK, tell virtio_ring.c to set up a virtqueue now we know its size | 294 | * OK, tell virtio_ring.c to set up a virtqueue now we know its size |
295 | * and we've got a pointer to its pages. | 295 | * and we've got a pointer to its pages. Note that we set weak_barriers |
296 | * to 'true': the host just a(nother) SMP CPU, so we only need inter-cpu | ||
297 | * barriers. | ||
296 | */ | 298 | */ |
297 | vq = vring_new_virtqueue(lvq->config.num, LGUEST_VRING_ALIGN, | 299 | vq = vring_new_virtqueue(lvq->config.num, LGUEST_VRING_ALIGN, vdev, |
298 | vdev, lvq->pages, lg_notify, callback, name); | 300 | true, lvq->pages, lg_notify, callback, name); |
299 | if (!vq) { | 301 | if (!vq) { |
300 | err = -ENOMEM; | 302 | err = -ENOMEM; |
301 | goto unmap; | 303 | goto unmap; |
diff --git a/drivers/s390/kvm/kvm_virtio.c b/drivers/s390/kvm/kvm_virtio.c index 8af868bab20b..7bc1955337ea 100644 --- a/drivers/s390/kvm/kvm_virtio.c +++ b/drivers/s390/kvm/kvm_virtio.c | |||
@@ -198,7 +198,7 @@ static struct virtqueue *kvm_find_vq(struct virtio_device *vdev, | |||
198 | goto out; | 198 | goto out; |
199 | 199 | ||
200 | vq = vring_new_virtqueue(config->num, KVM_S390_VIRTIO_RING_ALIGN, | 200 | vq = vring_new_virtqueue(config->num, KVM_S390_VIRTIO_RING_ALIGN, |
201 | vdev, (void *) config->address, | 201 | vdev, true, (void *) config->address, |
202 | kvm_notify, callback, name); | 202 | kvm_notify, callback, name); |
203 | if (!vq) { | 203 | if (!vq) { |
204 | err = -ENOMEM; | 204 | err = -ENOMEM; |
diff --git a/drivers/virtio/virtio_mmio.c b/drivers/virtio/virtio_mmio.c index 0269717436af..01d6dc250d5c 100644 --- a/drivers/virtio/virtio_mmio.c +++ b/drivers/virtio/virtio_mmio.c | |||
@@ -310,8 +310,8 @@ static struct virtqueue *vm_setup_vq(struct virtio_device *vdev, unsigned index, | |||
310 | vm_dev->base + VIRTIO_MMIO_QUEUE_PFN); | 310 | vm_dev->base + VIRTIO_MMIO_QUEUE_PFN); |
311 | 311 | ||
312 | /* Create the vring */ | 312 | /* Create the vring */ |
313 | vq = vring_new_virtqueue(info->num, VIRTIO_MMIO_VRING_ALIGN, | 313 | vq = vring_new_virtqueue(info->num, VIRTIO_MMIO_VRING_ALIGN, vdev, |
314 | vdev, info->queue, vm_notify, callback, name); | 314 | true, info->queue, vm_notify, callback, name); |
315 | if (!vq) { | 315 | if (!vq) { |
316 | err = -ENOMEM; | 316 | err = -ENOMEM; |
317 | goto error_new_virtqueue; | 317 | goto error_new_virtqueue; |
diff --git a/drivers/virtio/virtio_pci.c b/drivers/virtio/virtio_pci.c index baabb7937ec2..688b42d28dad 100644 --- a/drivers/virtio/virtio_pci.c +++ b/drivers/virtio/virtio_pci.c | |||
@@ -414,8 +414,8 @@ static struct virtqueue *setup_vq(struct virtio_device *vdev, unsigned index, | |||
414 | vp_dev->ioaddr + VIRTIO_PCI_QUEUE_PFN); | 414 | vp_dev->ioaddr + VIRTIO_PCI_QUEUE_PFN); |
415 | 415 | ||
416 | /* create the vring */ | 416 | /* create the vring */ |
417 | vq = vring_new_virtqueue(info->num, VIRTIO_PCI_VRING_ALIGN, | 417 | vq = vring_new_virtqueue(info->num, VIRTIO_PCI_VRING_ALIGN, vdev, |
418 | vdev, info->queue, vp_notify, callback, name); | 418 | true, info->queue, vp_notify, callback, name); |
419 | if (!vq) { | 419 | if (!vq) { |
420 | err = -ENOMEM; | 420 | err = -ENOMEM; |
421 | goto out_activate_queue; | 421 | goto out_activate_queue; |
diff --git a/drivers/virtio/virtio_ring.c b/drivers/virtio/virtio_ring.c index c7a2c208f6ea..50da92046092 100644 --- a/drivers/virtio/virtio_ring.c +++ b/drivers/virtio/virtio_ring.c | |||
@@ -28,17 +28,20 @@ | |||
28 | #ifdef CONFIG_SMP | 28 | #ifdef CONFIG_SMP |
29 | /* Where possible, use SMP barriers which are more lightweight than mandatory | 29 | /* Where possible, use SMP barriers which are more lightweight than mandatory |
30 | * barriers, because mandatory barriers control MMIO effects on accesses | 30 | * barriers, because mandatory barriers control MMIO effects on accesses |
31 | * through relaxed memory I/O windows (which virtio does not use). */ | 31 | * through relaxed memory I/O windows (which virtio-pci does not use). */ |
32 | #define virtio_mb() smp_mb() | 32 | #define virtio_mb(vq) \ |
33 | #define virtio_rmb() smp_rmb() | 33 | do { if ((vq)->weak_barriers) smp_mb(); else mb(); } while(0) |
34 | #define virtio_wmb() smp_wmb() | 34 | #define virtio_rmb(vq) \ |
35 | do { if ((vq)->weak_barriers) smp_rmb(); else rmb(); } while(0) | ||
36 | #define virtio_wmb(vq) \ | ||
37 | do { if ((vq)->weak_barriers) smp_rmb(); else rmb(); } while(0) | ||
35 | #else | 38 | #else |
36 | /* We must force memory ordering even if guest is UP since host could be | 39 | /* We must force memory ordering even if guest is UP since host could be |
37 | * running on another CPU, but SMP barriers are defined to barrier() in that | 40 | * running on another CPU, but SMP barriers are defined to barrier() in that |
38 | * configuration. So fall back to mandatory barriers instead. */ | 41 | * configuration. So fall back to mandatory barriers instead. */ |
39 | #define virtio_mb() mb() | 42 | #define virtio_mb(vq) mb() |
40 | #define virtio_rmb() rmb() | 43 | #define virtio_rmb(vq) rmb() |
41 | #define virtio_wmb() wmb() | 44 | #define virtio_wmb(vq) wmb() |
42 | #endif | 45 | #endif |
43 | 46 | ||
44 | #ifdef DEBUG | 47 | #ifdef DEBUG |
@@ -77,6 +80,9 @@ struct vring_virtqueue | |||
77 | /* Actual memory layout for this queue */ | 80 | /* Actual memory layout for this queue */ |
78 | struct vring vring; | 81 | struct vring vring; |
79 | 82 | ||
83 | /* Can we use weak barriers? */ | ||
84 | bool weak_barriers; | ||
85 | |||
80 | /* Other side has made a mess, don't try any more. */ | 86 | /* Other side has made a mess, don't try any more. */ |
81 | bool broken; | 87 | bool broken; |
82 | 88 | ||
@@ -245,14 +251,14 @@ void virtqueue_kick(struct virtqueue *_vq) | |||
245 | START_USE(vq); | 251 | START_USE(vq); |
246 | /* Descriptors and available array need to be set before we expose the | 252 | /* Descriptors and available array need to be set before we expose the |
247 | * new available array entries. */ | 253 | * new available array entries. */ |
248 | virtio_wmb(); | 254 | virtio_wmb(vq); |
249 | 255 | ||
250 | old = vq->vring.avail->idx; | 256 | old = vq->vring.avail->idx; |
251 | new = vq->vring.avail->idx = old + vq->num_added; | 257 | new = vq->vring.avail->idx = old + vq->num_added; |
252 | vq->num_added = 0; | 258 | vq->num_added = 0; |
253 | 259 | ||
254 | /* Need to update avail index before checking if we should notify */ | 260 | /* Need to update avail index before checking if we should notify */ |
255 | virtio_mb(); | 261 | virtio_mb(vq); |
256 | 262 | ||
257 | if (vq->event ? | 263 | if (vq->event ? |
258 | vring_need_event(vring_avail_event(&vq->vring), new, old) : | 264 | vring_need_event(vring_avail_event(&vq->vring), new, old) : |
@@ -314,7 +320,7 @@ void *virtqueue_get_buf(struct virtqueue *_vq, unsigned int *len) | |||
314 | } | 320 | } |
315 | 321 | ||
316 | /* Only get used array entries after they have been exposed by host. */ | 322 | /* Only get used array entries after they have been exposed by host. */ |
317 | virtio_rmb(); | 323 | virtio_rmb(vq); |
318 | 324 | ||
319 | i = vq->vring.used->ring[vq->last_used_idx%vq->vring.num].id; | 325 | i = vq->vring.used->ring[vq->last_used_idx%vq->vring.num].id; |
320 | *len = vq->vring.used->ring[vq->last_used_idx%vq->vring.num].len; | 326 | *len = vq->vring.used->ring[vq->last_used_idx%vq->vring.num].len; |
@@ -337,7 +343,7 @@ void *virtqueue_get_buf(struct virtqueue *_vq, unsigned int *len) | |||
337 | * the read in the next get_buf call. */ | 343 | * the read in the next get_buf call. */ |
338 | if (!(vq->vring.avail->flags & VRING_AVAIL_F_NO_INTERRUPT)) { | 344 | if (!(vq->vring.avail->flags & VRING_AVAIL_F_NO_INTERRUPT)) { |
339 | vring_used_event(&vq->vring) = vq->last_used_idx; | 345 | vring_used_event(&vq->vring) = vq->last_used_idx; |
340 | virtio_mb(); | 346 | virtio_mb(vq); |
341 | } | 347 | } |
342 | 348 | ||
343 | END_USE(vq); | 349 | END_USE(vq); |
@@ -366,7 +372,7 @@ bool virtqueue_enable_cb(struct virtqueue *_vq) | |||
366 | * entry. Always do both to keep code simple. */ | 372 | * entry. Always do both to keep code simple. */ |
367 | vq->vring.avail->flags &= ~VRING_AVAIL_F_NO_INTERRUPT; | 373 | vq->vring.avail->flags &= ~VRING_AVAIL_F_NO_INTERRUPT; |
368 | vring_used_event(&vq->vring) = vq->last_used_idx; | 374 | vring_used_event(&vq->vring) = vq->last_used_idx; |
369 | virtio_mb(); | 375 | virtio_mb(vq); |
370 | if (unlikely(more_used(vq))) { | 376 | if (unlikely(more_used(vq))) { |
371 | END_USE(vq); | 377 | END_USE(vq); |
372 | return false; | 378 | return false; |
@@ -393,7 +399,7 @@ bool virtqueue_enable_cb_delayed(struct virtqueue *_vq) | |||
393 | /* TODO: tune this threshold */ | 399 | /* TODO: tune this threshold */ |
394 | bufs = (u16)(vq->vring.avail->idx - vq->last_used_idx) * 3 / 4; | 400 | bufs = (u16)(vq->vring.avail->idx - vq->last_used_idx) * 3 / 4; |
395 | vring_used_event(&vq->vring) = vq->last_used_idx + bufs; | 401 | vring_used_event(&vq->vring) = vq->last_used_idx + bufs; |
396 | virtio_mb(); | 402 | virtio_mb(vq); |
397 | if (unlikely((u16)(vq->vring.used->idx - vq->last_used_idx) > bufs)) { | 403 | if (unlikely((u16)(vq->vring.used->idx - vq->last_used_idx) > bufs)) { |
398 | END_USE(vq); | 404 | END_USE(vq); |
399 | return false; | 405 | return false; |
@@ -453,6 +459,7 @@ EXPORT_SYMBOL_GPL(vring_interrupt); | |||
453 | struct virtqueue *vring_new_virtqueue(unsigned int num, | 459 | struct virtqueue *vring_new_virtqueue(unsigned int num, |
454 | unsigned int vring_align, | 460 | unsigned int vring_align, |
455 | struct virtio_device *vdev, | 461 | struct virtio_device *vdev, |
462 | bool weak_barriers, | ||
456 | void *pages, | 463 | void *pages, |
457 | void (*notify)(struct virtqueue *), | 464 | void (*notify)(struct virtqueue *), |
458 | void (*callback)(struct virtqueue *), | 465 | void (*callback)(struct virtqueue *), |
@@ -476,6 +483,7 @@ struct virtqueue *vring_new_virtqueue(unsigned int num, | |||
476 | vq->vq.vdev = vdev; | 483 | vq->vq.vdev = vdev; |
477 | vq->vq.name = name; | 484 | vq->vq.name = name; |
478 | vq->notify = notify; | 485 | vq->notify = notify; |
486 | vq->weak_barriers = weak_barriers; | ||
479 | vq->broken = false; | 487 | vq->broken = false; |
480 | vq->last_used_idx = 0; | 488 | vq->last_used_idx = 0; |
481 | vq->num_added = 0; | 489 | vq->num_added = 0; |
diff --git a/include/linux/virtio_ring.h b/include/linux/virtio_ring.h index 36be0f6e18a9..e338730c2660 100644 --- a/include/linux/virtio_ring.h +++ b/include/linux/virtio_ring.h | |||
@@ -168,6 +168,7 @@ struct virtqueue; | |||
168 | struct virtqueue *vring_new_virtqueue(unsigned int num, | 168 | struct virtqueue *vring_new_virtqueue(unsigned int num, |
169 | unsigned int vring_align, | 169 | unsigned int vring_align, |
170 | struct virtio_device *vdev, | 170 | struct virtio_device *vdev, |
171 | bool weak_barriers, | ||
171 | void *pages, | 172 | void *pages, |
172 | void (*notify)(struct virtqueue *vq), | 173 | void (*notify)(struct virtqueue *vq), |
173 | void (*callback)(struct virtqueue *vq), | 174 | void (*callback)(struct virtqueue *vq), |
diff --git a/tools/virtio/linux/virtio.h b/tools/virtio/linux/virtio.h index 669bcdd45805..953db2abf6b9 100644 --- a/tools/virtio/linux/virtio.h +++ b/tools/virtio/linux/virtio.h | |||
@@ -214,6 +214,7 @@ void *virtqueue_detach_unused_buf(struct virtqueue *vq); | |||
214 | struct virtqueue *vring_new_virtqueue(unsigned int num, | 214 | struct virtqueue *vring_new_virtqueue(unsigned int num, |
215 | unsigned int vring_align, | 215 | unsigned int vring_align, |
216 | struct virtio_device *vdev, | 216 | struct virtio_device *vdev, |
217 | bool weak_barriers, | ||
217 | void *pages, | 218 | void *pages, |
218 | void (*notify)(struct virtqueue *vq), | 219 | void (*notify)(struct virtqueue *vq), |
219 | void (*callback)(struct virtqueue *vq), | 220 | void (*callback)(struct virtqueue *vq), |
diff --git a/tools/virtio/virtio_test.c b/tools/virtio/virtio_test.c index 74d3331bdaf9..0740284396c1 100644 --- a/tools/virtio/virtio_test.c +++ b/tools/virtio/virtio_test.c | |||
@@ -92,7 +92,8 @@ static void vq_info_add(struct vdev_info *dev, int num) | |||
92 | assert(r >= 0); | 92 | assert(r >= 0); |
93 | memset(info->ring, 0, vring_size(num, 4096)); | 93 | memset(info->ring, 0, vring_size(num, 4096)); |
94 | vring_init(&info->vring, num, info->ring, 4096); | 94 | vring_init(&info->vring, num, info->ring, 4096); |
95 | info->vq = vring_new_virtqueue(info->vring.num, 4096, &dev->vdev, info->ring, | 95 | info->vq = vring_new_virtqueue(info->vring.num, 4096, &dev->vdev, |
96 | true, info->ring, | ||
96 | vq_notify, vq_callback, "test"); | 97 | vq_notify, vq_callback, "test"); |
97 | assert(info->vq); | 98 | assert(info->vq); |
98 | info->vq->priv = info; | 99 | info->vq->priv = info; |