diff options
author | Linus Torvalds | 2015-09-04 12:22:09 -0500 |
---|---|---|
committer | Linus Torvalds | 2015-09-04 12:22:09 -0500 |
commit | 88a99886c26fec8bf662e7b6bc080431a8660326 (patch) | |
tree | 615b9a9a959ab093f6d8d0dd94d3bbc5299fc4c6 /CREDITS | |
parent | 8d2faea672606827c2018143ec7d88c760f2d6de (diff) | |
parent | 1ab36387ea4face01aac3560b396b1e2ce07c4ff (diff) | |
download | kernel-omap-88a99886c26fec8bf662e7b6bc080431a8660326.tar.gz kernel-omap-88a99886c26fec8bf662e7b6bc080431a8660326.tar.xz kernel-omap-88a99886c26fec8bf662e7b6bc080431a8660326.zip |
Merge tag 'pinctrl-v4.3-1' of git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-pinctrl
Pull pin control updates from Linus Walleij:
"This is the bulk of pin control changes for the v4.3 development
cycle.
Like with GPIO it's a lot of stuff. If my subsystems are any sign of
the overall tempo of the kernel v4.3 will be a gigantic diff.
[ It looks like 4.3 is calmer than 4.2 in most other subsystems, but
we'll see - Linus ]
Core changes:
- It is possible configure groups in debugfs.
- Consolidation of chained IRQ handler install/remove replacing all
call sites where irq_set_handler_data() and
irq_set_chained_handler() were done in succession with a combined
call to irq_set_chained_handler_and_data(). This series was
created by Thomas Gleixner after the problem was observed by
Russell King.
- Tglx also made another series of patches switching
__irq_set_handler_locked() for irq_set_handler_locked() which is
way cleaner.
- Tglx also wrote a good bunch of patches to make use of
irq_desc_get_xxx() accessors and avoid looking up irq_descs from
IRQ numbers. The goal is to get rid of the irq number from the
handlers in the IRQ flow which is nice.
Driver feature enhancements:
- Power management support for the SiRF SoC Atlas 7.
- Power down support for the Qualcomm driver.
- Intel Cherryview and Baytrail: switch drivers to use raw spinlocks
in IRQ handlers to play nice with the realtime patch set.
- Rework and new modes handling for Qualcomm SPMI-MPP.
- Pinconf power source config for SH PFC.
New drivers and subdrivers:
- A new driver for Conexant Digicolor CX92755.
- A new driver for UniPhier PH1-LD4, PH1-Pro4, PH1-sLD8, PH1-Pro5,
ProXtream2 and PH1-LD6b SoC pin control support.
- Reverse-egineered the S/PDIF settings for the Allwinner sun4i
driver.
- Support for Qualcomm Technologies QDF2xxx ARM64 SoCs
- A new Freescale i.mx6ul subdriver.
Cleanup:
- Remove platform data support in a number of SH PFC subdrivers"
* tag 'pinctrl-v4.3-1' of git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-pinctrl: (95 commits)
pinctrl: at91: fix null pointer dereference
pinctrl: mediatek: Implement wake handler and suspend resume
pinctrl: mediatek: Fix multiple registration issue.
pinctrl: sh-pfc: r8a7794: add USB pin groups
pinctrl: at91: Use generic irq_{request,release}_resources()
pinctrl: cherryview: Use raw_spinlock for locking
pinctrl: baytrail: Use raw_spinlock for locking
pinctrl: imx6ul: Remove .owner field
pinctrl: zynq: Fix typos in smc0_nand_grp and smc0_nor_grp
pinctrl: sh-pfc: Implement pinconf power-source param for voltage switching
clk: rockchip: add pclk_pd_pmu to the list of rk3288 critical clocks
pinctrl: sun4i: add spdif to pin description.
pinctrl: atlas7: clear ugly branch statements for pull and drivestrength
pinctrl: baytrail: Serialize all register access
pinctrl: baytrail: Drop FSF mailing address
pinctrl: rockchip: only enable gpio clock when it setting
pinctrl/mediatek: fix spelling mistake in dev_err error message
pinctrl: cherryview: Serialize all register access
pinctrl: UniPhier: PH1-Pro5: add I2C ch6 pin-mux setting
pinctrl: nomadik: reflect current input value
...
Diffstat (limited to 'CREDITS')
-rw-r--r-- | CREDITS | 4 |
1 files changed, 4 insertions, 0 deletions
@@ -20,6 +20,10 @@ D: One of assisting postmasters for vger.kernel.org's lists | |||
20 | S: (ask for current address) | 20 | S: (ask for current address) |
21 | S: Finland | 21 | S: Finland |
22 | 22 | ||
23 | N: Thomas Abraham | ||
24 | E: thomas.ab@samsung.com | ||
25 | D: Samsung pin controller driver | ||
26 | |||
23 | N: Dragos Acostachioaie | 27 | N: Dragos Acostachioaie |
24 | E: dragos@iname.com | 28 | E: dragos@iname.com |
25 | W: http://www.arbornet.org/~dragos | 29 | W: http://www.arbornet.org/~dragos |