diff options
author | Linus Torvalds | 2012-12-13 14:14:47 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-13 14:14:47 -0600 |
commit | 193c0d682525987db59ac3a24531a77e4947aa95 (patch) | |
tree | 7b58346171c4d07e2c2ee6c3c469c325495149a4 /Documentation/ABI | |
parent | 8b0cab14951fbf8126795ab301835a8f8126a988 (diff) | |
parent | 1cb73f8c479e66541fefd3f7fa547b1fa56cdc54 (diff) | |
download | kernel-omap-193c0d682525987db59ac3a24531a77e4947aa95.tar.gz kernel-omap-193c0d682525987db59ac3a24531a77e4947aa95.tar.xz kernel-omap-193c0d682525987db59ac3a24531a77e4947aa95.zip |
Merge tag 'for-3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/helgaas/pci
Pull PCI update from Bjorn Helgaas:
"Host bridge hotplug:
- Untangle _PRT from struct pci_bus (Bjorn Helgaas)
- Request _OSC control before scanning root bus (Taku Izumi)
- Assign resources when adding host bridge (Yinghai Lu)
- Remove root bus when removing host bridge (Yinghai Lu)
- Remove _PRT during hot remove (Yinghai Lu)
SRIOV
- Add sysfs knobs to control numVFs (Don Dutile)
Power management
- Notify devices when power resource turned on (Huang Ying)
Bug fixes
- Work around broken _SEG on HP xw9300 (Bjorn Helgaas)
- Keep runtime PM enabled for unbound PCI devices (Huang Ying)
- Fix Optimus dual-GPU runtime D3 suspend issue (Dave Airlie)
- Fix xen frontend shutdown issue (David Vrabel)
- Work around PLX PCI 9050 BAR alignment erratum (Ian Abbott)
Miscellaneous
- Add GPL license for drivers/pci/ioapic (Andrew Cooks)
- Add standard PCI-X, PCIe ASPM register #defines (Bjorn Helgaas)
- NumaChip remote PCI support (Daniel Blueman)
- Fix PCIe Link Capabilities Supported Link Speed definition (Jingoo
Han)
- Convert dev_printk() to dev_info(), etc (Joe Perches)
- Add support for non PCI BAR ROM data (Matthew Garrett)
- Add x86 support for host bridge translation offset (Mike Yoknis)
- Report success only when every driver supports AER (Vijay
Pandarathil)"
Fix up trivial conflicts.
* tag 'for-3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/helgaas/pci: (48 commits)
PCI: Use phys_addr_t for physical ROM address
x86/PCI: Add NumaChip remote PCI support
ath9k: Use standard #defines for PCIe Capability ASPM fields
iwlwifi: Use standard #defines for PCIe Capability ASPM fields
iwlwifi: collapse wrapper for pcie_capability_read_word()
iwlegacy: Use standard #defines for PCIe Capability ASPM fields
iwlegacy: collapse wrapper for pcie_capability_read_word()
cxgb3: Use standard #defines for PCIe Capability ASPM fields
PCI: Add standard PCIe Capability Link ASPM field names
PCI/portdrv: Use PCI Express Capability accessors
PCI: Use standard PCIe Capability Link register field names
x86: Use PCI setup data
PCI: Add support for non-BAR ROMs
PCI: Add pcibios_add_device
EFI: Stash ROMs if they're not in the PCI BAR
PCI: Add and use standard PCI-X Capability register names
PCI/PM: Keep runtime PM enabled for unbound PCI devices
xen-pcifront: Handle backend CLOSED without CLOSING
PCI: SRIOV control and status via sysfs (documentation)
PCI/AER: Report success only when every device has AER-aware driver
...
Diffstat (limited to 'Documentation/ABI')
-rw-r--r-- | Documentation/ABI/testing/sysfs-bus-pci | 34 |
1 files changed, 34 insertions, 0 deletions
diff --git a/Documentation/ABI/testing/sysfs-bus-pci b/Documentation/ABI/testing/sysfs-bus-pci index dff1f48d252d..1ce5ae329c04 100644 --- a/Documentation/ABI/testing/sysfs-bus-pci +++ b/Documentation/ABI/testing/sysfs-bus-pci | |||
@@ -222,3 +222,37 @@ Description: | |||
222 | satisfied too. Reading this attribute will show the current | 222 | satisfied too. Reading this attribute will show the current |
223 | value of d3cold_allowed bit. Writing this attribute will set | 223 | value of d3cold_allowed bit. Writing this attribute will set |
224 | the value of d3cold_allowed bit. | 224 | the value of d3cold_allowed bit. |
225 | |||
226 | What: /sys/bus/pci/devices/.../sriov_totalvfs | ||
227 | Date: November 2012 | ||
228 | Contact: Donald Dutile <ddutile@redhat.com> | ||
229 | Description: | ||
230 | This file appears when a physical PCIe device supports SR-IOV. | ||
231 | Userspace applications can read this file to determine the | ||
232 | maximum number of Virtual Functions (VFs) a PCIe physical | ||
233 | function (PF) can support. Typically, this is the value reported | ||
234 | in the PF's SR-IOV extended capability structure's TotalVFs | ||
235 | element. Drivers have the ability at probe time to reduce the | ||
236 | value read from this file via the pci_sriov_set_totalvfs() | ||
237 | function. | ||
238 | |||
239 | What: /sys/bus/pci/devices/.../sriov_numvfs | ||
240 | Date: November 2012 | ||
241 | Contact: Donald Dutile <ddutile@redhat.com> | ||
242 | Description: | ||
243 | This file appears when a physical PCIe device supports SR-IOV. | ||
244 | Userspace applications can read and write to this file to | ||
245 | determine and control the enablement or disablement of Virtual | ||
246 | Functions (VFs) on the physical function (PF). A read of this | ||
247 | file will return the number of VFs that are enabled on this PF. | ||
248 | A number written to this file will enable the specified | ||
249 | number of VFs. A userspace application would typically read the | ||
250 | file and check that the value is zero, and then write the number | ||
251 | of VFs that should be enabled on the PF; the value written | ||
252 | should be less than or equal to the value in the sriov_totalvfs | ||
253 | file. A userspace application wanting to disable the VFs would | ||
254 | write a zero to this file. The core ensures that valid values | ||
255 | are written to this file, and returns errors when values are not | ||
256 | valid. For example, writing a 2 to this file when sriov_numvfs | ||
257 | is not 0 and not 2 already will return an error. Writing a 10 | ||
258 | when the value of sriov_totalvfs is 8 will return an error. | ||