diff options
author | Stanislav Kinsbursky | 2013-01-04 17:34:50 -0600 |
---|---|---|
committer | Linus Torvalds | 2013-01-04 18:11:45 -0600 |
commit | 03f595668017f1a1fb971c02fc37140bc6e7bb1c (patch) | |
tree | 3aa5c4b32b5fd396f0d74679548de8c09ca195a1 /Documentation | |
parent | 9afdacda0252fc1ddb7907728e878518edbcdfce (diff) | |
download | kernel-omap-03f595668017f1a1fb971c02fc37140bc6e7bb1c.tar.gz kernel-omap-03f595668017f1a1fb971c02fc37140bc6e7bb1c.tar.xz kernel-omap-03f595668017f1a1fb971c02fc37140bc6e7bb1c.zip |
ipc: add sysctl to specify desired next object id
Add 3 new variables and sysctls to tune them (by one "next_id" variable
for messages, semaphores and shared memory respectively). This variable
can be used to set desired id for next allocated IPC object. By default
it's equal to -1 and old behaviour is preserved. If this variable is
non-negative, then desired idr will be extracted from it and used as a
start value to search for free IDR slot.
Notes:
1) this patch doesn't guarantee that the new object will have desired
id. So it's up to user space how to handle new object with wrong id.
2) After a sucessful id allocation attempt, "next_id" will be set back
to -1 (if it was non-negative).
[akpm@linux-foundation.org: checkpatch fixes]
Signed-off-by: Stanislav Kinsbursky <skinsbursky@parallels.com>
Cc: Serge Hallyn <serge.hallyn@canonical.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Cc: Pavel Emelyanov <xemul@parallels.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com>
Cc: Michael Kerrisk <mtk.manpages@gmail.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'Documentation')
-rw-r--r-- | Documentation/sysctl/kernel.txt | 19 |
1 files changed, 19 insertions, 0 deletions
diff --git a/Documentation/sysctl/kernel.txt b/Documentation/sysctl/kernel.txt index 2907ba6c3607..51b953a1b149 100644 --- a/Documentation/sysctl/kernel.txt +++ b/Documentation/sysctl/kernel.txt | |||
@@ -38,6 +38,7 @@ show up in /proc/sys/kernel: | |||
38 | - l2cr [ PPC only ] | 38 | - l2cr [ PPC only ] |
39 | - modprobe ==> Documentation/debugging-modules.txt | 39 | - modprobe ==> Documentation/debugging-modules.txt |
40 | - modules_disabled | 40 | - modules_disabled |
41 | - msg_next_id [ sysv ipc ] | ||
41 | - msgmax | 42 | - msgmax |
42 | - msgmnb | 43 | - msgmnb |
43 | - msgmni | 44 | - msgmni |
@@ -62,7 +63,9 @@ show up in /proc/sys/kernel: | |||
62 | - rtsig-max | 63 | - rtsig-max |
63 | - rtsig-nr | 64 | - rtsig-nr |
64 | - sem | 65 | - sem |
66 | - sem_next_id [ sysv ipc ] | ||
65 | - sg-big-buff [ generic SCSI device (sg) ] | 67 | - sg-big-buff [ generic SCSI device (sg) ] |
68 | - shm_next_id [ sysv ipc ] | ||
66 | - shm_rmid_forced | 69 | - shm_rmid_forced |
67 | - shmall | 70 | - shmall |
68 | - shmmax [ sysv ipc ] | 71 | - shmmax [ sysv ipc ] |
@@ -320,6 +323,22 @@ to false. | |||
320 | 323 | ||
321 | ============================================================== | 324 | ============================================================== |
322 | 325 | ||
326 | msg_next_id, sem_next_id, and shm_next_id: | ||
327 | |||
328 | These three toggles allows to specify desired id for next allocated IPC | ||
329 | object: message, semaphore or shared memory respectively. | ||
330 | |||
331 | By default they are equal to -1, which means generic allocation logic. | ||
332 | Possible values to set are in range {0..INT_MAX}. | ||
333 | |||
334 | Notes: | ||
335 | 1) kernel doesn't guarantee, that new object will have desired id. So, | ||
336 | it's up to userspace, how to handle an object with "wrong" id. | ||
337 | 2) Toggle with non-default value will be set back to -1 by kernel after | ||
338 | successful IPC object allocation. | ||
339 | |||
340 | ============================================================== | ||
341 | |||
323 | nmi_watchdog: | 342 | nmi_watchdog: |
324 | 343 | ||
325 | Enables/Disables the NMI watchdog on x86 systems. When the value is | 344 | Enables/Disables the NMI watchdog on x86 systems. When the value is |