aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorLinus Torvalds2013-01-24 14:42:50 -0600
committerLinus Torvalds2013-01-24 14:42:50 -0600
commit1496ec13a1ae92cea305d266ff73f850138f92c7 (patch)
tree906a88476ca654e6446502c83882b76ef067ae80 /Documentation
parentba2ab41f3d68f277860768b2c5b197768b196332 (diff)
parent3836414f45b01486b9b50c627a329010573ad0f4 (diff)
downloadkernel-omap-1496ec13a1ae92cea305d266ff73f850138f92c7.tar.gz
kernel-omap-1496ec13a1ae92cea305d266ff73f850138f92c7.tar.xz
kernel-omap-1496ec13a1ae92cea305d266ff73f850138f92c7.zip
Merge tag 'fixes-for-linus2' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc
Pull ARM SoC fixes from Olof Johansson: "Here's a long-pending fixes pull request for arm-soc (I didn't send one in the -rc4 cycle). The larger deltas are from: - A fixup of error paths in the mvsdio driver - Header file move for a driver that hadn't been properly converted to multiplatform on i.MX, which was causing build failures when included - Device tree updates for at91 dealing mostly with their new pinctrl setup merged in 3.8 and mistakes in those initial configs The rest are the normal mix of small fixes all over the place; sunxi, omap, imx, mvebu, etc, etc." * tag 'fixes-for-linus2' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: (40 commits) mfd: vexpress-sysreg: Don't skip initialization on probe ARM: vexpress: Enable A7 cores in V2P-CA15_A7's Device Tree ARM: vexpress: extend the MPIDR range used for pen release check ARM: at91/dts: correct comment in at91sam9x5.dtsi for mii ARM: at91/at91_dt_defconfig: add at91sam9n12 SoC to DT defconfig ARM: at91/at91_dt_defconfig: remove memory specification to cmdline ARM: at91/dts: add macb mii pinctrl config for kizbox ARM: at91: rm9200: remake the BGA as default version ARM: at91: fix gpios on i2c-gpio for RM9200 DT ARM: at91/at91sam9x5 DTS: add SCK USART pins ARM: at91/at91sam9x5 DTS: correct wrong PIO BANK values on u(s)arts ARM: at91/at91-pinctrl documentation: fix typo and add some details ARM: kirkwood: fix missing #interrupt-cells property mmc: mvsdio: use devm_ API to simplify/correct error paths. clk: mvebu/clk-cpu.c: fix memory leakage ARM: OMAP2+: omap4-panda: add UART2 muxing for WiLink shared transport ARM: OMAP2+: DT node Timer iteration fix ARM: OMAP2+: Fix section warning for omap_init_ocp2scp() ARM: OMAP2+: fix build break for omapdrm ARM: OMAP2: Fix missing omap2xxx_clkt_vps_late_init function calls ...
Diffstat (limited to 'Documentation')
-rw-r--r--Documentation/devicetree/bindings/pinctrl/atmel,at91-pinctrl.txt5
1 files changed, 3 insertions, 2 deletions
diff --git a/Documentation/devicetree/bindings/pinctrl/atmel,at91-pinctrl.txt b/Documentation/devicetree/bindings/pinctrl/atmel,at91-pinctrl.txt
index 3a268127b054..bc50899e0c81 100644
--- a/Documentation/devicetree/bindings/pinctrl/atmel,at91-pinctrl.txt
+++ b/Documentation/devicetree/bindings/pinctrl/atmel,at91-pinctrl.txt
@@ -81,7 +81,8 @@ PA31 TXD4
81Required properties for pin configuration node: 81Required properties for pin configuration node:
82- atmel,pins: 4 integers array, represents a group of pins mux and config 82- atmel,pins: 4 integers array, represents a group of pins mux and config
83 setting. The format is atmel,pins = <PIN_BANK PIN_BANK_NUM PERIPH CONFIG>. 83 setting. The format is atmel,pins = <PIN_BANK PIN_BANK_NUM PERIPH CONFIG>.
84 The PERIPH 0 means gpio. 84 The PERIPH 0 means gpio, PERIPH 1 is periph A, PERIPH 2 is periph B...
85 PIN_BANK 0 is pioA, PIN_BANK 1 is pioB...
85 86
86Bits used for CONFIG: 87Bits used for CONFIG:
87PULL_UP (1 << 0): indicate this pin need a pull up. 88PULL_UP (1 << 0): indicate this pin need a pull up.
@@ -126,7 +127,7 @@ pinctrl@fffff400 {
126 pinctrl_dbgu: dbgu-0 { 127 pinctrl_dbgu: dbgu-0 {
127 atmel,pins = 128 atmel,pins =
128 <1 14 0x1 0x0 /* PB14 periph A */ 129 <1 14 0x1 0x0 /* PB14 periph A */
129 1 15 0x1 0x1>; /* PB15 periph with pullup */ 130 1 15 0x1 0x1>; /* PB15 periph A with pullup */
130 }; 131 };
131 }; 132 };
132}; 133};