diff options
author | Glauber Costa | 2012-12-18 16:22:04 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-18 17:02:12 -0600 |
commit | 50bdd430c20566b13d8bc59946184b08f5875de6 (patch) | |
tree | 15ccc558002367c3d2c6b092ccc1d49e6d14acf1 /Documentation | |
parent | 6a1a0d3b625a4091e7a0eb249aefc6a644385149 (diff) | |
download | kernel-omap-50bdd430c20566b13d8bc59946184b08f5875de6.tar.gz kernel-omap-50bdd430c20566b13d8bc59946184b08f5875de6.tar.xz kernel-omap-50bdd430c20566b13d8bc59946184b08f5875de6.zip |
res_counter: return amount of charges after res_counter_uncharge()
It is useful to know how many charges are still left after a call to
res_counter_uncharge. While it is possible to issue a res_counter_read
after uncharge, this can be racy.
If we need, for instance, to take some action when the counters drop down
to 0, only one of the callers should see it. This is the same semantics
as the atomic variables in the kernel.
Since the current return value is void, we don't need to worry about
anything breaking due to this change: nobody relied on that, and only
users appearing from now on will be checking this value.
Signed-off-by: Glauber Costa <glommer@parallels.com>
Reviewed-by: Michal Hocko <mhocko@suse.cz>
Acked-by: Kamezawa Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Acked-by: David Rientjes <rientjes@google.com>
Cc: Johannes Weiner <hannes@cmpxchg.org>
Cc: Suleiman Souhlal <suleiman@google.com>
Cc: Tejun Heo <tj@kernel.org>
Cc: Christoph Lameter <cl@linux.com>
Cc: Frederic Weisbecker <fweisbec@redhat.com>
Cc: Greg Thelen <gthelen@google.com>
Cc: JoonSoo Kim <js1304@gmail.com>
Cc: Mel Gorman <mel@csn.ul.ie>
Cc: Pekka Enberg <penberg@cs.helsinki.fi>
Cc: Rik van Riel <riel@redhat.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'Documentation')
-rw-r--r-- | Documentation/cgroups/resource_counter.txt | 7 |
1 files changed, 4 insertions, 3 deletions
diff --git a/Documentation/cgroups/resource_counter.txt b/Documentation/cgroups/resource_counter.txt index 0c4a344e78fa..c4d99ed0b418 100644 --- a/Documentation/cgroups/resource_counter.txt +++ b/Documentation/cgroups/resource_counter.txt | |||
@@ -83,16 +83,17 @@ to work with it. | |||
83 | res_counter->lock internally (it must be called with res_counter->lock | 83 | res_counter->lock internally (it must be called with res_counter->lock |
84 | held). The force parameter indicates whether we can bypass the limit. | 84 | held). The force parameter indicates whether we can bypass the limit. |
85 | 85 | ||
86 | e. void res_counter_uncharge[_locked] | 86 | e. u64 res_counter_uncharge[_locked] |
87 | (struct res_counter *rc, unsigned long val) | 87 | (struct res_counter *rc, unsigned long val) |
88 | 88 | ||
89 | When a resource is released (freed) it should be de-accounted | 89 | When a resource is released (freed) it should be de-accounted |
90 | from the resource counter it was accounted to. This is called | 90 | from the resource counter it was accounted to. This is called |
91 | "uncharging". | 91 | "uncharging". The return value of this function indicate the amount |
92 | of charges still present in the counter. | ||
92 | 93 | ||
93 | The _locked routines imply that the res_counter->lock is taken. | 94 | The _locked routines imply that the res_counter->lock is taken. |
94 | 95 | ||
95 | f. void res_counter_uncharge_until | 96 | f. u64 res_counter_uncharge_until |
96 | (struct res_counter *rc, struct res_counter *top, | 97 | (struct res_counter *rc, struct res_counter *top, |
97 | unsinged long val) | 98 | unsinged long val) |
98 | 99 | ||