diff options
author | Haavard Skinnemoen | 2008-02-08 06:21:00 -0600 |
---|---|---|
committer | Linus Torvalds | 2008-02-08 11:22:37 -0600 |
commit | a1cfac48ba4c7481bb749e0f4f37c85cb871b2d1 (patch) | |
tree | dcce72478ff110f40a393755133b08ce096a83e5 /MAINTAINERS | |
parent | b4bd7d59451960d4e1d994c01581b31b08fe3720 (diff) | |
download | kernel-omap-a1cfac48ba4c7481bb749e0f4f37c85cb871b2d1.tar.gz kernel-omap-a1cfac48ba4c7481bb749e0f4f37c85cb871b2d1.tar.xz kernel-omap-a1cfac48ba4c7481bb749e0f4f37c85cb871b2d1.zip |
MAINTAINERS: add Haavard as maintainer of the atmel_serial driver
The following patchset cleans up the atmel_serial driver a bit, moves a
significant portion of the interrupt handler into a tasklet, and adds DMA
support. This is the result of a combined effort by Chip Coldwell, Remy
Bohmer and me. The patches should apply cleanly onto Linus' latest git tree,
and I've also tested it on -mm (with a couple of avr32 fixes applied to make
the rest of the tree compile.)
With DMA, I see transfer rates around 92 kbps when transferring a big file
using ZModem (both directions are roughly the same.) I've also tested the same
thing with a bunch of debug options enabled. The transfer rate is slightly
lower, but no errors are reported.
Note that break and error handling doesn't work too well with DMA enabled.
This is a common problem with all the efforts I've seen adding DMA support to
this driver (including my own). The PDC error handling also accesses icount
without locking. I'm tempted to just ignore the problem for now and hopefully
come up with a solution later.
This patch:
The atmel_serial driver never had a MAINTAINERS entry, although Andrew Victor
has effectively been acting as a maintainer since he got the driver merged
into mainline in the first place.
I'll keep Cc'ing Andrew on all patches, but I'm going to take the main
responsibility for getting things moving upstream from now on.
Signed-off-by: Haavard Skinnemoen <hskinnemoen@atmel.com>
Acked-by: Andrew Victor <linux@maxim.org.za>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'MAINTAINERS')
-rw-r--r-- | MAINTAINERS | 6 |
1 files changed, 6 insertions, 0 deletions
diff --git a/MAINTAINERS b/MAINTAINERS index e91eeba3f3e3..a24631f4eab1 100644 --- a/MAINTAINERS +++ b/MAINTAINERS | |||
@@ -688,6 +688,12 @@ W: http://www.atmel.com/products/AT91/ | |||
688 | W: http://www.at91.com/ | 688 | W: http://www.at91.com/ |
689 | S: Maintained | 689 | S: Maintained |
690 | 690 | ||
691 | ATMEL AT91 / AT32 SERIAL DRIVER | ||
692 | P: Haavard Skinnemoen | ||
693 | M: hskinnemoen@atmel.com | ||
694 | L: linux-kernel@vger.kernel.org | ||
695 | S: Supported | ||
696 | |||
691 | ATMEL LCDFB DRIVER | 697 | ATMEL LCDFB DRIVER |
692 | P: Nicolas Ferre | 698 | P: Nicolas Ferre |
693 | M: nicolas.ferre@atmel.com | 699 | M: nicolas.ferre@atmel.com |