aboutsummaryrefslogtreecommitdiffstats
path: root/README
diff options
context:
space:
mode:
authorMichael Witten2012-04-03 14:20:02 -0500
committerJiri Kosina2012-04-17 03:23:31 -0500
commita20e3a795b1a1975f09f7f729ba2b6fc74f4a54a (patch)
treefbedf9f750c4584623abb5edc9ee00224e39f5c6 /README
parent5b4285fbd4692928ed41992b9aba55c7d1efd723 (diff)
downloadkernel-omap-a20e3a795b1a1975f09f7f729ba2b6fc74f4a54a.tar.gz
kernel-omap-a20e3a795b1a1975f09f7f729ba2b6fc74f4a54a.tar.xz
kernel-omap-a20e3a795b1a1975f09f7f729ba2b6fc74f4a54a.zip
README: Grammar: `me has' -> `I have'
Signed-off-by: Michael Witten <mfwitten@gmail.com> Acked-by: Randy Dunlap <rdunlap@xenotime.net> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
Diffstat (limited to 'README')
-rw-r--r--README2
1 files changed, 1 insertions, 1 deletions
diff --git a/README b/README
index c03dc56e1872..15acb0a6ae67 100644
--- a/README
+++ b/README
@@ -89,7 +89,7 @@ INSTALLING the kernel source:
89 source tree, _in_order_, and you should be ok. You may want to remove 89 source tree, _in_order_, and you should be ok. You may want to remove
90 the backup files (some-file-name~ or some-file-name.orig), and make sure 90 the backup files (some-file-name~ or some-file-name.orig), and make sure
91 that there are no failed patches (some-file-name# or some-file-name.rej). 91 that there are no failed patches (some-file-name# or some-file-name.rej).
92 If there are, either you or me has made a mistake. 92 If there are, either you or I have made a mistake.
93 93
94 Unlike patches for the 3.x kernels, patches for the 3.x.y kernels 94 Unlike patches for the 3.x kernels, patches for the 3.x.y kernels
95 (also known as the -stable kernels) are not incremental but instead apply 95 (also known as the -stable kernels) are not incremental but instead apply