diff options
author | Tobias Klauser | 2005-09-10 02:26:58 -0500 |
---|---|---|
committer | Linus Torvalds | 2005-09-10 12:06:31 -0500 |
commit | 9dcbb32f1654e79c212c20d9cd9d48509ee1eaf7 (patch) | |
tree | b0663a525fbb0f24acc6304d6869b71d0c0c991c /REPORTING-BUGS | |
parent | 96757701336365e30bea9fccdfac087338954e09 (diff) | |
download | kernel-omap-9dcbb32f1654e79c212c20d9cd9d48509ee1eaf7.tar.gz kernel-omap-9dcbb32f1654e79c212c20d9cd9d48509ee1eaf7.tar.xz kernel-omap-9dcbb32f1654e79c212c20d9cd9d48509ee1eaf7.zip |
[PATCH] Spelling and whitespace fixes for REPORTING-BUGS
The attached patch fixes some spelling errors in REPORTING-BUGS and also
removes all trailing whitespaces.
Signed-off-by: Tobias Klauser <tklauser@nuerscht.ch>
Signed-off-by: Domen Puncer <domen@coderock.org>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Diffstat (limited to 'REPORTING-BUGS')
-rw-r--r-- | REPORTING-BUGS | 14 |
1 files changed, 7 insertions, 7 deletions
diff --git a/REPORTING-BUGS b/REPORTING-BUGS index 224c34741d32..f9da827a0c18 100644 --- a/REPORTING-BUGS +++ b/REPORTING-BUGS | |||
@@ -9,7 +9,7 @@ screen please read "Documentation/oops-tracing.txt" before posting your | |||
9 | bug report. This explains what you should do with the "Oops" information | 9 | bug report. This explains what you should do with the "Oops" information |
10 | to make it useful to the recipient. | 10 | to make it useful to the recipient. |
11 | 11 | ||
12 | Send the output the maintainer of the kernel area that seems to | 12 | Send the output to the maintainer of the kernel area that seems to |
13 | be involved with the problem. Don't worry too much about getting the | 13 | be involved with the problem. Don't worry too much about getting the |
14 | wrong person. If you are unsure send it to the person responsible for the | 14 | wrong person. If you are unsure send it to the person responsible for the |
15 | code relevant to what you were doing. If it occurs repeatably try and | 15 | code relevant to what you were doing. If it occurs repeatably try and |
@@ -18,15 +18,15 @@ The list of maintainers is in the MAINTAINERS file in this directory. | |||
18 | 18 | ||
19 | If it is a security bug, please copy the Security Contact listed | 19 | If it is a security bug, please copy the Security Contact listed |
20 | in the MAINTAINERS file. They can help coordinate bugfix and disclosure. | 20 | in the MAINTAINERS file. They can help coordinate bugfix and disclosure. |
21 | See Documentation/SecurityBugs for more infomation. | 21 | See Documentation/SecurityBugs for more information. |
22 | 22 | ||
23 | If you are totally stumped as to whom to send the report, send it to | 23 | If you are totally stumped as to whom to send the report, send it to |
24 | linux-kernel@vger.kernel.org. (For more information on the linux-kernel | 24 | linux-kernel@vger.kernel.org. (For more information on the linux-kernel |
25 | mailing list see http://www.tux.org/lkml/). | 25 | mailing list see http://www.tux.org/lkml/). |
26 | 26 | ||
27 | This is a suggested format for a bug report sent to the Linux kernel mailing | 27 | This is a suggested format for a bug report sent to the Linux kernel mailing |
28 | list. Having a standardized bug report form makes it easier for you not to | 28 | list. Having a standardized bug report form makes it easier for you not to |
29 | overlook things, and easier for the developers to find the pieces of | 29 | overlook things, and easier for the developers to find the pieces of |
30 | information they're really interested in. Don't feel you have to follow it. | 30 | information they're really interested in. Don't feel you have to follow it. |
31 | 31 | ||
32 | First run the ver_linux script included as scripts/ver_linux, which | 32 | First run the ver_linux script included as scripts/ver_linux, which |
@@ -35,9 +35,9 @@ the command "sh scripts/ver_linux". | |||
35 | 35 | ||
36 | Use that information to fill in all fields of the bug report form, and | 36 | Use that information to fill in all fields of the bug report form, and |
37 | post it to the mailing list with a subject of "PROBLEM: <one line | 37 | post it to the mailing list with a subject of "PROBLEM: <one line |
38 | summary from [1.]>" for easy identification by the developers | 38 | summary from [1.]>" for easy identification by the developers. |
39 | 39 | ||
40 | [1.] One line summary of the problem: | 40 | [1.] One line summary of the problem: |
41 | [2.] Full description of the problem/report: | 41 | [2.] Full description of the problem/report: |
42 | [3.] Keywords (i.e., modules, networking, kernel): | 42 | [3.] Keywords (i.e., modules, networking, kernel): |
43 | [4.] Kernel version (from /proc/version): | 43 | [4.] Kernel version (from /proc/version): |