diff options
author | Kees Cook | 2017-06-23 17:08:57 -0500 |
---|---|---|
committer | Greg Kroah-Hartman | 2017-06-29 05:48:50 -0500 |
commit | 1d3d0f8b7cf758136ed36b30620442d989601737 (patch) | |
tree | 0b812c7d3390e1622f7b356c5847731d7ca5f8a8 /fs | |
parent | 22da7ca81a3aad1af021c770b578acad86d63681 (diff) | |
download | kernel-omap-1d3d0f8b7cf758136ed36b30620442d989601737.tar.gz kernel-omap-1d3d0f8b7cf758136ed36b30620442d989601737.tar.xz kernel-omap-1d3d0f8b7cf758136ed36b30620442d989601737.zip |
fs/exec.c: account for argv/envp pointers
commit 98da7d08850fb8bdeb395d6368ed15753304aa0c upstream.
When limiting the argv/envp strings during exec to 1/4 of the stack limit,
the storage of the pointers to the strings was not included. This means
that an exec with huge numbers of tiny strings could eat 1/4 of the stack
limit in strings and then additional space would be later used by the
pointers to the strings.
For example, on 32-bit with a 8MB stack rlimit, an exec with 1677721
single-byte strings would consume less than 2MB of stack, the max (8MB /
4) amount allowed, but the pointers to the strings would consume the
remaining additional stack space (1677721 * 4 == 6710884).
The result (1677721 + 6710884 == 8388605) would exhaust stack space
entirely. Controlling this stack exhaustion could result in
pathological behavior in setuid binaries (CVE-2017-1000365).
[akpm@linux-foundation.org: additional commenting from Kees]
Fixes: b6a2fea39318 ("mm: variable length argument support")
Link: http://lkml.kernel.org/r/20170622001720.GA32173@beast
Signed-off-by: Kees Cook <keescook@chromium.org>
Acked-by: Rik van Riel <riel@redhat.com>
Acked-by: Michal Hocko <mhocko@suse.com>
Cc: Alexander Viro <viro@zeniv.linux.org.uk>
Cc: Qualys Security Advisory <qsa@qualys.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Diffstat (limited to 'fs')
-rw-r--r-- | fs/exec.c | 28 |
1 files changed, 24 insertions, 4 deletions
@@ -206,8 +206,26 @@ static struct page *get_arg_page(struct linux_binprm *bprm, unsigned long pos, | |||
206 | 206 | ||
207 | if (write) { | 207 | if (write) { |
208 | unsigned long size = bprm->vma->vm_end - bprm->vma->vm_start; | 208 | unsigned long size = bprm->vma->vm_end - bprm->vma->vm_start; |
209 | unsigned long ptr_size; | ||
209 | struct rlimit *rlim; | 210 | struct rlimit *rlim; |
210 | 211 | ||
212 | /* | ||
213 | * Since the stack will hold pointers to the strings, we | ||
214 | * must account for them as well. | ||
215 | * | ||
216 | * The size calculation is the entire vma while each arg page is | ||
217 | * built, so each time we get here it's calculating how far it | ||
218 | * is currently (rather than each call being just the newly | ||
219 | * added size from the arg page). As a result, we need to | ||
220 | * always add the entire size of the pointers, so that on the | ||
221 | * last call to get_arg_page() we'll actually have the entire | ||
222 | * correct size. | ||
223 | */ | ||
224 | ptr_size = (bprm->argc + bprm->envc) * sizeof(void *); | ||
225 | if (ptr_size > ULONG_MAX - size) | ||
226 | goto fail; | ||
227 | size += ptr_size; | ||
228 | |||
211 | acct_arg_size(bprm, size / PAGE_SIZE); | 229 | acct_arg_size(bprm, size / PAGE_SIZE); |
212 | 230 | ||
213 | /* | 231 | /* |
@@ -225,13 +243,15 @@ static struct page *get_arg_page(struct linux_binprm *bprm, unsigned long pos, | |||
225 | * to work from. | 243 | * to work from. |
226 | */ | 244 | */ |
227 | rlim = current->signal->rlim; | 245 | rlim = current->signal->rlim; |
228 | if (size > ACCESS_ONCE(rlim[RLIMIT_STACK].rlim_cur) / 4) { | 246 | if (size > READ_ONCE(rlim[RLIMIT_STACK].rlim_cur) / 4) |
229 | put_page(page); | 247 | goto fail; |
230 | return NULL; | ||
231 | } | ||
232 | } | 248 | } |
233 | 249 | ||
234 | return page; | 250 | return page; |
251 | |||
252 | fail: | ||
253 | put_page(page); | ||
254 | return NULL; | ||
235 | } | 255 | } |
236 | 256 | ||
237 | static void put_arg_page(struct page *page) | 257 | static void put_arg_page(struct page *page) |