diff options
author | Sahitya Tummala | 2017-07-10 17:50:00 -0500 |
---|---|---|
committer | Greg Kroah-Hartman | 2017-07-21 00:44:56 -0500 |
commit | 68b0f5d85b3a25ee452424e18fe06b93da8dd4d2 (patch) | |
tree | 6d321b722d4b790388e8637dec804dc96ec0f71d /fs | |
parent | 2d0db02d2e8f45e215fd2e646820c669c6e70159 (diff) | |
download | kernel-omap-68b0f5d85b3a25ee452424e18fe06b93da8dd4d2.tar.gz kernel-omap-68b0f5d85b3a25ee452424e18fe06b93da8dd4d2.tar.xz kernel-omap-68b0f5d85b3a25ee452424e18fe06b93da8dd4d2.zip |
fs/dcache.c: fix spin lockup issue on nlru->lock
commit b17c070fb624cf10162cf92ea5e1ec25cd8ac176 upstream.
__list_lru_walk_one() acquires nlru spin lock (nlru->lock) for longer
duration if there are more number of items in the lru list. As per the
current code, it can hold the spin lock for upto maximum UINT_MAX
entries at a time. So if there are more number of items in the lru
list, then "BUG: spinlock lockup suspected" is observed in the below
path:
spin_bug+0x90
do_raw_spin_lock+0xfc
_raw_spin_lock+0x28
list_lru_add+0x28
dput+0x1c8
path_put+0x20
terminate_walk+0x3c
path_lookupat+0x100
filename_lookup+0x6c
user_path_at_empty+0x54
SyS_faccessat+0xd0
el0_svc_naked+0x24
This nlru->lock is acquired by another CPU in this path -
d_lru_shrink_move+0x34
dentry_lru_isolate_shrink+0x48
__list_lru_walk_one.isra.10+0x94
list_lru_walk_node+0x40
shrink_dcache_sb+0x60
do_remount_sb+0xbc
do_emergency_remount+0xb0
process_one_work+0x228
worker_thread+0x2e0
kthread+0xf4
ret_from_fork+0x10
Fix this lockup by reducing the number of entries to be shrinked from
the lru list to 1024 at once. Also, add cond_resched() before
processing the lru list again.
Link: http://marc.info/?t=149722864900001&r=1&w=2
Link: http://lkml.kernel.org/r/1498707575-2472-1-git-send-email-stummala@codeaurora.org
Signed-off-by: Sahitya Tummala <stummala@codeaurora.org>
Suggested-by: Jan Kara <jack@suse.cz>
Suggested-by: Vladimir Davydov <vdavydov.dev@gmail.com>
Acked-by: Vladimir Davydov <vdavydov.dev@gmail.com>
Cc: Alexander Polakov <apolyakov@beget.ru>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Diffstat (limited to 'fs')
-rw-r--r-- | fs/dcache.c | 5 |
1 files changed, 3 insertions, 2 deletions
diff --git a/fs/dcache.c b/fs/dcache.c index 849c1c1e787b..3000cbb54949 100644 --- a/fs/dcache.c +++ b/fs/dcache.c | |||
@@ -1128,11 +1128,12 @@ void shrink_dcache_sb(struct super_block *sb) | |||
1128 | LIST_HEAD(dispose); | 1128 | LIST_HEAD(dispose); |
1129 | 1129 | ||
1130 | freed = list_lru_walk(&sb->s_dentry_lru, | 1130 | freed = list_lru_walk(&sb->s_dentry_lru, |
1131 | dentry_lru_isolate_shrink, &dispose, UINT_MAX); | 1131 | dentry_lru_isolate_shrink, &dispose, 1024); |
1132 | 1132 | ||
1133 | this_cpu_sub(nr_dentry_unused, freed); | 1133 | this_cpu_sub(nr_dentry_unused, freed); |
1134 | shrink_dentry_list(&dispose); | 1134 | shrink_dentry_list(&dispose); |
1135 | } while (freed > 0); | 1135 | cond_resched(); |
1136 | } while (list_lru_count(&sb->s_dentry_lru) > 0); | ||
1136 | } | 1137 | } |
1137 | EXPORT_SYMBOL(shrink_dcache_sb); | 1138 | EXPORT_SYMBOL(shrink_dcache_sb); |
1138 | 1139 | ||