diff options
author | Linus Torvalds | 2012-12-17 15:39:11 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-17 15:39:11 -0600 |
commit | 9228ff90387e276ad67b10c0eb525c9d6a57d5e9 (patch) | |
tree | e7c87b68daba7cf7ca4c342c6b52165bd78fbe16 /init | |
parent | 9360b53661a2c7754517b2925580055bacc8ec38 (diff) | |
parent | d2ec180c23a5a1bfe34d8638b0342a47c00cf70f (diff) | |
download | kernel-omap-9228ff90387e276ad67b10c0eb525c9d6a57d5e9.tar.gz kernel-omap-9228ff90387e276ad67b10c0eb525c9d6a57d5e9.tar.xz kernel-omap-9228ff90387e276ad67b10c0eb525c9d6a57d5e9.zip |
Merge branch 'for-3.8/drivers' of git://git.kernel.dk/linux-block
Pull block driver update from Jens Axboe:
"Now that the core bits are in, here are the driver bits for 3.8. The
branch contains:
- A huge pile of drbd bits that were dumped from the 3.7 merge
window. Following that, it was both made perfectly clear that
there is going to be no more over-the-wall pulls and how the
situation on individual pulls can be improved.
- A few cleanups from Akinobu Mita for drbd and cciss.
- Queue improvement for loop from Lukas. This grew into adding a
generic interface for waiting/checking an even with a specific
lock, allowing this to be pulled out of md and now loop and drbd is
also using it.
- A few fixes for xen back/front block driver from Roger Pau Monne.
- Partition improvements from Stephen Warren, allowing partiion UUID
to be used as an identifier."
* 'for-3.8/drivers' of git://git.kernel.dk/linux-block: (609 commits)
drbd: update Kconfig to match current dependencies
drbd: Fix drbdsetup wait-connect, wait-sync etc... commands
drbd: close race between drbd_set_role and drbd_connect
drbd: respect no-md-barriers setting also when changed online via disk-options
drbd: Remove obsolete check
drbd: fixup after wait_even_lock_irq() addition to generic code
loop: Limit the number of requests in the bio list
wait: add wait_event_lock_irq() interface
xen-blkfront: free allocated page
xen-blkback: move free persistent grants code
block: partition: msdos: provide UUIDs for partitions
init: reduce PARTUUID min length to 1 from 36
block: store partition_meta_info.uuid as a string
cciss: use check_signature()
cciss: cleanup bitops usage
drbd: use copy_highpage
drbd: if the replication link breaks during handshake, keep retrying
drbd: check return of kmalloc in receive_uuids
drbd: Broadcast sync progress no more often than once per second
drbd: don't try to clear bits once the disk has failed
...
Diffstat (limited to 'init')
-rw-r--r-- | init/do_mounts.c | 61 |
1 files changed, 40 insertions, 21 deletions
diff --git a/init/do_mounts.c b/init/do_mounts.c index f8a66424360d..1d1b6348f903 100644 --- a/init/do_mounts.c +++ b/init/do_mounts.c | |||
@@ -69,23 +69,28 @@ __setup("ro", readonly); | |||
69 | __setup("rw", readwrite); | 69 | __setup("rw", readwrite); |
70 | 70 | ||
71 | #ifdef CONFIG_BLOCK | 71 | #ifdef CONFIG_BLOCK |
72 | struct uuidcmp { | ||
73 | const char *uuid; | ||
74 | int len; | ||
75 | }; | ||
76 | |||
72 | /** | 77 | /** |
73 | * match_dev_by_uuid - callback for finding a partition using its uuid | 78 | * match_dev_by_uuid - callback for finding a partition using its uuid |
74 | * @dev: device passed in by the caller | 79 | * @dev: device passed in by the caller |
75 | * @data: opaque pointer to a 36 byte char array with a UUID | 80 | * @data: opaque pointer to the desired struct uuidcmp to match |
76 | * | 81 | * |
77 | * Returns 1 if the device matches, and 0 otherwise. | 82 | * Returns 1 if the device matches, and 0 otherwise. |
78 | */ | 83 | */ |
79 | static int match_dev_by_uuid(struct device *dev, void *data) | 84 | static int match_dev_by_uuid(struct device *dev, void *data) |
80 | { | 85 | { |
81 | u8 *uuid = data; | 86 | struct uuidcmp *cmp = data; |
82 | struct hd_struct *part = dev_to_part(dev); | 87 | struct hd_struct *part = dev_to_part(dev); |
83 | 88 | ||
84 | if (!part->info) | 89 | if (!part->info) |
85 | goto no_match; | 90 | goto no_match; |
86 | 91 | ||
87 | if (memcmp(uuid, part->info->uuid, sizeof(part->info->uuid))) | 92 | if (strncasecmp(cmp->uuid, part->info->uuid, cmp->len)) |
88 | goto no_match; | 93 | goto no_match; |
89 | 94 | ||
90 | return 1; | 95 | return 1; |
91 | no_match: | 96 | no_match: |
@@ -95,7 +100,7 @@ no_match: | |||
95 | 100 | ||
96 | /** | 101 | /** |
97 | * devt_from_partuuid - looks up the dev_t of a partition by its UUID | 102 | * devt_from_partuuid - looks up the dev_t of a partition by its UUID |
98 | * @uuid: min 36 byte char array containing a hex ascii UUID | 103 | * @uuid: char array containing ascii UUID |
99 | * | 104 | * |
100 | * The function will return the first partition which contains a matching | 105 | * The function will return the first partition which contains a matching |
101 | * UUID value in its partition_meta_info struct. This does not search | 106 | * UUID value in its partition_meta_info struct. This does not search |
@@ -106,38 +111,41 @@ no_match: | |||
106 | * | 111 | * |
107 | * Returns the matching dev_t on success or 0 on failure. | 112 | * Returns the matching dev_t on success or 0 on failure. |
108 | */ | 113 | */ |
109 | static dev_t devt_from_partuuid(char *uuid_str) | 114 | static dev_t devt_from_partuuid(const char *uuid_str) |
110 | { | 115 | { |
111 | dev_t res = 0; | 116 | dev_t res = 0; |
117 | struct uuidcmp cmp; | ||
112 | struct device *dev = NULL; | 118 | struct device *dev = NULL; |
113 | u8 uuid[16]; | ||
114 | struct gendisk *disk; | 119 | struct gendisk *disk; |
115 | struct hd_struct *part; | 120 | struct hd_struct *part; |
116 | int offset = 0; | 121 | int offset = 0; |
122 | bool clear_root_wait = false; | ||
123 | char *slash; | ||
117 | 124 | ||
118 | if (strlen(uuid_str) < 36) | 125 | cmp.uuid = uuid_str; |
119 | goto done; | ||
120 | 126 | ||
127 | slash = strchr(uuid_str, '/'); | ||
121 | /* Check for optional partition number offset attributes. */ | 128 | /* Check for optional partition number offset attributes. */ |
122 | if (uuid_str[36]) { | 129 | if (slash) { |
123 | char c = 0; | 130 | char c = 0; |
124 | /* Explicitly fail on poor PARTUUID syntax. */ | 131 | /* Explicitly fail on poor PARTUUID syntax. */ |
125 | if (sscanf(&uuid_str[36], | 132 | if (sscanf(slash + 1, |
126 | "/PARTNROFF=%d%c", &offset, &c) != 1) { | 133 | "PARTNROFF=%d%c", &offset, &c) != 1) { |
127 | printk(KERN_ERR "VFS: PARTUUID= is invalid.\n" | 134 | clear_root_wait = true; |
128 | "Expected PARTUUID=<valid-uuid-id>[/PARTNROFF=%%d]\n"); | ||
129 | if (root_wait) | ||
130 | printk(KERN_ERR | ||
131 | "Disabling rootwait; root= is invalid.\n"); | ||
132 | root_wait = 0; | ||
133 | goto done; | 135 | goto done; |
134 | } | 136 | } |
137 | cmp.len = slash - uuid_str; | ||
138 | } else { | ||
139 | cmp.len = strlen(uuid_str); | ||
135 | } | 140 | } |
136 | 141 | ||
137 | /* Pack the requested UUID in the expected format. */ | 142 | if (!cmp.len) { |
138 | part_pack_uuid(uuid_str, uuid); | 143 | clear_root_wait = true; |
144 | goto done; | ||
145 | } | ||
139 | 146 | ||
140 | dev = class_find_device(&block_class, NULL, uuid, &match_dev_by_uuid); | 147 | dev = class_find_device(&block_class, NULL, &cmp, |
148 | &match_dev_by_uuid); | ||
141 | if (!dev) | 149 | if (!dev) |
142 | goto done; | 150 | goto done; |
143 | 151 | ||
@@ -158,6 +166,13 @@ static dev_t devt_from_partuuid(char *uuid_str) | |||
158 | no_offset: | 166 | no_offset: |
159 | put_device(dev); | 167 | put_device(dev); |
160 | done: | 168 | done: |
169 | if (clear_root_wait) { | ||
170 | pr_err("VFS: PARTUUID= is invalid.\n" | ||
171 | "Expected PARTUUID=<valid-uuid-id>[/PARTNROFF=%%d]\n"); | ||
172 | if (root_wait) | ||
173 | pr_err("Disabling rootwait; root= is invalid.\n"); | ||
174 | root_wait = 0; | ||
175 | } | ||
161 | return res; | 176 | return res; |
162 | } | 177 | } |
163 | #endif | 178 | #endif |
@@ -174,6 +189,10 @@ done: | |||
174 | * used when disk name of partitioned disk ends on a digit. | 189 | * used when disk name of partitioned disk ends on a digit. |
175 | * 6) PARTUUID=00112233-4455-6677-8899-AABBCCDDEEFF representing the | 190 | * 6) PARTUUID=00112233-4455-6677-8899-AABBCCDDEEFF representing the |
176 | * unique id of a partition if the partition table provides it. | 191 | * unique id of a partition if the partition table provides it. |
192 | * The UUID may be either an EFI/GPT UUID, or refer to an MSDOS | ||
193 | * partition using the format SSSSSSSS-PP, where SSSSSSSS is a zero- | ||
194 | * filled hex representation of the 32-bit "NT disk signature", and PP | ||
195 | * is a zero-filled hex representation of the 1-based partition number. | ||
177 | * 7) PARTUUID=<UUID>/PARTNROFF=<int> to select a partition in relation to | 196 | * 7) PARTUUID=<UUID>/PARTNROFF=<int> to select a partition in relation to |
178 | * a partition with a known unique id. | 197 | * a partition with a known unique id. |
179 | * | 198 | * |