aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorRusty Russell2013-03-14 23:34:17 -0500
committerRusty Russell2013-03-14 23:39:43 -0500
commitb92021b09df70c1609e3547f3d6128dd560be97f (patch)
tree0203752a738c71718f5141b84f5143d1dc8b431d /kernel/modsign_certificate.S
parent4febd95a8a85dd38b1a71fcf9726e19c7fd20039 (diff)
downloadkernel-omap-b92021b09df70c1609e3547f3d6128dd560be97f.tar.gz
kernel-omap-b92021b09df70c1609e3547f3d6128dd560be97f.tar.xz
kernel-omap-b92021b09df70c1609e3547f3d6128dd560be97f.zip
CONFIG_SYMBOL_PREFIX: cleanup.
We have CONFIG_SYMBOL_PREFIX, which three archs define to the string "_". But Al Viro broke this in "consolidate cond_syscall and SYSCALL_ALIAS declarations" (in linux-next), and he's not the first to do so. Using CONFIG_SYMBOL_PREFIX is awkward, since we usually just want to prefix it so something. So various places define helpers which are defined to nothing if CONFIG_SYMBOL_PREFIX isn't set: 1) include/asm-generic/unistd.h defines __SYMBOL_PREFIX. 2) include/asm-generic/vmlinux.lds.h defines VMLINUX_SYMBOL(sym) 3) include/linux/export.h defines MODULE_SYMBOL_PREFIX. 4) include/linux/kernel.h defines SYMBOL_PREFIX (which differs from #7) 5) kernel/modsign_certificate.S defines ASM_SYMBOL(sym) 6) scripts/modpost.c defines MODULE_SYMBOL_PREFIX 7) scripts/Makefile.lib defines SYMBOL_PREFIX on the commandline if CONFIG_SYMBOL_PREFIX is set, so that we have a non-string version for pasting. (arch/h8300/include/asm/linkage.h defines SYMBOL_NAME(), too). Let's solve this properly: 1) No more generic prefix, just CONFIG_HAVE_UNDERSCORE_SYMBOL_PREFIX. 2) Make linux/export.h usable from asm. 3) Define VMLINUX_SYMBOL() and VMLINUX_SYMBOL_STR(). 4) Make everyone use them. Signed-off-by: Rusty Russell <rusty@rustcorp.com.au> Reviewed-by: James Hogan <james.hogan@imgtec.com> Tested-by: James Hogan <james.hogan@imgtec.com> (metag)
Diffstat (limited to 'kernel/modsign_certificate.S')
-rw-r--r--kernel/modsign_certificate.S13
1 files changed, 3 insertions, 10 deletions
diff --git a/kernel/modsign_certificate.S b/kernel/modsign_certificate.S
index 246b4c6e6135..4a9a86d12c8b 100644
--- a/kernel/modsign_certificate.S
+++ b/kernel/modsign_certificate.S
@@ -1,15 +1,8 @@
1/* SYMBOL_PREFIX defined on commandline from CONFIG_SYMBOL_PREFIX */ 1#include <linux/export.h>
2#ifndef SYMBOL_PREFIX
3#define ASM_SYMBOL(sym) sym
4#else
5#define PASTE2(x,y) x##y
6#define PASTE(x,y) PASTE2(x,y)
7#define ASM_SYMBOL(sym) PASTE(SYMBOL_PREFIX, sym)
8#endif
9 2
10#define GLOBAL(name) \ 3#define GLOBAL(name) \
11 .globl ASM_SYMBOL(name); \ 4 .globl VMLINUX_SYMBOL(name); \
12 ASM_SYMBOL(name): 5 VMLINUX_SYMBOL(name):
13 6
14 .section ".init.data","aw" 7 .section ".init.data","aw"
15 8