aboutsummaryrefslogtreecommitdiffstats
path: root/lib
diff options
context:
space:
mode:
authorOleg Nesterov2012-12-17 18:01:36 -0600
committerLinus Torvalds2012-12-17 19:15:18 -0600
commit9390ef0c85fd065f01045fef708b046c98cda04c (patch)
tree22ae17e0d07a9386cd494a869f60df757cfc56d7 /lib
parenta1fd3e24d8a484b3265a6d485202afe093c058f3 (diff)
downloadkernel-omap-9390ef0c85fd065f01045fef708b046c98cda04c.tar.gz
kernel-omap-9390ef0c85fd065f01045fef708b046c98cda04c.tar.xz
kernel-omap-9390ef0c85fd065f01045fef708b046c98cda04c.zip
percpu_rw_semaphore: kill ->writer_mutex, add ->write_ctr
percpu_rw_semaphore->writer_mutex was only added to simplify the initial rewrite, the only thing it protects is clear_fast_ctr() which otherwise could be called by multiple writers. ->rw_sem is enough to serialize the writers. Kill this mutex and add "atomic_t write_ctr" instead. The writers increment/decrement this counter, the readers check it is zero instead of mutex_is_locked(). Move atomic_add(clear_fast_ctr(), slow_read_ctr) under down_write() to avoid the race with other writers. This is a bit sub-optimal, only the first writer needs this and we do not need to exclude the readers at this stage. But this is simple, we do not want another internal lock until we add more features. And this speeds up the write-contended case. Before this patch the racing writers sleep in synchronize_sched_expedited() sequentially, with this patch multiple synchronize_sched_expedited's can "overlap" with each other. Note: we can do more optimizations, this is only the first step. Signed-off-by: Oleg Nesterov <oleg@redhat.com> Cc: Anton Arapov <anton@redhat.com> Cc: Ingo Molnar <mingo@elte.hu> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Michal Marek <mmarek@suse.cz> Cc: Mikulas Patocka <mpatocka@redhat.com> Cc: "Paul E. McKenney" <paulmck@linux.vnet.ibm.com> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Srikar Dronamraju <srikar@linux.vnet.ibm.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'lib')
-rw-r--r--lib/percpu-rwsem.c34
1 files changed, 16 insertions, 18 deletions
diff --git a/lib/percpu-rwsem.c b/lib/percpu-rwsem.c
index 2e03bcfe48f9..ce92ab563a08 100644
--- a/lib/percpu-rwsem.c
+++ b/lib/percpu-rwsem.c
@@ -1,4 +1,4 @@
1#include <linux/mutex.h> 1#include <linux/atomic.h>
2#include <linux/rwsem.h> 2#include <linux/rwsem.h>
3#include <linux/percpu.h> 3#include <linux/percpu.h>
4#include <linux/wait.h> 4#include <linux/wait.h>
@@ -13,8 +13,8 @@ int percpu_init_rwsem(struct percpu_rw_semaphore *brw)
13 if (unlikely(!brw->fast_read_ctr)) 13 if (unlikely(!brw->fast_read_ctr))
14 return -ENOMEM; 14 return -ENOMEM;
15 15
16 mutex_init(&brw->writer_mutex);
17 init_rwsem(&brw->rw_sem); 16 init_rwsem(&brw->rw_sem);
17 atomic_set(&brw->write_ctr, 0);
18 atomic_set(&brw->slow_read_ctr, 0); 18 atomic_set(&brw->slow_read_ctr, 0);
19 init_waitqueue_head(&brw->write_waitq); 19 init_waitqueue_head(&brw->write_waitq);
20 return 0; 20 return 0;
@@ -28,7 +28,7 @@ void percpu_free_rwsem(struct percpu_rw_semaphore *brw)
28 28
29/* 29/*
30 * This is the fast-path for down_read/up_read, it only needs to ensure 30 * This is the fast-path for down_read/up_read, it only needs to ensure
31 * there is no pending writer (!mutex_is_locked() check) and inc/dec the 31 * there is no pending writer (atomic_read(write_ctr) == 0) and inc/dec the
32 * fast per-cpu counter. The writer uses synchronize_sched_expedited() to 32 * fast per-cpu counter. The writer uses synchronize_sched_expedited() to
33 * serialize with the preempt-disabled section below. 33 * serialize with the preempt-disabled section below.
34 * 34 *
@@ -44,7 +44,7 @@ void percpu_free_rwsem(struct percpu_rw_semaphore *brw)
44 * If this helper fails the callers rely on the normal rw_semaphore and 44 * If this helper fails the callers rely on the normal rw_semaphore and
45 * atomic_dec_and_test(), so in this case we have the necessary barriers. 45 * atomic_dec_and_test(), so in this case we have the necessary barriers.
46 * 46 *
47 * But if it succeeds we do not have any barriers, mutex_is_locked() or 47 * But if it succeeds we do not have any barriers, atomic_read(write_ctr) or
48 * __this_cpu_add() below can be reordered with any LOAD/STORE done by the 48 * __this_cpu_add() below can be reordered with any LOAD/STORE done by the
49 * reader inside the critical section. See the comments in down_write and 49 * reader inside the critical section. See the comments in down_write and
50 * up_write below. 50 * up_write below.
@@ -54,7 +54,7 @@ static bool update_fast_ctr(struct percpu_rw_semaphore *brw, unsigned int val)
54 bool success = false; 54 bool success = false;
55 55
56 preempt_disable(); 56 preempt_disable();
57 if (likely(!mutex_is_locked(&brw->writer_mutex))) { 57 if (likely(!atomic_read(&brw->write_ctr))) {
58 __this_cpu_add(*brw->fast_read_ctr, val); 58 __this_cpu_add(*brw->fast_read_ctr, val);
59 success = true; 59 success = true;
60 } 60 }
@@ -101,9 +101,8 @@ static int clear_fast_ctr(struct percpu_rw_semaphore *brw)
101} 101}
102 102
103/* 103/*
104 * A writer takes ->writer_mutex to exclude other writers and to force the 104 * A writer increments ->write_ctr to force the readers to switch to the
105 * readers to switch to the slow mode, note the mutex_is_locked() check in 105 * slow mode, note the atomic_read() check in update_fast_ctr().
106 * update_fast_ctr().
107 * 106 *
108 * After that the readers can only inc/dec the slow ->slow_read_ctr counter, 107 * After that the readers can only inc/dec the slow ->slow_read_ctr counter,
109 * ->fast_read_ctr is stable. Once the writer moves its sum into the slow 108 * ->fast_read_ctr is stable. Once the writer moves its sum into the slow
@@ -114,11 +113,10 @@ static int clear_fast_ctr(struct percpu_rw_semaphore *brw)
114 */ 113 */
115void percpu_down_write(struct percpu_rw_semaphore *brw) 114void percpu_down_write(struct percpu_rw_semaphore *brw)
116{ 115{
117 /* also blocks update_fast_ctr() which checks mutex_is_locked() */ 116 /* tell update_fast_ctr() there is a pending writer */
118 mutex_lock(&brw->writer_mutex); 117 atomic_inc(&brw->write_ctr);
119
120 /* 118 /*
121 * 1. Ensures mutex_is_locked() is visible to any down_read/up_read 119 * 1. Ensures that write_ctr != 0 is visible to any down_read/up_read
122 * so that update_fast_ctr() can't succeed. 120 * so that update_fast_ctr() can't succeed.
123 * 121 *
124 * 2. Ensures we see the result of every previous this_cpu_add() in 122 * 2. Ensures we see the result of every previous this_cpu_add() in
@@ -130,25 +128,25 @@ void percpu_down_write(struct percpu_rw_semaphore *brw)
130 */ 128 */
131 synchronize_sched_expedited(); 129 synchronize_sched_expedited();
132 130
131 /* exclude other writers, and block the new readers completely */
132 down_write(&brw->rw_sem);
133
133 /* nobody can use fast_read_ctr, move its sum into slow_read_ctr */ 134 /* nobody can use fast_read_ctr, move its sum into slow_read_ctr */
134 atomic_add(clear_fast_ctr(brw), &brw->slow_read_ctr); 135 atomic_add(clear_fast_ctr(brw), &brw->slow_read_ctr);
135 136
136 /* block the new readers completely */
137 down_write(&brw->rw_sem);
138
139 /* wait for all readers to complete their percpu_up_read() */ 137 /* wait for all readers to complete their percpu_up_read() */
140 wait_event(brw->write_waitq, !atomic_read(&brw->slow_read_ctr)); 138 wait_event(brw->write_waitq, !atomic_read(&brw->slow_read_ctr));
141} 139}
142 140
143void percpu_up_write(struct percpu_rw_semaphore *brw) 141void percpu_up_write(struct percpu_rw_semaphore *brw)
144{ 142{
145 /* allow the new readers, but only the slow-path */ 143 /* release the lock, but the readers can't use the fast-path */
146 up_write(&brw->rw_sem); 144 up_write(&brw->rw_sem);
147
148 /* 145 /*
149 * Insert the barrier before the next fast-path in down_read, 146 * Insert the barrier before the next fast-path in down_read,
150 * see W_R case in the comment above update_fast_ctr(). 147 * see W_R case in the comment above update_fast_ctr().
151 */ 148 */
152 synchronize_sched_expedited(); 149 synchronize_sched_expedited();
153 mutex_unlock(&brw->writer_mutex); 150 /* the last writer unblocks update_fast_ctr() */
151 atomic_dec(&brw->write_ctr);
154} 152}