diff options
author | Linus Torvalds | 2012-10-12 20:20:11 -0500 |
---|---|---|
committer | Linus Torvalds | 2012-10-12 20:20:11 -0500 |
commit | ade0899b298ba2c43bfd6abd8cbc2545944cde0c (patch) | |
tree | a448dfb440b3b958b6306bb43620cd5d76f504bf /tools/perf/Makefile | |
parent | 871a0596cb2f51b57dc583d1a7c4be0186582fe7 (diff) | |
parent | 95cf59ea72331d0093010543b8951bb43f262cac (diff) | |
download | kernel-omap-ade0899b298ba2c43bfd6abd8cbc2545944cde0c.tar.gz kernel-omap-ade0899b298ba2c43bfd6abd8cbc2545944cde0c.tar.xz kernel-omap-ade0899b298ba2c43bfd6abd8cbc2545944cde0c.zip |
Merge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip
Pull perf updates from Ingo Molnar:
"This tree includes some late late perf items that missed the first
round:
tools:
- Bash auto completion improvements, now we can auto complete the
tools long options, tracepoint event names, etc, from Namhyung Kim.
- Look up thread using tid instead of pid in 'perf sched'.
- Move global variables into a perf_kvm struct, from David Ahern.
- Hists refactorings, preparatory for improved 'diff' command, from
Jiri Olsa.
- Hists refactorings, preparatory for event group viewieng work, from
Namhyung Kim.
- Remove double negation on optional feature macro definitions, from
Namhyung Kim.
- Remove several cases of needless global variables, on most
builtins.
- misc fixes
kernel:
- sysfs support for IBS on AMD CPUs, from Robert Richter.
- Support for an upcoming Intel CPU, the Xeon-Phi / Knights Corner
HPC blade PMU, from Vince Weaver.
- misc fixes"
* 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: (46 commits)
perf: Fix perf_cgroup_switch for sw-events
perf: Clarify perf_cpu_context::active_pmu usage by renaming it to ::unique_pmu
perf/AMD/IBS: Add sysfs support
perf hists: Add more helpers for hist entry stat
perf hists: Move he->stat.nr_events initialization to a template
perf hists: Introduce struct he_stat
perf diff: Removing the total_period argument from output code
perf tool: Add hpp interface to enable/disable hpp column
perf tools: Removing hists pair argument from output path
perf hists: Separate overhead and baseline columns
perf diff: Refactor diff displacement possition info
perf hists: Add struct hists pointer to struct hist_entry
perf tools: Complete tracepoint event names
perf/x86: Add support for Intel Xeon-Phi Knights Corner PMU
perf evlist: Remove some unused methods
perf evlist: Introduce add_newtp method
perf kvm: Move global variables into a perf_kvm struct
perf tools: Convert to BACKTRACE_SUPPORT
perf tools: Long option completion support for each subcommands
perf tools: Complete long option names of perf command
...
Diffstat (limited to 'tools/perf/Makefile')
-rw-r--r-- | tools/perf/Makefile | 83 |
1 files changed, 29 insertions, 54 deletions
diff --git a/tools/perf/Makefile b/tools/perf/Makefile index 9546ff58f024..247264502fb7 100644 --- a/tools/perf/Makefile +++ b/tools/perf/Makefile | |||
@@ -45,6 +45,8 @@ include config/utilities.mak | |||
45 | # | 45 | # |
46 | # Define NO_LIBUNWIND if you do not want libunwind dependency for dwarf | 46 | # Define NO_LIBUNWIND if you do not want libunwind dependency for dwarf |
47 | # backtrace post unwind. | 47 | # backtrace post unwind. |
48 | # | ||
49 | # Define NO_BACKTRACE if you do not want stack backtrace debug feature | ||
48 | 50 | ||
49 | $(OUTPUT)PERF-VERSION-FILE: .FORCE-PERF-VERSION-FILE | 51 | $(OUTPUT)PERF-VERSION-FILE: .FORCE-PERF-VERSION-FILE |
50 | @$(SHELL_PATH) util/PERF-VERSION-GEN $(OUTPUT) | 52 | @$(SHELL_PATH) util/PERF-VERSION-GEN $(OUTPUT) |
@@ -185,7 +187,7 @@ strip-libs = $(filter-out -l%,$(1)) | |||
185 | PYTHON_EXT_SRCS := $(shell grep -v ^\# util/python-ext-sources) | 187 | PYTHON_EXT_SRCS := $(shell grep -v ^\# util/python-ext-sources) |
186 | PYTHON_EXT_DEPS := util/python-ext-sources util/setup.py | 188 | PYTHON_EXT_DEPS := util/python-ext-sources util/setup.py |
187 | 189 | ||
188 | $(OUTPUT)python/perf.so: $(PYRF_OBJS) $(PYTHON_EXT_SRCS) $(PYTHON_EXT_DEPS) | 190 | $(OUTPUT)python/perf.so: $(PYTHON_EXT_SRCS) $(PYTHON_EXT_DEPS) |
189 | $(QUIET_GEN)CFLAGS='$(BASIC_CFLAGS)' $(PYTHON_WORD) util/setup.py \ | 191 | $(QUIET_GEN)CFLAGS='$(BASIC_CFLAGS)' $(PYTHON_WORD) util/setup.py \ |
190 | --quiet build_ext; \ | 192 | --quiet build_ext; \ |
191 | mkdir -p $(OUTPUT)python && \ | 193 | mkdir -p $(OUTPUT)python && \ |
@@ -447,20 +449,6 @@ BUILTIN_OBJS += $(OUTPUT)builtin-inject.o | |||
447 | 449 | ||
448 | PERFLIBS = $(LIB_FILE) $(LIBTRACEEVENT) | 450 | PERFLIBS = $(LIB_FILE) $(LIBTRACEEVENT) |
449 | 451 | ||
450 | # Files needed for the python binding, perf.so | ||
451 | # pyrf is just an internal name needed for all those wrappers. | ||
452 | # This has to be in sync with what is in the 'sources' variable in | ||
453 | # tools/perf/util/setup.py | ||
454 | |||
455 | PYRF_OBJS += $(OUTPUT)util/cpumap.o | ||
456 | PYRF_OBJS += $(OUTPUT)util/ctype.o | ||
457 | PYRF_OBJS += $(OUTPUT)util/evlist.o | ||
458 | PYRF_OBJS += $(OUTPUT)util/evsel.o | ||
459 | PYRF_OBJS += $(OUTPUT)util/python.o | ||
460 | PYRF_OBJS += $(OUTPUT)util/thread_map.o | ||
461 | PYRF_OBJS += $(OUTPUT)util/util.o | ||
462 | PYRF_OBJS += $(OUTPUT)util/xyarray.o | ||
463 | |||
464 | # | 452 | # |
465 | # Platform specific tweaks | 453 | # Platform specific tweaks |
466 | # | 454 | # |
@@ -487,7 +475,13 @@ ifneq ($(call try-cc,$(SOURCE_LIBELF),$(FLAGS_LIBELF)),y) | |||
487 | NO_DWARF := 1 | 475 | NO_DWARF := 1 |
488 | NO_DEMANGLE := 1 | 476 | NO_DEMANGLE := 1 |
489 | endif | 477 | endif |
490 | endif | 478 | else |
479 | FLAGS_DWARF=$(ALL_CFLAGS) -ldw -lelf $(ALL_LDFLAGS) $(EXTLIBS) | ||
480 | ifneq ($(call try-cc,$(SOURCE_DWARF),$(FLAGS_DWARF)),y) | ||
481 | msg := $(warning No libdw.h found or old libdw.h found or elfutils is older than 0.138, disables dwarf support. Please install new elfutils-devel/libdw-dev); | ||
482 | NO_DWARF := 1 | ||
483 | endif # Dwarf support | ||
484 | endif # SOURCE_LIBELF | ||
491 | endif # NO_LIBELF | 485 | endif # NO_LIBELF |
492 | 486 | ||
493 | ifndef NO_LIBUNWIND | 487 | ifndef NO_LIBUNWIND |
@@ -512,8 +506,6 @@ ifneq ($(OUTPUT),) | |||
512 | endif | 506 | endif |
513 | 507 | ||
514 | ifdef NO_LIBELF | 508 | ifdef NO_LIBELF |
515 | BASIC_CFLAGS += -DNO_LIBELF_SUPPORT | ||
516 | |||
517 | EXTLIBS := $(filter-out -lelf,$(EXTLIBS)) | 509 | EXTLIBS := $(filter-out -lelf,$(EXTLIBS)) |
518 | 510 | ||
519 | # Remove ELF/DWARF dependent codes | 511 | # Remove ELF/DWARF dependent codes |
@@ -528,17 +520,12 @@ BUILTIN_OBJS := $(filter-out $(OUTPUT)builtin-probe.o,$(BUILTIN_OBJS)) | |||
528 | LIB_OBJS += $(OUTPUT)util/symbol-minimal.o | 520 | LIB_OBJS += $(OUTPUT)util/symbol-minimal.o |
529 | 521 | ||
530 | else # NO_LIBELF | 522 | else # NO_LIBELF |
523 | BASIC_CFLAGS += -DLIBELF_SUPPORT | ||
531 | 524 | ||
532 | ifneq ($(call try-cc,$(SOURCE_ELF_MMAP),$(FLAGS_COMMON)),y) | 525 | ifeq ($(call try-cc,$(SOURCE_ELF_MMAP),$(FLAGS_COMMON)),y) |
533 | BASIC_CFLAGS += -DLIBELF_NO_MMAP | 526 | BASIC_CFLAGS += -DLIBELF_MMAP |
534 | endif | 527 | endif |
535 | 528 | ||
536 | FLAGS_DWARF=$(ALL_CFLAGS) -ldw -lelf $(ALL_LDFLAGS) $(EXTLIBS) | ||
537 | ifneq ($(call try-cc,$(SOURCE_DWARF),$(FLAGS_DWARF)),y) | ||
538 | msg := $(warning No libdw.h found or old libdw.h found or elfutils is older than 0.138, disables dwarf support. Please install new elfutils-devel/libdw-dev); | ||
539 | NO_DWARF := 1 | ||
540 | endif # Dwarf support | ||
541 | |||
542 | ifndef NO_DWARF | 529 | ifndef NO_DWARF |
543 | ifeq ($(origin PERF_HAVE_DWARF_REGS), undefined) | 530 | ifeq ($(origin PERF_HAVE_DWARF_REGS), undefined) |
544 | msg := $(warning DWARF register mappings have not been defined for architecture $(ARCH), DWARF support disabled); | 531 | msg := $(warning DWARF register mappings have not been defined for architecture $(ARCH), DWARF support disabled); |
@@ -551,38 +538,33 @@ endif # PERF_HAVE_DWARF_REGS | |||
551 | endif # NO_DWARF | 538 | endif # NO_DWARF |
552 | endif # NO_LIBELF | 539 | endif # NO_LIBELF |
553 | 540 | ||
554 | ifdef NO_LIBUNWIND | 541 | ifndef NO_LIBUNWIND |
555 | BASIC_CFLAGS += -DNO_LIBUNWIND_SUPPORT | 542 | BASIC_CFLAGS += -DLIBUNWIND_SUPPORT |
556 | else | ||
557 | EXTLIBS += $(LIBUNWIND_LIBS) | 543 | EXTLIBS += $(LIBUNWIND_LIBS) |
558 | BASIC_CFLAGS := $(LIBUNWIND_CFLAGS) $(BASIC_CFLAGS) | 544 | BASIC_CFLAGS := $(LIBUNWIND_CFLAGS) $(BASIC_CFLAGS) |
559 | BASIC_LDFLAGS := $(LIBUNWIND_LDFLAGS) $(BASIC_LDFLAGS) | 545 | BASIC_LDFLAGS := $(LIBUNWIND_LDFLAGS) $(BASIC_LDFLAGS) |
560 | LIB_OBJS += $(OUTPUT)util/unwind.o | 546 | LIB_OBJS += $(OUTPUT)util/unwind.o |
561 | endif | 547 | endif |
562 | 548 | ||
563 | ifdef NO_LIBAUDIT | 549 | ifndef NO_LIBAUDIT |
564 | BASIC_CFLAGS += -DNO_LIBAUDIT_SUPPORT | ||
565 | else | ||
566 | FLAGS_LIBAUDIT = $(ALL_CFLAGS) $(ALL_LDFLAGS) -laudit | 550 | FLAGS_LIBAUDIT = $(ALL_CFLAGS) $(ALL_LDFLAGS) -laudit |
567 | ifneq ($(call try-cc,$(SOURCE_LIBAUDIT),$(FLAGS_LIBAUDIT)),y) | 551 | ifneq ($(call try-cc,$(SOURCE_LIBAUDIT),$(FLAGS_LIBAUDIT)),y) |
568 | msg := $(warning No libaudit.h found, disables 'trace' tool, please install audit-libs-devel or libaudit-dev); | 552 | msg := $(warning No libaudit.h found, disables 'trace' tool, please install audit-libs-devel or libaudit-dev); |
569 | BASIC_CFLAGS += -DNO_LIBAUDIT_SUPPORT | ||
570 | else | 553 | else |
554 | BASIC_CFLAGS += -DLIBAUDIT_SUPPORT | ||
571 | BUILTIN_OBJS += $(OUTPUT)builtin-trace.o | 555 | BUILTIN_OBJS += $(OUTPUT)builtin-trace.o |
572 | EXTLIBS += -laudit | 556 | EXTLIBS += -laudit |
573 | endif | 557 | endif |
574 | endif | 558 | endif |
575 | 559 | ||
576 | ifdef NO_NEWT | 560 | ifndef NO_NEWT |
577 | BASIC_CFLAGS += -DNO_NEWT_SUPPORT | ||
578 | else | ||
579 | FLAGS_NEWT=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) -lnewt | 561 | FLAGS_NEWT=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) -lnewt |
580 | ifneq ($(call try-cc,$(SOURCE_NEWT),$(FLAGS_NEWT)),y) | 562 | ifneq ($(call try-cc,$(SOURCE_NEWT),$(FLAGS_NEWT)),y) |
581 | msg := $(warning newt not found, disables TUI support. Please install newt-devel or libnewt-dev); | 563 | msg := $(warning newt not found, disables TUI support. Please install newt-devel or libnewt-dev); |
582 | BASIC_CFLAGS += -DNO_NEWT_SUPPORT | ||
583 | else | 564 | else |
584 | # Fedora has /usr/include/slang/slang.h, but ubuntu /usr/include/slang.h | 565 | # Fedora has /usr/include/slang/slang.h, but ubuntu /usr/include/slang.h |
585 | BASIC_CFLAGS += -I/usr/include/slang | 566 | BASIC_CFLAGS += -I/usr/include/slang |
567 | BASIC_CFLAGS += -DNEWT_SUPPORT | ||
586 | EXTLIBS += -lnewt -lslang | 568 | EXTLIBS += -lnewt -lslang |
587 | LIB_OBJS += $(OUTPUT)ui/setup.o | 569 | LIB_OBJS += $(OUTPUT)ui/setup.o |
588 | LIB_OBJS += $(OUTPUT)ui/browser.o | 570 | LIB_OBJS += $(OUTPUT)ui/browser.o |
@@ -604,17 +586,15 @@ else | |||
604 | endif | 586 | endif |
605 | endif | 587 | endif |
606 | 588 | ||
607 | ifdef NO_GTK2 | 589 | ifndef NO_GTK2 |
608 | BASIC_CFLAGS += -DNO_GTK2_SUPPORT | ||
609 | else | ||
610 | FLAGS_GTK2=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) $(shell pkg-config --libs --cflags gtk+-2.0 2>/dev/null) | 590 | FLAGS_GTK2=$(ALL_CFLAGS) $(ALL_LDFLAGS) $(EXTLIBS) $(shell pkg-config --libs --cflags gtk+-2.0 2>/dev/null) |
611 | ifneq ($(call try-cc,$(SOURCE_GTK2),$(FLAGS_GTK2)),y) | 591 | ifneq ($(call try-cc,$(SOURCE_GTK2),$(FLAGS_GTK2)),y) |
612 | msg := $(warning GTK2 not found, disables GTK2 support. Please install gtk2-devel or libgtk2.0-dev); | 592 | msg := $(warning GTK2 not found, disables GTK2 support. Please install gtk2-devel or libgtk2.0-dev); |
613 | BASIC_CFLAGS += -DNO_GTK2_SUPPORT | ||
614 | else | 593 | else |
615 | ifeq ($(call try-cc,$(SOURCE_GTK2_INFOBAR),$(FLAGS_GTK2)),y) | 594 | ifeq ($(call try-cc,$(SOURCE_GTK2_INFOBAR),$(FLAGS_GTK2)),y) |
616 | BASIC_CFLAGS += -DHAVE_GTK_INFO_BAR | 595 | BASIC_CFLAGS += -DHAVE_GTK_INFO_BAR |
617 | endif | 596 | endif |
597 | BASIC_CFLAGS += -DGTK2_SUPPORT | ||
618 | BASIC_CFLAGS += $(shell pkg-config --cflags gtk+-2.0 2>/dev/null) | 598 | BASIC_CFLAGS += $(shell pkg-config --cflags gtk+-2.0 2>/dev/null) |
619 | EXTLIBS += $(shell pkg-config --libs gtk+-2.0 2>/dev/null) | 599 | EXTLIBS += $(shell pkg-config --libs gtk+-2.0 2>/dev/null) |
620 | LIB_OBJS += $(OUTPUT)ui/gtk/browser.o | 600 | LIB_OBJS += $(OUTPUT)ui/gtk/browser.o |
@@ -622,7 +602,7 @@ else | |||
622 | LIB_OBJS += $(OUTPUT)ui/gtk/util.o | 602 | LIB_OBJS += $(OUTPUT)ui/gtk/util.o |
623 | LIB_OBJS += $(OUTPUT)ui/gtk/helpline.o | 603 | LIB_OBJS += $(OUTPUT)ui/gtk/helpline.o |
624 | # Make sure that it'd be included only once. | 604 | # Make sure that it'd be included only once. |
625 | ifneq ($(findstring -DNO_NEWT_SUPPORT,$(BASIC_CFLAGS)),) | 605 | ifeq ($(findstring -DNEWT_SUPPORT,$(BASIC_CFLAGS)),) |
626 | LIB_OBJS += $(OUTPUT)ui/setup.o | 606 | LIB_OBJS += $(OUTPUT)ui/setup.o |
627 | LIB_OBJS += $(OUTPUT)ui/util.o | 607 | LIB_OBJS += $(OUTPUT)ui/util.o |
628 | endif | 608 | endif |
@@ -763,23 +743,18 @@ ifeq ($(NO_PERF_REGS),0) | |||
763 | ifeq ($(ARCH),x86) | 743 | ifeq ($(ARCH),x86) |
764 | LIB_H += arch/x86/include/perf_regs.h | 744 | LIB_H += arch/x86/include/perf_regs.h |
765 | endif | 745 | endif |
766 | else | 746 | BASIC_CFLAGS += -DHAVE_PERF_REGS |
767 | BASIC_CFLAGS += -DNO_PERF_REGS | ||
768 | endif | 747 | endif |
769 | 748 | ||
770 | ifdef NO_STRLCPY | 749 | ifndef NO_STRLCPY |
771 | BASIC_CFLAGS += -DNO_STRLCPY | 750 | ifeq ($(call try-cc,$(SOURCE_STRLCPY),),y) |
772 | else | 751 | BASIC_CFLAGS += -DHAVE_STRLCPY |
773 | ifneq ($(call try-cc,$(SOURCE_STRLCPY),),y) | ||
774 | BASIC_CFLAGS += -DNO_STRLCPY | ||
775 | endif | 752 | endif |
776 | endif | 753 | endif |
777 | 754 | ||
778 | ifdef NO_BACKTRACE | 755 | ifndef NO_BACKTRACE |
779 | BASIC_CFLAGS += -DNO_BACKTRACE | 756 | ifeq ($(call try-cc,$(SOURCE_BACKTRACE),),y) |
780 | else | 757 | BASIC_CFLAGS += -DBACKTRACE_SUPPORT |
781 | ifneq ($(call try-cc,$(SOURCE_BACKTRACE),),y) | ||
782 | BASIC_CFLAGS += -DNO_BACKTRACE | ||
783 | endif | 758 | endif |
784 | endif | 759 | endif |
785 | 760 | ||