diff options
author | David Howells | 2012-11-19 16:21:03 -0600 |
---|---|---|
committer | David Howells | 2012-11-19 16:21:03 -0600 |
commit | d2709c7ce4c513ab7f4ca9a106a930621811f2d3 (patch) | |
tree | da6e14e27b02b2d234aad0eb1ccf5bbfa06d0cb8 /tools/perf/Makefile | |
parent | f2d9cae9ea9e0228f6eb4d4c5ab4f548d0270d1a (diff) | |
download | kernel-omap-d2709c7ce4c513ab7f4ca9a106a930621811f2d3.tar.gz kernel-omap-d2709c7ce4c513ab7f4ca9a106a930621811f2d3.tar.xz kernel-omap-d2709c7ce4c513ab7f4ca9a106a930621811f2d3.zip |
perf: Make perf build for x86 with UAPI disintegration applied
Make perf build for x86 once the UAPI disintegration patches for that arch
have been applied by adding the appropriate -I flags - in the right order -
and then converting some #includes that use ../.. notation to find main kernel
headerfiles to use <asm/foo.h> and <linux/foo.h> instead.
Note that -Iarch/foo/include/uapi is present _before_ -Iarch/foo/include.
This makes sure we get the userspace version of the pt_regs struct. Ideally,
we wouldn't have the latter -I flag at all, but unfortunately we want
asm/svm.h and asm/vmx.h in builtin-kvm.c and these aren't part of the UAPI -
at least not for x86. I wonder if the bits outside of the __KERNEL__ guards
*should* be transferred there.
I note also that perf seems to do its dependency handling manually by listing
all the header files it might want to use in LIB_H in the Makefile. Can this
be changed to use -MD?
Note that to do make this work, we need to export and UAPI disintegrate
linux/hw_breakpoint.h, which I think should've been exported previously so that
perf can access the bits. We have to do this in the same patch to maintain
bisectability.
Signed-off-by: David Howells <dhowells@redhat.com>
Diffstat (limited to 'tools/perf/Makefile')
-rw-r--r-- | tools/perf/Makefile | 29 |
1 files changed, 28 insertions, 1 deletions
diff --git a/tools/perf/Makefile b/tools/perf/Makefile index 00deed4d6159..0a619af5be43 100644 --- a/tools/perf/Makefile +++ b/tools/perf/Makefile | |||
@@ -169,7 +169,34 @@ endif | |||
169 | 169 | ||
170 | ### --- END CONFIGURATION SECTION --- | 170 | ### --- END CONFIGURATION SECTION --- |
171 | 171 | ||
172 | BASIC_CFLAGS = -Iutil/include -Iarch/$(ARCH)/include -I$(OUTPUT)util -I$(TRACE_EVENT_DIR) -D_LARGEFILE64_SOURCE -D_FILE_OFFSET_BITS=64 -D_GNU_SOURCE | 172 | ifeq ($(srctree),) |
173 | srctree := $(patsubst %/,%,$(dir $(shell pwd))) | ||
174 | srctree := $(patsubst %/,%,$(dir $(srctree))) | ||
175 | #$(info Determined 'srctree' to be $(srctree)) | ||
176 | endif | ||
177 | |||
178 | ifneq ($(objtree),) | ||
179 | #$(info Determined 'objtree' to be $(objtree)) | ||
180 | endif | ||
181 | |||
182 | ifneq ($(OUTPUT),) | ||
183 | #$(info Determined 'OUTPUT' to be $(OUTPUT)) | ||
184 | endif | ||
185 | |||
186 | BASIC_CFLAGS = \ | ||
187 | -Iutil/include \ | ||
188 | -Iarch/$(ARCH)/include \ | ||
189 | $(if $(objtree),-I$(objtree)/arch/$(ARCH)/include/generated/uapi) \ | ||
190 | -I$(srctree)/arch/$(ARCH)/include/uapi \ | ||
191 | -I$(srctree)/arch/$(ARCH)/include \ | ||
192 | $(if $(objtree),-I$(objtree)/include/generated/uapi) \ | ||
193 | -I$(srctree)/include/uapi \ | ||
194 | -I$(srctree)/include \ | ||
195 | -I$(OUTPUT)util \ | ||
196 | -Iutil \ | ||
197 | -I. \ | ||
198 | -I$(TRACE_EVENT_DIR) \ | ||
199 | -D_LARGEFILE64_SOURCE -D_FILE_OFFSET_BITS=64 -D_GNU_SOURCE | ||
173 | BASIC_LDFLAGS = | 200 | BASIC_LDFLAGS = |
174 | 201 | ||
175 | # Guard against environment variables | 202 | # Guard against environment variables |