diff options
author | Linus Torvalds | 2012-12-11 20:14:31 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-11 20:14:31 -0600 |
commit | 090f8ccba37034cec5a5972a70abeaae7eb0222b (patch) | |
tree | 0b7cf8a4bb94601816399acfb336835fbf309a2a /tools/perf/builtin-stat.c | |
parent | aefb058b0c27dafb15072406fbfd92d2ac2c8790 (diff) | |
parent | cc1b39dbf9f55a438e8a21a694394c20e6a17129 (diff) | |
download | kernel-omap-090f8ccba37034cec5a5972a70abeaae7eb0222b.tar.gz kernel-omap-090f8ccba37034cec5a5972a70abeaae7eb0222b.tar.xz kernel-omap-090f8ccba37034cec5a5972a70abeaae7eb0222b.zip |
Merge branch 'perf-core-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip
Pull perf updates from Ingo Molnar:
"Lots of activity:
211 files changed, 8328 insertions(+), 4116 deletions(-)
most of it on the tooling side.
Main changes:
* ftrace enhancements and fixes from Steve Rostedt.
* uprobes fixes, cleanups and preparation for the ARM port from Oleg
Nesterov.
* UAPI fixes, from David Howels - prepares the arch/x86 UAPI
transition
* Separate perf tests into multiple objects, one per test, from Jiri
Olsa.
* Make hardware event translations available in sysfs, from Jiri
Olsa.
* Fixes to /proc/pid/maps parsing, preparatory to supporting data
maps, from Namhyung Kim
* Implement ui_progress for GTK, from Namhyung Kim
* Add framework for automated perf_event_attr tests, where tools with
different command line options will be run from a 'perf test', via
python glue, and the perf syscall will be intercepted to verify
that the perf_event_attr fields set by the tool are those expected,
from Jiri Olsa
* Add a 'link' method for hists, so that we can have the leader with
buckets for all the entries in all the hists. This new method is
now used in the default 'diff' output, making the sum of the
'baseline' column be 100%, eliminating blind spots.
* libtraceevent fixes for compiler warnings trying to make perf it
build on some distros, like fedora 14, 32-bit, some of the warnings
really pointed to real bugs.
* Add a browser for 'perf script' and make it available from the
report and annotate browsers. It does filtering to find the
scripts that handle events found in the perf.data file used. From
Feng Tang
* perf inject changes to allow showing where a task sleeps, from
Andrew Vagin.
* Makefile improvements from Namhyung Kim.
* Add --pre and --post command hooks in 'stat', from Peter Zijlstra.
* Don't stop synthesizing threads when one vanishes, this is for the
existing threads when we start a tool like trace.
* Use sched:sched_stat_runtime to provide a thread summary, this
produces the same output as the 'trace summary' subcommand of
tglx's original "trace" tool.
* Support interrupted syscalls in 'trace'
* Add an event duration column and filter in 'trace'.
* There are references to the man pages in some tools, so try to
build Documentation when installing, warning the user if that is
not possible, from Borislav Petkov.
* Give user better message if precise is not supported, from David
Ahern.
* Try to find cross-built objdump path by using the session
environment information in the perf.data file header, from Irina
Tirdea, original patch and idea by Namhyung Kim.
* Diplays more output on features check for make V=1, so that one can
figure out what is happening by looking at gcc output, etc. From
Jiri Olsa.
* Add on_exit implementation for systems without one, e.g. Android,
from Bernhard Rosenkraenzer.
* Only process events for vcpus of interest, helps handling large
number of events, from David Ahern.
* Cross compilation fixes for Android, from Irina Tirdea.
* Add documentation on compiling for Android, from Irina Tirdea.
* perf diff improvements from Jiri Olsa.
* Target (task/user/cpu/syswide) handling improvements, from Namhyung
Kim.
* Add support in 'trace' for tracing workload given by command line,
from Namhyung Kim.
* ... and much more."
* 'perf-core-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: (194 commits)
uprobes: Use percpu_rw_semaphore to fix register/unregister vs dup_mmap() race
perf evsel: Introduce is_group_member method
perf powerpc: Use uapi/unistd.h to fix build error
tools: Pass the target in descend
tools: Honour the O= flag when tool build called from a higher Makefile
tools: Define a Makefile function to do subdir processing
perf ui: Always compile browser setup code
perf ui: Add ui_progress__finish()
perf ui gtk: Implement ui_progress functions
perf ui: Introduce generic ui_progress helper
perf ui tui: Move progress.c under ui/tui directory
perf tools: Add basic event modifier sanity check
perf tools: Omit group members from perf_evlist__disable/enable
perf tools: Ensure single disable call per event in record comand
perf tools: Fix 'disabled' attribute config for record command
perf tools: Fix attributes for '{}' defined event groups
perf tools: Use sscanf for parsing /proc/pid/maps
perf tools: Add gtk.<command> config option for launching GTK browser
perf tools: Fix compile error on NO_NEWT=1 build
perf hists: Initialize all of he->stat with zeroes
...
Diffstat (limited to 'tools/perf/builtin-stat.c')
-rw-r--r-- | tools/perf/builtin-stat.c | 54 |
1 files changed, 41 insertions, 13 deletions
diff --git a/tools/perf/builtin-stat.c b/tools/perf/builtin-stat.c index 93b9011fa3e2..c247faca7127 100644 --- a/tools/perf/builtin-stat.c +++ b/tools/perf/builtin-stat.c | |||
@@ -57,6 +57,7 @@ | |||
57 | #include "util/thread.h" | 57 | #include "util/thread.h" |
58 | #include "util/thread_map.h" | 58 | #include "util/thread_map.h" |
59 | 59 | ||
60 | #include <stdlib.h> | ||
60 | #include <sys/prctl.h> | 61 | #include <sys/prctl.h> |
61 | #include <locale.h> | 62 | #include <locale.h> |
62 | 63 | ||
@@ -83,6 +84,9 @@ static const char *csv_sep = NULL; | |||
83 | static bool csv_output = false; | 84 | static bool csv_output = false; |
84 | static bool group = false; | 85 | static bool group = false; |
85 | static FILE *output = NULL; | 86 | static FILE *output = NULL; |
87 | static const char *pre_cmd = NULL; | ||
88 | static const char *post_cmd = NULL; | ||
89 | static bool sync_run = false; | ||
86 | 90 | ||
87 | static volatile int done = 0; | 91 | static volatile int done = 0; |
88 | 92 | ||
@@ -125,8 +129,7 @@ static struct stats runtime_itlb_cache_stats[MAX_NR_CPUS]; | |||
125 | static struct stats runtime_dtlb_cache_stats[MAX_NR_CPUS]; | 129 | static struct stats runtime_dtlb_cache_stats[MAX_NR_CPUS]; |
126 | static struct stats walltime_nsecs_stats; | 130 | static struct stats walltime_nsecs_stats; |
127 | 131 | ||
128 | static int create_perf_stat_counter(struct perf_evsel *evsel, | 132 | static int create_perf_stat_counter(struct perf_evsel *evsel) |
129 | struct perf_evsel *first) | ||
130 | { | 133 | { |
131 | struct perf_event_attr *attr = &evsel->attr; | 134 | struct perf_event_attr *attr = &evsel->attr; |
132 | bool exclude_guest_missing = false; | 135 | bool exclude_guest_missing = false; |
@@ -149,7 +152,8 @@ retry: | |||
149 | return 0; | 152 | return 0; |
150 | } | 153 | } |
151 | 154 | ||
152 | if (!perf_target__has_task(&target) && (!group || evsel == first)) { | 155 | if (!perf_target__has_task(&target) && |
156 | !perf_evsel__is_group_member(evsel)) { | ||
153 | attr->disabled = 1; | 157 | attr->disabled = 1; |
154 | attr->enable_on_exec = 1; | 158 | attr->enable_on_exec = 1; |
155 | } | 159 | } |
@@ -265,10 +269,10 @@ static int read_counter(struct perf_evsel *counter) | |||
265 | return 0; | 269 | return 0; |
266 | } | 270 | } |
267 | 271 | ||
268 | static int run_perf_stat(int argc __maybe_unused, const char **argv) | 272 | static int __run_perf_stat(int argc __maybe_unused, const char **argv) |
269 | { | 273 | { |
270 | unsigned long long t0, t1; | 274 | unsigned long long t0, t1; |
271 | struct perf_evsel *counter, *first; | 275 | struct perf_evsel *counter; |
272 | int status = 0; | 276 | int status = 0; |
273 | int child_ready_pipe[2], go_pipe[2]; | 277 | int child_ready_pipe[2], go_pipe[2]; |
274 | const bool forks = (argc > 0); | 278 | const bool forks = (argc > 0); |
@@ -328,10 +332,8 @@ static int run_perf_stat(int argc __maybe_unused, const char **argv) | |||
328 | if (group) | 332 | if (group) |
329 | perf_evlist__set_leader(evsel_list); | 333 | perf_evlist__set_leader(evsel_list); |
330 | 334 | ||
331 | first = perf_evlist__first(evsel_list); | ||
332 | |||
333 | list_for_each_entry(counter, &evsel_list->entries, node) { | 335 | list_for_each_entry(counter, &evsel_list->entries, node) { |
334 | if (create_perf_stat_counter(counter, first) < 0) { | 336 | if (create_perf_stat_counter(counter) < 0) { |
335 | /* | 337 | /* |
336 | * PPC returns ENXIO for HW counters until 2.6.37 | 338 | * PPC returns ENXIO for HW counters until 2.6.37 |
337 | * (behavior changed with commit b0a873e). | 339 | * (behavior changed with commit b0a873e). |
@@ -405,6 +407,32 @@ static int run_perf_stat(int argc __maybe_unused, const char **argv) | |||
405 | return WEXITSTATUS(status); | 407 | return WEXITSTATUS(status); |
406 | } | 408 | } |
407 | 409 | ||
410 | static int run_perf_stat(int argc __maybe_unused, const char **argv) | ||
411 | { | ||
412 | int ret; | ||
413 | |||
414 | if (pre_cmd) { | ||
415 | ret = system(pre_cmd); | ||
416 | if (ret) | ||
417 | return ret; | ||
418 | } | ||
419 | |||
420 | if (sync_run) | ||
421 | sync(); | ||
422 | |||
423 | ret = __run_perf_stat(argc, argv); | ||
424 | if (ret) | ||
425 | return ret; | ||
426 | |||
427 | if (post_cmd) { | ||
428 | ret = system(post_cmd); | ||
429 | if (ret) | ||
430 | return ret; | ||
431 | } | ||
432 | |||
433 | return ret; | ||
434 | } | ||
435 | |||
408 | static void print_noise_pct(double total, double avg) | 436 | static void print_noise_pct(double total, double avg) |
409 | { | 437 | { |
410 | double pct = rel_stddev_stats(total, avg); | 438 | double pct = rel_stddev_stats(total, avg); |
@@ -1069,8 +1097,7 @@ static int add_default_attributes(void) | |||
1069 | 1097 | ||
1070 | int cmd_stat(int argc, const char **argv, const char *prefix __maybe_unused) | 1098 | int cmd_stat(int argc, const char **argv, const char *prefix __maybe_unused) |
1071 | { | 1099 | { |
1072 | bool append_file = false, | 1100 | bool append_file = false; |
1073 | sync_run = false; | ||
1074 | int output_fd = 0; | 1101 | int output_fd = 0; |
1075 | const char *output_name = NULL; | 1102 | const char *output_name = NULL; |
1076 | const struct option options[] = { | 1103 | const struct option options[] = { |
@@ -1114,6 +1141,10 @@ int cmd_stat(int argc, const char **argv, const char *prefix __maybe_unused) | |||
1114 | OPT_BOOLEAN(0, "append", &append_file, "append to the output file"), | 1141 | OPT_BOOLEAN(0, "append", &append_file, "append to the output file"), |
1115 | OPT_INTEGER(0, "log-fd", &output_fd, | 1142 | OPT_INTEGER(0, "log-fd", &output_fd, |
1116 | "log output to fd, instead of stderr"), | 1143 | "log output to fd, instead of stderr"), |
1144 | OPT_STRING(0, "pre", &pre_cmd, "command", | ||
1145 | "command to run prior to the measured command"), | ||
1146 | OPT_STRING(0, "post", &post_cmd, "command", | ||
1147 | "command to run after to the measured command"), | ||
1117 | OPT_END() | 1148 | OPT_END() |
1118 | }; | 1149 | }; |
1119 | const char * const stat_usage[] = { | 1150 | const char * const stat_usage[] = { |
@@ -1238,9 +1269,6 @@ int cmd_stat(int argc, const char **argv, const char *prefix __maybe_unused) | |||
1238 | fprintf(output, "[ perf stat: executing run #%d ... ]\n", | 1269 | fprintf(output, "[ perf stat: executing run #%d ... ]\n", |
1239 | run_idx + 1); | 1270 | run_idx + 1); |
1240 | 1271 | ||
1241 | if (sync_run) | ||
1242 | sync(); | ||
1243 | |||
1244 | status = run_perf_stat(argc, argv); | 1272 | status = run_perf_stat(argc, argv); |
1245 | } | 1273 | } |
1246 | 1274 | ||