aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDavid Howells2012-11-05 15:02:08 -0600
committerDavid Howells2012-11-19 16:10:30 -0600
commitbf35182ffcd00d8b36d56210ffdac110e5624d7d (patch)
tree222537ccd17378d77de88702aa35a4d671f64aeb /tools/scripts
parentca9dfc6cc45a8ae0297188f5fed23af242cc8a8d (diff)
downloadkernel-omap-bf35182ffcd00d8b36d56210ffdac110e5624d7d.tar.gz
kernel-omap-bf35182ffcd00d8b36d56210ffdac110e5624d7d.tar.xz
kernel-omap-bf35182ffcd00d8b36d56210ffdac110e5624d7d.zip
tools: Honour the O= flag when tool build called from a higher Makefile
Honour the O= flag that was passed to a higher level Makefile and then passed down as part of a tool build. To make this work, the top-level Makefile passes the original O= flag and subdir=tools to the tools/Makefile, and that in turn passes subdir=$(O)/$(subdir)/foodir when building tool foo in directory $(O)/$(subdir)/foodir (where the intervening slashes aren't added if an element is missing). For example, take perf. This is found in tools/perf/. Assume we're building into directory ~/zebra/, so we pass O=~/zebra to make. Dependening on where we run the build from, we see: make run in dir $(OUTPUT) dir ======================= ================== linux ~/zebra/tools/perf/ linux/tools ~/zebra/perf/ linux/tools/perf ~/zebra/ and if O= is not set, we get: make run in dir $(OUTPUT) dir ======================= ================== linux linux/tools/perf/ linux/tools linux/tools/perf/ linux/tools/perf linux/tools/perf/ The output directories are created by the descend function if they don't already exist. Signed-off-by: David Howells <dhowells@redhat.com> Cc: Borislav Petkov <bp@amd64.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/r/1378.1352379110@warthog.procyon.org.uk Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
Diffstat (limited to 'tools/scripts')
-rw-r--r--tools/scripts/Makefile.include17
1 files changed, 13 insertions, 4 deletions
diff --git a/tools/scripts/Makefile.include b/tools/scripts/Makefile.include
index 4a9e3176f743..87467b17e05c 100644
--- a/tools/scripts/Makefile.include
+++ b/tools/scripts/Makefile.include
@@ -1,8 +1,11 @@
1ifeq ("$(origin O)", "command line") 1ifeq ($(origin O), command line)
2 dummy := $(if $(shell test -d $(O) || echo $(O)),$(error O=$(O) does not exist),) 2 dummy := $(if $(shell test -d $(O) || echo $(O)),$(error O=$(O) does not exist),)
3 ABSOLUTE_O := $(shell cd $(O) ; pwd) 3 ABSOLUTE_O := $(shell cd $(O) ; pwd)
4 OUTPUT := $(ABSOLUTE_O)/ 4 OUTPUT := $(ABSOLUTE_O)/$(if $(subdir),$(subdir)/)
5 COMMAND_O := O=$(ABSOLUTE_O) 5 COMMAND_O := O=$(ABSOLUTE_O)
6ifeq ($(objtree),)
7 objtree := $(O)
8endif
6endif 9endif
7 10
8ifneq ($(OUTPUT),) 11ifneq ($(OUTPUT),)
@@ -47,9 +50,10 @@ endif
47# Call by doing: $(call descend,directory[,target]) 50# Call by doing: $(call descend,directory[,target])
48# 51#
49descend = \ 52descend = \
50 $(QUIET_SUBDIR0)$(1) $(QUIET_SUBDIR1) $(2) 53 +mkdir -p $(OUTPUT)$(1) && \
54 $(MAKE) $(COMMAND_O) subdir=$(if $(subdir),$(subdir)/$(1),$(1)) $(PRINT_DIR) -C $(1)
51 55
52QUIET_SUBDIR0 = +$(MAKE) -C # space to separate -C and subdir 56QUIET_SUBDIR0 = +$(MAKE) $(COMMAND_O) -C # space to separate -C and subdir
53QUIET_SUBDIR1 = 57QUIET_SUBDIR1 =
54 58
55ifneq ($(findstring $(MAKEFLAGS),s),s) 59ifneq ($(findstring $(MAKEFLAGS),s),s)
@@ -64,5 +68,10 @@ ifndef V
64 $(MAKE) $(PRINT_DIR) -C $$subdir 68 $(MAKE) $(PRINT_DIR) -C $$subdir
65 QUIET_FLEX = @echo ' ' FLEX $@; 69 QUIET_FLEX = @echo ' ' FLEX $@;
66 QUIET_BISON = @echo ' ' BISON $@; 70 QUIET_BISON = @echo ' ' BISON $@;
71
72 descend = \
73 @echo ' ' DESCEND $(1); \
74 mkdir -p $(OUTPUT)$(1) && \
75 $(MAKE) $(COMMAND_O) subdir=$(if $(subdir),$(subdir)/$(1),$(1)) $(PRINT_DIR) -C $(1)
67endif 76endif
68endif 77endif