diff options
author | Steven Rostedt | 2011-12-22 20:37:22 -0600 |
---|---|---|
committer | Steven Rostedt | 2011-12-22 21:02:35 -0600 |
commit | 9cc9e091ed4c70535309dd9336a5ea5c2c5920aa (patch) | |
tree | 514c7d65b55f5cc3df3487bbc89a79dc35d1fd24 /tools/testing/ktest | |
parent | b5f4aea687797bf9ab24f59643f88f82443b01fa (diff) | |
download | kernel-omap-9cc9e091ed4c70535309dd9336a5ea5c2c5920aa.tar.gz kernel-omap-9cc9e091ed4c70535309dd9336a5ea5c2c5920aa.tar.xz kernel-omap-9cc9e091ed4c70535309dd9336a5ea5c2c5920aa.zip |
ktest: Detect typos in option names
It becomes quite annoying when you go to run a test and then
realize that you typed an option name wrong, and the test starts
doing the default action and not what you expected it to do.
It is even more annoying when you wake up the next day after
running the test over night when you discover this.
By testing if all options specified in a config file are
used by either ktest or were used in one of the option's values
we can see if there are any dangling options that were not used.
In such a case, show the user the options that were not used
and ask them if they want to continue or not.
The option IGNORE_UNUSED was also added to allow the user to
override this feature.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Diffstat (limited to 'tools/testing/ktest')
-rwxr-xr-x | tools/testing/ktest/ktest.pl | 208 | ||||
-rw-r--r-- | tools/testing/ktest/sample.conf | 11 |
2 files changed, 139 insertions, 80 deletions
diff --git a/tools/testing/ktest/ktest.pl b/tools/testing/ktest/ktest.pl index 5ba9ad4248d7..f360cbdbf00f 100755 --- a/tools/testing/ktest/ktest.pl +++ b/tools/testing/ktest/ktest.pl | |||
@@ -58,6 +58,9 @@ my %default = ( | |||
58 | "SSH_USER" => "root", | 58 | "SSH_USER" => "root", |
59 | "BUILD_TARGET" => "arch/x86/boot/bzImage", | 59 | "BUILD_TARGET" => "arch/x86/boot/bzImage", |
60 | "TARGET_IMAGE" => "/boot/vmlinuz-test", | 60 | "TARGET_IMAGE" => "/boot/vmlinuz-test", |
61 | |||
62 | "LOG_FILE" => undef, | ||
63 | "IGNORE_UNUSED" => 0, | ||
61 | ); | 64 | ); |
62 | 65 | ||
63 | my $ktest_config; | 66 | my $ktest_config; |
@@ -176,6 +179,92 @@ my %force_config; | |||
176 | # do not force reboots on config problems | 179 | # do not force reboots on config problems |
177 | my $no_reboot = 1; | 180 | my $no_reboot = 1; |
178 | 181 | ||
182 | my %option_map = ( | ||
183 | "MACHINE" => \$machine, | ||
184 | "SSH_USER" => \$ssh_user, | ||
185 | "TMP_DIR" => \$tmpdir, | ||
186 | "OUTPUT_DIR" => \$outputdir, | ||
187 | "BUILD_DIR" => \$builddir, | ||
188 | "TEST_TYPE" => \$test_type, | ||
189 | "BUILD_TYPE" => \$build_type, | ||
190 | "BUILD_OPTIONS" => \$build_options, | ||
191 | "PRE_BUILD" => \$pre_build, | ||
192 | "POST_BUILD" => \$post_build, | ||
193 | "PRE_BUILD_DIE" => \$pre_build_die, | ||
194 | "POST_BUILD_DIE" => \$post_build_die, | ||
195 | "POWER_CYCLE" => \$power_cycle, | ||
196 | "REBOOT" => \$reboot, | ||
197 | "BUILD_NOCLEAN" => \$noclean, | ||
198 | "MIN_CONFIG" => \$minconfig, | ||
199 | "OUTPUT_MIN_CONFIG" => \$output_minconfig, | ||
200 | "START_MIN_CONFIG" => \$start_minconfig, | ||
201 | "IGNORE_CONFIG" => \$ignore_config, | ||
202 | "TEST" => \$run_test, | ||
203 | "ADD_CONFIG" => \$addconfig, | ||
204 | "REBOOT_TYPE" => \$reboot_type, | ||
205 | "GRUB_MENU" => \$grub_menu, | ||
206 | "POST_INSTALL" => \$post_install, | ||
207 | "NO_INSTALL" => \$no_install, | ||
208 | "REBOOT_SCRIPT" => \$reboot_script, | ||
209 | "REBOOT_ON_ERROR" => \$reboot_on_error, | ||
210 | "SWITCH_TO_GOOD" => \$switch_to_good, | ||
211 | "SWITCH_TO_TEST" => \$switch_to_test, | ||
212 | "POWEROFF_ON_ERROR" => \$poweroff_on_error, | ||
213 | "DIE_ON_FAILURE" => \$die_on_failure, | ||
214 | "POWER_OFF" => \$power_off, | ||
215 | "POWERCYCLE_AFTER_REBOOT" => \$powercycle_after_reboot, | ||
216 | "POWEROFF_AFTER_HALT" => \$poweroff_after_halt, | ||
217 | "SLEEP_TIME" => \$sleep_time, | ||
218 | "BISECT_SLEEP_TIME" => \$bisect_sleep_time, | ||
219 | "PATCHCHECK_SLEEP_TIME" => \$patchcheck_sleep_time, | ||
220 | "IGNORE_WARNINGS" => \$ignore_warnings, | ||
221 | "BISECT_MANUAL" => \$bisect_manual, | ||
222 | "BISECT_SKIP" => \$bisect_skip, | ||
223 | "CONFIG_BISECT_GOOD" => \$config_bisect_good, | ||
224 | "BISECT_RET_GOOD" => \$bisect_ret_good, | ||
225 | "BISECT_RET_BAD" => \$bisect_ret_bad, | ||
226 | "BISECT_RET_SKIP" => \$bisect_ret_skip, | ||
227 | "BISECT_RET_ABORT" => \$bisect_ret_abort, | ||
228 | "BISECT_RET_DEFAULT" => \$bisect_ret_default, | ||
229 | "STORE_FAILURES" => \$store_failures, | ||
230 | "STORE_SUCCESSES" => \$store_successes, | ||
231 | "TEST_NAME" => \$test_name, | ||
232 | "TIMEOUT" => \$timeout, | ||
233 | "BOOTED_TIMEOUT" => \$booted_timeout, | ||
234 | "CONSOLE" => \$console, | ||
235 | "DETECT_TRIPLE_FAULT" => \$detect_triplefault, | ||
236 | "SUCCESS_LINE" => \$success_line, | ||
237 | "REBOOT_SUCCESS_LINE" => \$reboot_success_line, | ||
238 | "STOP_AFTER_SUCCESS" => \$stop_after_success, | ||
239 | "STOP_AFTER_FAILURE" => \$stop_after_failure, | ||
240 | "STOP_TEST_AFTER" => \$stop_test_after, | ||
241 | "BUILD_TARGET" => \$build_target, | ||
242 | "SSH_EXEC" => \$ssh_exec, | ||
243 | "SCP_TO_TARGET" => \$scp_to_target, | ||
244 | "CHECKOUT" => \$checkout, | ||
245 | "TARGET_IMAGE" => \$target_image, | ||
246 | "LOCALVERSION" => \$localversion, | ||
247 | |||
248 | "BISECT_GOOD" => \$bisect_good, | ||
249 | "BISECT_BAD" => \$bisect_bad, | ||
250 | "BISECT_TYPE" => \$bisect_type, | ||
251 | "BISECT_START" => \$bisect_start, | ||
252 | "BISECT_REPLAY" => \$bisect_replay, | ||
253 | "BISECT_FILES" => \$bisect_files, | ||
254 | "BISECT_REVERSE" => \$bisect_reverse, | ||
255 | "BISECT_CHECK" => \$bisect_check, | ||
256 | |||
257 | "CONFIG_BISECT" => \$config_bisect, | ||
258 | "CONFIG_BISECT_TYPE" => \$config_bisect_type, | ||
259 | |||
260 | "PATCHCHECK_TYPE" => \$patchcheck_type, | ||
261 | "PATCHCHECK_START" => \$patchcheck_start, | ||
262 | "PATCHCHECK_END" => \$patchcheck_end, | ||
263 | ); | ||
264 | |||
265 | # Options may be used by other options, record them. | ||
266 | my %used_options; | ||
267 | |||
179 | # default variables that can be used | 268 | # default variables that can be used |
180 | chomp ($variable{"PWD"} = `pwd`); | 269 | chomp ($variable{"PWD"} = `pwd`); |
181 | 270 | ||
@@ -427,6 +516,10 @@ sub process_variables { | |||
427 | } else { | 516 | } else { |
428 | # put back the origin piece. | 517 | # put back the origin piece. |
429 | $retval = "$retval\$\{$var\}"; | 518 | $retval = "$retval\$\{$var\}"; |
519 | # This could be an option that is used later, save | ||
520 | # it so we don't warn if this option is not one of | ||
521 | # ktests options. | ||
522 | $used_options{$var} = 1; | ||
430 | } | 523 | } |
431 | $value = $end; | 524 | $value = $end; |
432 | } | 525 | } |
@@ -850,6 +943,37 @@ sub read_config { | |||
850 | $opt{$default} = $default{$default}; | 943 | $opt{$default} = $default{$default}; |
851 | } | 944 | } |
852 | } | 945 | } |
946 | |||
947 | if ($opt{"IGNORE_UNUSED"} == 1) { | ||
948 | return; | ||
949 | } | ||
950 | |||
951 | my %not_used; | ||
952 | |||
953 | # check if there are any stragglers (typos?) | ||
954 | foreach my $option (keys %opt) { | ||
955 | my $op = $option; | ||
956 | # remove per test labels. | ||
957 | $op =~ s/\[.*\]//; | ||
958 | if (!exists($option_map{$op}) && | ||
959 | !exists($default{$op}) && | ||
960 | !exists($used_options{$op})) { | ||
961 | $not_used{$op} = 1; | ||
962 | } | ||
963 | } | ||
964 | |||
965 | if (%not_used) { | ||
966 | my $s = "s are"; | ||
967 | $s = " is" if (keys %not_used == 1); | ||
968 | print "The following option$s not used; could be a typo:\n"; | ||
969 | foreach my $option (keys %not_used) { | ||
970 | print "$option\n"; | ||
971 | } | ||
972 | print "Set IGRNORE_UNUSED = 1 to have ktest ignore unused variables\n"; | ||
973 | if (!read_yn "Do you want to continue?") { | ||
974 | exit -1; | ||
975 | } | ||
976 | } | ||
853 | } | 977 | } |
854 | 978 | ||
855 | sub __eval_option { | 979 | sub __eval_option { |
@@ -3321,86 +3445,10 @@ for (my $i = 1; $i <= $opt{"NUM_TESTS"}; $i++) { | |||
3321 | 3445 | ||
3322 | my $makecmd = set_test_option("MAKE_CMD", $i); | 3446 | my $makecmd = set_test_option("MAKE_CMD", $i); |
3323 | 3447 | ||
3324 | $machine = set_test_option("MACHINE", $i); | 3448 | # Load all the options into their mapped variable names |
3325 | $ssh_user = set_test_option("SSH_USER", $i); | 3449 | foreach my $opt (keys %option_map) { |
3326 | $tmpdir = set_test_option("TMP_DIR", $i); | 3450 | ${$option_map{$opt}} = set_test_option($opt, $i); |
3327 | $outputdir = set_test_option("OUTPUT_DIR", $i); | 3451 | } |
3328 | $builddir = set_test_option("BUILD_DIR", $i); | ||
3329 | $test_type = set_test_option("TEST_TYPE", $i); | ||
3330 | $build_type = set_test_option("BUILD_TYPE", $i); | ||
3331 | $build_options = set_test_option("BUILD_OPTIONS", $i); | ||
3332 | $pre_build = set_test_option("PRE_BUILD", $i); | ||
3333 | $post_build = set_test_option("POST_BUILD", $i); | ||
3334 | $pre_build_die = set_test_option("PRE_BUILD_DIE", $i); | ||
3335 | $post_build_die = set_test_option("POST_BUILD_DIE", $i); | ||
3336 | $power_cycle = set_test_option("POWER_CYCLE", $i); | ||
3337 | $reboot = set_test_option("REBOOT", $i); | ||
3338 | $noclean = set_test_option("BUILD_NOCLEAN", $i); | ||
3339 | $minconfig = set_test_option("MIN_CONFIG", $i); | ||
3340 | $output_minconfig = set_test_option("OUTPUT_MIN_CONFIG", $i); | ||
3341 | $start_minconfig = set_test_option("START_MIN_CONFIG", $i); | ||
3342 | $ignore_config = set_test_option("IGNORE_CONFIG", $i); | ||
3343 | $run_test = set_test_option("TEST", $i); | ||
3344 | $addconfig = set_test_option("ADD_CONFIG", $i); | ||
3345 | $reboot_type = set_test_option("REBOOT_TYPE", $i); | ||
3346 | $grub_menu = set_test_option("GRUB_MENU", $i); | ||
3347 | $post_install = set_test_option("POST_INSTALL", $i); | ||
3348 | $no_install = set_test_option("NO_INSTALL", $i); | ||
3349 | $reboot_script = set_test_option("REBOOT_SCRIPT", $i); | ||
3350 | $reboot_on_error = set_test_option("REBOOT_ON_ERROR", $i); | ||
3351 | $switch_to_good = set_test_option("SWITCH_TO_GOOD", $i); | ||
3352 | $switch_to_test = set_test_option("SWITCH_TO_TEST", $i); | ||
3353 | $poweroff_on_error = set_test_option("POWEROFF_ON_ERROR", $i); | ||
3354 | $die_on_failure = set_test_option("DIE_ON_FAILURE", $i); | ||
3355 | $power_off = set_test_option("POWER_OFF", $i); | ||
3356 | $powercycle_after_reboot = set_test_option("POWERCYCLE_AFTER_REBOOT", $i); | ||
3357 | $poweroff_after_halt = set_test_option("POWEROFF_AFTER_HALT", $i); | ||
3358 | $sleep_time = set_test_option("SLEEP_TIME", $i); | ||
3359 | $bisect_sleep_time = set_test_option("BISECT_SLEEP_TIME", $i); | ||
3360 | $patchcheck_sleep_time = set_test_option("PATCHCHECK_SLEEP_TIME", $i); | ||
3361 | $ignore_warnings = set_test_option("IGNORE_WARNINGS", $i); | ||
3362 | $bisect_manual = set_test_option("BISECT_MANUAL", $i); | ||
3363 | $bisect_skip = set_test_option("BISECT_SKIP", $i); | ||
3364 | $config_bisect_good = set_test_option("CONFIG_BISECT_GOOD", $i); | ||
3365 | $bisect_ret_good = set_test_option("BISECT_RET_GOOD", $i); | ||
3366 | $bisect_ret_bad = set_test_option("BISECT_RET_BAD", $i); | ||
3367 | $bisect_ret_skip = set_test_option("BISECT_RET_SKIP", $i); | ||
3368 | $bisect_ret_abort = set_test_option("BISECT_RET_ABORT", $i); | ||
3369 | $bisect_ret_default = set_test_option("BISECT_RET_DEFAULT", $i); | ||
3370 | $store_failures = set_test_option("STORE_FAILURES", $i); | ||
3371 | $store_successes = set_test_option("STORE_SUCCESSES", $i); | ||
3372 | $test_name = set_test_option("TEST_NAME", $i); | ||
3373 | $timeout = set_test_option("TIMEOUT", $i); | ||
3374 | $booted_timeout = set_test_option("BOOTED_TIMEOUT", $i); | ||
3375 | $console = set_test_option("CONSOLE", $i); | ||
3376 | $detect_triplefault = set_test_option("DETECT_TRIPLE_FAULT", $i); | ||
3377 | $success_line = set_test_option("SUCCESS_LINE", $i); | ||
3378 | $reboot_success_line = set_test_option("REBOOT_SUCCESS_LINE", $i); | ||
3379 | $stop_after_success = set_test_option("STOP_AFTER_SUCCESS", $i); | ||
3380 | $stop_after_failure = set_test_option("STOP_AFTER_FAILURE", $i); | ||
3381 | $stop_test_after = set_test_option("STOP_TEST_AFTER", $i); | ||
3382 | $build_target = set_test_option("BUILD_TARGET", $i); | ||
3383 | $ssh_exec = set_test_option("SSH_EXEC", $i); | ||
3384 | $scp_to_target = set_test_option("SCP_TO_TARGET", $i); | ||
3385 | $checkout = set_test_option("CHECKOUT", $i); | ||
3386 | $target_image = set_test_option("TARGET_IMAGE", $i); | ||
3387 | $localversion = set_test_option("LOCALVERSION", $i); | ||
3388 | |||
3389 | $bisect_good = set_test_option("BISECT_GOOD", $i); | ||
3390 | $bisect_bad = set_test_option("BISECT_BAD", $i); | ||
3391 | $bisect_type = set_test_option("BISECT_TYPE", $i); | ||
3392 | $bisect_start = set_test_option("BISECT_START", $i); | ||
3393 | $bisect_replay = set_test_option("BISECT_REPLAY", $i); | ||
3394 | $bisect_files = set_test_option("BISECT_FILES", $i); | ||
3395 | $bisect_reverse = set_test_option("BISECT_REVERSE", $i); | ||
3396 | $bisect_check = set_test_option("BISECT_CHECK", $i); | ||
3397 | |||
3398 | $config_bisect = set_test_option("CONFIG_BISECT", $i); | ||
3399 | $config_bisect_type = set_test_option("CONFIG_BISECT_TYPE", $i); | ||
3400 | |||
3401 | $patchcheck_type = set_test_option("PATCHCHECK_TYPE", $i); | ||
3402 | $patchcheck_start = set_test_option("PATCHCHECK_START", $i); | ||
3403 | $patchcheck_end = set_test_option("PATCHCHECK_END", $i); | ||
3404 | 3452 | ||
3405 | $start_minconfig_defined = 1; | 3453 | $start_minconfig_defined = 1; |
3406 | 3454 | ||
diff --git a/tools/testing/ktest/sample.conf b/tools/testing/ktest/sample.conf index c8dc7575c2f5..86ce62c3fdca 100644 --- a/tools/testing/ktest/sample.conf +++ b/tools/testing/ktest/sample.conf | |||
@@ -727,6 +727,17 @@ | |||
727 | # (default 1) | 727 | # (default 1) |
728 | #DETECT_TRIPLE_FAULT = 0 | 728 | #DETECT_TRIPLE_FAULT = 0 |
729 | 729 | ||
730 | # All options in the config file should be either used by ktest | ||
731 | # or could be used within a value of another option. If an option | ||
732 | # in the config file is not used, ktest will warn about it and ask | ||
733 | # if you want to continue. | ||
734 | # | ||
735 | # If you don't care if there are non-used options, enable this | ||
736 | # option. Be careful though, a non-used option is usually a sign | ||
737 | # of an option name being typed incorrectly. | ||
738 | # (default 0) | ||
739 | #IGNORE_UNUSED = 1 | ||
740 | |||
730 | #### Per test run options #### | 741 | #### Per test run options #### |
731 | # The following options are only allowed in TEST_START sections. | 742 | # The following options are only allowed in TEST_START sections. |
732 | # They are ignored in the DEFAULTS sections. | 743 | # They are ignored in the DEFAULTS sections. |