aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorDoug Ledford2012-05-31 18:26:34 -0500
committerLinus Torvalds2012-05-31 19:49:31 -0500
commit50069a5851323ba5def0e414a21e234345016870 (patch)
treeb7a6af308f2416e0da77adc7b59bfa5e84d61989 /tools/testing/selftests
parentcef0184c115e5e4e10498f6548d9526465e72478 (diff)
downloadkernel-omap-50069a5851323ba5def0e414a21e234345016870.tar.gz
kernel-omap-50069a5851323ba5def0e414a21e234345016870.tar.xz
kernel-omap-50069a5851323ba5def0e414a21e234345016870.zip
selftests: add mq_open_tests
Add a directory to house POSIX message queue subsystem specific tests. Add first test which checks the operation of mq_open() under various corner conditions. Signed-off-by: Doug Ledford <dledford@redhat.com> Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com> Cc: Doug Ledford <dledford@redhat.com> Cc: Joe Korty <joe.korty@ccur.com> Cc: Amerigo Wang <amwang@redhat.com> Cc: Serge E. Hallyn <serue@us.ibm.com> Cc: Jiri Slaby <jslaby@suse.cz> Cc: Manfred Spraul <manfred@colorfullife.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'tools/testing/selftests')
-rw-r--r--tools/testing/selftests/Makefile2
-rw-r--r--tools/testing/selftests/mqueue/Makefile8
-rw-r--r--tools/testing/selftests/mqueue/mq_open_tests.c492
3 files changed, 501 insertions, 1 deletions
diff --git a/tools/testing/selftests/Makefile b/tools/testing/selftests/Makefile
index 28bc57ee757c..14972017a43e 100644
--- a/tools/testing/selftests/Makefile
+++ b/tools/testing/selftests/Makefile
@@ -1,4 +1,4 @@
1TARGETS = breakpoints vm 1TARGETS = breakpoints mqueue vm
2 2
3all: 3all:
4 for TARGET in $(TARGETS); do \ 4 for TARGET in $(TARGETS); do \
diff --git a/tools/testing/selftests/mqueue/Makefile b/tools/testing/selftests/mqueue/Makefile
new file mode 100644
index 000000000000..bd74142a173f
--- /dev/null
+++ b/tools/testing/selftests/mqueue/Makefile
@@ -0,0 +1,8 @@
1all:
2 gcc -O2 -lrt mq_open_tests.c -o mq_open_tests
3
4run_tests:
5 ./mq_open_tests /test1
6
7clean:
8 rm -f mq_open_tests
diff --git a/tools/testing/selftests/mqueue/mq_open_tests.c b/tools/testing/selftests/mqueue/mq_open_tests.c
new file mode 100644
index 000000000000..711cc2923047
--- /dev/null
+++ b/tools/testing/selftests/mqueue/mq_open_tests.c
@@ -0,0 +1,492 @@
1/*
2 * This application is Copyright 2012 Red Hat, Inc.
3 * Doug Ledford <dledford@redhat.com>
4 *
5 * mq_open_tests is free software: you can redistribute it and/or modify
6 * it under the terms of the GNU General Public License as published by
7 * the Free Software Foundation, version 3.
8 *
9 * mq_open_tests is distributed in the hope that it will be useful,
10 * but WITHOUT ANY WARRANTY; without even the implied warranty of
11 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
12 * GNU General Public License for more details.
13 *
14 * For the full text of the license, see <http://www.gnu.org/licenses/>.
15 *
16 * mq_open_tests.c
17 * Tests the various situations that should either succeed or fail to
18 * open a posix message queue and then reports whether or not they
19 * did as they were supposed to.
20 *
21 */
22#include <stdio.h>
23#include <stdlib.h>
24#include <unistd.h>
25#include <fcntl.h>
26#include <string.h>
27#include <limits.h>
28#include <errno.h>
29#include <sys/types.h>
30#include <sys/time.h>
31#include <sys/resource.h>
32#include <sys/stat.h>
33#include <mqueue.h>
34
35static char *usage =
36"Usage:\n"
37" %s path\n"
38"\n"
39" path Path name of the message queue to create\n"
40"\n"
41" Note: this program must be run as root in order to enable all tests\n"
42"\n";
43
44char *DEF_MSGS = "/proc/sys/fs/mqueue/msg_default";
45char *DEF_MSGSIZE = "/proc/sys/fs/mqueue/msgsize_default";
46char *MAX_MSGS = "/proc/sys/fs/mqueue/msg_max";
47char *MAX_MSGSIZE = "/proc/sys/fs/mqueue/msgsize_max";
48
49int default_settings;
50struct rlimit saved_limits, cur_limits;
51int saved_def_msgs, saved_def_msgsize, saved_max_msgs, saved_max_msgsize;
52int cur_def_msgs, cur_def_msgsize, cur_max_msgs, cur_max_msgsize;
53FILE *def_msgs, *def_msgsize, *max_msgs, *max_msgsize;
54char *queue_path;
55mqd_t queue = -1;
56
57static inline void __set(FILE *stream, int value, char *err_msg);
58void shutdown(int exit_val, char *err_cause, int line_no);
59static inline int get(FILE *stream);
60static inline void set(FILE *stream, int value);
61static inline void getr(int type, struct rlimit *rlim);
62static inline void setr(int type, struct rlimit *rlim);
63void validate_current_settings();
64static inline void test_queue(struct mq_attr *attr, struct mq_attr *result);
65static inline int test_queue_fail(struct mq_attr *attr, struct mq_attr *result);
66
67static inline void __set(FILE *stream, int value, char *err_msg)
68{
69 rewind(stream);
70 if (fprintf(stream, "%d", value) < 0)
71 perror(err_msg);
72}
73
74
75void shutdown(int exit_val, char *err_cause, int line_no)
76{
77 static int in_shutdown = 0;
78
79 /* In case we get called recursively by a set() call below */
80 if (in_shutdown++)
81 return;
82
83 seteuid(0);
84
85 if (queue != -1)
86 if (mq_close(queue))
87 perror("mq_close() during shutdown");
88 if (queue_path)
89 /*
90 * Be silent if this fails, if we cleaned up already it's
91 * expected to fail
92 */
93 mq_unlink(queue_path);
94 if (default_settings) {
95 if (saved_def_msgs)
96 __set(def_msgs, saved_def_msgs,
97 "failed to restore saved_def_msgs");
98 if (saved_def_msgsize)
99 __set(def_msgsize, saved_def_msgsize,
100 "failed to restore saved_def_msgsize");
101 }
102 if (saved_max_msgs)
103 __set(max_msgs, saved_max_msgs,
104 "failed to restore saved_max_msgs");
105 if (saved_max_msgsize)
106 __set(max_msgsize, saved_max_msgsize,
107 "failed to restore saved_max_msgsize");
108 if (exit_val)
109 error(exit_val, errno, "%s at %d", err_cause, line_no);
110 exit(0);
111}
112
113static inline int get(FILE *stream)
114{
115 int value;
116 rewind(stream);
117 if (fscanf(stream, "%d", &value) != 1)
118 shutdown(4, "Error reading /proc entry", __LINE__ - 1);
119 return value;
120}
121
122static inline void set(FILE *stream, int value)
123{
124 int new_value;
125
126 rewind(stream);
127 if (fprintf(stream, "%d", value) < 0)
128 return shutdown(5, "Failed writing to /proc file",
129 __LINE__ - 1);
130 new_value = get(stream);
131 if (new_value != value)
132 return shutdown(5, "We didn't get what we wrote to /proc back",
133 __LINE__ - 1);
134}
135
136static inline void getr(int type, struct rlimit *rlim)
137{
138 if (getrlimit(type, rlim))
139 shutdown(6, "getrlimit()", __LINE__ - 1);
140}
141
142static inline void setr(int type, struct rlimit *rlim)
143{
144 if (setrlimit(type, rlim))
145 shutdown(7, "setrlimit()", __LINE__ - 1);
146}
147
148void validate_current_settings()
149{
150 int rlim_needed;
151
152 if (cur_limits.rlim_cur < 4096) {
153 printf("Current rlimit value for POSIX message queue bytes is "
154 "unreasonably low,\nincreasing.\n\n");
155 cur_limits.rlim_cur = 8192;
156 cur_limits.rlim_max = 16384;
157 setr(RLIMIT_MSGQUEUE, &cur_limits);
158 }
159
160 if (default_settings) {
161 rlim_needed = (cur_def_msgs + 1) * (cur_def_msgsize + 1 +
162 2 * sizeof(void *));
163 if (rlim_needed > cur_limits.rlim_cur) {
164 printf("Temporarily lowering default queue parameters "
165 "to something that will work\n"
166 "with the current rlimit values.\n\n");
167 set(def_msgs, 10);
168 cur_def_msgs = 10;
169 set(def_msgsize, 128);
170 cur_def_msgsize = 128;
171 }
172 } else {
173 rlim_needed = (cur_max_msgs + 1) * (cur_max_msgsize + 1 +
174 2 * sizeof(void *));
175 if (rlim_needed > cur_limits.rlim_cur) {
176 printf("Temporarily lowering maximum queue parameters "
177 "to something that will work\n"
178 "with the current rlimit values in case this is "
179 "a kernel that ties the default\n"
180 "queue parameters to the maximum queue "
181 "parameters.\n\n");
182 set(max_msgs, 10);
183 cur_max_msgs = 10;
184 set(max_msgsize, 128);
185 cur_max_msgsize = 128;
186 }
187 }
188}
189
190/*
191 * test_queue - Test opening a queue, shutdown if we fail. This should
192 * only be called in situations that should never fail. We clean up
193 * after ourselves and return the queue attributes in *result.
194 */
195static inline void test_queue(struct mq_attr *attr, struct mq_attr *result)
196{
197 int flags = O_RDWR | O_EXCL | O_CREAT;
198 int perms = DEFFILEMODE;
199
200 if ((queue = mq_open(queue_path, flags, perms, attr)) == -1)
201 shutdown(1, "mq_open()", __LINE__);
202 if (mq_getattr(queue, result))
203 shutdown(1, "mq_getattr()", __LINE__);
204 if (mq_close(queue))
205 shutdown(1, "mq_close()", __LINE__);
206 queue = -1;
207 if (mq_unlink(queue_path))
208 shutdown(1, "mq_unlink()", __LINE__);
209}
210
211/*
212 * Same as test_queue above, but failure is not fatal.
213 * Returns:
214 * 0 - Failed to create a queue
215 * 1 - Created a queue, attributes in *result
216 */
217static inline int test_queue_fail(struct mq_attr *attr, struct mq_attr *result)
218{
219 int flags = O_RDWR | O_EXCL | O_CREAT;
220 int perms = DEFFILEMODE;
221
222 if ((queue = mq_open(queue_path, flags, perms, attr)) == -1)
223 return 0;
224 if (mq_getattr(queue, result))
225 shutdown(1, "mq_getattr()", __LINE__);
226 if (mq_close(queue))
227 shutdown(1, "mq_close()", __LINE__);
228 queue = -1;
229 if (mq_unlink(queue_path))
230 shutdown(1, "mq_unlink()", __LINE__);
231 return 1;
232}
233
234int main(int argc, char *argv[])
235{
236 struct mq_attr attr, result;
237
238 if (argc != 2) {
239 fprintf(stderr, "Must pass a valid queue name\n\n");
240 fprintf(stderr, usage, argv[0]);
241 exit(1);
242 }
243
244 /*
245 * Although we can create a msg queue with a non-absolute path name,
246 * unlink will fail. So, if the name doesn't start with a /, add one
247 * when we save it.
248 */
249 if (*argv[1] == '/')
250 queue_path = strdup(argv[1]);
251 else {
252 queue_path = malloc(strlen(argv[1]) + 2);
253 if (!queue_path) {
254 perror("malloc()");
255 exit(1);
256 }
257 queue_path[0] = '/';
258 queue_path[1] = 0;
259 strcat(queue_path, argv[1]);
260 }
261
262 if (getuid() != 0) {
263 fprintf(stderr, "Not running as root, but almost all tests "
264 "require root in order to modify\nsystem settings. "
265 "Exiting.\n");
266 exit(1);
267 }
268
269 /* Find out what files there are for us to make tweaks in */
270 def_msgs = fopen(DEF_MSGS, "r+");
271 def_msgsize = fopen(DEF_MSGSIZE, "r+");
272 max_msgs = fopen(MAX_MSGS, "r+");
273 max_msgsize = fopen(MAX_MSGSIZE, "r+");
274
275 if (!max_msgs)
276 shutdown(2, "Failed to open msg_max", __LINE__);
277 if (!max_msgsize)
278 shutdown(2, "Failed to open msgsize_max", __LINE__);
279 if (def_msgs || def_msgsize)
280 default_settings = 1;
281
282 /* Load up the current system values for everything we can */
283 getr(RLIMIT_MSGQUEUE, &saved_limits);
284 cur_limits = saved_limits;
285 if (default_settings) {
286 saved_def_msgs = cur_def_msgs = get(def_msgs);
287 saved_def_msgsize = cur_def_msgsize = get(def_msgsize);
288 }
289 saved_max_msgs = cur_max_msgs = get(max_msgs);
290 saved_max_msgsize = cur_max_msgsize = get(max_msgsize);
291
292 /* Tell the user our initial state */
293 printf("\nInitial system state:\n");
294 printf("\tUsing queue path:\t\t%s\n", queue_path);
295 printf("\tRLIMIT_MSGQUEUE(soft):\t\t%d\n", saved_limits.rlim_cur);
296 printf("\tRLIMIT_MSGQUEUE(hard):\t\t%d\n", saved_limits.rlim_max);
297 printf("\tMaximum Message Size:\t\t%d\n", saved_max_msgsize);
298 printf("\tMaximum Queue Size:\t\t%d\n", saved_max_msgs);
299 if (default_settings) {
300 printf("\tDefault Message Size:\t\t%d\n", saved_def_msgsize);
301 printf("\tDefault Queue Size:\t\t%d\n", saved_def_msgs);
302 } else {
303 printf("\tDefault Message Size:\t\tNot Supported\n");
304 printf("\tDefault Queue Size:\t\tNot Supported\n");
305 }
306 printf("\n");
307
308 validate_current_settings();
309
310 printf("Adjusted system state for testing:\n");
311 printf("\tRLIMIT_MSGQUEUE(soft):\t\t%d\n", cur_limits.rlim_cur);
312 printf("\tRLIMIT_MSGQUEUE(hard):\t\t%d\n", cur_limits.rlim_max);
313 printf("\tMaximum Message Size:\t\t%d\n", cur_max_msgsize);
314 printf("\tMaximum Queue Size:\t\t%d\n", cur_max_msgs);
315 if (default_settings) {
316 printf("\tDefault Message Size:\t\t%d\n", cur_def_msgsize);
317 printf("\tDefault Queue Size:\t\t%d\n", cur_def_msgs);
318 }
319
320 printf("\n\nTest series 1, behavior when no attr struct "
321 "passed to mq_open:\n");
322 if (!default_settings) {
323 test_queue(NULL, &result);
324 printf("Given sane system settings, mq_open without an attr "
325 "struct succeeds:\tPASS\n");
326 if (result.mq_maxmsg != cur_max_msgs ||
327 result.mq_msgsize != cur_max_msgsize) {
328 printf("Kernel does not support setting the default "
329 "mq attributes,\nbut also doesn't tie the "
330 "defaults to the maximums:\t\t\tPASS\n");
331 } else {
332 set(max_msgs, ++cur_max_msgs);
333 set(max_msgsize, ++cur_max_msgsize);
334 test_queue(NULL, &result);
335 if (result.mq_maxmsg == cur_max_msgs &&
336 result.mq_msgsize == cur_max_msgsize)
337 printf("Kernel does not support setting the "
338 "default mq attributes and\n"
339 "also ties system wide defaults to "
340 "the system wide maximums:\t\t"
341 "FAIL\n");
342 else
343 printf("Kernel does not support setting the "
344 "default mq attributes,\n"
345 "but also doesn't tie the defaults to "
346 "the maximums:\t\t\tPASS\n");
347 }
348 } else {
349 printf("Kernel supports setting defaults separately from "
350 "maximums:\t\tPASS\n");
351 /*
352 * While we are here, go ahead and test that the kernel
353 * properly follows the default settings
354 */
355 test_queue(NULL, &result);
356 printf("Given sane values, mq_open without an attr struct "
357 "succeeds:\t\tPASS\n");
358 if (result.mq_maxmsg != cur_def_msgs ||
359 result.mq_msgsize != cur_def_msgsize)
360 printf("Kernel supports setting defaults, but does "
361 "not actually honor them:\tFAIL\n\n");
362 else {
363 set(def_msgs, ++cur_def_msgs);
364 set(def_msgsize, ++cur_def_msgsize);
365 /* In case max was the same as the default */
366 set(max_msgs, ++cur_max_msgs);
367 set(max_msgsize, ++cur_max_msgsize);
368 test_queue(NULL, &result);
369 if (result.mq_maxmsg != cur_def_msgs ||
370 result.mq_msgsize != cur_def_msgsize)
371 printf("Kernel supports setting defaults, but "
372 "does not actually honor them:\t"
373 "FAIL\n");
374 else
375 printf("Kernel properly honors default setting "
376 "knobs:\t\t\t\tPASS\n");
377 }
378 set(def_msgs, cur_max_msgs + 1);
379 cur_def_msgs = cur_max_msgs + 1;
380 set(def_msgsize, cur_max_msgsize + 1);
381 cur_def_msgsize = cur_max_msgsize + 1;
382 if (cur_def_msgs * (cur_def_msgsize + 2 * sizeof(void *)) >=
383 cur_limits.rlim_cur) {
384 cur_limits.rlim_cur = (cur_def_msgs + 2) *
385 (cur_def_msgsize + 2 * sizeof(void *));
386 cur_limits.rlim_max = 2 * cur_limits.rlim_cur;
387 setr(RLIMIT_MSGQUEUE, &cur_limits);
388 }
389 if (test_queue_fail(NULL, &result)) {
390 if (result.mq_maxmsg == cur_max_msgs &&
391 result.mq_msgsize == cur_max_msgsize)
392 printf("Kernel properly limits default values "
393 "to lesser of default/max:\t\tPASS\n");
394 else
395 printf("Kernel does not properly set default "
396 "queue parameters when\ndefaults > "
397 "max:\t\t\t\t\t\t\t\tFAIL\n");
398 } else
399 printf("Kernel fails to open mq because defaults are "
400 "greater than maximums:\tFAIL\n");
401 set(def_msgs, --cur_def_msgs);
402 set(def_msgsize, --cur_def_msgsize);
403 cur_limits.rlim_cur = cur_limits.rlim_max = cur_def_msgs *
404 cur_def_msgsize;
405 setr(RLIMIT_MSGQUEUE, &cur_limits);
406 if (test_queue_fail(NULL, &result))
407 printf("Kernel creates queue even though defaults "
408 "would exceed\nrlimit setting:"
409 "\t\t\t\t\t\t\t\tFAIL\n");
410 else
411 printf("Kernel properly fails to create queue when "
412 "defaults would\nexceed rlimit:"
413 "\t\t\t\t\t\t\t\tPASS\n");
414 }
415
416 /*
417 * Test #2 - open with an attr struct that exceeds rlimit
418 */
419 printf("\n\nTest series 2, behavior when attr struct is "
420 "passed to mq_open:\n");
421 cur_max_msgs = 32;
422 cur_max_msgsize = cur_limits.rlim_max >> 4;
423 set(max_msgs, cur_max_msgs);
424 set(max_msgsize, cur_max_msgsize);
425 attr.mq_maxmsg = cur_max_msgs;
426 attr.mq_msgsize = cur_max_msgsize;
427 if (test_queue_fail(&attr, &result))
428 printf("Queue open in excess of rlimit max when euid = 0 "
429 "succeeded:\t\tFAIL\n");
430 else
431 printf("Queue open in excess of rlimit max when euid = 0 "
432 "failed:\t\tPASS\n");
433 attr.mq_maxmsg = cur_max_msgs + 1;
434 attr.mq_msgsize = 10;
435 if (test_queue_fail(&attr, &result))
436 printf("Queue open with mq_maxmsg > limit when euid = 0 "
437 "succeeded:\t\tPASS\n");
438 else
439 printf("Queue open with mq_maxmsg > limit when euid = 0 "
440 "failed:\t\tFAIL\n");
441 attr.mq_maxmsg = 1;
442 attr.mq_msgsize = cur_max_msgsize + 1;
443 if (test_queue_fail(&attr, &result))
444 printf("Queue open with mq_msgsize > limit when euid = 0 "
445 "succeeded:\t\tPASS\n");
446 else
447 printf("Queue open with mq_msgsize > limit when euid = 0 "
448 "failed:\t\tFAIL\n");
449 attr.mq_maxmsg = 65536;
450 attr.mq_msgsize = 65536;
451 if (test_queue_fail(&attr, &result))
452 printf("Queue open with total size > 2GB when euid = 0 "
453 "succeeded:\t\tFAIL\n");
454 else
455 printf("Queue open with total size > 2GB when euid = 0 "
456 "failed:\t\t\tPASS\n");
457 seteuid(99);
458 attr.mq_maxmsg = cur_max_msgs;
459 attr.mq_msgsize = cur_max_msgsize;
460 if (test_queue_fail(&attr, &result))
461 printf("Queue open in excess of rlimit max when euid = 99 "
462 "succeeded:\t\tFAIL\n");
463 else
464 printf("Queue open in excess of rlimit max when euid = 99 "
465 "failed:\t\tPASS\n");
466 attr.mq_maxmsg = cur_max_msgs + 1;
467 attr.mq_msgsize = 10;
468 if (test_queue_fail(&attr, &result))
469 printf("Queue open with mq_maxmsg > limit when euid = 99 "
470 "succeeded:\t\tFAIL\n");
471 else
472 printf("Queue open with mq_maxmsg > limit when euid = 99 "
473 "failed:\t\tPASS\n");
474 attr.mq_maxmsg = 1;
475 attr.mq_msgsize = cur_max_msgsize + 1;
476 if (test_queue_fail(&attr, &result))
477 printf("Queue open with mq_msgsize > limit when euid = 99 "
478 "succeeded:\t\tFAIL\n");
479 else
480 printf("Queue open with mq_msgsize > limit when euid = 99 "
481 "failed:\t\tPASS\n");
482 attr.mq_maxmsg = 65536;
483 attr.mq_msgsize = 65536;
484 if (test_queue_fail(&attr, &result))
485 printf("Queue open with total size > 2GB when euid = 99 "
486 "succeeded:\t\tFAIL\n");
487 else
488 printf("Queue open with total size > 2GB when euid = 99 "
489 "failed:\t\t\tPASS\n");
490
491 shutdown(0,"",0);
492}