aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorSteven Rostedt2012-05-21 23:10:12 -0500
committerSteven Rostedt2012-05-21 23:10:12 -0500
commit3a7bef7917f8fd103197b4cc5969a3125d45deec (patch)
tree3fed056b98af6bfeb0cc40e649aca0eba3dd68be /tools/testing
parent6d76f469c8ac9ef0d769cca0d9cee4375b3d6293 (diff)
downloadkernel-omap-3a7bef7917f8fd103197b4cc5969a3125d45deec.tar.gz
kernel-omap-3a7bef7917f8fd103197b4cc5969a3125d45deec.tar.xz
kernel-omap-3a7bef7917f8fd103197b4cc5969a3125d45deec.zip
ktest: Add kvm.conf example config
Add an example config that explains how to use ktest with a virtual guest as the target. Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Diffstat (limited to 'tools/testing')
-rw-r--r--tools/testing/ktest/examples/kvm.conf88
1 files changed, 88 insertions, 0 deletions
diff --git a/tools/testing/ktest/examples/kvm.conf b/tools/testing/ktest/examples/kvm.conf
new file mode 100644
index 000000000000..831c7c5395f1
--- /dev/null
+++ b/tools/testing/ktest/examples/kvm.conf
@@ -0,0 +1,88 @@
1#
2# This config is an example usage of ktest.pl with a kvm guest
3#
4# The guest is called 'Guest' and this would be something that
5# could be run on the host to test a virtual machine target.
6
7MACHINE = Guest
8
9
10# Use virsh to read the serial console of the guest
11CONSOLE = virsh console ${MACHINE}
12
13#*************************************#
14# This part is the same as test.conf #
15#*************************************#
16
17# The include files will set up the type of test to run. Just set TEST to
18# which test you want to run.
19#
20# TESTS = patchcheck, randconfig, boot, test, config-bisect, bisect, min-config
21#
22# See the include/*.conf files that define these tests
23#
24TEST := patchcheck
25
26# Some tests may have more than one test to run. Define MULTI := 1 to run
27# the extra tests.
28MULTI := 0
29
30# In case you want to differentiate which type of system you are testing
31BITS := 64
32
33# REBOOT = none, error, fail, empty
34# See include/defaults.conf
35REBOOT := empty
36
37
38# The defaults file will set up various settings that can be used by all
39# machine configs.
40INCLUDE include/defaults.conf
41
42
43#*************************************#
44# Now we are different from test.conf #
45#*************************************#
46
47
48# The example here assumes that Guest is running a Fedora release
49# that uses dracut for its initfs. The POST_INSTALL will be executed
50# after the install of the kernel and modules are complete.
51#
52POST_INSTALL = ${SSH} /sbin/dracut -f /boot/initramfs-test.img $KERNEL_VERSION
53
54# Guests sometimes get stuck on reboot. We wait 3 seconds after running
55# the reboot command and then do a full power-cycle of the guest.
56# This forces the guest to restart.
57#
58POWERCYCLE_AFTER_REBOOT = 3
59
60# We do the same after the halt command, but this time we wait 20 seconds.
61POWEROFF_AFTER_HALT = 20
62
63
64# As the defaults.conf file has a POWER_CYCLE option already defined,
65# and options can not be defined in the same section more than once
66# (all DEFAULTS sections are considered the same). We use the
67# DEFAULTS OVERRIDE to tell ktest.pl to ignore the previous defined
68# options, for the options set in the OVERRIDE section.
69#
70DEFAULTS OVERRIDE
71
72# Instead of using the default POWER_CYCLE option defined in
73# defaults.conf, we use virsh to cycle it. To do so, we destroy
74# the guest, wait 5 seconds, and then start it up again.
75# Crude, but effective.
76#
77POWER_CYCLE = virsh destroy ${MACHINE}; sleep 5; virsh start ${MACHINE}
78
79
80DEFAULTS
81
82# The following files each handle a different test case.
83# Having them included allows you to set up more than one machine and share
84# the same tests.
85INCLUDE include/patchcheck.conf
86INCLUDE include/tests.conf
87INCLUDE include/bisect.conf
88INCLUDE include/min-config.conf